Skip navigation

community

Embedded ARM Development Blog

1 Post tagged with the stm32f103_ tag
0

STM32F103ZE ARM Cortex-M3 Board

Posted by kennyxie Nov 11, 2009

For more details, please feel free to visit: http://www.embedinfo.com/en/list.asp?id=31.

 

The STM32F103ZEH6 is an ARM embedded evaluation board produced by Embest, integrate the STMicroelectronic ARM Cortex-M3 core-based processor STM32F103ZE, operating at a 72 MHz frequency. The board features USB, CAN, SD Card interface, TFT-LCD, RS232 serial interface, four 26-pin user extended interface, etc. Plenty of software examples, which can be used in Keil MDK environment, are accompanied in CDROM.

  • 512KB Flash memory, 64KB SRAM
  • uCOS-II v2.86 ported
  • Source code of example program
  •  

    Hardware Specifications:

    The connectors on the STM32F103ZEH6 ARM evaluation board provide easy access to many of the STM32F103ZE's on-chip peripherals.

    • Serial Port
      A standard DB9 connector is on the STM32F103ZEH6 board for the STM32F103ZE's built-in UART interfaces. This is a full duplex, serial port.
    • CAN Port
      A standard DB9 connector for applications requiring CAN communications.
    • USB Port
      A standard USB Type B connector for applications requiring USB communications.
    • LCD Display
      A detachable, 240x320 TFT, color LCD display. You may use this graphic display device to show real-time debug and program status messages.
    • On-board Battery
      A removable, lithium battery is included on the STM32F103ZEH6 to maintain power to the real-time clock when the board disconnects from the main power supply.
    • Analog Voltage Control for ADC Input
      An adjustable analog voltage source for testing the Analog to Digital converter built into the STM32F103ZEH6.
    • External Memory
      The STM32F103ZEH6 board includes 1 Mbyte of external static RAM and 8 Mbytes of external SPI Flash memory.
    • MicroSD Card Connector
      A MicroSD Card connector for developing applications requiring access to MicroSD Cards.
    • ETM Trace Debug
      An ETM connector for on-chip debugging via the Embedded Trace Macrocell capabilities of the STM32F103 device.
    • JTAG Download and Debug
      A JTAG on-chip debug interface, coupled with the ULINK USB-JTAG adapter, provides flash programming and real-time in-circuit emulation of the STM32F103 device.



    kennyxie

    kennyxie

    Member since: Nov 10, 2009

    This blog will introduce you to the world of embedded arm development, it could contain the relevant industry news, the hot arm development tools, the embedded development knowledge and fun stories. Warmly welcome to drop by my Blog!

    View kennyxie's profile