Skip navigation

community

Previous Next

Jim's FAQ's

October 2009
0

            Inductive sensors use a magnetic field to detect objects.  Capacitive sensors use an electric field.  In order to be sensed by an inductive sensor an object must be conductive. This limits suitable targets to metal objects (for the most part). In order to be sensed by a capacitive sensor the target doesn’t need to be conductive. A capacitive sensor will react to an object acting as a dielectric material as well as a conductive object. This makes metal and non-metal objects suitable targets.

0

            The fans from the Multicomp brand that feature the “Vapo Bearing” have an extra magnet in the motor and shaft area. This extra magnet helps to stabilize the rotating fan reducing friction between the shaft and the bearing.  In this increases the life of the fan while reducing motor noise.