Skip navigation

community

Currently Being Moderated

Are the contacts included with the D38999 series 3 connectors, or ordered separately?

Posted by jhayden on Mar 16, 2010 10:24:57 AM

            Contacts are normally included with the D38999 series of connectors, however a number of exceptions do exist.  One of them is when the part number used to order the connector has an “-LC” suffix at the end.   Another exception is how the part number is assembled.  Normally at the end of the part number there’s a “P” or ‘S” to denote the gender of the contacts used in the connector (“P” for pins, “S” for sockets).  If these are switch to an “A” or “B”, then the contacts are again omitted and must be purchased separately.   Some example part numbers are shown below.

These 2 part numbers include contacts.

D38999/20JE26PN

D38999/20JE26SN

While the 3 below do not include the contacts

D38999/20JE26PN-LC

D38999/20JE26AN

D38999/20JE26BN

Please review the manufacture’s documentation for full ordering details as well as options for specific applications.

Attributes

Comments (0)