Skip navigation

community

Jim's FAQ's

3 Posts tagged with the faq tag
0

            Inductive sensors use a magnetic field to detect objects.  Capacitive sensors use an electric field.  In order to be sensed by an inductive sensor an object must be conductive. This limits suitable targets to metal objects (for the most part). In order to be sensed by a capacitive sensor the target doesn’t need to be conductive. A capacitive sensor will react to an object acting as a dielectric material as well as a conductive object. This makes metal and non-metal objects suitable targets.

0

            The fans from the Multicomp brand that feature the “Vapo Bearing” have an extra magnet in the motor and shaft area. This extra magnet helps to stabilize the rotating fan reducing friction between the shaft and the bearing.  In this increases the life of the fan while reducing motor noise.

0

What is a “Peltier”?

Posted by jhayden Sep 29, 2009

A “Peltier” is a solid state Thermoelectric Module.  When powered, it acts like a solid state heat pump (thanks to the Peltier effect) that transfers heat from one side of the device to the other.  Computer enthusiasts sometimes place the wafer like device on top of the processor of their computer with the hot side facing a water block to enhance the cooling of the processor.  Thermoelectric Modules ratings include max temperature difference and max cooling capacity, among others.



jhayden

jhayden

Member since: Dec 3, 2008

Answers to various technical inquiries received over the years.

View jhayden's profile

Recent Comments

No recent comments.