Skip navigation

community

Jim's FAQ's

2 Posts tagged with the sensor tag
0

Photoelectric sensors consist of an emitter and receiver, the emitter sends out a beam of light for the receiver to sense.  With the diffused and retro reflective type of sensors both the emitter and receiver are placed in the same housing and are configured for light to be reflected back to the sensor.

Retro reflective sensors use a target to reflect light back to the sensor and will sense an object that breaks the beam’s path.  The diffuse reflective type senses an object when the light beam is reflected back to the sensor.  Additional features as well as different form factors will vary from series to series.

0

            Inductive sensors use a magnetic field to detect objects.  Capacitive sensors use an electric field.  In order to be sensed by an inductive sensor an object must be conductive. This limits suitable targets to metal objects (for the most part). In order to be sensed by a capacitive sensor the target doesn’t need to be conductive. A capacitive sensor will react to an object acting as a dielectric material as well as a conductive object. This makes metal and non-metal objects suitable targets.



jhayden

jhayden

Member since: Dec 3, 2008

Answers to various technical inquiries received over the years.

View jhayden's profile

Recent Comments

No recent comments.