Skip navigation

community

Jim's FAQ's

2 Posts tagged with the sensors tag
0

     The outputs of some sensors will behave like transistors, when a sensor senses an object it will trigger the transistor controlling the output (which essentially acts like a switch) and depending on its design it’ll act as an NPN or PNP type transistor.  An NPN output is commonly called a “sinking” output.  When the sensor senses an object it will connect the output to the negative supply.  A PNP output is commonly called a “sourcing” output. When it senses an object it will connect the output to the positive supply.  If you’re unsure of which output type you need, a number of manufactures produce sensors with configurable outputs. In this case the sensor can be configured to operate as an NPN or PNP type.  NPN, PNP, and Configurable type sensors come in a Normally Closed and Normally Open configurations.

0

            Inductive sensors use a magnetic field to detect objects.  Capacitive sensors use an electric field.  In order to be sensed by an inductive sensor an object must be conductive. This limits suitable targets to metal objects (for the most part). In order to be sensed by a capacitive sensor the target doesn’t need to be conductive. A capacitive sensor will react to an object acting as a dielectric material as well as a conductive object. This makes metal and non-metal objects suitable targets.



jhayden

jhayden

Member since: Dec 3, 2008

Answers to various technical inquiries received over the years.

View jhayden's profile

Recent Comments

No recent comments.