Skip navigation

community

Jim's FAQ's

2 Posts tagged with the supply_rail tag
0

            While op-amps are designed to reject noise and other disturbances in the supply rails, shifts in the supply voltage can affect the output of the op-amp.  Just how much the op-amp may be affected depends on a number of factors (noise, frequency, temperature, degree of change in voltage, etc). The op-amp’s power supply rejection ratio (or PSRR) can give a good estimation of how much an output can be affected by noise or changes in the supply rail.  The PSRR is frequency dependant so its value will change under different circumstances. The voltage delivered to the op-amp’s supply pins should be kept constant, within the manufacture’s specifications, and as noise free as possible.

0
     Many op-amps can work off of a range of voltages; however, some characteristics of the op-amp may behave differently at different supply voltages.  Check the manufacture’s datasheet for details on the working specifications for the device at the voltage you want to run it at. The supply voltage should not exceed the specifications given by the manufacture and should remain constant.  Special considerations may apply to particularly low voltage levels.


jhayden

jhayden

Member since: Dec 3, 2008

Answers to various technical inquiries received over the years.

View jhayden's profile

Recent Comments

No recent comments.