Skip navigation

community

Transportation

3 Posts tagged with the fuel tag
0

Question: What does your everyday Ford Focus, Nissan Altera, VW Passat and virtually every other mass produced vehicle on the road have that a NASCAR race car doesn’t?


Answer: Electronic fuel injection. That’s right, NASCAR still uses carburetors, same as your father’s Oldsmobile from the 1950s.

 

Fuel injection delivers an even flow of gas to the engine, something that a carburetor can't always manage. Sensors in the engine regulate the fuel intake and make sure it is dispersed properly.

 

Which is one of several reasons why after decades of using carburetors and long after they were relegated to the junk heap by the world’s automakers  (production vehicles haven't had carburetors since 1989) NASCAR teams will use fuel injection in 2012, starting with the Daytona 500.

 

Each team will pay about $26,000 per car to use a system developed by McLaren Electronic Systems and Freescale Semiconductor, which produce the engine control units.  Apart from the performance benefits expected to accrue NASCAR reports use of electronic fuel injection will also allow officials to better police how teams power their engines.

 

The Sprint Cup car manufacturers — Chevrolet, Dodge, Ford and Toyota— all underwent on-track testing of fuel injection racecars last week at Kentucky Speedway.

 

The new system is expected to also provide better fuel mileage, which could give a team an edge in a sport where extending the number of laps run between pit stops can make a difference in how high up in the field a car finishes.

0

110606-01-01.jpg


The charge anxiety of an Electric Vehicle (EV) has deterred many from purchase. With few places to recharge, the possibility of being stranded is high. Nissan and the Japan Automobile Federation (JAF) announced a roadside recharging service for all EVs that has lost power. Nissan developed a few roadside vehicles equipped with EV recharging equipment that can be deployed from a Kanagawa branch office. Of course this one office will not service all of Japan, it is first being tested in an extremely limited area. It is a first step in promoting green technology, EVs, and to provide a "safety net" for all EV owners.

 

Nissan VP of External and Government affairs, Hitoshi Kawaguchi, had this to say about the effort, "As EVs gain wider consumer acceptance, it is important to create a roadside assistance system that can help motorists driving EVs which have run out of battery power, as well as to build a charging infrastructure. Nissan is leveraging the development and trial operation of this roadside service vehicle with charging equipment – and the accompanying staff training – to strengthen cooperation with JAF and to benefit customers. This will build confidence in EV use and contribute toward achieving a society with low carbon emissions."

 

With the countless towing companies in the world, I can see the same group of people fitted with EV recharging equipment becoming instantly accepted as the first thought in an EV charge emergency. Most gasoline based emergency vehicles are equipped with 300A alternators, a 3-phase AC source at either 12 or 24V. More than enough for a quick charge.


I personally think every EV should come with the "Bat Hook" power line leech, and carte blanche to use it.


 

Eavesdropper

0

by Cherif Assad

CherifAssad.JPG

 

The debate for performance has always been a passionate one in the engineering community. In the semiconductor industry, nearly every competitor claims to have the most innovate architecture that offers the highest performance.

 

Let’s make an attempt to sort out the requirements of a relative performance evaluation. The intrinsic core performance and workload behavior are important, but not enough. The interaction with the peripheral set –analog to digital, digital to analog conversion, multiplexing, bus switch to memory access – is the litmus test to determine the real value behind a piece of silicon. The compiler is provided by a software tools vendor, which may help to optimize the source code execution to come to the result expected. Now remains the essential element about the methodology for an objective assessment.

 

You can select a software benchmark given for generic tests, and you can also use algorithms dedicated for special functions or to measure signal processing capability. In automotive, specifically powertrain, there are several key parameters calling for high performance microcontrollers (MCUs) to determine real time position: the engine’s cog, angle-to-time conversion, road speed calculation, and lookup tables.

 

 

Interested? Read the complete entry