Skip navigation

community

Transportation

6 Posts tagged with the in:automotive tag
0

avicosreplac.jpg

(Image via Technische Universitaet Muenchen)

 

I did not know how to turn off the change oil light in my car, it was not in the manual. What did I do? I checked youtube for the answer. Technische Universitaet Muenchen (TU) and Audi are about to bring a video manual you can talk to on all new model Audi cars.

 

The Avatar-based Virtual Co-driver System (AviCoS) is a animated avatar that can give the driver, or anyone in the car, detailed information on the vehicle using "natural-language dialog." Simply ask a question, and the system will deliver the answer. AviCoS uses an AI that can analyze complete sentences and answer using audio, images, or video on a embedded screen in the car. The avatar can also visually guide the user through the car, or point to areas of interest.

 

If the user is unfamiliar with a certain feature of the car, the touch screen lets the user enter the "Touch & Tell Mode." The user touches the area of the car where more information is needed, the avatar provides all the background information. While driving, all animations and graphical outputs are suppressed to avoid distracting the driver. However, voice communication will still work. " Overall, AviCoS provides comfortable and interactive access to multimedia content that goes far beyond the information contained in printed manuals. The self-explanatory system can be used without training, making it easy to get familiar with the operation of a vehicle," said TU Institute for Business Informatics' Dr Michael Schermann.

 

The development team stated that the next step is to sense the drivers mood through elevated speech patterns or tone of voice. When angry, the animations are suppressed.  In a time a difficulty, I would not care to see flashy animations, I suppose.

 

Eavesdropper

0

by Rainer Makowitz

RainerMakowitz.JPG

 

RADAR has been quickly adopted as the foundation of the new Advanced Driver Assistance Systems (ADAS) that are being introduced by vehicle  manufacturers around the globe.

 

The RADAR technology has several benefits over other forward-facing  sensor technologies, like cameras. It can operate under adverse weather  conditions, can ‘see through’ objects to detect smaller targets and is  the primary method to determine speed of objects around the car. What  was used in police cruisers to provide hard evidence against speed limit  offenders has now come to be used as a preventive means to make driving  safer.

 

The choice of 76-81 GHz as the operating  frequency band was made by a standards organization to obtain  exceptional resolution and also to have a globally agreed frequency band  exclusively for this application.

 

At the Freescale Technology Forum (20-24 June, 2011) in San  Antonio, Astyx and Freescale demonstrated a high resolution 77GHz RADAR  sensor that is designed to be used in the next generation of automotive  ADAS systems. New technological advancements over conventional  automotive RADAR systems include:

- Digital beam forming using multiple receive channels
- Full 2D object detection
- High resolution in space and velocity
- Highly integrated RF components

 

Digital beam forming requires many receiver channels, which made it  costly and complex to implement in the past. This demo has implemented  unprecedented 16 receiver channels integrated into four Freescale BiCMOS  receiver chips driving high-resolution imaging. The high dynamics  requirements of automotive use case require fast frequency sweep in the  transmitter. The Freescale transmitter implementation represents the  market leading trade-off between frequency stability and fast sweep  operation.

 

The flexible Digital Beam Forming RADAR  sensor architecture designed  by Astyx allows several sensor ‘personalities’ (short range – up to  50m, or long range – 250m) to be defined by software options only.

 

 

Interested? Read the complete entry

2

by Mike Garrard

MikeGarrard.JPG

 

Without doubt, electric vehicles have sex appeal. Not in the same way that a five litre 480hp V8 Mustang at full throttle does. The benefit is more cerebral.  They are the future, quiet and clean. Driving one comes with a feel good factor of saving the planet. I have one, and I love it, see here. It might even breed a certain little sanctimonious corner of the grey matter that makes one park it on the drive rather than put it in the garage.

 

Do we need them? Most certainly.  I don’t believe it is possible for the planet’s resources to support all of China and India at the consumption rates in the West, an astounding 200kWh per head, every day. If China were like the USA they would be buying 60M cars per year: that’s the entire world car production in 2009. Something has to change.


Even the most optimistic people, which I rashly assume is the US Geological Society, say peak oil will be somewhere around 2030; IEA thinks we’ve flatlined and others say that we’ve peaked already. For mass consumption, oil shale may not be the significant low cost oil replacement we want it to be.  Your children, or theirs, may be the last petrol heads on the planet.

 

 

Interested? Read the complete entry

0

by Marc Osajda

MarcOsajda.JPG

 

Powered two wheelers account for only one percent of European traffic, but represent 16 percent of the road fatalities, according to a study led by the European Association of Motorcycle Manufacturers. The risk of being killed in motorcycle accident is 20 times higher than in a regular passenger car. More than half of the death causes are due to upper body area injuries in the thorax, abdomen and spine.


Scary data, isn’t it?

 

Bering, a well-known manufacturer of motorcycle clothes is now launching an innovative motorcycle airbag jacket intended to reduce bikers’ injuries and fatalities, the Bering Wireless Airbag Safety System.

 

The system is innovative for several reasons. It uses proven automotive crash sensors to detect real impact with other road users, dedicated sensors to detect if the motorcycle is sliding (cornering on a slippery road, for example) and the command to inflate the airbag jacket is transmitted wirelessly in less than 0.05 seconds. The full protection is achieved in less than 0.08 seconds. The reason why I’m proud of this safety equipment is because the solution is designed around Freescale Xtrinsic MEMS sensors and Freescale microcontrollers – proven automotive technology used in millions of passenger car airbag systems around the world.

 

Interested? Read the complete entry

1

by Mike Stanley

MikeStanley.JPG


Expanding on the topic of “active safety,” Freescale recently announced advanced Xtrinsic sensors for use in Electronic Stability Control (ESC). ESC works by comparing vehicle responses to user control inputs. If the two are inconsistent, ESC applies the individual wheel brakes of the car to bring things back in line. ESC is standard in high end vehicles today, but the technology is moving into the mainstream market as well. The U.S. National Highway Traffic Safety Administration will require the technology in most 2012 model vehicles. ESC has the potential to prevent nearly one-third of all fatal car accidents and 70 percent of fatal accidents of light trucks and vans.

 

The MMA690xQ dual-axis (X/Y) low-g accelerometers were designed specifically for safety critical applications. The devices are controlled via a standard SPI interface. Built with safety requirements in mind, the SPI module checks data parity and number of clock edges in a packet and flags errors to the host. The MMA690xQ also monitors critical internal voltages, on-chip clock frequencies, device temperature and programmed data integrity. The integrated self-test feature can apply an electrostatic force to stimulate and confirm accelerometer mechanical movement.

 

 

Interested? Read the complete entry

4

 

I just finished reading an article about the new Nissan leaf, which Nissan tout as the “first real world Electric Car”, but have we been here before I wonder, and is an electric car a truly viable alternative to the internal combustion engine (ICE). Given the time required to recharge the batteries between journeys, I still can’t see how this could be accepted as a viable alternative by most users. Nissan claim the Leaf has a range of approximately 100 miles on a full charge, but even as early as 1911 the Detroit Electric from the Anderson Carriage Company had a range of 80 miles (all be it at a top speed of 20 miles per hour). Has so little change in battery technology in all this time that we still find it difficult to produce a practical battery powered car with compelling range? Even though the lithium-ion cells used in the Leaf can be fast charged to 80% capacity in 30mins, a full overnight charge still takes around 8 hours.

 

This started me wondering, where are we with viable alternatives? I recall seeing an item on the UKs Top Gear program presented by James May about a Honda Fuel cell car somewhere in California, and set off to do some web investigation. What I discovered was very interesting. Honda have for some years, been leasing (in what I might term experimental quantities) their FCX Clarity, to a select group of customers there. Not to be out done, Mercedes Benz has recently announced the introduction of their B Class F-Cell for 2010. The initial production run will be limited to just 200 cars, so I assume this is much more about information gathering than a practical real world product. Capable of developing 136hp from the electric motor and a range of 250miles with a performance to match its 2.0 litre petrol counterpart, the future of Hydrogen fuel cell cars looks to be on the horizon.

 

Today’s practical solution however is clearly the HEV (Hybrid Electric Vehicle). The HEV at present is synonymous with the Toyota Prius, but an ever increasing number of suppliers are offering or planning to offer HEVs including Honda, Lexus, Nissan, Ford, Mercury and Saturn. The great benefit with the HEV of course is the fact that if you don’t get stuck if you battery goes flat, because the ICE is still the primary drive. The electric motor assists the ICE during acceleration, and doubles up as a generator under braking to recharge the batteries. In addition to the regenerative breaking power management is also a big feature of the HEV, to improve overall efficiency, emissions and MPG.

 

Having said all this, even HEV sales currently represent less than 1% of global unit sales, but is predicted to have strong growth in the coming years to an estimated four and half million units by around 2013 (The Freedonia Group).

 

All of this is I think great news for electronics engineers. The growth of the markets for these technologies will drive the electronics content of vehicles ever skyward with intelligent drives to propel the vehicles and, power management to maximise fuel efficiency as we integrate systems, such as adaptive cruise control, collision mitigation, blind-spot detection, collision warning systems, lane departure warning systems, rear-view cameras, Digital Instrument Clusters, infotainment, navigation and communication systems. The need for the oily bits experts looks to be diminishing and the future brighter for the electronics design engineers, is this the real start of the automotive electric revolution?

 

(You can find a good overview and links to useful information on battery technology and charging here http://www.element-14.com/community/docs/DOC-13354).