Skip navigation

community

Transportation

13 Posts tagged with the transportation tag
0

By Stephan Lehmann — Many in the automotive industry believe that the automobile will undergo more changes in the next 15 years than it has since its inception 125 year ago. Through partnerships, this industry is working towards fuel efficiency and a world without accidents. Vehicles will connect to each other and to the cloud creating opportunities beyond imagination.

 

In this video, Tim Nixon, Karla Wallace and Mike Grimes from GM, as well as John Schneider from Ford, share incredible energy, excitement and passion for the progress being made in the automotive industry and the future evolution of the connected car.

 

Mike Grimes summarizes it nicely: “I thought I would have retired with technology that actually has already occurred. So, I’m already beyond my retirement point and now I’m just having fun!”

 

Read more about it

0

4e52b5a738a06.image.jpg

(via AP Photo/Paul Sancya)

 

Two of my favorite car companies have partnered together, Ford and Toyota, to work on my favorite drive topology, rear-wheel drive, with everyone's favorite engine system, the hybrid.

 

● The partnership sets the two companies on equal footing in an effort to create and advanced hybrid system for rear-wheel drive light trucks and SUVs.

● The goal is to deliver greater fuel efficiency while not compromising the performance of the vehicles.

● The team will also work towards developing the next-generation standards for in vehicle internet and digital communication systems.

● Ford and Toyota pledge to deliver the new tech within the coming decade.

 

I like where their minds are at. However, I would like to see this same hybrid RWD system come to consumer and sport cars. I believe I am not the only one. Perhaps market demand with usher in a new revival for RWD. We can only hope.

 

Cabe

1

Auto -inflating tires are given in science fiction futures, if the vehicles have wheels that is. Look at the film Demolition Man, which features Wesley Snipe's character using voice commands to auto-inflate a tire. It seems like a simple idea, only now is it made?

 

From Goodyear Tire & Rubber Company comes the Air Maintenance Technology (AMT). The entire system is housed inside the tire. There will be no need for external intervention. Goodyear senior vice president and chief technical officer Jean-Claude Kihn elaborated, "While the technology is complex, the idea behind the AMT system is relatively simple and powered by the tire itself as it rolls down the road."

 

The U.S. Department of Energy (DOE)Office of Vehicle Technology awarded Goodyear with $1.5 million USD for further research in using the AMT system on commercial truck tires. Tires not properly inflated will cause up to a 3.3% drop in fuel economy. The DOE's angle is to lessen the demand for foreign oil by the 3.3%. The average semi-truck drives up to 1 million miles in its life time. The 3.3% improvement could mean a savings of $6,000 USD in the end. (3.3% ~= 0.12 cents per . With a liberal 20 mpg, the savings comes up to $6.000 at current gasoline prices.)

 

The grant also applies to a Goodyear and PPG Industries partnership on improving rolling resistance and fuel efficiencies of tires.

 

There is no date or pricing on the AMT system's release. Goodyear is also very hush on how the technology works. I am going to guess it is very similar to the SIT (self inflating tire) from 2008.


 

Cabe

1

EV breaks distance records

Posted by Eavesdropper Aug 17, 2011

Why  does every electric car that boasts a world record range on a single  charge always looks like it is from an ugly Buck Rogers future?

42520_90409_2.jpgbluebird-team-wants--1_460x0w.jpg

Buck Rogers Rocket Ship (left)  Bluebird EV capable of 500 mph (Right)

 

1-boozerevsets.jpgboozerevsets.jpg

Schluckspecht E (left) and with the Schluckspecht Team (right)  (via Team Schluckspecht)


Team  Schluckspecht just barely does away with the outer-space fairing look  with their new world record holding electric vehicle (EV), the  "Schluckspecht E" or "Boozer E" in English. On a single charge the EV  travelled 1,013.8 miles (1,631.5 km) over a span of 36 hours and 12  minutes. The efficiency comes from taking as much mass out of the EV's  chassis, only having one seat, and evenly dividing the power demand  equally between 14 individual lithium-cobalt batteries. Drive in applied  directly via two motors, one on each front wheel, which does away with a  transmission. However, the team did not break any land-speed records.  The Boozer could only reach 28 mph (45 km/h). The test took place at the Bosch corporate race track in Boxberg, Germany.

 

I  would stomach driving this EV if it could go 65 mph. I am sure much of  the range will be lost adding a transmission, but it would still best  every EV available today.

 

Eavesdropper

0

avicosreplac.jpg

(Image via Technische Universitaet Muenchen)

 

I did not know how to turn off the change oil light in my car, it was not in the manual. What did I do? I checked youtube for the answer. Technische Universitaet Muenchen (TU) and Audi are about to bring a video manual you can talk to on all new model Audi cars.

 

The Avatar-based Virtual Co-driver System (AviCoS) is a animated avatar that can give the driver, or anyone in the car, detailed information on the vehicle using "natural-language dialog." Simply ask a question, and the system will deliver the answer. AviCoS uses an AI that can analyze complete sentences and answer using audio, images, or video on a embedded screen in the car. The avatar can also visually guide the user through the car, or point to areas of interest.

 

If the user is unfamiliar with a certain feature of the car, the touch screen lets the user enter the "Touch & Tell Mode." The user touches the area of the car where more information is needed, the avatar provides all the background information. While driving, all animations and graphical outputs are suppressed to avoid distracting the driver. However, voice communication will still work. " Overall, AviCoS provides comfortable and interactive access to multimedia content that goes far beyond the information contained in printed manuals. The self-explanatory system can be used without training, making it easy to get familiar with the operation of a vehicle," said TU Institute for Business Informatics' Dr Michael Schermann.

 

The development team stated that the next step is to sense the drivers mood through elevated speech patterns or tone of voice. When angry, the animations are suppressed.  In a time a difficulty, I would not care to see flashy animations, I suppose.

 

Eavesdropper

0

HEV Solutions Guide is intended to help you explore TI's IC solutions as the various sectors become increasingly electrified on a path toward energy efficiency and sustainability.

Guide includes: System block diagrams, followed by details about key devices and support functions

 

hev.jpg

0

 

Self taught, Terry Hope has made his own solar power generating electric bicycle. Hope fitted the stock Specialized FRS 18 speed bike with a front grill and windshield for mounting eighteen 6"x6" mono crystalline sollar cells. Approximately 4 watt (@ 8.7v) output on each cell. Totaling 72 watts if all conditions are ideal. A 24V motor controller moves the 1 HP motor at the core of the project. Batteries are 6s1p 5000mah LIPO as the main, and two 4s1p LIPO 5000mah as "booster packs" which are wired in series. I assume he uses the "boosters" to overdrive the motor. Across the handle bars are several buttons used to turn the solar on or off for direct use, button for the booster, and the all important red E-stop. Hope added toggles to use solar for battery charging.

 

The motor itself drives the main sprocket. As with most multi-speed bicycles, the pedals are not engaged by the motor. The drive system is very unique compared to other electric bicycles. However, this is not ready for mass production. It is still very much a labor of love. I like the smaller electric bicycle Hope has made more than the 18 speed, see his launch page.

 

Can we do better? Help me build an electric bicycle with the rest of the community.

 

Cabe

0

26 November 2003 was the last flight for the commercial Concorde supersonic airliner. Global dreams of traveling 3 times faster than anything else were seemingly dashed forever.

 

That was until the 2011 Paris Air Show. Two supersonic jet concepts were announced from EADS and new player HyperMach Europe Aeronautics. Both claim speeds fasters than the Concorde. Both are decades away. More notably, both are promoting these jets as being "green."

 

EADS, the European Aeronautic Defence and Space Company N.V., teased their concept called the ZEHST (Zero Emissions Hypersonic Transport). The jet contains three different types of purpulsion systems that will engage at different stages in flight, each quite green. The takeoff enginers use a algae based biofuel. At an altitude of 6km, the Ariane (rocket type) engine using cryogenically stored hydrogen and oxygen liquid fuels. At an altitude of 32km onboard ramjets take over the flight also using hydrogen as the fuel, taking the craft to speeds of up to mach 4 and possibly 5, high enough to not allow for sonic-booms. EADS claims that this method of propulsion will be cost-effective and environmentally friendly.

 

EADS spokesman Grgor von Kurell said, " We think the three different propulsion types we're considering - one of which we have perfected for the Ariane rocket - could make this achievable by 2050." EADS also claims a London to Tokyo flight of just over 2 hours.



 

HyberMach's jet concept called the SonicStar differentiates itself distinctly by giving a release date of 2021. This all depends on whether or not they get the funding and partnership. The S-MagJet 4000X engine that pushes this craft is 30% more efficient than the Concorde engine and at twice the speed, Mach 3.6. Another big feature claims it can adjust the sound footprint of the jet, and if need be suppress a sonic-boom.

 

The SonicStar, using conventional engine technology does seem to be poised for sooner realization. However, in its current design, the SonicStar is only designed to carry 10-20 passengers. Again, putting supersonic flight out of the reach of the global dreamers.


 

Eavesdropper

2

6a00d8341c4fbe53ef012875d07ee4970c-800wi.png

Kinergy Flywheel

 

 

A weighted 9" disc spins at 60,000 rpm, who's surface is traveling twice the speed of sound, may just power hybrid vehicles in the near future. British company Ricardo has designed a flywheel energy storage system to use in future hybrid vehicles. The system called Kinergy, stores the energy in breaking into the carbon fibre laced flywheels. The energy stored is then used as a torque assist in accelerating the vehicle. The flywheel is house in a vacuum sealed container and placed on magnetic bushings to reduce all friction to the near zero. A magnetic gearing and coupling mechanism gathers the energy from the flywheel and applies it, with no mechanical contact, to the transmission. Each flywheel produces approximately 30 kW of power from the 4.5 kg discs.

 

6a00d8341c4fbe53ef012875d0887e970c-800wi.png

Flybus with Kinergy system, rear cutaway

 

Currently the Kinergy system is being tested on Flybus buses at airports, with a goal of 20% fuel savings. Another test involved using a Kinergy storage system paired with a Torotrak Continuously Variable Transmission on a Optare Solo bus. The future has Ricardo leading the KinerStor project with a consortium of other companies to bring the Kinergy system to other hybrid vehicles with a goal of 30% efficiency increase.

 

Flywheels already help regulate large volumes of power, by not in cars too?

 

Eavesdropper

 

2

 

Inside a non-transparent box that is moving, one may feel secure. Ignorance is bliss. But placed in a clear box that is moving, impending doom could be seen. Airbus wants to make a clear box airplane for the future. Much like the observation car on a train, a section of the new airplane will be mostly transparent showing the entirety of the outside. The ability to look straight ahead into the direction of the plane will show objects approaching at whatever speed the plane is moving. 700 mph bugs and birds hitting the windshield, in other words. Though ambitious as it seems, it most likely will not happen in the same way shown above.

 

The body heat absorbing seats seems a little useless, when coating the entire plane is solar active cells would produce so much more. I do hope to see the holographic display that floats in mid air. Who knows what 2050 will hold, the projected release date for the plane form Airbus.

 

Eavesdropper

1

MIDE_13.jpgMIDE_01.jpg

 

 

Here is a perfect example of, "I can not believe this has not been done already."

 

Aalto University in Finland is testing the use of hybrid technology in non-road, mobile industrial machinery. Think Prius versions of cranes, bulldozers, tractors, and diggers. Their concept is to capture of the energy from the work being performed by each machine that is lost when in operation. Like in hybrid cars, deceleration, braking energies are being absorbed as well as energy from such tasks as lowering a load. For the record, no one has attempted making hybrids in this area.

 

Head researchers Professor Jussi Suomela spoke of the impetus of the project, "These heavy duty machines are operated for long periods of time, so by the end of the day emissions and fuel consumption have added up. Being able to target them is a significant improvement." From recent experimental data, Suomela has show that involving such combustion/electric hybrids in work machinery has the potential to save 50% of the fuel costs in stand alone operation, and even more if the system is plugged into the power grid.

 

Now it is not a question of can it be done, but when can it be implemented. Great work, Aalto University.

 

Eavesdropper

0

110606-01-01.jpg


The charge anxiety of an Electric Vehicle (EV) has deterred many from purchase. With few places to recharge, the possibility of being stranded is high. Nissan and the Japan Automobile Federation (JAF) announced a roadside recharging service for all EVs that has lost power. Nissan developed a few roadside vehicles equipped with EV recharging equipment that can be deployed from a Kanagawa branch office. Of course this one office will not service all of Japan, it is first being tested in an extremely limited area. It is a first step in promoting green technology, EVs, and to provide a "safety net" for all EV owners.

 

Nissan VP of External and Government affairs, Hitoshi Kawaguchi, had this to say about the effort, "As EVs gain wider consumer acceptance, it is important to create a roadside assistance system that can help motorists driving EVs which have run out of battery power, as well as to build a charging infrastructure. Nissan is leveraging the development and trial operation of this roadside service vehicle with charging equipment – and the accompanying staff training – to strengthen cooperation with JAF and to benefit customers. This will build confidence in EV use and contribute toward achieving a society with low carbon emissions."

 

With the countless towing companies in the world, I can see the same group of people fitted with EV recharging equipment becoming instantly accepted as the first thought in an EV charge emergency. Most gasoline based emergency vehicles are equipped with 300A alternators, a 3-phase AC source at either 12 or 24V. More than enough for a quick charge.


I personally think every EV should come with the "Bat Hook" power line leech, and carte blanche to use it.


 

Eavesdropper

1

Sphere drone robot

Posted by Eavesdropper Jun 10, 2011

 

The Japanese Ministry of Self-Defense went to the geek capitol of Akihabara, a section of Tokyo, to source parts for this "reconnaissance drone." In its current form, it can travel 40 mph for up to 8 minutes. Since the drone if built inside of a protective sphere, it can withstand the sudden impact of drop after losing power. 8 separate fins around the sphere control the direction, and it seems to handle quick turns very well. The 42cm, diameter, drone weighs only 350 grams with all the components and onboard camera. All the parts, collectively, cost approximately $975 USD.

 

The simplicity, low cost, and versatility of this drone is sure to inspire more and better version. Add thin-cell solar to the roll cage, increase the battery size, and these things will be everywhere. On one hand, these could be used to watch and control people. On the other, they could keep people safe, guide them through cities, or lead them to locations. Either way, I'm all for them.

 

Eavesdropper