Skip navigation

community

1 2 Previous Next

Medical Device Design & Equipment Development

16 Posts tagged with the medical tag
1

-006.jpg

Image that was controlled via Kinect during operation. (via Microsoft)

 

The Kinect imaging sensor has been used in some technically innovative projects such as Queen’s University’s 3D video conferencing system to Microsoft’s own augmented reality MirageTable. It’s even found its way into the medical field with a recent successful operation involving the repair of an aneurism at Guy’s and St Thomas’ hospital in London.

 

Surgeons involved in complex operations occasionally need to refer to reference material to help them through certain procedures. This is typically done by using an assistant to bring up the materials on a laptop so the doctor can remain at the operating table without having to waste time re-scrubbing because of contamination. This is where a new 3D imaging system that was developed by Microsoft Research Cambridge with Guy’s and St Thomas’ hospital can be invaluable as it was used for the first time by assistant surgeon Tom Carrell to perform heart surgery.

 

mg21428655.200-1_300.jpg

Promotional image of the Kinect during surgery. (via Microsoft & St. Thomas' Hospital)

 

The system was used to compare a 3D model of an aorta with a live-feed 2D image of the patient's by using a fluoroscopic x-ray camera to help Carrell navigate through the delicate procedure. The 3D model could also be manipulated through a series of minimal gestures that include the ability to rotate the image using the palm of your hand and placing a marker simply by pointing and using a voice command. These simple gestures can be performed using only one hand leaving the other to continue the surgery while others, such as panning, rotating or zooming in/out need the use of both hands. Not only can the system be used in confined spaces commonly found in operating theaters, it also saves valuable time in eliminating the need to take a break to consult reference material.

 

Cabe

http://twitter.com/Cabe_e14

0

connected scale.jpg

Composite image of the two companies technologies (via Withings & BodyMedia)

 

When it comes to weight loss, most people could use all the help they can get. The companies Withings and BodyMedia, Inc. are teaming up to provide those who wish to get fit and stay in shape with as much assistance as they can muster. The partnership is designed to bring together the functions of the Withings Wi-Fi Body Scale and the BodyMedia FIT system.

 

 

The Withings scale can collect data on the user’s body weight, lean mass and fat mass and body mass index (BMI). It allows 8 users at a time to store their information and access it through the Withings smartphone app or your own secure web page. The BodyMedia FIT armbands collect all sorts of physiological data like heat flux, skin temperature, motion and galvanic skin response at over 5,000 readings per minute.

 

 

Now, both of these devices automatically transmit all of their acquired data to the BodyMedia FIT Activity Monitor via their built in Wi-Fi making it extremely convenient to create graphs and charts of data and, one would hope, the motivation or value that would impulse one into exercising. The Withings scale is even able to update tweets and your facebook status with details of your getting healthy journey to get as much support from your friends online.

 

 

The Withings Wi-Fi Scale will set you back $160, and the BodyMedia FIT system equipment array is paralleling the price.

 

 

Cabe

http://twitter.com/Cabe_e14

1

illu-isir04.gif

(via The Institute for Intelligent Systems and Robotics (ISIR))

 

Technology that helps robots navigate and interact with their environment may soon help blind people in much the same way. A new type of glasses that takes advantage of 3D navigation that some robots use are currently being designed by Edwige Pissaloux and his team from the Institute of Intelligent Systems and Robotics located in France. The design uses a headset imaging system that takes 3D images and sends them to a handheld device that converts it to braille that the user can read which gives the blind a different way to see their environment. The headset consists of two cameras mounted on either side of the wearer which in tandem takes 3D images. A processor then analyzes the images and identifies various objects in the cameras field of view such as walls and other objects and builds a 3D map of the area. A series of accelerometers and gyroscopes monitors the user’s location and speed to determine the wearer’s relative position in relation to the 3D map. The compiled data is then sent to a tactile feedback display that produces a constant 3D map in braille form (at a rate of ten maps per-second) the gives the user a way of ‘seeing’ their environment in real-time.

 

The IISR team in France is also looking to combine their system with software being developed by engineers at the University of Nevada that was initially used to tell robots how far they have travelled based on its sensors (accelerometer/gyroscope). Their system uses smartphones internal sensors along with available 2D in-door maps and synthetic speech (SIRI?) to help the blind navigate. In order for the system to be effective, the phone must be calibrated to the users stride. This is done touching a series of stationary markers such as walls, hallway entrances and other obstacles. Both systems combined would greatly benefit the user’s ability to navigate just about anywhere in an urban environment. As to when this system/s will become readily available is anyone’s guess but then again ‘seeing is believing’.

 

It seems the scientific community is bent on technology returning sight to the blind. Read about more efforts in the area after this link.

 

Cabe

http://twitter.com/Cabe_e14

0

Bionic Vision, At Last

Posted by Cabe Atwell May 9, 2012

Bionic-Eye.jpg

Bionic Eye concept (via Bionic Vision Australia)

 

Most of us go our days taking for granted our sense of vision, but loss of this sense changes everything. Even though vision loss can occur for many different reasons, there is little medical science can do to fix most cases of blindness. However, technology is catching up. Retinal implants are already here, and next year a computer aided “bionic” eye will be tested on a human patient.

 

 

An Australian company, Bionic Vision Australia is teaming up with scientists from a new $2.5 million facility, the Rs.12.76 Crore Fabrication Facility, found at the University of New South Wales to develop prototype bionic eyes. These first prototypes will be helpful to patients with degenerative retinal conditions. To benefit from one of these bionic eyes, patients need to have a complete and functioning visual pathway from the retina to the brain and some intact retinal cells.

 

 

These prototypes are intended to give patients limited visual capabilities. This will be accomplished by use of a chip inside the transplant, which is connected to the nerve cells in the retina that send signals to the visual cortex. Impressively, the signal is captured via a video camera found on a pair of glasses worn by the patient that wirelessly relay it to a processing computer, and even a smartphone could do the job. After processing, it is sent to the bionic eye’s chip connected to retinal cells.

 

 

The sensor is made of biocompatible material and includes 98 electrodes that stimulate surviving nerve cells. Development and manufacture of the bionic eye will be greatly accelerated at the Rs.12.76 Fabrication Facility where the two prototypes are in development. This facility is stacked with state of the art equipment including laser cutters, plasma reactors, high temperature presses, probing machines and even a “clean room” for manufacturing electrical components.

 

 

The first prototype is a “wide-view” device that will help some visually impaired to easily detect between light and dark and allow them to see outlines of big objects for easier navigation around their environment. The second prototype is a “high-acuity” bionic eye that will provide a higher definition and will allow patients to read large fonts and recognize faces. They hope to have the second prototype ready for testing in four years.

 

 

Cabe

http://twitter.com/Cabe_e14

1

111 implant in place.JPG14634_Retina_scan_showing_chip__c__Oxford_Eye_Hospital.jpg

(Left) Implant behind eye. (Right) Retinal scan showing the sensor chip in place. (via University of Oxford)

 

Diagnosed with retinitis pigmentosa, the first symptom was night blindness. A few years later, vision was drastically reduced. Finally, another disease brought complete blindness in the left eye and the inability to distinguish light on the right. Chris James, a fifty-four year old council worker in Wiltshire U.K., had his life completely changed by his complications. He said, "It’s something you have to come to terms with and make the best of what you’ve got."

 

Chris James's new eye was switched on for the first time. The digital circuits flood with electricity. James could see light against a black background for the first time in decades. The retinal implants were a success. "As soon as I had this flash in my eye, this confirmed that my optic nerves are functioning properly which is a really promising sign. It was like someone taking a photo with a flashbulb, a pulsating light, I recognized it instantly."

 

Chris James was one of the first patients (along with Robin Millar, a 60 year old music producer) suffering from retinitis pigmentosa to receive retinal implanted circuitry to detect light and images from a collaboration between the University of Oxford (UO) and the company "Retina Implants" form Germany. A team led by ophthalmology professor Robert MacLaren were able to help the patients regain some semblance of vision. As the patients continue to use the implants, their vision continues to improve. Currently, the patients can see light differences and basic shapes.

 

111 retinal implant.jpg

X-ray image of the complete system installed into Chris James. (via University of Oxford)

 

The implant is a 3mm square chip containing 1,500 light sensitive diodes. The chip is attached to the back of the eye where a signal can be sent between electrodes and the patient's optical nerves. The system is powered by an implanted power supply buried behind the ear, similar to some cochlear devices. Professor MacLaren explained that the sensor will "stimulate the overlying nerves to create a pixellated image." He continued, "Apart from a hearing aid like device behind the ear, you would not know a patient had one implanted.  We are all delighted with these initial results. The vision is different to normal , and it requires a different type of brain processing. We hope, however, that the electronic chips will provide independence for many people who are blind from retinitis pigmentosa."

 

The U.K based trials will continue with 12 patients overall thanks to funding from the National Institute of Health Research and the Oxford Biomedical Research Centre.

 

Cabe

http://twitter.com/Cabe_e14

0

technology_infographic.jpg

Technology overview (via MicroChips Inc.)

 

Daily injections of medicine may be crucial for patients who suffer from certain diseases.  However, the pain involved may deter some patients from following their prescribed regiments , and this can lead to ineffective treatment. The company Microchips Inc., along with two other commercial companies, scientists at Harvard, MIT and the Case Western Reserve are developing a microchip system that could deliver individual doses of medicine while monitoring levels in the blood wirelessly.

 

 

The device was implanted and tried successfully in seven women who suffered from postmenopausal osteoporosis.  The drug to treat osteoporosis, teriparatide, is to be injected daily for two years , and it works to build bone if given intermittently so it was the ideal candidate for preliminary testing of this device.

 

 

A single microchip is 1/15’’ thick, ½’’ long and 1/5’’ wide and is implanted using local anesthetics under the skin of the abdomen. The entire system is 2 ¼’’ long and 1 ½’’ wide and made up of two chips located on the surface of its titanium housing. Each chip contains 10 individual cubic reservoirs, each measuring 0.04 in wide, capable of holding 600 nanoliters of the medicine.

 

 

Each reservoir faces the patient’s skin and is covered with a metallic membrane made of a titanium and platinum composite. These membranes are connected to internal circuits, which deliver currents to the membranes to dissolve them and release the drug.

 

in vivo chip.jpg

A close up of how the system works (via MicroChips Inc.)

 

This drug delivery system could be used to treat multiple sclerosis and chronic pain, but limitations to this device are clear in that they cannot be used to treat Diabetics because there is not enough room in the chip to store all the insulin needed. The company estimates that it will take 2 years to develop a chip that can deliver medicine for 365 days.

 

 

Many more human trials are needed to prove this technology is safe. Microchips Inc plans to file for FDA approval in 2014 , but the device will need 2 more years of clinical studies so it will not be available commercially until late in the decade.

No toxic effects were observed in the trial, although a faulty circuit prevented the drug from being released in the 8th patient. Blood tests showed that the quantity of the automatic doses was more consistent than shots and the drug was effective in generating bone growth.

 

 

Robert Farra, President and CEO of Microchips Inc announced that the cost of the implant and treatment would be around $10,000-12,000, which is very similar to price of standard injections.

 

 

Cabe

http://twitter.com/Cabe_e14

0

Fig-1.jpg

Cochlear implant concept (via University of Utah)

 

Cochlear implants have improved the hearing for over 220,000 deaf people around the globe, but they have their drawbacks. Not being able to swim or wear helmets comfortably due to the delicate microphone and related electronics worn on the outside of the ear are just some of the tip of the limitation. A team of engineers, led by Associate Professor Darrin Young from the University of Utah, are looking to fix those issues by implanting the cochlear microphone inside the ear itself, giving the user an increased level of freedom in otherwise damaging environments.

 

Typical implants house the microphone, signal processor and transmitter coil in a plastic shroud worn behind the ear. The mic picks up sound and sends it to an internal receiver-stimulator attached to bone under the skin by the microphone housing. From there, sound is sent to electrodes attached to cochlea which in-turn stimulates auditory nerves making it possible for the user to hear. Young’s design places all the external components normally worn outside the ear inside by placing an accelerometer sensor that’s attached to a chip on the ears umbo part of the tympanic membrane to detect vibration. This converts sound into electrical signals that are then sent to the electrodes attached to the cochlea which is powered by an implanted battery enabling the user to hear.

 

Recharging the battery is done at night while the user sleeps using a charger located behind the user’s ear in much the same fashion as wearing a typical cochlear implant. Successful testing was done using several cadavers (yes, you read that right) implanted with the new cochlear system. A laser was then used to measure the vibration on bones inside the ear to see which one was more efficient at picking up normal-level sound after which it was found that the umbo was the most successful. In order to test this device, the implanted microphone was wired to speakers with Beethoven’s Ninth Symphony acting as the test medium. While the sound was ‘muffled,’ Young states that ‘the muffling can be filtered out’. The team hopes to improve the overall sound quality in future versions so clinical trials are still a few years away but anything that can assist the disabled is still a hopeful future.

 

Cabe

http://twitter.com/Cabe_e14

1

It’s annoying when you are working at home and the power goes out for a couple of minutes, perhaps causing you to lose a document you were working on,  But if you are a patient in a hospital the effect of a power loss, even for a minute, is more than annoying., It could be fatal. For that reason in hospitals and other medical facilities which control machines keeping people alive require a medical grade UPS (uninterruptible power supply). A medical grade UPS will maintain power voltage and frequency variations in electrical equipment not only in the event of complete power failure, but also as a result of fluctuations in the power supply like those caused by surges, brown-outs and storms and car accidents that take down power lines. 

 

Commercially available power supplies are generally manufactured to the IEC-950 or UL-1950 standards. But because it may operate near patients medical-grade power supplies differ from the standard commercial variety and must comply with IEC601-1 or UL2601-1 relating to  design and test criteria that seek to eliminate the shock hazard to patients and medical attendants. For electrical equipment operated from the AC mains, the IEC standard focuses on two issues: high voltage breakdown and current leakage. Current leakage directly affects the patient, while breakdown can indirectly affect the patient by increasing leakage in their vicinity.

 

For UPS product standard commercial UPS systems can have earth leakage of no more than 3mA, and with EMC filters employed UPS systems have earth leakage in the 1 to 2mA region. Medical standards, on the other hand call for earth leakage to be no more than 300 microamps, about  one-tenth of the levels allowed by specifications aimed at commercial-grade supplies

Sophisticated medical equipment such as ultrasound systems, laboratory equipment, and other health care devices also need optimal power protection from noise, sags and surges.  A medical grade UPS should be able to withstand an electrostatic discharge compliant to ENC61000-4-2, level 4 relating to the immunity of electrical and electronic equipment to repetitive electrical fast transient s without damage and without affecting the connected load.

 

All switching power supplies draw current from the line in narrow, high-amplitude pulses instead of a smooth, sinusoidal flow from the ac mains. As such medical-grade supplies also must satisfy standards for power factor correction. IEC 60601-1-2 requires PFC in power supplies above 75 W. By way of review power factor is the ratio of real power (Pr) to apparent power (Pa). The power factor of a typical switching power supply is 0.6 to 0.7. The power factor of a corrected power supply is typically 0.95 or greater.

0

(repost)

sound system concept.jpgacousticr.jpg

(Left) Concept of the system (Right) Drawing of the MEMS generator (Via Purdue University)

 

A new medical pressure sensitive implant, microelectromechanical system (MEMS), is out that uses sound as a power source. This MEMS device is a sensor that monitors the pressure of the urinary ladder and in the sack of blood vessel damages by an aneurism. Purdue University researches invented the MEMS to one day treat people with aneurism or incontinence due to paralysis patients.

 

The MEMS device uses a vibrating cantilever that is connected to the bottom of the heart by a thin. The cantilever vibrates when music is within the range of frequencies of 200-500 hertz. When the cantilever vibrates it generates electricity, and that charge is stored in a small onboard supercapacitor. When the frequency falls out of the useful range, the cantilever stops vibrating and will automatically send the electrical charge to the sensor. At the same time, the system will take the pressure readings and transmits the data wirelessly.

 

ziaie-music2.jpg

MEMS generator (via Purdue University)

 

The cantilever beam is a ceramic based lead zirconate titante material, a piezoelectric (PZT)element. The sensor is about two centimeters long. Researcher even tested the device in a water-filled balloon to see if still worked, and the test was a success. To get this device powered you can use batteries or an external transmitter.

 

The four genres tested with the MEMS were rap, blues, jazz, and rock. Among the four genres of music tested, rap rise above all when being the most effective. "Rap is the best because it contains a lot of low frequency sound, notably the bass," Purdue professor Babak Ziaie said. In rap, the vulgar words and the deep bass are put together for the listener to understand the true power of the message, which does not give the rap genre the best reputation. Soon, doctors using the device will understand the true power of Tupac songs.

 

Cabe

http://twitter.com/Cabe_e14

0

(repost)

 

RIBA-II-02.jpg

 

Japanese company Riken has partnered up with Tokai Rubber in the creation of the RIBA II nursing assistant robot. At the joint laboratory RTC, RIKEN-TRI Collaboration Center for Human-Interactive Robot Research, they have taken the RIBA Robot, from 2008, and upgraded the lifting abilities (by 41 lbs) and control interface to the point where it will be a tool for medical use.

 

I know a few hospital volunteers that say they have to lift elderly, sick, and disabled people in and out of beds and chairs routinely throughout the day. Depending on the condition of the patient, they say it can be an extremely difficult and cumbersome task to handle. This is where the RIBA II come in to play.

 

The 507 lbs (230 kg) robot can handle patients of up to 176 lbs (80 kg). Each are in covered in soft rubber, and has 7 degrees of freedom. The head has 3, waist has 2, and the omni-directional base has 3 more degrees of freedom. A touchscreen on the RIBA II bot's back will allow nurses to direct the bot to locations. Onboard laser range finders, proximity sensors, bumper sensors, and voice commands will help the RIBA II avoid obstacles and prevent accidents.

 

RIBA-II-spec1.gif03.jpg

 

 

Direct control of the RIBA II is the most innovative addition to the platform. The robot is covered in "Smart Rubber" that is the world's first capacitive touch rubber surface.  The sensors are on the bot's upper arms, forearms, hands, and chest. A nurse can then physically guide the bot quickly and make adjustments on the fly for hoisting the patient. Like the RIBA I, the RIBA II's Tokai Rubber also detect slippage and will adjust on its own to keep the patient comfortable.

 

RIBA II has the same "bear" head that was on the original RIBA. The designers claim this is to not scare the patient. The original lifting bot RI-MAN, which could only handle 41 lbs (18 kg), was a little scary. I question the use of either head. It is just a tool, right? A human forklift, in other words. Make it as non-anthropomorphized as possible, in my opinion.

RIMAN-header.jpg

(RI-MAN by RIKEN)

 

 

When available in 2015, the RIBA II will cost $77,000 USD (6,000,000 JPY). Much more expensive than the free volunteers most hospitals depend on.


video via youtube member kmoriyama

 

(All pictures via RIKEN)

0

(repost)

 

Showa Hanako is a dental training robot developed by the department of Orthodontics at the Showa University (SU) in Japan. The PVC skinned bot would move in a limited fashion using a hydraulic system. Limited movement and speech capabilities were built in. This bot was the 3rd generation of the University's line of training robots. Some of the complaints were the un-lifelike skin, odd stare, and the motion of the overall system. The Showa Hanako was never available for wide spread distribution due to the designer  Tmsuk's inability to handle  global repair issues. But all this is soon to change.

 

Showa University is going to attempt wide spread sales of their new upgraded Showa Hanako 2 dental training robot. This new bot swaps the PVC skin for realistic silicon skin. It now has an upgraded mouth with 2 degrees of movement for the tongue. The whole body has switch to motor actuation. The bot blinks, sneezes, coughs, shakes its head, gets tired of holding its mouth open, and has an expanding vocabulary. The smooth realistic oral cavity is currently being put through the patent process. IT software company, RayTron, has built in a voice recognition system able to hear a masked dentist and respond accordingly.

 

The sudden upgrade of parts comes from the Japanese company Orient Industries (OI), famous for "love dolls." OI has been build human shaped dolls since 1977. Their "Real Love Doll" line has figures with silicon skin with every joint movable in natural human positions. SU even admitted they needed OI's help in creating a realistic patient down to every detail. "Even the smallest mistake would be unforgivable."

 

More on the Showa Hanako 2 :

The Showa Hanako 2 even vomits when a student user touches the uvula (sensor).

 


0

DNA nanorobot from Wyss Institute on Vimeo

 

 

Star Trek's "Borg" use nano-probes for cell-repair and to fight unwanted intrusion inside their human/robot bodies. It sounds like an effective way of fighting damaged cells, but it is science fiction. However, this Star Treks technology may be brought into reality for fighting off diseased cells (cancer) with the help of DNA origami. Designed by Paul Rothemund at CIT (California Institute of Technology), DNA origami is the folding of a single DNA strand into various two and three dimensional shapes.

 

dna_nanorobot-275x389.jpg

Programmable DNA nanorobot concept model. (via Wyss Institute & Campbell Strong, Shawn Douglas, and Gaël McGill using Molecular Maya and cadnano)

 

These can be made into a different number of things such as miniature images or even a programmable robot. Harvard University's Wyss Institute researcher Shawn Douglas, and his team, have created a barrel-like nano-robot that can deliver a dose of medicine to diseased cells. The ‘barrel’ is held shut by two DNA ‘latches’ that only release and introduce the medicine when they encounter specific cell proteins found in cancer. The team has tested this application with both leukemia and lymphoma cells that were mixed in with non-diseased cells. The nano-robots were programmed to seek out and deliver their payload known to kill those disease cells respectively. After a three day test period, the robots effectively killed around half of the cancerous cells without harming the healthy ones. Think of it as a super-mechanical white blood cell that homes in on cells that are in distress and targets them for termination.

 

This method is by no means and end-all to the cancer problem as it is still in the development stage and has not been run through clinical trials. The team has encountered some challenges along the way as to programming, shape of the nano-robot, method of medicine delivery and a host of other problems. However, any hope for an effective treatment for battling cancer is excellent news and should be viewed as such.

 

Cabe

http://twitter.com/Cabe_e14

1

One of the first thoughts that come to our minds when we hear the words “Pulse Oximeter” is a person lying in a hospital bed wearing a finger sensor and being monitored by a nurse or a doctor. A pulse oximeter is a device capable of measuring oxygen saturation in arterial blood, and in some models pulse rate as well. It is true, that one of the most relevant application fields for a pulse oximeter lies in the hospital area as being a part of important medical devices, like vital signs monitors and anesthesia units. However, pulse oximeters can also help keep you away from the hospital.

 

An excellent example of how a Pulse Oximeter can save lives outside the operating room is in aeronautics. In 2003 a PA-28R-200 crashed after a pilot started to make erratic decisions due to hypoxia caused by altitude. At 14,000 feet, blood oxygen saturation falls to 85% (normal values are 95-99%) causing judgment, memory, and thought degradation. The pilot flew above 14,000 feet for 1 hour 49 minutes without supplementary oxygen or a blood oxygen saturation monitor.

 

Oxygen saturation monitoring has also helped mountain climbers to determine the appropriate altitude to start using their oxygen tanks and avoid “altitude sickness” which is usually over 8,000 feet. Some athletes also use a pulse oximeter for monitoring their oxygen saturation and pulsations per minute while exercising.

 

As you can see, pulse oximeters like other medical devices, have a large application field outside the hospital and more can be accomplished when these devices become portable. Freescale is aware of this, and they have developed the MED-SPO2. This is a pulse oximeter reference design as an Analog Front End (AFE) development board.

 

The MED-SPO2 is designed to be used together with the Freescale Tower System, compatible with the Tower system development boards (TWR-S08MM128 for 8-bits, TWR-MCF51MM256 and TWR-K53N512 for 32-bits portfolios) enables the developer to create a fast and low-cost solution for pulse oximeter applications. The MED-SPO2 is reduced in size and components, decreases design time for engineers.

 

Making pulse oximeter devices as portable as possible with highly integrated hardware solutions like Freescale medical oriented microcontrollers, improves the way in which people integrate these solutions in their daily lives, even outside the operating room.

 

So next time you see a pulse oximeter, think in all the possible solutions that it can bring not only in the hospital area, but also in your daily life. Portable medical devices help people to make their lives safer and easier.

1

 

Imagine being told you or your loved one will never be able to walk again, the devastation, the shock …

 

Well, there may be hope after-all.  In a lab at Duke University doctors, engineers, neuroscientists and physiologists from Brazil, Switzerland, Germany and the United States are all actively working on what many might call a miracle, a “prosthetic exoskeleton” that would allow those immobilized by injury or illness to walk again.  Their goal is to demonstrate that they could bypass the body’s complex network of nerve endings and supply the sensation of touch right to the brains of monkeys.

 

Dr Nicolelis, a Brazilian-born physician and neuroscientist, is bringing together brain science and engineering or sensory feedback and brain control devices to be combined in real time and in a useful way.  Kip Ludwig, who has funded some of Nicolelis’ work, states, “Before, they’ve always been separate.”  He also states that, ideally, the long-term goal would be a prosthetic that would send all the sensory information – touch, position and temperature- to a body part that would add meaning to it."

 

Nicolelis’ team has “recruited” two female monkeys, from southern Asia, to demonstrate the feasibility of their ideas. The team is sending electrical signals to the monkey’s brain to distinguish between three identical circles with different textures.  These sensations will come from coded electrical currents sent to each monkey’s sensory cortex, or outer layer of the brain, by four filaments the width of hair.

 

1939817.jpg


 

Nicolelis explained the brain the motor drive purpose, “The team is starting with simple experiments for Mango and Nectarine, (the monkeys) so that when the experiments move to humans he or she will not only learn quickly how to initiate and repeat movements using thought alone, but the prosthetic should interface so seamlessly with the intelligent human brain that the patient will begin to see the prosthetic as a natural extension of him or herself.... It would be just like a car…only a little tighter.”

 

Now, when is this determined and industrious goal expected to happen you ask?  This wonderful team that Nicolelis has put together, hopes to send a young quadriplegic striding out to midfield to open the 2014 World Cup soccer tournament in Brazil, suited up in an “prosthetic exoskeleton."

 

How is that for ambitious?

 

Eavesdropper

 

Pictures and video via Duke University

0

kjh.jpg

The biological logic gate Via Professor Kitney

 

This is a Re-Post from the DIT Blog.

 

An AND logic gate made from Escherichia Coli (E.Coli) and DNA was made at the Imperial College London, demonstrating the much hypothesized concept of the biological computer. The experiment also showed how several of these gates can be connected to for other more complex forms, such as a NAND. The foundation is set, in-body biological computing is close.

 

Co-author of the paper, Professor Richard Kitney explained the concept further, "Logic gates are the fundamental building blocks in silicon circuitry that our entire digital age is based on. Without them, we could not process digital information. Now that we have demonstrated that we can replicate these parts using bacteria and DNA, we hope that our work could lead to a new generation of biological processors, whose applications in information processing could be as important as their electronic equivalents.”

 

The development team stated that their vision will lead such biological computers to searching out the body's ailments and handling them accordingly. For example, using a bio-circuit to find cancer cells and destroy them. In the meantime, the group is looking into building more complex organizations of the gates. 

 

I can only imagine a 1-trillion gate biological processor would be too large to move through the blood stream. I am more curious about how the team will tackle that obstacle. 

 

Eavesdropper

1 2 Previous Next