Skip navigation

community

1 2 3 ... 55 Previous Next

News

819 Posts
1

tband antenna.jpg

T-ray antenna (via Tokyo Institute of Technology)

 

It may seem sometimes that we have exploited the vast reaches of the electromagnetic spectrum, but technologies like WiGig, are showing this notion is not correct at all. T-rays, or electromagnetic waves found in the terahertz band, have traditionally been used for imaging research like X-rays, but now researchers from the Tokyo Institute of Technology are developing a system to apply this technology to ultra fast data transmission.

 

 

The terahertz band actually makes use of the 300 GHz to 3 THz frequencies a range currently unregulated by telecommunication authorities. Using a frequency of 542 GHz the team achieved data transfers of 3 Gb/s using a device called a resonant tunneling diode (RTD). These results are higher than anything achieved so far in the terahertz band.

 

 

This device is revolutionary in the terahertz data transmission because of its small size of only 1 mm-squared and low power necessities.  RTDs are unusual in that the voltage across them can be decreased as the current increases. The RTDs generate waves in the terahertz band by making the diode inside them resonate.

 

 

Due to the energy usage, the Tokyo researchers hope to some day implement them in hand held devices for short-range data transfers. It is likely that terahertz Internet would work only in short distances of up to 10 m (33 ft), and this short range is something the researchers are trying to improve by making their devices resonate at higher frequencies, but this will also require more power.

 

 

It will take a long time before these devices are put in any device consumers can hold, but the future hopes for speeds of up to 100Gb/s, which blows current transfer rates out of the water at 15 greater than 802.11ac Wi-Fi.

 

Eavesdropper

0

 

Yet another example of how to enter the bigtime with your electrical ideas. Learn form example:

 

MIT Media Lab researchers Jay Silver and Eric Rosenbaum have designed an Arduino input device that lets you use any electricity-conducting material as a touchpad. Called ‘Makey Makey’, the device works by completing an electrical circuit with any conductive material such as vegitables, pencil lead or one's self to interact with the internet or programs on your computer. For example; you could play games Super Mario Bros by connecting the alligator clips to Play Doh buttons or play a piano program using bananas as the keys.

 

The research team designed Makey Makey around an Atmel ATMega32u4 8-bit AVR RISC-based microcontroller that runs Arduino Leonardo boot-loader and uses a USB 2.0 port to interface with a computer running an up to date OS (Windows XP, Vista, 7 and Mac OSX). The touchpad device requires no software to run as the PC recognizes it as a regular input device such as a keyboard or mouse and ,therefore, can run anything that uses those peripheral input devices. The team used Kickstarter to fund the Makey Makey project and was successful in reaching over $190,000 US with a target goal of $25,000. The device sells for $35 US (through Kickstarter) and comes with the board, USB cable, a set of alligator clips and your imagination.

 

Cabe

http://twitter.com/Cabe_e14

1

http://aperture.adfero.co.uk/Image/Original/7010714

 

Google's high-profile acquisition of Motorola Mobility is set to go ahead after regulators in China gave their official backing for the move. The deal, which is worth as much as $12.5 billion, means that Google will soon seize control of Motorola's patents.

 

Consequently, Google's ongoing battle with Apple has moved up another notch. Of course, Larry Page, the Google co-founder, is determined to ensure that the search engine giant soon competes on an even footing with Apple's iPhone, which currently dominates the lucrative smartphone market. Google has ambitious plans to extend its hardware business and this deal is seen as a key component of that.

 

Similarly, the takeover is seen as significant in terms of the continuing disputes over patents. Google is, of course, already the world's biggest maker of smartphone software and as a result of the acquisition, it will soon gain control of around 17,000 additional patents. With the new patents under its control, Google will be in a stronger position to protect Android devices in legal disputes with competitors, such as Apple.

 

The deal was first announced in 2011, but Google have been waiting on regulatory approval in China. In a statement, Google said: "Our stance since we agreed to acquire Motorola has not changed and we look forward to closing the deal."

 

Interestingly, though, the deal now puts Google in direct competition with other handset makers, like HTC, which work on the Android operating system. Under the terms of the deal, the Chinese Ministry of Commerce said that Android software versions must be free and open over the next five years.

 

Additionally, it has been confirmed that Google will be required to report to an independent monitor in China on its progress in meeting the terms of the agreement.

1

tumblr_m44kzh25YX1qe2k72.jpg

Attendees at the TEDx conference (via TEDxMogadishu)

 

Somalia’s capital city Mogadishu hosted their first ever TEDx (Technology, Entertainment and Design) conference earlier in March of this year. Between 50 and 100 people from diverse backgrounds attended the conference, held at the First Somali Bank, and discussed how to best to rebuild the war-torn capital and bring in new businesses after two decades of conflicts.

 

The forum was also a way of changing the world’s opinion about the country to show that there is more going on than terrorism and piracy in the hopes that new businesses will bring forth foreign investors (capitalists?). The event (called ‘Rebirth’) featured short films, music and speakers that included a University founder, property developers and health-care specialists. Only those who were invited (most of the invitee’s never heard of the TEDx conference) attended the talks due to security concerns, however, the forum was broadcasted over the internet for those who were interested. The talks came with mixed reviews as some thought that rebuilding Mogadishu gave them hope while others thought the focus should have been on rebuilding the country of Somalia itself. Still, no matter how you look at it any step forward is a monumental undertaking and a beacon of hope for that country.

 

 

Cabe

http://twitter.com/Cabe_e14

1

 

There’s good news for those of you who need to destroy your data stored on your SSD’s quickly and efficiently in an emergency situation. RunCore (manufacturer of SSD’s) has unveiled their new line of InVincible Solid State Disc drives which feature two ways to ensure data destruction.

 

The first capability the drives feature is ‘Intelligent’ destruction which over-writes the data and returns the drive back to its factory default setting. According to the company there is no possible way to recover the original data stored on the drive once the drive is reset. This is the rather mundane approach as the second option for data elimination is much more fun and effective (as well as costly).

 

The second option of data deletion the drives feature is self-destruction. Essentially the drive over-volts itself and physically damages the NAND chips inside rendering the drive useless (like a bad CPU overclocking job). To initiate both data erasure and destruction, the InVincible drives feature a two push-button system that is physically attached to the drive with the green button for erasing and a red button for meltdown.

 

These new drives were designed for the military, as well as other companies and institutions where sensitive data is being used or stored, and come in varying sizes and capacities that can withstand a temperature range of -45 to 200 degrees Fahrenheit. The company hasn’t said when the InVincible line of will be available or how much they will go for, but chances are they will cost more than current SSD’s and be available before the year is out.

 

Cabe

http://twitter.com/Cabe_e14

0

http://aperture.adfero.co.uk/Image/Original/7075531

 

Advanced Micro Devices (AMD) has just unveiled its new Trinity processor family, which it claims offers "twice the performance per watt" of Llano chips. AMD explained that the update features four CPU (central processing unit) cores and a single GPU (graphics processing unit).

 

The update is seen as particularly significant for people connected to the gaming community, with AMD saying that it will provide players with a significantly improved experience.

 

It has already been confirmed that the Hewlett Packard 'Sleekbook' - which is set to go on sale next month - will be the first consumer product to feature the chip. AMD, which is popular among computer manufacturers, explained that the chip can be set to run off as low as 17 watts, precisely half the minimum amount possible using its predecessor, Llano.

 

"Over the past decade, several test chips successfully demonstrated a variety of resonant clocking implementations," Joe Macri, AMD's chief technology officer, explained. "None, however, has achieved integration into a commercial processor due to various practicality or cost issues. AMD has managed to overcome these challenges.

 

"[It] results in a reduction in total core power consumption of up to ten percent."

 

For gaming fans in particular, the new chip is set to be especially beneficial, according to Sasa Markinkovic, the head of desktop and software product marketing. Indeed, AMD is intent on pushing Trinity's ability to manage high definition games on systems that are not kitted out with discrete graphics cards.

 

"When you look at Ivy Bridge it is a step forward for Intel in terms of graphics performance, but it's still not good enough for HD gaming - and that makes the difference between playable and not playable," he added.

 

Despite this, some analysts, including Sergis Mushell, processor expert at the tech analysis firm Gartner, have cast doubt over whether AMD will be able to compete with Intel, its long-term rival.

0

Nanofiber Energy Harvesting

Posted by gervasi May 21, 2012

ZnONanofiber.jpgI had the opportunity last week to talk to Dr. Xudong Wang from the University of Wisconsin about his research into energy harvesting using nanfibers.  By coincidence this came just a week after I talked to Dr. Krupenkin about his energy harvesting technology.  They are similar in that they generate energy using the electrostatic force to move current rather than by moving a wire through a magnetic field as in a traditional generator.

 

Nanofiber energy harvesting uses materials that develop a charge when mechanical compression deforms their crystalline structure.  This happens in materials made of atoms with a high disparity of charge.  The compression causes one side of the material to have more atoms of a positive charge while the other side has more negatively charged atoms.  PVDF is common material with this property.  It can develop several volts when compressed.

 

Dr. Wang is researching ZnO because it can be grown into nanofibers and it is not toxic to the human body, so it may therefore lend itself to powering medical implants.  Nanofibers can be located in an assembly in which wires or other nanofibers brush against them, causing them to develop a charge.  This charge can be collected and stored in a battery or capacitor. 

PiezoMatrixHarvest.jpg

The ZnO nanofibers typically only develop hundreds of millivolts, which makes it harder to harness than energy from PVDF.  How to collect charge efficiently from low-voltage sources is outside Dr. Wang's focus.

 

PVDFMicrobelt.jpgThe energy from airflow can be harvested from a thin film using this property by allowing the film to oscillate in the wind.  This has been demonstrated with PVDF.  If researchers can make this work with very thin films using nanotechnology, tiny amounts of power could be harvested from the airflow associated with respiration.  It would be good to see a productive use for a phenomenon that has become a metaphor for general engineering failure owing to the case of Galloping Gertie.   

 

This technology touches me personally because my mother-in-law has a pacemaker.  Her doctors are monitoring its battery's charge.  Replacing the battery requires surgery, which can always be risky in people with health problems.  So deciding at which point to change the battery becomes tricky decision.  One application Dr. Wang talked about was pacemakers.  The heart undergoes a lot of motion from which energy could be harvested.  If this technology could provide even some of the power for a pacemaker, it would be a huge benefit to patients. 

 

As with all energy harvesting, my impression is someone needs to find a "killer app" for it.  I'm not clear whether enough charge could be collected from nanofibers to put a dent in a pacemaker's energy budget.  It will likely find applications that the reasearchers haven't even considered. 

1

dragon_pica.jpg

Dragon capsule (via SpaceX)

 

SpaceX (Space Exploration Technologies Corp.) has recently announced that they will launch their Dragon free-flying reusable space craft on Tuesday May 22nd. This will mark the first time in history that a commercial company has launched a manned space vehicle into space to rendezvous with the International Space Station.

 

The Dragon re-usable space craft was designed using three main components which feature a nosecone that’s used as a shield during lift-off and houses the docking adapter needed to connect to external hatches found on the ISS. The second component featured is the spacecraft itself and was designed to be configured based on payload specifications and houses the avionics, RCS (Reaction Control System or thruster control systems) system, parachutes and other un-pressurized cargo/systems. The third component featured on the spacecraft is the Trunk which is used for un-pressurized cargo, solar arrays and thermal radiators needed to power the craft.

 

The re-usable vehicle will be launched atop of SpaceX’s Falcon 9 two-stage heavy-lift rocket which uses 10 Merlin 1C liquid oxygen and kerosene motors (9 on the first stage and 1 on the second). The mission will bring much needed supplies to the ISS as well as challenge the Dragon in a series of tests designed to test the feasibility of using commercial craft for future missions contracted through NASA and other organizations. If all goes well the launch will take place at Cape Canaveral at 4:15 AM Eastern Time and is expected to return a few hundred miles off the coast of California two weeks later. For those interested in watching the launch head over to SpaceX.com which will start broadcasting 40 minutes prior to launch.

 

Update: The rocket was scheduled to launch this past Saturday, the 19th. However, the team discovered a faulty check valve on the "Merlin Engine." The component was swapped, and not the historic flight will take place this Tuesday, the 22nd. The post was updated to reflect the change.

 

Update 2: The Falcon 9 is now in orbit. The launch was successful.

 

Cabe

http://twitter.com/Cabe_e14

1

 

Digital language translators are used every day. However, there is one dialect that still eludes the automation.

 

 

Engineering students, Ranjay Krishna, Seonwoo Lee and Si Ping Wang, from Cornell University are attempting to develop a very different type of translator, one that helps those who cannot make use of auditory signals. The students have created a sign language translator that converts hand gestures to their corresponding letter symbol and sound.

 

 

This translator is in the form of a glove for the hand and circuitry that fasten to the forearm. The glove itself contains nine flex sensors, four contact sensors, one x-y axis accelerometers and one z-axis accelerometer. The flex sensors are positioned around the upper/lower knuckles and the contact sensors at the tips of the fingers to distinguish between gestures. The accelerometers are needed because some letters vary only on movements of the hands and other letters vary only on the orientation of the hand.

 

 

An ATMega644 Microcontroller is used to analyze the signal from the electromechanical sensors and send transmission requests to the transmitter. The device is made wireless using a Radiotronix transceiver. All of this makes up what they call the Detection Unit, and it is simply strapped to the forearm.  The signal is then received by the base station with outputs the results to an LCD screen as well as transmits the signal to a computer via USB where it can also be outputted as sound through the computer speakers. The students used Matlab, Java and C for all their coding.

 

 

As far as can be seen, this device only converts gestures to letters so more development is needed for those gestures that represent nouns or actions but no doubt this is a start towards a world where we can all communicate a little easier.

 

Cabe

http://twitter.com/Cabe_e14

0

CortexA9.jpg

ARM Cortex A-9 (via TSMC)

 

Today's processor industry is largely controlled by two companies, Intel and ARM Holdings. Intel produces processors running in most of today’s laptops, desktops, and servers. On the other hand, ARM largely dominates the quickly growing mobile industry. Both are looking to invade each others markets soon by developing processors with high performance and low power consumption, or a strong performance per watt ratio.

 

 

Taiwan Semiconductor Manufacturing Company (TSMC) may have just made ARM Holdings future in the CPU market a bit more promising. At TSMC, they have recently ran a 28nm dual-core ARM Cortex A-9 processor at a max speed of 3.1GHz. The clock speed is 55% higher than present and is about twice as fast as its 40nm counterpart at TSMC. Additionally, the ARM chips also have the advantage of very little heat dissipation, giving them the ability to be densely packed together with one another.

 

 

Two of ARM's many partners include Nvidia and Calxeda, are both looking to produce ARM based processors to compete with Intel. Calxeda is working on producing chips for servers that work more efficiently. Such as implementing overlapping operations during each clock cycle to allow better speed handling. The method gives them an efficiency boost and may work to an advantage for large data retrieving applications such as web hosting.

 

 

TSMC also produces mobile chips for Nvidia. The successful high speed processing test can also mean good things for Nvidia. Nvidia is working on a custom ARM based processor to use in desktops and laptops to compete with Intel. The CPU project dubbed Project Denver has already been in development for some time, but TSMC's latest breakthrough could give the project a large boost.

 

 

The coming products produced from this “competition” should give us some interesting products in the future. Both companies will not easily be letting other companies invade their markets. The server market is worth $50 billion due to the rise of cloud computing and use of social networking. In addition, everyone can see the rise in the uses of tablets and smart phones.  The competition will lead us into the future of processor technology, which will be developed with these two companies paving the way.

 

Cabe

http://twitter.com/Cabe_e14

1

 

Microsoft has unveiled a revolutionary piece of kit that could transform the consumer electronic market over coming years. Using the new augmented reality system, consumers working in different locations would be able to collaborate on tabletop projects. The device, in essence, allows them to share objects that they can both handle.

 

The device, which is known as MirageTable, has been demonstrated at a conference in Austin, Texas. The firm also outlined details of the project on the firm's research site. The impressive system gives the illusion that the two parties are working together seamlessly. However, Microsoft researchers concede that even more work needs to be conducted before the kit can reach the consumer market.

 

Details of how the system works are provided on Microsoft's research site. The firm explained that using a 3D-video projector, consumers are able to beam images onto a sheet of curved white plastic. Thereafter, camera sensors are used to track the direction of each person's stare. They are also used to capture the shape and appearance of objects. And using shutter glasses, consumers are able to see the object in three dimensions, thereby rendering geographic boundaries obsolete for some people.

 

In a statement, the researchers said they were "motivated by a simple idea: can we enable the user to interact with 3D digital objects alongside real objects in the same physically realistic way and without wearing any additional trackers, gloves or gear".

 

Although the prospect of the MirageTable reaching the consumer market remains some way off, Microsoft researchers are optimistic about the future of the project.

 

"In our system, the user can hold a virtual object, move it, or knock it down, since all virtual and real objects participate in a real-world physics simulation," the research team said. "The unique benefit of this setup is that two users share not only the 3D image of each other, but also the tabletop task space in front of them."

 

However, the research team's positivity surrounding the project was tempered somewhat by the acknowledgement that simulating realistic grasping behaviours given depth camera input "remains an open research problem".

0

 

A tear-jerking introduction of the technology

 

A cerebrally controlled robotic system is being developed by a team of researchers from Brown University, Harvard Medical School, Massachusetts General Hospital and a host of others could give paralyzed people the ability to use robotic limbs to manipulate objects for themselves. Called ‘BrainGate’, the brain-controlled system allows the user to control a robotic limb through thought. To do this, the team implants a wireless microelectrode array (Neural Interface System) at 4 X 4mm directly on the motor cortex portion of the brain that controls motor function. The series of electrodes (100 in all) on the chip pick up the brain's activity associated with arm movement and sends the signals to a series of computers that use software (unknown at this time) to decode the brains activity. The computers then translate those signals into a series of instructions that tell a robotic arm to move and grasp an object based on the user’s desired intentions. The researchers are presently using two types of robotic arms, which are being continuously developed by DLR Institute of Robotics and Mechatronics and DEKA Research and Development Corporation.

 

HASy_01_Freigestellt200x300.jpg

DLR robotic hand/arm concept


The bigger of the two robotic arms being used by the researchers is DLR’s Hand Arm System, which is an external robotic arm made for more robust applications where impacts with heavy objects are nonconsequential (factory and warehouse work?).  The arm consists of a series of mechatronic compliance actuators with 52 drives and over 100 position sensors. The units hand alone features 38 individual tendons with each connected to an individual motor to provide tension and stiffness. The fingers use a similar configuration that uses two separate motors for individual grasping and tension based on the object being manipulated. The arm is so robust that you can actually beat it with a baseball bat without damaging any of the electronics.

 

deka_arm.jpg

Deka arm system

 

The second arm that the team is working with is DEKA Research and Development’s ‘Luke’ Arm (named after Luke Skywalker's mechanical hand). The arm is actually a robotic prosthesis that was designed for amputee patients and was developed as a DARPA tetraplegia project. The titanium Arm was designed to be roughly the same size as a typical human appendage and houses all of its electronics, motors and actuators inside (exactly how and what technology was used is currently unknown). The prosthesis features 18 degrees of movement which was accomplished by using rigid-to-flex circuit boards that were folded into ‘origami’ shapes placed inside the titanium housing. A vibrational motor at the top of the arm lets the user know how much pressure is needed to grasp an object through varying degrees vibration depending if the wearer is holding an egg or a brick.

 

Cabe

http://twitter.com/Cabe_e14

 

(All images and video courtesy of Crown Institute for Brain Science)

1

solar boat.JPG

PlanetSolar leaving Vieux Port (Via marcovdz)

 

Sometimes a simple idea or dream can lead to massive accomplishments. For Rapheal Domjan, his thought of  building a solar ship did just that.  MS Tûranor PlanetSolar, a unconventional yacht, traveled around the globe in 585 days using only solar energy to power its journey. In a quadruple record breaking feat, the ship stopped at 28 countries along the way promoting solar energy and exploiting its power. The ships demonstration of solar power will lead to many new boating innovations and will revolutionize the way ships are built.

 

 

Craig Loomes and his team designed the 40 person 'PlanetSolar' optimizing energy collection, aerodynamics, propulsion, and materials used. The ship is extremely durable , and light due to its carbon structure and also is the biggest solar powered ship built to date. Additionally, it is 35 meters long and 23 meters wide and boasts a large array of solar panels upon its top, nearly every surface. The solar panels bring in a 22.6% yield that allows for a maximum engine output of 120 kW and an average output of 20 kW. The solar panels charge a row of 6 large lithium-ion batteries that give them a maximum energy density. With the impressive completion of the solar only commute, soon many ships will be equipped with solar powered systems similar.

 

 

Working on the ship brought together a team of diverse people including electrical engineers, physicians, sea captains, and ship builders. Navigating around the globe brought them to many different places along the way. Though most of the stops were around the equator for maximum sunshine harvesting. The global adventure showed just how powerful solar energy can be. For now, the ship is resting at Hercule Harbour in Monaco soaking up rays in the sun. Solar energy is an option that may be too appealing to pass on for the future of sea faring ships.

 

Cabe

http://twitter.com/Cabe_e14

1

mit multi brain.JPG005.jpg

(Left) Erin Treacy Solovey wearing the Brainput device (Right) Artistic concept (via MIT & Erin Solovey)

 

When it comes to multitasking we as humans try the best we can. While we all have a modicum of ability, some are better than others. It suffices to say, we could all use a boost to become more efficient in our multitude of multitasking efforts, which is why a team of researchers has developed an unconventional solution to the problem. Led by Erin Solovey from MIT’s Humans and Automation Lab, the team has designed a system called ‘Brainput’ that can off-load some of our brains multitasking skills to a computer which is way more efficient at doing multiple things than we could ever hope to be. They system uses a portable low-cost version of a functional magnetic resonance imager called ‘fNIRS’ (functional Near-Infrared Spectroscopy) to measure the activity going on in the brain. The measurements are monitored and processed (using two probes) in real-time using Boxy software (from ISS). The information is then analyzed by a software engine (created using both Matlab and Weka tools) to look for specific patterns associated when the individual is multitasking. When the system has learned these patterns the software kicks in and is able to help the user with the task at hand.

 

A maze was created to test Brainputs effectiveness where a subject had to navigate through using two robots simultaneously. The operator using the fNIRS system was constantly switching back and forth between them and once the software learned the patterns it was able to engage sensors in the robots to help the user with their guidance. While the robots were autonomous, the test subject’s performance did indeed improve. While Brainput is still in its early development stages, it could be implemented into many applications in the future like helping you drive while you’re momentarily distracted or used during surgery with robotic assistance. What if the system could be used wirelessly? If you have an automated laundry machine, you could be slaving at work and washing your laundry at home at the same time! The possibilities are endless.

 

Cabe

http://twitter.com/Cabe_e14

1

01 tokyo hotaru2.jpg

LED Wishing Star art show (via Tokyo Hotaru)

 

LEDs have been used to create some of the world’s most interesting art. One of the more impressive pieces was showcased at the Licht Festival in Belgium last year, showcasing the cathedral of light. This year brought another large display of LEDs from Panasonic for Tokyo’s Hotaru Festival (Firefly Festival) which celebrates an age old tradition of…well…watching fireflies along river-banks. Panasonic took part in the ‘Symphony of Light’ celebration by releasing 100,000 ‘wishing star’ LED free-floating balls into Tokyo’s Sumida river which was complemented by the illuminated Tokyo Sky Tree. Each ball contains an individual LED which is powered by a tiny solar-cell and rechargeable battery making them fully self-sustainable and reusable. The piece is strikingly similar to what Mother Nature does naturally with bioluminescence.

 

01349158.jpg

Bioluminescent bloom of plankton, Maldives (via Doug Perrine)

 

Illuminating art can be found in nature and also uses self-sustainable energy like Panasonic’s ‘wishing star’ LED balls. These however rely on a chemical reactions (chemiluminescence) rather than solar to emit light. Plankton (much like the firefly) use a group of chemicals, known as luciferins, that oxidize and set off a catalyst called luciferase which produces ‘cold light’. Many of this plankton wash up on various shores where lucky on-lookers can appreciate a fantastic light-show like that recently found on Vaadhoo Island in the Maldives. Both of the displays were impressive in their own right, but only one of them was edible which edges Mother Nature as the winner of the illuminated art shows!

 

Cabe

http://twitter.com/Cabe_e14

 

More of the Panasonic Tokyo art show:

 

1 2 3 ... 55 Previous Next