Skip navigation

community

1 2 3 ... 12 Previous Next

News

175 Posts tagged with the alternative_energy tag
1

solar boat.JPG

PlanetSolar leaving Vieux Port (Via marcovdz)

 

Sometimes a simple idea or dream can lead to massive accomplishments. For Rapheal Domjan, his thought of  building a solar ship did just that.  MS Tûranor PlanetSolar, a unconventional yacht, traveled around the globe in 585 days using only solar energy to power its journey. In a quadruple record breaking feat, the ship stopped at 28 countries along the way promoting solar energy and exploiting its power. The ships demonstration of solar power will lead to many new boating innovations and will revolutionize the way ships are built.

 

 

Craig Loomes and his team designed the 40 person 'PlanetSolar' optimizing energy collection, aerodynamics, propulsion, and materials used. The ship is extremely durable , and light due to its carbon structure and also is the biggest solar powered ship built to date. Additionally, it is 35 meters long and 23 meters wide and boasts a large array of solar panels upon its top, nearly every surface. The solar panels bring in a 22.6% yield that allows for a maximum engine output of 120 kW and an average output of 20 kW. The solar panels charge a row of 6 large lithium-ion batteries that give them a maximum energy density. With the impressive completion of the solar only commute, soon many ships will be equipped with solar powered systems similar.

 

 

Working on the ship brought together a team of diverse people including electrical engineers, physicians, sea captains, and ship builders. Navigating around the globe brought them to many different places along the way. Though most of the stops were around the equator for maximum sunshine harvesting. The global adventure showed just how powerful solar energy can be. For now, the ship is resting at Hercule Harbour in Monaco soaking up rays in the sun. Solar energy is an option that may be too appealing to pass on for the future of sea faring ships.

 

Cabe

http://twitter.com/Cabe_e14

2

-010.jpg

(via Microsoft)

 

With the recent uncovering of toxic e-waste destroying the environment in Guiyu China, it was only a matter of time before huge companies started to rethink of what it actually means to be ‘green’. One such company is taking it rather seriously and is stepping up, becoming more environmentally conscious in every aspect of their business; Microsoft. The company will become completely carbon neutral by the beginning of the fiscal year, which starts on July 1st of this year (2012).

 

To do so, the company says that they are implementing an internal ‘carbon fee’ for each of their operations buildings in over 100 countries. Meaning each representative institution will be required to pay a fine (to Microsoft headquarters in Redmond) for carbon emissions based on renewable energy and carbon offsets. This will create an incentive among the data centers, office buildings and development labs to reduce or eliminate their carbon emissions. Some of the steps taken by Microsoft to become more environmentally friendly include ‘a smarter buldings pilot’ which entailed using software and technology to make Microsoft’s Redmond campus more energy efficient. Another step included using Carbonsystems Enterprise Sustainability Platform (ESP), which is an application that collects data from smart-meters, energy suppliers, waste processors and internal business systems to learn ways of reducing the global impact of carbon waste. Microsoft is even going as far as purchasing more renewable power agreements from various green conscious power companies and reducing air travel for business trips through based on the benefits incurred as each flight produces 1000kg of carbon emissions per trip. So far Microsoft is leading the way for a greener future , but we will have to wait and see if other companies follow suit in carbon-emission reduction.

 

Cabe

http://twitter.com/Cabe_e14

0

solium-550x300.jpg

Sodium in the raw (stock photography)

 

Batteries are a key part to developing green and more energy sustainable products. Lithium-ion batteries power almost everything we use today. A short list of applications; smart phones, laptops, GPS units, and electric vehicles. However, lithium is expensive and rare. So, having an alternative option to support those applications is a logical decision, especially due to China's dominance in the production of rare earth minerals. A recent project is making table-salt, sodium, an appealing choice for a lithium replacement.

 

 

Researchers from Tokyo University have recently created an innovative sodium-ion battery using a new electrode composition consisting of manganese, iron, and sodium oxides. The new metal mix composition allowed the researchers to create  sodium based battery that held a charge close to that of lithium. Lithium batteries are still more powerful due to lithium atoms naturally releasing more energy when they lose an electron. To match this power difference, the new batteries created consisted of a positive electrode that held more ions allowing it to reach energy densities close to that of lithium batteries by using the new metal material as the cathode (positive electrode) and sodium as the anode (negative electrode).

 

 

The metal mix was created by mixing the chemicals together and smashing them into a pellet sized shape. From there, the composition was heated at 900 °C for 12 hours. The result was a product with an average voltage of 2.75V and capacity of 190 milliAmp-hours/gram that decreased over 30 cycles. Furthermore, the energy density was very similar to that of the lithium electrodes around 520 mWhr/g. As of now the new batteries will not be smaller or longer lasting than the lithium ones (power density is around 1200 W/kg). However, they are cheaper and provide a nice alternative to their rare earth counterparts. The new finding will help further the development of battery technology, and may create an explosive new battery for consumer products. Let's hope no water is allowed to come in contact with the sodium; instant disaster.

 

Eavesdropper

2

Lilliputian_USB_MPS_270x166.jpg

Large and small fuel-cell charger (via Lilliputain)

 

Lilliputian Systems has recently announced their partnership with Brookstone (retailers of everything) to sell their portable Silicon Power Cell system that is capable of re-charging just about every mobile device with one butane cartridge, for several weeks at a time. The smaller charger can supposedly handle recharging a smartphone 10 times, and the larger charger can handle 20 times (3W output on both). The portable charger, a little bigger than a pack of cigarettes, houses a chip that takes advantage of a solid oxide fuel cell which converts butane into electricity with only a tiny amount of CO2 and water-vapor as a by-product. Although the internal temperature reaches 750 °C (1380 °F), the heated core is insulated so well that it can be touched. Conveniently, the butane cartridges are about the size of a cigarette lighter and come in various sizes with the smallest being able to provide ten charges before needing to be replaced.

 

A series of LED’s lets you know what’s happening with the device: Green lets you know your device is charging, Red to let you know your low on fuel, and Blue to inform you that a new cartridge has been inserted and ready to go. The portable charger is equipped with a USB port that allows for just about any mobile device such as phones, tablets, MP3 players and cameras to get a boost when you need it (especially at trade shows). There’s no word yet on the exact MSRP will be, but the charger is rumored to run anywhere from $150 US to $200 with the recyclable recharging butane cartridges going for $2 to $5 US depending on the size. An interesting sidenote is that the company states that you will be able to carry these butane filled chargers on airplanes, but regular lighters are still not allowed. It’s unknown at this time as to exactly when Lilliputian’s Silicon Power Cell will be available , but chances are that it will be out within a few months.

 

Cabe

http://twitter.com/Cabe_e14

0

liquid-solar-cell.jpg

Glass treated with nanocrystal solar element (via University of Southern California and Dietmar Quistorf)

 

As the dominance of solar power in today's energy market grows, so does competition within innovation and production of this technology. A recent addition to the solar mix is the advancements being made in liquid nanocrystals solar cells. These nanocrystal cells have their main advantages over their single crystal wafer counterparts in their cost and size. However, the low efficiency of nanocrystal solar cells has been holding back their expansion. Now, scientists from the University of Southern California have found a way to improve the efficiency of liquid nanocrystal solar cells to make them more competitive and solar energy more prominent.

 

 

The liquid nanocrystals used in the production of these PV cells are about 4 nanometers across. These cells must be stabilized and kept apart from one another. To do this, scientists used organic ligands that attached to the nanocrystals. Unfortunately, these organic ligands also acted as insulators that impeded conductivity between the crystals. To over come this, scientists at USC have engineered synthetic ligands that perform the same function as the organic ones but also improve the conductivity between the crystals and thus improve the efficiency and effectiveness of liquid nanocrystal solar cells.

 

 

This type of solar panel is cheaper to make than the traditional single-crystal silicon wafer partly due to their small size. These liquid crystals can exist as paint or ink that will not melt. Liquid nanocrystals can be applied to plastic surfaces, which can be shaped to fit in more places than traditional glass surfaces. Using liquid nanocrystals, solar panels can be made to be extremely thin and flexible. However, more research is needed to find more suitable materials to make these crystals. Currently, cadmium selenide is used in their manufacture but this chemical is commercially restricted due to its high toxicity. The commercialization of this technology is still years away but is a leader in the next generation solar cells.

 

Cabe

http://twitter.com/Cabe_e14

3

 

 

With all the smart-devices in our homes it only makes sense that Microsoft would come up with a way to control them all within a centralized hub. Devices like smart-fridges, automated coffee makers, motion sensors and mobile phones can all be manipulated through the use of Microsoft’s HomeOS software which turns your home into a sort of smart-house. Researchers designed the software using what they call ‘PC-like abstraction’ which is a fancy term for their specialized software kernel (written using C# and Net 4.0) that gives our appliances the ability to communicate to a computer as well as being remotely-operated through mobile devices. For the past 8 months, researchers have been testing HomeOS in 12 homes with promising results according to Microsoft. In fact over 50 students have already been writing various apps for the software with some letting the user control gaming consoles and Blu-ray players directly from your mobile phones and tablets which will be available on Microsoft’s HomeStore in the near future. As of now, the HomeOS SDK is available for free to any academic institutions (schools) to encourage teaching on automated homes with no word yet as to when it will become available to the general public.


logo-only-green.png

HomeOS logo (via Microsoft)

 

 

Eavesdropper

 

See some other "smart-home" tech:

Health monitoring home

Nissan's alternative energy home

2

bio-solar-cell.jpg

Spinach based solar cell prototype (via Vanderbilt School of Engineering)

 

Engineering students from the Vanderbilt School of Engineering have recently received a $90,000 US grant from the EPA (Environmental Protection Agency) to continue development of a hybrid bio-solar panel that makes use of a protein found in spinach. Their solar-panel design makes use of photosynthetic proteins extracted from spinach as an alternative to silicon-based photovoltaic cells to produce electricity. The solar panel is comprised of 24 centimeter-sized cells deposited on a non-biological substrate that use PSI (Photosystem I) instead of silicon as the energy harvesting/conversion (photosynthesis) medium, which is coupled together with thin copper strips that also act as an electrical conduit. The next phase is to construct a 6' (1.8 meter) square panel consisting of 1,000 of the square centimeter cells (0.39" square).

 

biosolar-panel.gif

Full panel concept (via Vanderbilt School of Engineering)

 

The energy produced by this method is minimal at best. The tech could be used to power less demanding remote-based sensors, but it doesn’t rival the power produced by today's photovoltaic cells. The up-side is that the team hopes the future revisions would be both energy efficient as well as easier and cheaper to produce over silicon-based panels. As a result of winning the EPA-sponsored People, Prosperity and the Planet (P3) contest, where college students design projects for a sustainable future, the team was able to walk away with their sizable sum for further development of their spinach-powered solar panel.

 

Cabe

http://twitter.com/Cabe_e14

2

 

Sapping the energy out of wind usually involves wind turbines that stand between 27 and 94 meters from the earth's surface. Altaeros Energies thinks that’s not high enough to capture significant wind energy, so they’re looking to ‘float’ a newly designed wind turbine to new heights.

 

The energy company (created by former students from both MIT and Harvard) has designed a new prototype turbine that collects wind energy from altitudes at over 305 meters (~1000 ft) high where the wind is often stronger. Called the ‘Altaeros Airborne Wind Turbine,' the renewable energy generator uses a helium filled shell composed of aerostats (same material used for passenger blimps) that houses a Southwest Skystream wind turbine in its center  suspended by cabling. The whole inflatable structure is tethered by cables to the towable docking trailer that collects the energy for powering mobile diesel generators.

 

-001.jpg

Turbine by Altaeros Energies

 

The company recently tested the AWT at an altitude of 106 meters (350 ft) where it produced twice the power of comparable size generators found on the ground. After which, it landed safely all through a successful automated cycle. The only problem I can foresee with this novel approach at harnessing wind energy is interference from low-flying airplanes, which limits where the AWT can be deployed. Other than that, it seems like an ingenious idea.

 

For those who have read helium is becoming scarce and now question Altaeros Energies' turbine usefulness for the planet, the company has released this statement: "Helium is found in natural gas deposits. Industry leader CryoGas International reported in Oct 2011: "substantial world helium reserves exist in North America, the Middle East, Africa and Russia and that these could sustain the helium industry for hundreds of years." Over time, prices will likely rise, but helium is less than 5% of the cost of an Airborne Wind Turbine, and this will not significantly impact the product cost."

 

Cabe

http://twitter.com/Cabe_e14

0

shockabsorbe.jpg

Energy harvesting shock absorber with mechanical motion rectifier concept (via Lei Zuo)

 

Potholes and bumps in the road usually decrease the life of our vehicles shock absorbers over time, so we tend not to think of horrible road conditions as beneficial. Now we can.

 

A team of engineers from the State University of New York have designed a new type of shock absorber that actually harnesses the energy created by those rotten roads and turns it into electricity. The team, led by Professor Lei Zuo, recently designed the regenerative shock absorber (Mechanical Motion Rectifier) using a hydraulic system that turns a set of rotational gears through the cars vibration. The gears in-turn takes the irregular vibrational energy and transfers it to an electrical generator that converts it to electricity, which leads back to the vehicles alternator. The electricity is then used to recharge the vehicles battery as well as its electronics, which provides between 2 to 8 percent fuel efficiency over vehicles with standard shocks.

 

This translates into a fuel savings of 4% for vehicles that use an internal combustion engine and 8% in savings for hybrid vehicles. As an added benefit, the MMR shocks provide a smoother ride as they absorb more vibration over normal shocks. Professor Zuo says that the MMR’s could also be applied to train tracks which would power electrical devices such as lights and crossing gates as the trains vibrational energy is transferred. It stands to reason that only ‘good vibes’ can come from the MMR system being implemented into vehicles. Zuo states that if 5% of the 256,000,000 vehicles on the road today used the shocks we could reclaim more power than Niagara Falls produces per year. Every little bit adds up.

 

Professor Zuo's research was reported on back in July of 2010. In less than a year, Zuo and his team doubled the efficiencies from 1% to 8%. The boost was made by adoption a gear train generation over a

magnetic induction.

 

With the change, the shock absorber has an investor. The company Harvest Energy has licensed the tech. We may see the absorbers on buses and trucks in the near future. Progress is slow.

 

Cabe

http://twitter.com/Cabe_e14

0

 

If you remember the movie ‘Alien’, the crew was tasked with mining various planets and asteroids before their eventual demise on planet LV-426 (Everyone but the hero, that is). While that was science fiction, a new start-up company wants to make mining asteroids and other planetary bodies a reality.

 

Called Planetary Resources, the company is looking to explore the vastness of space. as well as mine valuable metals and water from resource-rich asteroids. To do this, the company will first deploy a low-cost ‘Arkyd-Series 100 Leo Space Telescope’ to search for near-earth asteroids that are rich in resources. Once potential asteroids are found, the ‘Arkyd-Series 200 Interceptor’ (a powered version of the 100) that houses additional scientific equipment will then head to the target and assume a geostationary orbit where it will collect further information on the suspected resources.

 

Once the information collected by the 200 series is confirmed, a ‘Arkyd-Series 300 Prospector’ with laser-based communications is sent out to survey the asteroid and collects information on its shape, density and surface/sub-surface composition in preparation for mining to begin. Initially, only asteroids that contain water will be mined as it can be broken down to its base components (hydrogen and oxygen) and used for fuel making the asteroid a kind of space gas station. The company hopes to use their Arkyd system as a cost-effective means of space exploration while simultaneously grabbing precious metals while doing so.

 

Technology-LEO-Web.pngTechnology-Intercept-Web.pngTechnology-Prospecting-Web.pngTechnology-Mining-Web.png

Concept art for the stages of mining: (1) Scan for targets (2) Up close data collection (3) In depth scan of asteroid (4) Actual mining operation

 

So far the company has no actual details of exactly how these planetary bodies will be mined (I have to go with the concept of Alien's Nostromo, send people there) and transported back to earth but the idea is intriguing to say the least.

 

The company was founded by X Prize board members Eric Anderson and Peter H. Diamandis. Although this effort seems far-fetched, several billionaire investors are banking on the quest. Director James Cameron, Google CEO Larry Page, Google chairman Eric Schmidt, Google executive Ram Shriram, Ross Perot Jr., and Microsoft executive/verteran astronaut Charles Simonyi, to name a few. With the potential operating income, who knows what the future holds for Planetary Resources.

 

Cabe

http://twitter.com/Cabe_e14

2

 

According to a recent survey people were found to love the idea of electric cars most due to lower impact on the environment, as well as the money saved on gas. However, 65% polled showed that they had ‘range anxiety’ (stranded with no power) that prevented them from purchasing an electric vehicle. It’s with the peoples concern that IBM started their ‘Battery 500 Project’ back in 2009, which could make future generations of batteries capable of traveling 500 miles on a single charge over the current generations’ 100 mile capacity.

 

Fast-forward to 2012 and Central Glass (materials manufacturing) along with Asahi Kasei (chemical manufacturing) have jumped on-board in developing a new type of lithium-air battery. Lithium-air batteries are designed to take in air (or breathe) as the vehicle is being driven which mixes with lithium-ions on the batteries anode (oxidation). This reaction produces lithium-peroxide which in-turn reduces the oxygen on the nan-carbon matrix layer of the battery thereby creating electricity and putting lithium back onto the anode. This process helps to extend the charge of the battery by storing the electricity created during the chemical reaction. While the development of the battery is still in its infancy, IBM is looking to release their final design to the automotive industry sometime around 2030.

 

Waiting almost two decades to get a 500 mile range electric car is not acceptable. Oil reserves, depending on who you ask, are predicted to be depleted within the next 12 - 40 years. Oil is an essential part of manufacturing, product composition, and farming. Wasting oil in human transportation, when there is an alternative close at hand, seems like a crime. The Tesla Roadster and Model S both have a 300 mile option already. Double the size of the battery, add solar, and suddenly there is a possible 700 mile electric car. Cost is the true problem. I am sure the IBM Lithium-Air battery will be comparatively expensive when it is released.

 

coda-battery-vga.jpg

Tesla Model S battery (in white/yellow area). Doubling that size does not seem out of the question. (via Tesla Motors)

 

Cabe

http://twitter.com/Cabe_e14

2

solarcity plan.JPGtesla box.png

(Left) SolarCity & Tesla's overall concept drawing (Right) The Tesla battery storage controls (via SolarCity)

 

In the transition to sustainable lifestyles, a big hurdle is staying "green" when renewable energy is not available. Elon Musk, CEO of Tesla other companies like PayPal and Space X is teaming up with his successful cousins Lyndon and Peter Rive  who are co-founders of SolarCity in tackling the problem of battery energy storage systems primarily for solar-roof panels.

 

 

After a few years of research, the team has concluded that the most doable configuration is a systems made up of stacks of thin lithium laptop-like batteries. The main source for batteries will be Panasonic, but other Asia based companies are on the short-list for back-up sources. The project is exciting because it plans to make use of funds from the California Public Utility Commission (CPUC) and Federal programs offering incentives for distributed energy generation to further drive the price for these systems low enough for wide consumer consideration.

 

 

Tesla and SolarCity have submitted 70 applications for funds from the CPUC’s Self Generation Incentive Program (SGIP) and funds offered by the Pacific Gas and Electric Company. Director of Communications for SolarCity, Jonathan Bass, says that there are many different projects with different applications. The applications have received a “conditional reservation” from the SGIP which means the companies will receive the funds once the systems are completed and operational. 

 

 

The projects have 18 month to be completed and operational. It is suspected that most will be done earlier. The cousins should have little trouble in producing some of these projects to the consumer shortly after.

 

Cabe

http://twitter.com/Cabe_e14

2

so-fi_bag.jpg

M Azzuro messenger bag (via so-fi)

 

On element 14, we have seen various attempts to merge technology with fashion. Finally, an attempt to merge these worlds has been recognized with a prestigious Red Dot Award for Product Design in the category of fashion, lifestyle and accessories. The winner was the M Azzurro messenger bag by so-fi ®. This bag’s special capabilities are harnessing solar power to charge smart phones, tables, MP3’s, digital cameras and other portable devices via a USB port located inside the bag.

 

 

Apart from this empowering feature, the award was won because of its sleek design, remarkable craftsmanship. The M Azzurro is made of high-density nylon and has a flexible, waterproof, crushproof solar panel made by UNI-SOLAR. The built in USB port stabilizes at 5.3 volts and delivers up to 550 mA of current. At this voltage, portable devices take between 2 to 4 hours to fully charge. However, the bag is capable of delivering power to any device as the sun is shining. The bag features 2 inside pockets, a zipper-pocket inside and one outside and one snap closure outside pocket.

 

 

The bag can be purchased from the so-fi website for around $200 dollars. Once you have it, you wont have to worry about forgetting your phone charger again, as long as it is sunny.

 

Cabe

http://twitter.com/Cabe_e14

1

 

Its no secret that when it comes to scientific innovation, products of nature have had millions of years of development.  Engineers are becoming quite aware of this. A perfect example is the simple and efficient propulsion method behind the jellyfish. Natures elegance is being replicated by Yonas Tadesse and his team at the University of Texas at Dallas and VirginiaTech . The Robojelly is born.

 

 

Robojelly is made from shape-memory alloy that returns to its original shape. When bent can be arranged to mimic the jellyfish propulsion movements. Robojelly is made up of eight moving segments covered in carbon nanotubes and coated with a platinum powder. The platinum powder is needed to chemically react with the hydrogen and oxygen in the water to create the heat that powers the Robojelly. The heat causes the alloy to change shape and repetition causes the jellyfish-like movement and propulsion. Tadesse, who is leading the creation of this robot announced, “to our knowledge this is the first successful powering of an underwater using external hydrogen as the fuel source.”

 

 

The robot holds high hopes for use in under water exploration, search and rescue operations, and surveillance. However, it still has a long way to go before it can be used. Current design restrictions limit the robot to move up only. The team is looking for methods to deliver hydrogen to specific parts of the robot independently, so it can eventually move in 3 dimensions. 

 

Eavesdropper

2

LP_CF_S_LPRIZE_EU-CLP-global-001.jpg

Promotional image of the L Prize winning bulb. (via Philips)

 

Back in 2007, the US Congress started what’s known as the L-Prize, which is a competition run by the Department of Energy to design efficient solid-state lights to replace the aging incandescent light-bulb. Contestants who take on the challenge are to design replacements for the PAR 38 halogen incandescent bulb ($5,000,000 US in prize money) as well as the standard 60 watt bulb ($10,000,000 US in winnings). Out of all the contestants that entered, Phillips took the top prize for the replacement of the 60 watt bulb as they were the only company who entered. Their L-Prize winning 60 watt LED bulb (with 940 lumens) only eats about 10 watts of power making it more efficient as well as cost effective by saving the consumers a whopping $8.00 annually (per bulb used). The newly designed bulb is set to go on sale on Earth Day (4/22) of this year (2012) at a price point of $50.00 US. This price may be reduced in the future if utility companies subsidize the bulb, which may in-turn offer rebates, which would bring the price down even further.

 

Seems like buying a "green" lightbulb is a major decision.

 

Eavesdropper

1 2 3 ... 12 Previous Next