Engineers become millionaires in less than 30 days; learn from their example.
Pebble Technology has recently entered into the Kickstarter hall of fame with their E-Paper watch gaining over $10,000,000 US in funding after only 26 hours of being put on the site. So, what makes the E-Paper watch so popular? It functions as a connection interface between your smartphone and as a wrist-mounted watch with app capabilities, a relatively simple embedded system.
Pebble Smartwatch (via Pebble)
The watch can be infinitely customized with different watch-faces (which is always on) and is compatible with both iPhone and Android (2.3 and higher) smartphones with a wide range of apps that let you check e-mail/text messages, caller ID and Facebook/Twitter accounts among others. The E-Paper watch connects to your smartphone through a Bluetooth 2.1+ EDR/4.0 connection and houses an ARM Cortex-M3 microcontroller which has over 8X more Flash memory and 12X more RAM than their previous inPulse Smartwatch. The ‘face’ is actually a high-resolution (144 X 168) black and white e-paper display and has a vibrating motor with a 3-axis accelerometer that’s capable of gestural detection. Charging the watch is the same as you would a smartphone by using a USB cable either for your PC/wall-outlet or mobile charging platform and has a life-span of 7 days before it needs to be re-charged. For those of you who love the water, E-paper is expected to be fully water-proofed to either 3 or 5 ATM (up to 165ft) if you can stand the pressure but make no mistake the watch IS NOT water-proof. Pebble Technology has sold out their first batch of 85,000 units, so the rest of us will just have to wait for E-Paper’s second coming.
Cabe