Skip navigation

community

News

8 Posts tagged with the development tag
1

 

Engineers become millionaires in less than 30 days; learn from their example.

 

Pebble Technology has recently entered into the Kickstarter hall of fame with their E-Paper watch gaining over $10,000,000 US in funding after only 26 hours of being put on the site. So, what makes the E-Paper watch so popular? It functions as a connection interface between your smartphone and as a wrist-mounted watch with app capabilities, a relatively simple embedded system.

 

photo-full.jpg

Pebble Smartwatch (via Pebble)

 

The watch can be infinitely customized with different watch-faces (which is always on) and is compatible with both iPhone and Android (2.3 and higher) smartphones with a wide range of apps that let you check e-mail/text messages, caller ID and Facebook/Twitter accounts among others. The E-Paper watch connects to your smartphone through a Bluetooth 2.1+ EDR/4.0 connection and houses an ARM Cortex-M3 microcontroller which has over 8X more Flash memory and 12X more RAM than their previous inPulse Smartwatch. The ‘face’ is actually a high-resolution (144 X 168) black and white e-paper display and has a vibrating motor with a 3-axis accelerometer that’s capable of gestural detection. Charging the watch is the same as you would a smartphone by using a USB cable either for your PC/wall-outlet or mobile charging platform and has a life-span of 7 days before it needs to be re-charged. For those of you who love the water, E-paper is expected to be fully water-proofed to either 3 or 5 ATM (up to 165ft) if you can stand the pressure but make no mistake the watch IS NOT water-proof. Pebble Technology has sold out their first batch of 85,000 units, so the rest of us will just have to wait for E-Paper’s second coming.

 

Cabe

http://twitter.com/Cabe_e14

2

AI mit google.jpgai book.JPG

(Left) Software interface. (via Google) App Inventor book by David Wolber (via Amazon)

 

Not being able to find an app, that can perform a specific task, can be frustrating. The only option is to develop it yourself. Google and the Massachusetts Institute of Technology (MIT) joined forces to help you get started.  The two came up with the "App Inventor" for android software toolset. The software allows your imagination to go wild in the Android app world as quick as possible.

 

If you have an idea for an app, but not very code savvy, don't sweat it. The App Inventor was invented for the pure purpose for users that have no prior knowledge of programming. They created easy to use developing app software for everyone.

 

Do not start whipping out your wallets yet, App Inventor is, according to MIT’s website. However, they said they will one day accept contributions for the software. The MIT team explained the goal, "[We] hope to nurture a robust and active open-source project but for now we don't want to distract the MIT developers from their efforts to complete and deploy the large-scale public server. In the meantime, we'll update the code periodically to match what's running at the latest MIT experimental system."

 

Google decided to shut down their App Inventor service due to recent service call, but the MIT team is still in full force. Download the App Inventor initial free (open-source) release at the project's main page. Not much support is available at the moment, but expect a deluge of examples and help to come in the next few months.

 

App Inventor uses the Apache License 2.0, which does allow for the selling of apps created with the software. Other restrictions may apply. Despite all this, App Inventor looks like an easy way to get started in the app-creation world.

 

Cabe

http://twitter.com/Cabe_e14

2

kinect for windows.JPG

Kinect for Windows v1.0 (via Microsoft)

 

The Microsoft Kinect is a widely popular object tracking camera system first released for the XBOX 360. It allows users to interface with games and menus without operating a controller. After its release, the "hacker" community quickly adapted the tech for use with computers. Simple tracking programs and art based developments soon followed. Due to the popularity, Microsoft started the Kinect Accelerator program, offering large cash prizes for further development with the Kinect.

Flash forward to today, Microsoft has released the Kinect for Windows version 1.0. Included in the release is a SDK and runtime environments. Most notable in the release is a "near-mode" for the new Kinect hardware, allowing tracking to be clear at 40 cm (approx 15 inches). Having one on a desk is completely feasible now. (With the XBOX setup, users have to be several meters away for accurate tracking.)


Improved tracking, controlling up to four Kinect sensors, improved speech recognition, and a driver update system is included in the release of v1 hardware and software. The SDK is meant for companies looking to develop software or other products for the Kinect, but it is available for anyone to download at the moment. Applications written in C++, C#, or Visual Basic in MS Visual Studios 2010 is supported right out of the box.


The Kinect for Windows hardware is planned to cost $250, and it is available now. An educational price of $150 will happen later this year. I sense a mad rush to be the first to market various control interfaces using Kinect. Hop in the dev-train now, or read more about the release at the
Kinect for Windows page.


Cabe

http://twitter.com/Cabe_e14

 

 

How will we look using Kinect for Windows? Find out in this week's Engineering On Friday.

 

 

More Kinect based projects:

Holodesk, the virtual 3D desktop

Control your robot with Kinect

Robotic shopping cart, follows its user around

Control the web and Windows 7 with Kinect

Kinect and Surface, virtual physics engine

Advanced robot tech for the masses

Upgraded humanoid service robot, buy it now

Autonomous robot plays catch

Surgeons of the future might use robotic nurses

0

6670104839_11eb706b84.jpg

Via SONY @ CES 2012

 

This year’s CES in downtown Las Vegas has, so far, been a showcase for screens of all kinds. From tablet and phone displays to massive multi-TV screens, the companies vying for king of the hill are endless. One company though says that the future of viewing displays is Crystal, and after seeing it I might have to agree.

 

The screen in question is Sony’s Crystal LED Display which is a massive 55 inch behemoth that houses an astounding six million (2mil of each color- RGB) edge-light LED’s! No, that wasn’t a typo, the Crystal screen is said to be superior to both Plasma and regular LCD displays, according to Sony. Rather than light the screen from behind with LED’s, Sony’s display has them mounted ‘IN’ the screen, which gives the display a better contrast and a wider range of color gamut over traditional LCD screens. Using LED’s instead of pixels also lowers the power consumption and increases the response time as well.

 

Whether or not we as consumer will ever see these types of displays in our homes is anyone’s guess, as some of you might remember we were supposed to have Samsung’s AMOLED transparent screens from CES 2011. Regardless, it is an impressive display and I hope Sony follows through with their prototype to bring us better resolution for the future.

 

Cabe

Follow my CES walk at:

http://twitter.com/Cabe_e14

0

 

Through software, two designers show how a contact microphone can detect particular sounds and trigger certain events. Bruno Zamborlin and Norbert Schnell designed the system around two ideas: convert vibration in direct sound, and certain sets of sounds triggering pre-determined audio tracks.

 

The project, dubbed Mogees, is developed in the Max/MSP environment with MuBu, a "multi-track container for sound description and motion capture data." Mogees has acted like an experiment demonstrating the team's goal of real-time interactive audio processing with MuBu. Both designers are key developers behind the MuBu project, as well. Be sure to take a look at their site.

 

I can already sense the legions of musical artists yearing to use Mogees in future projects. For those who think this will make for a new type of touchscreen, keep in mind that this technique can only sense sound and not position directly. Although, a different interpretation of the sound data could be used in a similar way to "surface acoustic wave" (SAW) touchscreens. Like in SAW tech, if the acoustic wave amplitude traveling along the surface of a material could be measured, position could be determined... But now I am getting ahead of Mogees purpose.

 

Cabe

http://twitter.com/Cabe_e14

0

phonegap.JPG

(Via PhoneGap)

 

Have idea for a simple phone app? Why not release it for the 4 big mobile operating systems at the same time: Windows Phone, Android, iOS, Blackberry, symbian, bada, and webOS.

 

PhoneGap 1.3 was recently released bringing along with it the most useful cross platform development environment to date. The new update mostly is to give Windows Phone 7.5 (Mango) full support of the features. The backbone of PhoneGap is based on web development standards, which innately bridges between the platforms already. The core relies  upon Java, HTML5, CSS and many native PhoneGap tools to get the job done. The best part is, PhoneGap is open-source. 

 

Originally developed by the company Nitobi, now part of Adobe, the PhoneGap framework (aka Apache Callback) has seen many contributors add to the project, most notably, RIM, IBM, and Microsoft. 

 

Unfortunately, according to the licensing agreement, PhoneGap can only be used on free apps. However, nothing says developers cannot make money with in-app advertisement. Take a look at the PhoneGap website to get started.

 

 

See more software development in the Knode OS forum.

 

Cabe

http://twitter.com/Cabe_e14

0

 

As motorcycle is to automobile, so is the Martin Jetpack to airplanes. The concept by, student, Glen Martin was conceived in 1981. Getting validation from the University of Canterbury's Mechanical Engineering Department, a successful prototype that exceeded the "Bell Rocket Belt" flight time of 20 seconds was built in 2005. This set the platform for public demonstrations in 2008, which ignited the media world.

 

The jetpack is based on a twin propeller design to gain flight, very similar to "light helicoptors." Plenty of safety features a built in, roll cage, auto stabilization, parachute, and avoidance systems. Now after 2,500 successful test flights, 100 combined engine hours, the Martin Jetpack is ready for public consumption. 43 minutes of Individual flight, at a time, can be gained for $100,000 USD. No pilots license is needed, however a Martin Aircraft training program is required. Waivers soon to follow as well.

 

The jet pack is being pushed for military and civil defense use. A unmanned, UAV, version is also in the works.

 

A remarkable 30 years of development soon to give a lot of people what they always dreamed of, a personal jet pack.

 

Eavesdropper

0

Robotic Media Center

Posted by Eavesdropper Apr 7, 2011

 

Reeti, a new robot home media center computer, seeks to bring a lot in a small package. Reeti's major feature over any other media device is its anthropomorphic appeal. Expressions are "endless," programmable, and alterable via an iOS device. The bot contains touch feedback, two microphones, and two HD cameras capable of 3D video all for the purpose of interaction.

 

Reeti is an open-platform running Ubuntu. Aside from the base applications, users are free to develop for the device. Pre-installed open-source libraries, and SDK, and middleware is provided to aid in application development. They really want people to like this bot.

 

Its core tech give it a lot to like. The processor is an Intel Atom Dual core at 1.8Ghz. 2GB DDR3 ram, Blu-ray reader, DVD burner, USB 2.0 and 3.0, Gigabit Ethernet, HDMI 1.3, 7.1 Audio, and Nvidia ION 2 HD and 3D round out the rest of its core features.

 

Into developing, watching movies, and robots? Reeti is just for you. Make a Netflix app when you get one.

 

Eavesdropper