Skip navigation

community

News

4 Posts tagged with the hybrid tag
0

shockabsorbe.jpg

Energy harvesting shock absorber with mechanical motion rectifier concept (via Lei Zuo)

 

Potholes and bumps in the road usually decrease the life of our vehicles shock absorbers over time, so we tend not to think of horrible road conditions as beneficial. Now we can.

 

A team of engineers from the State University of New York have designed a new type of shock absorber that actually harnesses the energy created by those rotten roads and turns it into electricity. The team, led by Professor Lei Zuo, recently designed the regenerative shock absorber (Mechanical Motion Rectifier) using a hydraulic system that turns a set of rotational gears through the cars vibration. The gears in-turn takes the irregular vibrational energy and transfers it to an electrical generator that converts it to electricity, which leads back to the vehicles alternator. The electricity is then used to recharge the vehicles battery as well as its electronics, which provides between 2 to 8 percent fuel efficiency over vehicles with standard shocks.

 

This translates into a fuel savings of 4% for vehicles that use an internal combustion engine and 8% in savings for hybrid vehicles. As an added benefit, the MMR shocks provide a smoother ride as they absorb more vibration over normal shocks. Professor Zuo says that the MMR’s could also be applied to train tracks which would power electrical devices such as lights and crossing gates as the trains vibrational energy is transferred. It stands to reason that only ‘good vibes’ can come from the MMR system being implemented into vehicles. Zuo states that if 5% of the 256,000,000 vehicles on the road today used the shocks we could reclaim more power than Niagara Falls produces per year. Every little bit adds up.

 

Professor Zuo's research was reported on back in July of 2010. In less than a year, Zuo and his team doubled the efficiencies from 1% to 8%. The boost was made by adoption a gear train generation over a

magnetic induction.

 

With the change, the shock absorber has an investor. The company Harvest Energy has licensed the tech. We may see the absorbers on buses and trucks in the near future. Progress is slow.

 

Cabe

http://twitter.com/Cabe_e14

0

BAE.jpg

(via BAE Systems)

 

Recently the US military has been increasing its use of ‘green’ technology in the last few years, but they have been in the area of renewable energy sources for some time. The armed forces are slowly but surely incorporating hybrid vehicles into their ranks. One such vehicle, being developed by the partnership of BAE systems and Northrop Grumman for the US Army, is both green and lethal. Called the Ground Combat Vehicle, the armored troop-carrier sports a hybrid-electric drive system that uses two electric motors (generating 1,400 horsepower) powered by a lithium-ion battery. Two diesel engines, which hold 255 gallons of fuel, provide back-up power as well as recharging the batteries when necessary. What makes the GCV a formidable threat is its ability to run completely on battery power, which makes it almost silent on the battlefield. Overall, the fuel efficiency of the tank gets a 10-20% boost over its stock counterpart. Another notable feature of the hybrid is the ability to ‘plug’ in electric-powered weapons systems such as LRADs (Long Range Acoustic Device) and microwave weapons which gives troops more options when it comes to load-outs.

 

The 70 ton hybrid can carry three crew members and nine passengers with a top speed of 43 Mph at a range of 186 miles. It’s also outfitted with a 7.62mm coaxial machine gun and 25mm auto-cannon as a base platform which can be upgraded with different weapons for depending on the scenario. The GCV looks like an updated hybrid Bradley Fighting Vehicle for the 21st century but with thicker armor and a completely different drive system. The Defense Department has approved for production at a cost of about $11,000,000 US each which would make the GCV a truly ‘Mean Green Killing Machine’!

 

Cabe

http://twitter.com/Cabe_e14

2

hiriko.jpgkirako 2.JPG

Hiriko concept images (via MIT)

 

Double saving with this car! You can save money and save room. Hiriko ("of the city") is the name of the double whammy car that can not only fold itself but runs on electric. The inventor is Jose Manual Barroso who is the president of the European Commission, in Brussels. Barroso is working on the project with the Spanish government and the USA's MIT Media Lab. Their goal is to have the Hiriko on Spanish streets by 2014.

 

Being a folding, do not except much room. The rear wheels simply fold right under the chassis, compressing the rear section forward, folding vertically. This makes the car only two-thirds the of the floor real estate of the Smart ForTwo. In other words, it is small when parked. There is only one door to get in and out this two-seater. The last car that opened up in the front was not much of a success, let us hope for the best with this one.

 

Hiriko’s power comes from a four in-wheel motor. Each wheel is independently driven and is steered by the “robot” electric motor. The oddest design feature stated is the system can tug at the drivers fingers via haptic feedback in the steering wheel. Aside from the haptic traditional shaped steering wheel, a joystick control will also be an option, which is undeniably a throw-back option similar to early model automobiles.

 

Unfortunately, you cannot get your hands on one. Only the 20 prototypes are rolling out to street testing in various European and American cities so far. However, in 2014, expect a price tag for the EV Hiriko to be in the $16,000 range.

 

Cabe

http://twitter.com/Cabe_e14

2

hydrogen_hybrid_cycle.jpg

The energy cycle (via Vattenfall)

 

In a time when the European Union is in financial turmoil, German, French and Swedish companies are showing that there is the undeniable potential of renewable energies. Creating a small “ecosystem” of energies, each supporting or complementing the other is a clear example of what scientists and engineers are capable of when given the right resources and are not doubted by investors or restricted by money.

 

While there are many ways of generating renewably energy, engineers have had trouble finding ways to store excess energy. This has always been a drawback to obvious renewable-energy  solutions like wind energy. However, a new innovative power plant in Germany has found a solution.

 

Many European companies, including Vattenfall, Siemens, Enertrag along with research institutions and environmental organizations are behind a project that has been operating since October in Prenzlau Germany, 75 miles north of Berlin. Their project is in the form of a Hybrid power plant that solves the storage problem by converting electrical energy generated by with wind turbine, into hydrogen. 

 

A hybrid power plant is the first of its kind in Europe, consisting of three wind turbines, a biogas unit, an electrolysis unit and two combined power plants that make use of waste heat. 

 

The turbines are capable of delivering 2 MW of electricity. This electricity is then converted into storable hydrogen by the electrolysis, a process that been theorized to be 80%-94% efficient.  The hydrogen can be distributed via pipeline and used like natural gas for heat; it can fuel hydrogen vehicles, and it can also co-fire the power plant along with the biogas to produce more electricity exactly when it is needed.

 

Vattenfall Innovation head Oliver Weinmann stated their mission best, "There is currently no system designed to compensate for the differences between supply and demand within the sector of renewable energy... But this project allows us to find a balance in the system and it’s also good business.”

 

Eavesdropper