Skip navigation

community

1 2 3 ... 6 Previous Next

News

82 Posts tagged with the medical tag
0

 

A tear-jerking introduction of the technology

 

A cerebrally controlled robotic system is being developed by a team of researchers from Brown University, Harvard Medical School, Massachusetts General Hospital and a host of others could give paralyzed people the ability to use robotic limbs to manipulate objects for themselves. Called ‘BrainGate’, the brain-controlled system allows the user to control a robotic limb through thought. To do this, the team implants a wireless microelectrode array (Neural Interface System) at 4 X 4mm directly on the motor cortex portion of the brain that controls motor function. The series of electrodes (100 in all) on the chip pick up the brain's activity associated with arm movement and sends the signals to a series of computers that use software (unknown at this time) to decode the brains activity. The computers then translate those signals into a series of instructions that tell a robotic arm to move and grasp an object based on the user’s desired intentions. The researchers are presently using two types of robotic arms, which are being continuously developed by DLR Institute of Robotics and Mechatronics and DEKA Research and Development Corporation.

 

HASy_01_Freigestellt200x300.jpg

DLR robotic hand/arm concept


The bigger of the two robotic arms being used by the researchers is DLR’s Hand Arm System, which is an external robotic arm made for more robust applications where impacts with heavy objects are nonconsequential (factory and warehouse work?).  The arm consists of a series of mechatronic compliance actuators with 52 drives and over 100 position sensors. The units hand alone features 38 individual tendons with each connected to an individual motor to provide tension and stiffness. The fingers use a similar configuration that uses two separate motors for individual grasping and tension based on the object being manipulated. The arm is so robust that you can actually beat it with a baseball bat without damaging any of the electronics.

 

deka_arm.jpg

Deka arm system

 

The second arm that the team is working with is DEKA Research and Development’s ‘Luke’ Arm (named after Luke Skywalker's mechanical hand). The arm is actually a robotic prosthesis that was designed for amputee patients and was developed as a DARPA tetraplegia project. The titanium Arm was designed to be roughly the same size as a typical human appendage and houses all of its electronics, motors and actuators inside (exactly how and what technology was used is currently unknown). The prosthesis features 18 degrees of movement which was accomplished by using rigid-to-flex circuit boards that were folded into ‘origami’ shapes placed inside the titanium housing. A vibrational motor at the top of the arm lets the user know how much pressure is needed to grasp an object through varying degrees vibration depending if the wearer is holding an egg or a brick.

 

Cabe

http://twitter.com/Cabe_e14

 

(All images and video courtesy of Crown Institute for Brain Science)

1

mit multi brain.JPG005.jpg

(Left) Erin Treacy Solovey wearing the Brainput device (Right) Artistic concept (via MIT & Erin Solovey)

 

When it comes to multitasking we as humans try the best we can. While we all have a modicum of ability, some are better than others. It suffices to say, we could all use a boost to become more efficient in our multitude of multitasking efforts, which is why a team of researchers has developed an unconventional solution to the problem. Led by Erin Solovey from MIT’s Humans and Automation Lab, the team has designed a system called ‘Brainput’ that can off-load some of our brains multitasking skills to a computer which is way more efficient at doing multiple things than we could ever hope to be. They system uses a portable low-cost version of a functional magnetic resonance imager called ‘fNIRS’ (functional Near-Infrared Spectroscopy) to measure the activity going on in the brain. The measurements are monitored and processed (using two probes) in real-time using Boxy software (from ISS). The information is then analyzed by a software engine (created using both Matlab and Weka tools) to look for specific patterns associated when the individual is multitasking. When the system has learned these patterns the software kicks in and is able to help the user with the task at hand.

 

A maze was created to test Brainputs effectiveness where a subject had to navigate through using two robots simultaneously. The operator using the fNIRS system was constantly switching back and forth between them and once the software learned the patterns it was able to engage sensors in the robots to help the user with their guidance. While the robots were autonomous, the test subject’s performance did indeed improve. While Brainput is still in its early development stages, it could be implemented into many applications in the future like helping you drive while you’re momentarily distracted or used during surgery with robotic assistance. What if the system could be used wirelessly? If you have an automated laundry machine, you could be slaving at work and washing your laundry at home at the same time! The possibilities are endless.

 

Cabe

http://twitter.com/Cabe_e14

1

decay sensor.jpg

Concept of the sensor (via MIT & Wiley Online Library)

 

The list of applications for carbon nanotubes seems to keep growing and growing. Scientists at MIT have found a way to give these nanotubes the capability of detecting gasses that are present during the process of ripening and rotting of fruits and vegetables.

 

 

These sensors consist of tens of thousands of carbon nanotubes that have been treated with copper atoms and polystyrene. Ethylene, a gas present during the ripening process, sticks to the copper and thus slows the flow of electrons through the carbon nanotubes. The higher the ethylene content in the air, the slower the electron flow is, and this can be correlated to determine the stage of ripening or rotting. Combining the sensor with an RFID chip allows for real time monitoring of produce. The sensor detects 0.5 parts per billion of ethylene in the air which makes it extremely sensitive. The sensor itself can be manufactured for only 25 cents, while the addition of an RFID chip increased the price to only $1 total per unit.

 

 

These sensors could change how produce is handled in stores like when it is put on clearance. This sensor can also be used to manage plants in new and beneficial ways. According to the USDA, 10% of produce is lost to spoilage annually.

 

 

The U.S. Army Office of Research funded the MIT research. The army is hoping this paves the way to more general electrochemical sensors such as mold or bacteria detectors.

 

Cabe

http://twitter.com/Cabe_e14

 

A brief collection of Carbon Nano-tube related news:

The 9 nanometer carbon nanotube transistor

First flexible carbon nanotube logic circuit printed

Graphene made cheap and green

Liquid smoke reformulated for new energy storage use

5 times the density in ICs

Biological enhancement to solar cells

Sensor detects one molecule of explosive

New scale able to weigh the light-weighted while you wait; the single atom scale

Carbon-nanotube based Ink-jet printer on the way

Wireless printed sensor detects explosives at a distance

Stretchable nanotube transistor material from DOE Berkely, a touch interface

1

inflate suit.jpg

Inflatable exo-suit (via Tokyo University of Science)

 

Those who have weak bodies can now become a virtual power-house.

 

For over a decade, exoskeletons have been used in the medical field to assist in either therapy or helping the disabled become more mobile (see Cyberdine’s HAL suit). These exosuits use some use varying sorts of hydraulic system to help the individual move and are rather bulky which limits the areas that they can be operated. A recent exoskeleton aimed at the medical field, called the ‘muscle suit’, uses a different approach to actuation by adapting air-bladders to help with mobility.

 

Designed by Dr. Hiroshi Kobayashi and a team from the Tokyo University of Science, the exosuit employs a series of artificial muscles attached to a frame that essentially simulate the muscles of the wearer. Deployed around the upper torso is a system of pressure and accelerator sensors which detect the user’s slight movements, which in-turn inflate or deflate the appropriate corresponding PAM’s (Pneumatic Artificial Muscles). Compressed air tank(s) powers the bladders when the sensors give a signal to a microprocessor. This gives the user the ability to lift or move an astounding 88 pounds!

 

The suit can also be controlled through simple voice commands i.e.: start/stop and the speed at which the PAM’s expand or contract can be adjusted through a regulator valve to further customize the suit to the user’s needs. The muscle suit comes in two versions with one (20lbs) aimed at places where extreme lifting is required while the smaller (11lbs) is meant for the medical industry with both being available for rent next year for around $185.00 US per month.

 

Cabe

http://twitter.com/Cabe_e14

2

darpa lens.jpeg

Innovega/DARPA AR Contact Lens concept (via DARPA)

 

As if calling in air-strikes with augmented reality glasses wasn't enough, now every soldier will get the virtual-world overlay on their eyes. DARPA is funding Innovega, a company looking to change the way we look at our digital and real worlds. The Air Force and Army both presently use head-up display (HUD) units to superimpose information about enemies, their environment, and other status updates in front of their field of view. However, Innovega offers a new technology that increases their field of view of the projection and greatly decreases the size of the product.

 

 

Innovega's system, called iOptik, uses contact lenses that have two different zones. This works by two different filters, an outer one used to see objects in your surrounding environment, and one at the very center that allows you to focus on very near objects with precise resolution. This dual-focus system will allow light rays to pass through the eye to the retina with two images in focus. The human eye has the amazing ability to choose which image it would like to see depending upon the user.

 

 

The system will also use small projectors placed on the side of the head near the ears to display the image on the lenses. According to Innovega, the image projected will appear very wide, similar to the experience of viewing a movie at an Imax. Additionally, the system can be used in different applications outside military purposes. It has a very big potential for 3D movies due to its ability show the eyes two different images at once. It can also be used to create augmented reality video games or superimpose digital information into the real world.

 

 

There are some eye-experts who are skeptical about the whole system, stating that it may cause a condition similar to motion sickness. On the other hand, not all people get motion sickness and Google's Project Glass is going to need some competition.

 

Eavesdropper

 


1

GOFilmonGlassSmall.jpg

Graphene filter (via University of Manchester)

 

Of all the uses of graphene, there is none more surprising than using it for alcohol distillation. Researchers from the University of Manchester (UK) have found that membranes made with graphene-oxide have impermeable qualities that prevent gasses and liquids from passing through them. On the other hand, water can easily pass through it when it evaporates as if the membrane wasn’t there at all.

 

The team, led by Dr. Rahul Nair, unexpectedly discovered their findings while conducting tests that involved taking sheets of graphene-oxide and using them to cover metal containers containing various liquids and gases that included helium. They then tested to see if any of the substances were permeable with extremely sensitive equipment. Nothing was detected until they tried ordinary water. What they found is that when the water was vaporized it could pass through the membrane like it wasn’t even there.

 

Nair explains that it can do this because the graphene sheets are arranged in such a way that there is enough space between them for a 1-molecule thick layer of water molecules to pass between. He states that the membrane’s ‘capillaries’ shrink when subjected to low humidity, which prevents molecules other than water from escaping (hence waters effectiveness). For a joke, the team then tried testing vodka and found that it became stronger the longer the evaporation process was performed. While none of the team drinks vodka, it soon became apparent that the new graphene-oxide membrane could have practical applications. Aside from making everyone's drink for effective, this also may make refining ethanol and other fuels easier and more cost effective in the future.

 

Cabe

http://twitter.com/Cabe_e14

 

Other graphene related news:

Scientists bring graphene to the semiconductor table

Girl Scout cookies to graphene

155Ghz graphene transistor

Graphene transistor from Nobel Prize winner

Transparent graphene transistor material stretches beyond all others

Graphene circuit auto-cool effect

Graphene made cheap and green

Cutting Costs and Cooling Efficiently With Graphene

Creating graphene with the help of pond scum

Researches can grow large sheets of graphene in one step

3

241P4LRYEB_00-APP-global-001_highres.jpg       Engineering On Friday ergosense shut up by Cabe Atwell.jpg

ErgoSensor concept (via Phillips)

 

Sitting and working at a computer all day takes its toll on our posture. Seriously, right now while I’m writing this, I’m hunched over at about a 45 degree angle and that can’t be good. So, for those of us who need help with this issue Phillips has designed a new monitor that lets us know were slouching and provides a procedure to correct it. The 24 inch LED monitor (1920 X 1080) is equipped with Phillips ‘ErgoSensor’ which measures the users position in relation to the monitor and provides feedback on distance to screen (optimal viewing distance), as well as neck-posture detection using an embedded sensor located in the display’s top bezel.

 

The sensor will alert you when you’re either too far/close to the screen, if your posture is wrong, and whether you’ve been at the display to long without taking a break (a coffee break?). The monitor also has some other unique functions such as powering off the monitor if nobody has been in front of it for a certain amount of time. This provides a power reduction of 80%, and there is a kill switch on the monitors back that lets you power-down to 0 watts (like the monitors off button on front?). The ErgoSensor monitor features standard adjustments as well i.e.: height, tilt and rotation. No word as of yet on the display’s cost, but my guess is in the $200 to $300 USD price range.

 

Cabe

http://twitter.com/Cabe_e14


Engineering On Friday takes the ErgoSense for a spin, annoyed by it.

1

gut-on-a-chip-250x326.jpg

"Gut-on-a-chip" (via Harvard University)

 

Sure it sounds creepy, but think of the education that can be had with pocket-sized living models of human organs. In order to get a different perspective on the way human intestines work, Dr. Donald Ingber and a team of researchers from the Wyss Institute for Biologically Inspired Engineering at Harvard University have designed a micro-sized living model based off of the human digestive tract.

 

Donald and his team created the ‘gut-on-a-chip’ by lining a series of tracts with living human intestinal cells that function the same as if they were inside the human body. The cells, which also grow digestive microbes as they would inside the human body, are placed on a flexible membrane which is housed inside a block of silicon about the size of a stick of computer ram. The membrane, which moves with the help of a vacuum system, acts as a recreation of the intestinal barrier which regulates the movement of antigens against bad burritos or other potentially toxic entities, as well as moving food along the digestive system.

 

The micro-design also replicates the movement of fluid, as well as blood through micro-capillaries, between the intestinal cell layers by pumping red and blue dye through separate channels that lead into the main channel which aids in giving a "more complete" view of how the intestinal system works. The team hopes that the ‘gut-on-a-chip’ will aid in diagnosing digestive disorders among other applications. It is better to test on a chip as opposed to a complete human being. Good job, Dr. Ingber.

 

Eavedropper

2

tricorder_mark2a_header.jpg

(via Dr. Peter Jensen)

 

Back in 2005 a sci-fi documentary came out called ‘How William Shatner Changed the World.' In it, Shatner describes how some gadgets and technology from the original series, as well as others, have become a reality in one form or another in today’s world. The one gadget that is predominantly showcased in every episode hasn’t made the transition from fantasy to reality, until now (no not ‘beaming’ tech). The multipurpose scanning "Tricorder."

 

Answering the call from Qualcomm to invent a Tricorder (Tricorder X-Prize contest), Dr. Peter Jensen has designed a series of functional prototypes that may win the $10,000,000 US cash prize. The first, called Science Tricorder Mark 1, features eleven different sensors grouped into three categories: spatial (GPS, accelerometer/gyroscope and distance), atmospheric (heat, pressure and humidity) and electromagnetic (magnetometer, colorimeter, non-contact IR thermometer, linear polarization filters and ambient light converter). Housed inside the ‘Star Trek-esque’ case is an impressive array of hardware which includes a Microchip DSPIC33FJ256MC710A-I/PF. processor, 2.7 inch Sony Reflective TFT display, Cirque TSM9957 touch-pad module with a Microchip 6S26 sensor board (originally made for the PS/2). Jenson used Microchip’s C30 compiler along with their MPLAB IDE software platform to code the Mark 1’s firmware. Total cost to develop and build the Mark 1 set Jensen (and a team of others from his school days at McMaster University in Canada) back around $500 US which is pretty impressive considering it’s based off of 23rd century technology (joking of course).

 

Next up is Jensen’s Mark 2 Tricorder which features most of the same hardware as the Mark 1 but with updated versions of the same sensors, electronics and the inclusion of an imaging sensor otherwise known as a cellphone camera. Another difference, or upgrade for that matter, over the Mark 1 is the inclusion of separate micro-controllers that make upgrading the sensors easier than its predecessor. The hardware for the Mark 2 has changed somewhat and includes an Amtel AT91RM9200 ARM-based processor along with two 2.8 inch OLED touchscreen displays.

 

Jensen's newer Tricorder design uses the Debian Linux OS for graphics rendering as well as a host of other applications. One of the noticeable differences the Mark 2 has over the original prototype is its casing. While the original looked like a crude silver cardboard cut-out, the Mark 2 is more stream-lined with a more ‘clean’ look giving it more of a Star Trek-like Tricorder aspect. Both are impressive, to say the least, and function as close to a futuristic Tricorder as possible. However, either of these Tricorders will not detect any alternate time-line fluctuations or alien pathogens, which is kind of a let-down.

 

Cabe

http://twitter.com/Cabe_e14

1

 

Wheelchairs have had some up-grades over the years. Various forms have come and gone, but they are typically limited to moving forward and backward. Those days are over as Masaharu Komori (from Kyoto University in Japan) has designed a new wheelchair that can not only travel forwards and backwards but also sideways. Called ‘Permoveh’ (Personal Mobile Vehicle) the wheelchair features a set of rollers housed inside the chairs wheels that lets the user travel in all directions, including diagonally as well as sideways. The rollers use a separate drive-train from the main wheels which gives the Permoveh its unique ability. This enables the disabled to move in tight or crowded areas with an impressive amount of maneuverability. The wheel innovation can also be adapted for other uses such as an upgrade for forklifts used in warehouses or adapted to robots that work in small places like my apartment. The downside to the Permoveh is that there are no plans to commercialize the chair as of yet but conceivably it could be on the market in the next few years.

 

01.jpg

Prototype chair and wheel concept (via Kyoto University)

 

The idea is nothing new, robotics competitions have had this exact tech for years. Whoever markets the wheels first will be treated as the inventor, so hop to it Masaharu Komori.

 

Eavesdropper

1

 

The practical beginnings of human-body augmentation are on us. GM and NASA have partnered to create a "Human Grip Assist" device,  which they are calling the Robo-Glove or K-Glove. The tech is pulled from the joint developed Robonaut 2 humanoid robot worker in the International Space Station.

 

Like in the Robonaut version, the glove is laden with sensors that help it decide what operations to perform. Pressure sensors let the Robo-Glove know it needs to start gripping. At which point the glove starts it actuators pulling in the synthetic tendons inside the glove. The team is boasting that 5-10 pound of human grip strength translates to 15-20 pounds of force in the glove. Actuation is produced via cords within the glove surface. A motor winds the cords up to pull the fingers into themselves. Very much like the tendon/muscle combo in human joints.

 

1331580905572.jpg1331580975857.jpg

Robo-Gloves in use and construction image (via NASA & GM)

 

GM is squarely fixed on applying the glove in the automotive industry.

 

GM manufacturing engineering director Dana Komin explained, "When fully developed, the Robo-Glove has the potential to reduce the amount of force that an auto worker would need to exert when operating a tool for an extended time or with repetitive motions. In so doing, it is expected to reduce the risk of repetitive stress injury. We are continuously looking for ways to improve safety and productivity on the shop floor. "

 

The Robo-Glove houses the actuators and tendons as mentioned above, but also a LCD for programming and diagnostic. A lithium-ion battery attached to the user's belt powers the gloves. Glove materials are constructed by the Oceaneering company (added link for those interested in similar projects). At the moment, third generation prototypes, the gloves weight 2 pounds each. The next gen, production models, are promised to be smaller and lighter than previous iterations.

 

Although great for workers, I believe medical applications will be a major user. Those who have lost their grip strength, now have it back.

 

Cabe

http://twitter.com/Cabe_e14

 

See behind the scenes at the Robo-Glove Test Procedures, from the view of Engineering On Friday after the link.

 

Robo-Glove fun facts:

The Robonaut 2 (R2) projects have given GM and NASA 46 patents.

- 21 of which are for the R2's hand.

- 4 apply to the Robo-Glove

0

755143-trevor-prideaux.jpg

(via Nokia)

 

"It’s not technology. It’s what you do with it." -Nokia

 

For some people with disabilities, using a smartphone can be a hassle. Just ask Trevor Prideaux. Born without his left arm, using a phone was like performing feats of acrobatics which usually entailed trying to balance his phone on his prosthetic arm while calling or texting. He decided to get in touch with some medical technicians from Exeter Mobility Centre (makers of custom prostheses) as well as Nokia to design a new prosthetic arm that has a smartphone docking station housed in the arm itself. The technicians carefully designed a limb around Nokia’s C7, placing the phone on the inside of his arm making it much easier to use. Trevor chose the C7 because of the fact that it has both a QWERTY keyboard as well as an alphanumeric giving him a wider range of options to use. This ingenious design will definitely open up new doors of mobile device technology for people who use prosthetic limbs. (Adding extended battery packs along with the mobile devices could also remove all worry for the user. Nokia, take it further!)

 

Cabe

http://twitter.com/Cabe_e14

0

dna usb.jpg

MinION (via Oxford Nanopore Technologies)

 

In the fast advancing technological world in which we live, it is only a matter of time before we can all readily have access to our human genome sequence. A firm in UK has built a small device that will bring us one step closer to that possibility. A surge in medical innovation may soon follow.

 

 

Oxford Nanopore Technologies has recently constructed a device that can sequence simple genomes through the USB port on your own computer. They call it the MinION, and it can sequence a genome in 2 hours. Within that time frame, it can sequence 10,000 base-pair long DNA strands."We just read the entire thing in one go," said chief technology officer Clive Brown.

 

 

The device is allowed to accomplish the enormous task of sequencing by nanopores, small organic molecules with a extremely small hole at their centers, only 10 nanometers wide. The nanopores are then placed into synthetic polymer membranes with exceedingly high electrical resistance. If a potential is applied across the membranes, it causes a current to flow through the small holes at the center of each nanopore.

 

 

When sequencing, DNA is added to a solution containing enzymes that are attracted to the ends of the DNA strands. The enzymes then attach to the ends of the nanopores, which act as a ratcheting device, feeding a  strand through one base pair at a time. Specific electrical characteristics of each of the four bases of the DNA cause a distortion in the current flow while passing through the nanopore. MinION is able to distinguish each of the four different disruptions in the current and record the sequence of DNA accordingly. The sensing components are integrated onto a small chip with approximately 512 nanopores, creating the potential to read up to 10,000 bases per second.

 

 

While other techniques currently exist to screen DNA, the MinION is superior in two unique ways. The device does not need to break apart individual strands in order to sequence them and can continuously sequence strands up to 10,000 bases. In addition, DNA does not need to be amplified to be accounted for. The MinION is expected to be out at the end of this year and will cost a customer around $900.

 

Cabe

http://twitter.com/Cabe_e14

1

Boston Dynamics "Petman" (via Boston Dynamics)

 

The Defense Advanced Research Projects Agency (DARPA) is set to develop breakthrough advancements in telepresence and remote operation of ground systems, by totally immersing soldier into robotic "Avatars." DARPA has dedicated $7 million of its 2012 budget to develop an avatar that can be used in combat and other tasks. Duties include, but are not limited to, "countering IEDs and mines, search and rescue missions, and recovering casualties during combat."

 

 

The effort is being called the "avatar program," undoubtedly inspired by the James Cameron movie, Avatar. Like the film, DARPA plans to have a soldier controlling a robot avatar from a safe location while still possessing the feeling of being present on the battlefield. The program will develop systems of communication between the avatar and soldier to effectively control the robot from some distance. If successful, it possesses the potential to save lives and reduce casualties. (At least for one side of the battle.)

 

 

DARPA is no stranger in the field of robotics. In the past, they have worked with Boston Dynamics and designed Petman, a semi-autonomous bi-pedal machine that is capable of walking similarly to humans. Additionally, AlphaDog is being built and tested to help assist soldiers in combat. AlphaDog is a large dog shaped robot that can carry up to 400 pounds and traverse 20 miles.There have also been successful investigations into robotics controlled by the mind. DARPA funded research into a prosthetic arm that was capable of many motions similar to the human arm. It has the ability to bend, twist and rotate 27 different ways, and is controlled by a microchip in the brain. It works by having the microchip record neuron activity and decode the signals to activate motor neurons that controlled the prosthetic arm.

 

Combine all these developments, the future is a grim, soulless, battlefield.

 

 

Cabe

http://twitter.com/Cabe_e14

1

01-1329998885-2084258.jpg

Jianhui and the controlled robotic limb (via Zhejiang University)

 

Animals are capable of much. Learning sign language or aiding with search and rescue immediately come to mind. One such test animal, the monkey Jianhui, is now adept at learning how to control robotics with their minds. Zheng Xiaoxiang and his team of researchers from Zhejiang University in Zijingang China were able to identify and decode the electrical signals in the area of the monkey’s brain used for hand movement. The researchers then surgically implanted two microchips, which are connected to over 200 neurons inside Jianhui’s brain, that interface with an external computer for deciphering the brain signals. The signals are then sent to an advanced robotic hand, which was developed by STMicroelectronics and the Bio-robotics Institute Scuola Superiore Sant’Anna, to mimic the monkey’s hand movements such as grabbing, pinching and holding. While animal rights activists may not agree with what Zheng Xiaoxiang and his team has done, the ‘Brain-Machine Interface’ does have practical implications such as enabling people with prosthetic limbs a more natural way of controlling them.

 

Jianhui is not the first to control a robot arm was controlled with thought. A similar system was already built and tested on a human subject with much success. However, that subject volunteered for the procedure, the monkey did not. It is a shame that animals get such a raw deal in science.

 

Cabe

http://twitter.com/Cabe_e14

1 2 3 ... 6 Previous Next