Skip navigation

community

1 2 3 Previous Next

News

43 Posts tagged with the military tag
2

-003.jpg

Cognisens concept diagram (via Cognisens)

 

SOF (Special Operations Forces) soldiers go through some pretty tough unending training to get their bodies into super-athlete condition to be able to handle the missions they’re tasked. However, it’s more of a matter of ‘mind’ than it is physical, as they need to be able to react to the environment around them.

 

Reconnaissance and FID (Foreign Internal Defense) plays a big part in the community , and that takes quite a bit of intelligence. To keep the mind sharp the SOF community employs a wide range of techniques and tools such as SOCOM’s (US, Special Operations Command) recent implementation of Cognisens NueroTracker. The system was actually designed for professional sports players to increase situational awareness and decreasing response time during game play. To do this Cognisens designed the system as a 3D environment where the participant wears 3D glasses to view 8 targets and has to track 4 designated targets for a period of 8 minutes.

 

It’s easier said than done as the series of targets increase over the period of sessions. This process becomes harder over time with 8 different gameplay difficulties with ‘Overload’ being the hardest level and ‘Challenger’ mode that pits two players against each other. The company states that just as lifting weights develops increased muscle capacity, NueroTracker ‘re-wires’ the part of the brain uses for memory and increases its performance. SOCOM says that this is the perfect tool in giving commandos the ability to track multiple targets with reduced response time and the ability to predict movement. While it doesn’t seem like the harsh, rigorous, training most operators go through, any tool that improves ability is certainly beneficial.

 

Cabe

http://twitter.com/Cabe_e14

1

nrl research lab.jpgLASR-exterior_46-12r_372x248.jpg

(Left) Captain Paul Stewart with an Asending Technologies Pelican quadrotor and "lucas" a mobile social robot (Right) the LASR facility building (via U.S. Naval Research Laboratory)

 

After two years of construction, the US Navy has opened its doors to their new Laboratory for Autonomous Systems Research (LASR) center. The facility will serve as the Navy’s primary laboratory for intelligent autonomous systems (robots), sensor systems, UAV’s and a host of other studies in multiple fields for future defense technology. The $17 million dollar building located in Washington DC contains multiple spaces for some of the more interesting labs that include a prototyping high-bay designed for testing both air and ground unmanned vehicles and features the world’s largest motion-capture system that allows scientists to collect accurate detailed data concerning said vehicles. There’s a littoral high-bay lab which contains a 45ft X 25ft pool that’s 5.5ft deep that features a wave-generator for water-borne unmanned vehicle testing in both calm and choppy simulated sea conditions. Another area contains a desert high-bay that has 18ft-high rock walls with a 40ft X 14ft area of sand that’s 2.5ft deep to test robots and sensors in an arid environment. Other environmental labs include the tropical high-bay which allows for testing systems in a greenhouse setting akin to southeast Asia, as well as an outdoor test range simulating a highland forest complete with waterfalls, streams and increasingly difficult terrain. There really is no area found on earth (besides the arctic regions) that the LASR hasn’t simulated for testing of all these systems.

 

LASR-desert-high-bay_46-12r_372x559.jpgtropical-high-bay-LASR_46-12r_372x559.jpg

(Left) Desert High-Bay with an 18-foot rock wall (Right) Tropical High-Bay simulating southeast asian rain forests (via U.S. Naval Research Laboratory)

 

The facility also contains various machine and electrical shops for all the labs as well as conference spaces for get-togethers to discuss wind-falls or complete disasters. Testing autonomous systems is nothing new to the Navy as the NRL (Naval Research Laboratory) has been testing these platforms since 1923 with the development of an electric dog that was controlled by a system of relays and a flight-control stick found in airplanes at the time. Other notable research done by the NRL includes remote-controlled battle ships in the 1930’s which were operated through selector switches based on teletype systems that used Baudot code. There were even anti-aircraft target drones that could be remote-controlled by people on other aircraft at distances of up to 25 miles away designed for a more realistic target for AA training. These testing platforms and developments created over the first half of the twentieth century eventually led to the development of guidance systems for missiles, like the sub-launched Polaris ballistic nuclear missile. With the Navy’s new LASR facility finally open it will be interesting to see what new developments come out of the first half of the current century. Can anyone say ‘Skynet’?

 

 

See more about robotics in element14's Robotics group

 

Eavesdropper

1

 

Playing with RC cars can be a lot of fun for kids, and as anyone who plays the Call of Duty games know, the army thinks they are fun as well. Now, a company called Boston Dynamics has revealed their latest take on the RC car. Unfortunately you will not find it at any Toy’s R Us. Boston Dynamics and the Army’s Rapid Equipping Force are behind this project because creating military bots is now more profitable than selling RC cars to kids.

 

 

Their creation is called the Sand Flea. It is a heavy duty all terrain RC car with a trick up its sleeve to overcome obstacles. Weighing only 11 pounds, the Sand Flea has an on board camera and CO2 piston-like launching mechanism all in a small package. The CO2 launch system propels it up to 30 feet in the air for gaining access to rooftops and clearing walls or obstacles. The Sand Flea jumps very accurately from a stationary position, so it can even get into open windows. The CO2 tank allows for 25 jumps before reloading. To assure a smooth landing and steady camera footage, the Sand Flea is also equipped with a stabilization system that levels it when it is in flight.

 

 

See more of Boston Dynamics work:

Advanced humanoid robot designed to test clothes

AlphaDog robot impresses and intimidates

 

 

Eavesdropper

 

See more robots is the element14 Robotics group

1

medium.jpg

 

The US ARMY has recently awarded Hewlett Packard the sum of $249,000,000 US for their integration of HP’s Enterprise Cloud Services. ECS incorporates servers, storage, networks and securities services all packaged together that are custom tailored to the customer’s needs. This will give the DoD, as well as other federal agencies, a secure centralized source for all their top-secret information needs. HP will provide the Army with two ‘suite’ versions with one designed to save the military a bundle of cash by outfitting a number of federal buildings with ECS that will keep the ‘Bradley Mannings’ out and the ‘for your eyes only’ in which will provide the DoD a more secure environment for classified information.

 

The second ‘suite’ will incorporate the use of ‘PODs’ (Performance-Optimized Data Centers) which can be deployed over-seas for tactical situations that require access to the US-based cloud hub. To get this service implemented HP will be working with ten (unknown at this time) small businesses and some wiz-kids over at Alabama’s A&M University. As to when the DoD’s cloud service will be coming online is currently unknown but be rest assured only those ‘in the loop’ will know.

 

Eavesdropper

1

ITvest.JPGconductive vest.jpg

(Left) Intelligent Textiles showing off their conductive "e-textiles" (Right) Conductive vest, looks exactly like its non-electrical original

 

Ask any soldier and they’ll tell you that the more gear you use when you ‘kit up’ the harder it is to move. Communication systems like the PRC-153, while smaller than their predecessors, take up a lot of real-estate on plate-carriers and tactical vests alike. Add up all the other electronic gadgets such as GPS units, tactical tablets and NVG systems and you’ll quickly get lost in the cluster that used to be your body-armor. Oh I almost forgot; each one of those ‘cool’ gadgets requires power, and this power usually (9 times out of 10) comes in the form of batteries, lots and lots of batteries.

 

To help free up some of the clutter and weight associated with these electronics, a UK company called "Intelligent Textiles" has designed an electrically conducive yarn that can be woven into uniforms or body-armor. The ‘e-textile’ allows for power to be transferred from a single battery pack to any location with a plug built-in to the fabric such as helmets, gloves, backpacks, sleeves or pant legs. The company states that even the soldier’s weapon can be outfitted to take advantage of the fabric and future versions will even come with a fold-out keyboard. This advanced electrical textile does away with a lot of the cable clutter as well as cutting all the batteries carried down to just one needed to power almost everything the soldier carries.

 

Intelligent textiles have fielded a prototype for testing purposes future versions will need to be waterproofed so the fabric doesn’t short-out or rust in wet environments. The company is currently in talks with BAE Systems with hopes to have their e-textile uniforms on the field by 2017.

 

This is not the first to propose conductive thread. A team of researchers assembled from different schools developed a wire with a cotton substrate. Their work was for everyday use, not just for the world's war fighters, thankfully.

 

Cabe

http://twitter.com/Cabe_e14

0

heat sig.JPG

(via Transformation thermodynamics: cloaking and concentrating heat flux paper)

 

Invisibility cloaks have been created to hide from magnetic detection, eyesight, radar waves and the IRS (just kidding). We can now add thermal cloaking to that list, with the recent research paper released by Sebastien Guenneau and his team from the Institut Fresnel in France. The theory outlined in ‘Transformation thermodynamics: cloaking and concentrating heat flux’ cloaks heat signatures from thermal optics typically used by militaries around the world.

 

The principle is based off of heat diffusion where an object is detected by infrared waves (thermal radiation) because of the heat associated with it. To make the object invisible, the team proposes using a system of ‘concentric rings’ made of both metal and plastic. These rings help isolate, and or, moves the heat energy away from the object being hidden. The metal rings are good at dissipating heat (heat sink?), whereas the plastic helps to direct the heat. This combination of alternating between metal and plastic rings with different diffusion rates helps to move the IR heat signature around the objects central region and, therefore, makes the objects temperature that of its surrounding area. On the other hand, the heat can be directed into a single focal point (apparently for ‘uncloaking’). So far, the team has only been able to cloak objects that are micrometers in size so don’t expect to see a ‘cloaked’ human being anytime soon.

 

Cabe

http://twitter.com/Cabe_e14

 

Engineering On Friday shows the military application for this tech.

1

futuristic_700.jpg

(Left) SUGAR high/freeze (Right) supersonic Boeing concept (via Boeing)

 

"Green" is becoming the norm in new design. Boeing is jumping on the bandwagon and looking to win a major contract from NASA to create new subsonic/supersonic aircraft that will be more environmentally friendly. Concepts for the subsonic aircraft (noted as N+3 for the next three generations of aircraft) are all derived from the project known as SUGAR (Subsonic Ultra Green Aircraft Research). These include "SUGAR free" and "refined SUGAR" (I’m not making this up these puns) that resembles current 737 designs. SUGAR high and the electric/gas hybrid SUGAR Volt are more of a futuristic design and SUGAR ray (a design that looks like a B2 stealth converted for passengers) bringing up the rear. Finally, the SUGAR freeze (based on the SUGAR high) runs on cryogenically frozen liquid natural gas, making it 64% more efficient than current Boeing 737-800 planes.

 

All planes in this category have been designed to decrease CO2 emissions in one way or another; however the SUGAR Volt stands out from the pack because of its battery/fuel hybrid engines which reduce its energy burn by 55% over the other designs.

 

sugar refined.jpgsugar ray.jpgsugar high.jpg

 

(Left) refined SUGAR (Middle) SUGAR ray (Right) SUGAR high (concepts via Boeing)

 

The supersonic designs are just as diverse as their slower moving brothers that include a swing-wing configuration, a fixed-wing design that uses a ‘v-tail’ concept (called Icon 2) and a joined-wing ‘scissor’ (1 wing joined at the fuselage that rotates on a pivot point) concept. All the supersonic crafts are designed to lessen or reduce the inevitable sonic boom created with super-fast flight. Yes, Boeing understands that while the supersonic models aren’t exactly up-to-speed (as it were) on the whole green initiative, they more than make up for it in raw speed alone. Conceptual designs were also submitted by Northrop Grumman and Lockheed Martin to NASA as well, all in the hopes of winning a contract. If all goes according to plan, the first group of next generation planes will hit the runway in 2030.

 

Cabe

http://twitter.com/Cabe_e14

1

See_Me_a.jpg

SeeMe concept (via DARPA)

 

In the military, it’s usually the SOF (Special Operations Forces) community are that get all the toys. For example, new body armor designs, improved weapons platforms and the latest electronic equipment are usually given to ‘Tier 1’ (the term is actually from the DOD’s budget rather than elite soldiers) operators. However, DARPA is seeking to develop and supply the average military units (as well as SOF) with the ability to recon over the horizon with cheap/disposable real-time satellite imagery.

 

Called ‘SeeMe’, DARPA’s project aims to use cheap already in-orbit satellites (about a dozen or so) that can be accessed with the push of a button and give the soldiers an area image within 90 minutes. DARPA is trying to combine the low-cost manufacturing processes from the cell-phone industry, propulsion systems designed by the auto-racing community, and valve tech from the medical field to get the SeeMe project off the ground (so to speak). The satellites are expected to cost around $500,000 US (which is pretty cheap as far as satellites go) and will remain in orbit anywhere from 60 to 90 day’s at which point the will re-enter the earth’s atmosphere and burn up on re-entry.

 

DARPA plans to use their ALASA (Airborne Launch Assist Space Access) platform to send these ‘prying eyes’ into space over conventional rocket deployment since the payload is expected to be 100Lbs or under. The company is hosting a get-together (called Proposers’ Day) on March 27 of this year to hear prospective proposals from interested parties interested in the SeeMe project. If you have an idea on how to make this happen, have a go at SeeMe. Maybe I will 'SeeYou' there!

 

Cabe

http://twitter.com/Cabe_e14

1

 

As citizens and politicians argue about how not to spend tax dollars, the U.S. navy seems to be gaining ground in persuading congress in spending hundreds of millions. A new type of gun that was previously thought as impractical and a waste of time, energy, and money may soon get back on the design track. This new weapon is called an electromagnetic rail gun and it works by accelerating a 20+ lb aluminum “bullet” around hypersonic speeds (Mach 5) towards the enemy.

 

 

Congress was skeptical as early designs did not include a barrel for the gun but new footage of preliminary tests by the company BEA Systems and the Office of Naval Research show a functioning rail gun with a barrel. These tests shot a 23 lb bullet at 5500 ft/s using 33 Mega Joules of energy. While these results have convinced the navy that this project should be pursued, there is still more development needed before battleships can handle these weapons.

 

 

The Navy wants guns that can shoot 10 times per minute, which means that the barrel will need to withstand the punishment. The firing needs to reduce the demand on the ships energy supplies. So additional energy-dense batteries for the gun will be need to be added. Each projectile has to be equipped with processing systems to guide its trajectory. Lastly, the blast cannot damage the onboard components. A new thermal managing systems are in development as well.

 

 

The companies BEA Systems and General Atomics are hard at work on this project. So far the effort has cost about $240 millions dollars, and it is expected to cost around twice this amount by the time it is complete and ready to buy. We may not have jobs in 2020, but the Navy counts on having these rail guns ready for war.

 

 

Eavesdropper

1

 

The iRobot team has recently released its newest ground robot the 110 FirstLook Scouting Unit. Unlike most robots, the First Look is capable of surviving 15 foot drops onto concrete, which allows it be thrown into buildings or onto out of reach places.

 

 

The robot is designed and marketed towards military and special ops teams. However, it is packed with awesome features that will appeal to any technical person with an inner child. The small robot is highly portable weighing in at only 5 pounds and measures 10'' long, 9'' wide, and 4'' tall allowing it to easily fit into a backpack. In addition, it features 4 cameras, one on each side that will give the user a 360 degree view of the environment. The cameras also feature IR illumination to enhance visualization while in low light situations.

 

 

The First Look gives the user the ability to navigate through rough terrain and dangerous situations at a safe distance. Worried about curbs or puddles of water causing navigating problems? The robot is waterproof up to 3 feet, and it can even overcome obstacles and steps up to 8 inches. The design is also convenient when needing to investigate hard to reach places, such as pipes, air ducts, or tunnels.

 

 

Controlling the robot requires a small 'tactical operating control' unit that includes a two way radio and screen for video feedback. The battery allows up to 6 hours of continuous operation and up to 10 hours of stationary video feedback.

 

 

Joint Improvised Explosive Device Defeat Organization has recently ordered a hundred of theses bots and will be testing them out for the first time within the next few months.

 

 

Just like with the ReconRobotics "Scout XT," if I saw this rolling towards me in even a mildly hostile environment, I would run in the opposite direction.

 

 

Eavesdropper

1

 

Cheetah_Concept.jpg

Cheeta concept drawing (via Boston Dynamics)

 

Robots are best known for their superhuman strength or computational prowess but not necessarily their speed. That’s all about to change with the introduction of DARPA’s new M3 (Maximum Mobility and Manipulation) robot. Called the Cheetah, the robot is the brainchild of Boston Dynamics and can reach speeds of 18 mph, which is a world record for multi-legged robots (unseating the previous contender from MIT). The Cheetah is designed after the animal of the same name and uses a mechanism, powered by a hydraulic pump, which flexes its back making the legs move (much like a muscle). Increasing the flexibility rate results in faster movement of the legs, but the robot needs to be held in place and run on a treadmill to do so at the moment. Outdoor testing without a leash will be done this year (2012) according to Boston Dynamics for further development. DARPA is funding the Cheetah and plans to adapt it to EOD teams, as well as other military applications, to help with IED disarmament and removal in rugged terrain that other robots ca not traverse. Sounds like a good project that would help save the lives of our ground-pounders. I just hope the final rendition of the Cheetah look like the concept graphic shown above.

 

Cabe

http://twitter.com/Cabe_e14

 

See some of Boston Dynamics other robots:

The AlphaDog, a heavy equipment carrier

Petman, the robotic human soldier

0

BAE.jpg

(via BAE Systems)

 

Recently the US military has been increasing its use of ‘green’ technology in the last few years, but they have been in the area of renewable energy sources for some time. The armed forces are slowly but surely incorporating hybrid vehicles into their ranks. One such vehicle, being developed by the partnership of BAE systems and Northrop Grumman for the US Army, is both green and lethal. Called the Ground Combat Vehicle, the armored troop-carrier sports a hybrid-electric drive system that uses two electric motors (generating 1,400 horsepower) powered by a lithium-ion battery. Two diesel engines, which hold 255 gallons of fuel, provide back-up power as well as recharging the batteries when necessary. What makes the GCV a formidable threat is its ability to run completely on battery power, which makes it almost silent on the battlefield. Overall, the fuel efficiency of the tank gets a 10-20% boost over its stock counterpart. Another notable feature of the hybrid is the ability to ‘plug’ in electric-powered weapons systems such as LRADs (Long Range Acoustic Device) and microwave weapons which gives troops more options when it comes to load-outs.

 

The 70 ton hybrid can carry three crew members and nine passengers with a top speed of 43 Mph at a range of 186 miles. It’s also outfitted with a 7.62mm coaxial machine gun and 25mm auto-cannon as a base platform which can be upgraded with different weapons for depending on the scenario. The GCV looks like an updated hybrid Bradley Fighting Vehicle for the 21st century but with thicker armor and a completely different drive system. The Defense Department has approved for production at a cost of about $11,000,000 US each which would make the GCV a truly ‘Mean Green Killing Machine’!

 

Cabe

http://twitter.com/Cabe_e14

1

Boston Dynamics "Petman" (via Boston Dynamics)

 

The Defense Advanced Research Projects Agency (DARPA) is set to develop breakthrough advancements in telepresence and remote operation of ground systems, by totally immersing soldier into robotic "Avatars." DARPA has dedicated $7 million of its 2012 budget to develop an avatar that can be used in combat and other tasks. Duties include, but are not limited to, "countering IEDs and mines, search and rescue missions, and recovering casualties during combat."

 

 

The effort is being called the "avatar program," undoubtedly inspired by the James Cameron movie, Avatar. Like the film, DARPA plans to have a soldier controlling a robot avatar from a safe location while still possessing the feeling of being present on the battlefield. The program will develop systems of communication between the avatar and soldier to effectively control the robot from some distance. If successful, it possesses the potential to save lives and reduce casualties. (At least for one side of the battle.)

 

 

DARPA is no stranger in the field of robotics. In the past, they have worked with Boston Dynamics and designed Petman, a semi-autonomous bi-pedal machine that is capable of walking similarly to humans. Additionally, AlphaDog is being built and tested to help assist soldiers in combat. AlphaDog is a large dog shaped robot that can carry up to 400 pounds and traverse 20 miles.There have also been successful investigations into robotics controlled by the mind. DARPA funded research into a prosthetic arm that was capable of many motions similar to the human arm. It has the ability to bend, twist and rotate 27 different ways, and is controlled by a microchip in the brain. It works by having the microchip record neuron activity and decode the signals to activate motor neurons that controlled the prosthetic arm.

 

Combine all these developments, the future is a grim, soulless, battlefield.

 

 

Cabe

http://twitter.com/Cabe_e14

0

FBOMB.jpgCOmonitorspy.jpg

(Left) F-Bomb in 3D printed enclosure (Right) F-Bomb hardware hidden in a CO monitor

 

 

Of all the mini computers available, this one might have the biggest potential of all. It is appropriately called the F-Bomb, which stands for, Falling or Ballistically-launched Object that Makes Backdoors. Malice Afterthought's Brendan O’Connor, a security researcher, has developed a system made from commercially available components and put together, costs less than 50 dollars and is capable of breaking into a network with the right software.

 

 

The purpose of the device is exactly as its name dictates. When dropped, the F-Bomb searches for networks within its range and infiltrates all the networks it finds. The size of this computer is 3.5 in by 4 in by 1 in. It is made using a Pogo Plug, 8 gig flash memory, small antennae, and a case made on a 3D printer. The components of the F-Bomb are so small that they can be easily be fitted inside any ordinary device, like a smoke detector, and covertly operate for as long as the batteries last.

 

 

The F-Bomb will be inexpensive, around $50 USD, on purpose. O'Connor explained why, "If some target is surrounded by bad men with guns, you don’t want to have to retrieve this, but you also don’t want to have to pay four or five hundred dollars for every use The idea is that it’s as close to free as possible. So you can throw a bunch of these sensors at a target and get away with losing a couple nodes in the process.”

 

 

In essence, the F-Bomb is a data collecting device. O’Connor designed it with Wi-Fi cracking software to create back doors into the network and collect private information. However, any applications and programs compatible with its Linux OS can run on the F-Bomb. With the correct sensors, it can performs other valuable data collections like meteorological or atmospheric information.

 

 

Originally, O'Connor won the DARPA awarded project "Reticle: Leaderless Command and Control" for the Cyber Fast Track program. F-Bomb was a follow up project, funded independently. The purpose of Reticle is on the hush-hush.

 

 

Cabe

http://twitter.com/Cabe_e14

0

Soldier prepares UAV for Afghanistan flight.png

Soldier sets up UAV communication system in Afganistan

 

Big bandwidth, 4G, wireless networks are popping up everywhere these days; it is almost hard to find an area that does not have a fast connection. That is not the case for our men and women fighting on foreign battlefields like Afghanistan. Wireless networks out there are hard to come by even at 3G speeds. Wars are won with information. Having soldiers connected is paramount.

 

Slow data speeds will soon be a problem of the past though as DARPA’s (Defense Advanced Research Projects Agency) STO (Strategic Technology Office) looks to bring 4G level connections to even the most remote of battlefields. To do this, DARPA plans on using their Mobile Hotspots program that uses a millimeter-wave communications platform (wavelength of 10 to 1mm.) This system will be implemented in air vehicles as well as ground and will be able to give the war-fighter the speed of a typical 4G fixed tower, which is about a gigabit per second, without the infrastructure (kind of hard to hide a cell-tower in a war zone). The Mobile Hotspots program will also utilize DARPA’s ‘Fixed Wireless at a Distance program' which is essentially a high-performance cell tower that’s placed in a protected area like a forward operating base (FOB). This work is being looked at to boost UAV transmission power in hopes to extend the range.

 

DARPA Program manager Dick Ridgway explained how they will get up and running, "Mobile Hotspots will require the development of steerable antennas, efficient millimeter-wave power amplifiers, and dynamic networking to establish and maintain the mobile data backhaul network. We anticipate using commercial radio protocols, such as WiFi, WiMax or LTE [Long Term Evolution], as a cost-effective demonstration of the high-capacity backbone.  However, the millimeter-wave mobile backbone developed during this program will be compatible with other military radios and protocols.”


 

"The principle of strategy is having one thing, to know ten thousand things." - Miyamoto Musashi (Book of Five Rings)

 

Cabe

http://twitter.com/Cabe_e14

1 2 3 Previous Next