Skip navigation

community

News

4 Posts tagged with the quantum_dot tag
1

flippingalig.jpg

Quantum Dot concept image (via the Optical Society Journal "Remote switching of cellular activity and cell signaling using light in conjunction with quantum dots"

 

Lih Lin and her research team at the University of Washington have been working with Quantum Dot based stimulation of cells within the brain with surprising results. Quantum Dots (QD) are small crystal shaped particles only a few nanometers wide that behave similarly to semiconductors. They are readily excited by light. When exposed to a light source, the QDs become negatively charged. The small size and composition give them extraordinary fluorescent optical properties, and are easily adjusted by changing the size or physical composition.

 

 

Lih Lin explained where the QDs are used, "Many brain disorders are caused by imbalanced neural activity... Manipulation of specific neurons could permit the restoration of normal activity levels."

 

 

The teams succeeded in creating action potentials within the neurons by exciting quantum dots nearby. The stimulation of the QD created a negative charged surrounding it and opened up the ion channels in the neurons. The ion channels are vital to stimulating the brain cells by allowing positive charges to flow into the cell and create an action potential. Additionally, the action potential in neurons is what sends messages to other neurons or nerve cells within the body allowing a form of communication to occur. The goal is to use quantum dots to control the abnormal signal firing within the brain cause by Parkinson's, for example.

 

 

QDs can be used to treat a wide variety of brain disorders from dementia to depression. Furthermore, they may be able to treat problems within the eye and possibly blindness. The only drawback right now is creating a way to shine a light on the quantum dots while they are in the brain.

 

 

The first use of QDs will likely happen in the eye, where light is constantly absorbed. However, QDs could be delivered to the brain through the veins where they could help balance out the neural activity. Quantum Dots have a bright future in the medical field treating disorders and can possibly do so without any dangerous or unwanted side effects that come along with current brain disorder treatments.

 

 

Cabe

http://twitter.com/Cabe_e14

1

mcontent-1323089923073.jpg

(Via Harvard)


A Quantum Dot (QD) is a semiconductor where excitons (bound stat of an electron and hole) are confined in all directions. Quantum Dots are already being used in communications and solar panels, to name a few. Even though QDs have outstanding optical properties, high extinction co-efficient, efficiency is not their strong suit.

 

 

Since the dots are nano-sized individual semiconductor elements, it is difficult to direct the electrical flow within them. Electrons have a tendency to be dissipated among the quantum dots instead of travelling between electrodes.

 

 

Researchers at Harvard University have published a paper detailing a process to improve on this efficiency. The remedy comes in a coating applied to these quantum dots. The author of the paper, Edward Likovich, visually describe the new process as putting QD’s in insulator egg cartons. This insulator separates the individual QD’s and prevents conduction between them.

 

 

To accomplish this, they create a single layer of QD’s, made up of a CdSe core and a ZnS shell, with hydrophobic octadecylamine ligands (QD coordinators). They then transfer this layer to an Al-doped ZnO (AZO) glass that acts at the bottom electrode of an LED. The insulator “egg carton” layer is made of Aluminum Oxide (Al2O3). To deposit this thin layer of Al2O3 over the QD’s, alternating sprays of water and an organometallic compound containing aluminum are applied at 150 degrees Celsius. Since the QD’s are positioned using hydrophobic ligands, only the oxygen adheres to create the layer of Al2O3. All of this is finally covered with an AZO top electrode.


Edward Likovich, author of the paper, explained, "The process provides a mechanical and energetic barrier between adjacent quantum dots, so the current tends to flow perpendicularly as opposed to being dissipated among dots in the layer... Also, because we have this mechanical barrier between the dots, we can do post-processing to remove the ligands while holding the dots in place, preventing agglomeration.”


 

A simple test using LEDs shows that the egg-carton does funnel electrons through the QD’s far better than untreated QD’s. Researchers believe the efficiency of these circuits can be improved by changing the ligands used to coordinate the position of the dots. Since the team assumes ligands become charged themselves and divert electrons from passing in between the electrodes.

 

 

Along with the solar cell based on QDs from NREL, perhaps Harvard's new QD system will usher in a new era of solar energy collection.

 

 

Eavesdropper

 

0

NREL.jpg

NREL facility (Via NREL)

 

Slowly, but surely, leaps and developments are being made that are making renewable energies competitive with fossil fuels. On December 16, 2011 an article was published in Science magazine by researchers at the National Renewable Energy Lab (NREL) that describes a new application of quantum mechanics in a solar cell, which improves the external quantum-mechanical  efficiency of the solar cell to 114%.

 

The NREL solar cell takes advantage of a quantum-mechanical effect called multiple excitation generation (MEG) by means of quantum dots (QD’s). The crystalline tiny semiconductor QDs, 1-20 nm, will exhibit many extreme effects of quantum physics; large band gap as size decreases, electron-hole excitation, "enhanced coupling" of electrons and positive holes.

 

The MEG effect is observed when a photon, from the high-energy spectrum of the sun, is absorbed by a semiconductor material inside the photocell. The result of the energy absorbed from one of these high-energy photons is the excitation of multiple electrons in the semiconductor atoms. As the electrons are excited by this photon, they move from the valence shell of the atom to the conductive shell where they are free to flow leaving behind electron-hole pairs in the atoms they used to occupy. The electron-hole pairs can be envisioned as voids that are theoretically left in the atom when the electron leaves the atom’s electron cloud. These electron-hole pairs, also called excitons, attract other excited electrons and this repetitive process can be used to create a current.

 

This solar cell has reached an external quantum efficiency of over 100%, which means that there are more electrons flowing in a circuit outside the solar cell than are photons of a specific solar spectrum flowing into the cell. Up to 130% efficiency was achieved by factoring in the reflection of photons and absorption of photons by the material.

 

This effect is significantly enhanced when it occurs in a quantum dot. Quantum dots are minute pieces of semiconductor that range from 1 to 20 nanometers. Due of their size they exhibit peculiar quantum mechanical properties that improve the efficiency of the MEG solar cell. One advantage is that the smaller they are, the higher the energy they release when an electron is excited from the valence band to the conducting band (higher bandgap) but in turn, this excitation must be done by higher energy photons. QD’s also allow for the formation of electron-hole pairs (excitations) at room temperature bringing a stronger attraction between electrons and electron holes.

 

QDotssolar_610x342.JPG

Giving off 2 electrons for every photon. (Via Science/AAAs)

 

By keeping these electrons within their minute volumes, quantum dots are able to capture higher energy photons that would normally be turned to heat and lost. The application of the multiple excitation generation, enhanced by the use of quantum dots, has allowed scientists to reach the point where there are more electrons flowing out of the solar cell then there are photons (of the adequate energy level) exciting them out of a quantum dot. Remember, this means that the whole solar spectrum is not used, just the photons that have enough energy but another advantage to the use of QD’s is their cheap cost and relatively easy manufacturing process.

 

Initially, electrons had a difficult time jumping from one quantum dot to the next to create a current. NREL scientists found the solution to this in a chemical coating of hydrazine and ethanedithiol that connects the dots with short organic chains and improves their conductivity. These quantum dots cover a layer of nano-structured zinc oxide, a transparent conductor proven to make MEG effective. They covered the top electrode of the solar cell in gold and covered the entire panel with anti-reflection glass. Due to this type of solar cell, which only uses the high-energy end of the solar spectrum, the over all efficiency of converting light to electricity was only 5%. However, Bruce Parkinson, a chemist from the University of Wyoming, Laramie, who confirmed the concept of an MEG solar cell, expressed this achievement “shows promise for the next generation [solar cell] designs.”

 

These third generation solar cells currently require 2.5 to 3 times the energy needed to excite electrons out if their valence shell to the conducting shell. Parkinson and NREL scientists agree that if they can lower this energy needed by creating more efficient quantum dots, they will see vast improvements in the efficiency of the MEG solar cell. Taking into account their cheap cost, MEG solar cells will make solar energy competitive with fossil fuels. NREL scientists had predicted that using MEG could increase the total thermodynamic energy conversion efficiency to around 55% compared to today’s standard solar cell efficiency of about 20%. While this peak has not yet been reached, their quantum dot solar cell confirmed previous MEG experimental results and promises a lot of room for improvement.


Eavesdropper

0

As copper interconnects reach their limit for transferring data, several solutions are popping up from industry leaders. Photonics seem to be the direction everyone is headed towards. Since fiber-optics have completely taken over for data backbones, optics will eventually reach the smallest interconnect. UCL and the London Centre for Nanaotechnology have created a contender, a quantum dot laser grow in a silicon substrate transmitting 10 Gbits/s at a 1.3 μm wavelength, geared towards being the first photonics link in telecommunications.  A quantum dot is a bit of semiconductor matter with electrical characteristics that are closely related to the size/shape of the crystals they are grown in. The smaller the crystal, the larger the band gap of energy, or the difference between the highest electron valence band and the lowest conduction band. Quantum dot lasers use the dots as the active medium in the light emitting portion.

 

Normally there is a dislocation in the crystal structure caused by contrast in the silicon and the compound semiconductor. However, the UCL overcame this issue by making layers that prevent dislocations. And they have successfully demonstrated the 1.3 μm laser by direct epitaxial growth on silicon, with an optical output of 15 mW per facet at 20-70°C. The size of the lasers make them ideal for use within chip, not external like Light Peak and other such options. Professor Alwyn Seeds, principal investigator in the London Center for Nanotechnology spoke of the groups next step, "The techniques that we have developed permit us to realize the Holy Grail of silicon photonics - an efficient, electrically pumped, semiconductor laser integrated on a silicon substrate. Our future work will be aimed at combining these lasers with waveguides and drive electronics leading to a comprehensive technology for the integration of photonics with silicon electronics."

 

Eavesdropper