Skip navigation

community

News

11 Posts tagged with the space tag
1

dragon_pica.jpg

Dragon capsule (via SpaceX)

 

SpaceX (Space Exploration Technologies Corp.) has recently announced that they will launch their Dragon free-flying reusable space craft on Tuesday May 22nd. This will mark the first time in history that a commercial company has launched a manned space vehicle into space to rendezvous with the International Space Station.

 

The Dragon re-usable space craft was designed using three main components which feature a nosecone that’s used as a shield during lift-off and houses the docking adapter needed to connect to external hatches found on the ISS. The second component featured is the spacecraft itself and was designed to be configured based on payload specifications and houses the avionics, RCS (Reaction Control System or thruster control systems) system, parachutes and other un-pressurized cargo/systems. The third component featured on the spacecraft is the Trunk which is used for un-pressurized cargo, solar arrays and thermal radiators needed to power the craft.

 

The re-usable vehicle will be launched atop of SpaceX’s Falcon 9 two-stage heavy-lift rocket which uses 10 Merlin 1C liquid oxygen and kerosene motors (9 on the first stage and 1 on the second). The mission will bring much needed supplies to the ISS as well as challenge the Dragon in a series of tests designed to test the feasibility of using commercial craft for future missions contracted through NASA and other organizations. If all goes well the launch will take place at Cape Canaveral at 4:15 AM Eastern Time and is expected to return a few hundred miles off the coast of California two weeks later. For those interested in watching the launch head over to SpaceX.com which will start broadcasting 40 minutes prior to launch.

 

Update: The rocket was scheduled to launch this past Saturday, the 19th. However, the team discovered a faulty check valve on the "Merlin Engine." The component was swapped, and not the historic flight will take place this Tuesday, the 22nd. The post was updated to reflect the change.

 

Update 2: The Falcon 9 is now in orbit. The launch was successful.

 

Cabe

http://twitter.com/Cabe_e14

0

 

If you remember the movie ‘Alien’, the crew was tasked with mining various planets and asteroids before their eventual demise on planet LV-426 (Everyone but the hero, that is). While that was science fiction, a new start-up company wants to make mining asteroids and other planetary bodies a reality.

 

Called Planetary Resources, the company is looking to explore the vastness of space. as well as mine valuable metals and water from resource-rich asteroids. To do this, the company will first deploy a low-cost ‘Arkyd-Series 100 Leo Space Telescope’ to search for near-earth asteroids that are rich in resources. Once potential asteroids are found, the ‘Arkyd-Series 200 Interceptor’ (a powered version of the 100) that houses additional scientific equipment will then head to the target and assume a geostationary orbit where it will collect further information on the suspected resources.

 

Once the information collected by the 200 series is confirmed, a ‘Arkyd-Series 300 Prospector’ with laser-based communications is sent out to survey the asteroid and collects information on its shape, density and surface/sub-surface composition in preparation for mining to begin. Initially, only asteroids that contain water will be mined as it can be broken down to its base components (hydrogen and oxygen) and used for fuel making the asteroid a kind of space gas station. The company hopes to use their Arkyd system as a cost-effective means of space exploration while simultaneously grabbing precious metals while doing so.

 

Technology-LEO-Web.pngTechnology-Intercept-Web.pngTechnology-Prospecting-Web.pngTechnology-Mining-Web.png

Concept art for the stages of mining: (1) Scan for targets (2) Up close data collection (3) In depth scan of asteroid (4) Actual mining operation

 

So far the company has no actual details of exactly how these planetary bodies will be mined (I have to go with the concept of Alien's Nostromo, send people there) and transported back to earth but the idea is intriguing to say the least.

 

The company was founded by X Prize board members Eric Anderson and Peter H. Diamandis. Although this effort seems far-fetched, several billionaire investors are banking on the quest. Director James Cameron, Google CEO Larry Page, Google chairman Eric Schmidt, Google executive Ram Shriram, Ross Perot Jr., and Microsoft executive/verteran astronaut Charles Simonyi, to name a few. With the potential operating income, who knows what the future holds for Planetary Resources.

 

Cabe

http://twitter.com/Cabe_e14

1

The-European-Envisat-satellite-Credits-ESA1.jpegenvisat.jpg

Envisat concept art (via European Space Agency)

 

April 8th began the troubles for the European Space Agency (ESA). At a scheduled time, Envisat, a large environment satellite, did not make its transmission of data back home. The satellite is the largest and most expensive non-military satellite orbiting Earth. It measures in at 30 feet long, 16 feet wide, and also carries a large solar array that is about 16 feet wide and 46 feet long and collectively weighs in around 17,600 pounds (about 8,000 kilograms).

 

 

Although Envisat is not communicating as of the moment, efforts are being made to restore contact with the satellite. It is still floating around in a stable orbit and will be for 150 more years unless some outside force interferes with its path. Envisat was only planned to have a five year mission collecting data on environmental factors such as air quality, land masses, sea ice, atmosphere, and ocean conditions. However, the satellite lasted twice as long as planned and scientist were hoping it would  last until its predecessors could be launched and calibrated around the year 2014. 

 

 

Envisat supplied data using 10 different sophisticated instruments. The instruments used include a spectrometer, a radio meter that can measure the oceans temperature, and a radar altimeter. In addition, it used an interferometer which is a Fourier transforming  infrared spectrometer which transmits data about pressure and temperature along with information about atmospheric gases.

 

 

Scientists are worried about the gap in data that the loss of this satellite will cause. Envisat was the most advanced information collecting system in space. An agreement with Canada to use two of their satellites to continue collecting data is being looked into, however those two satellites combined will still not fill in all the missing information that Envisat would have provided.

 

 

For now scientist will have to get by with what they got. ESA has already been planning to launch newer satellites into space called Sentinels. The program will launch 5 different satellites into space over a period of 6 to 7 years. Hopefully engineers can find a way to fix Envisat, or else it will would become a billion dollar, bus-sized piece of technology added to the space junk collection.

 

Cabe

http://twitter.com/Cabe_e14

2

The opening the Japanese animated series "Planetes," depicting the fictional first space debris collision on a commuter transport.

 

The earth has so much garbage in orbit that it’s becoming an increasing concern to not only NASA but to the US Air Force, as well. To help with the problem the Air Force has awarded preliminary contracts to both Lockheed Martin and Raytheon Corp. ($107,000,000 US. each) for the AF’s ‘Space Fence’ program which will be used to track small (1 to 10 centimeters in size) orbiting debris that can cause considerable damage to both satellites and space craft. Lockheed’s solution is to develop a ground-based radar system that will be able to locate and identify the tiny space junk. Their design will consist of two to three radar systems that use the S-band range in the electromagnetic spectrum which will enable them to track objects or microsatellites in low-earth orbit at about the size of a basketball. These radar stations will be placed strategically around the globe which will provide ‘Fence’ coverage even in the southern hemisphere.

 

1320434318303.jpg

Ground based radar tracking system for space debris (via Lockheed Martin)

 

Raytheon has a similar approach to Lockheed which also uses a system of ground-based S-band radars to help in low-orbit earth detection of space garbage. However, Raytheon’s prototype system is already in the testing phase, actively tracking space debris, and was demonstrated to the Air Force back in January of 2012. Both systems so far have been successful in preliminary tracking tests and are more than capable of the task for which they were designed, but there can only be one winner. The victor will be chosen later this year with the winning system fully implemented by 2017. Lets hope a space debris solution is chosen before regular civilian commuter flights head into orbit.

 

Cabe

http://twitter.com/Cabe_e14

 

Other Space Debris Cleanup related news:

New satellite aims to chase down and clean up space debris

NASA to shoot lasers at space debris

SETI to re-start looking for life elsewhere, and track garbage

Space debris threatens the Space Station

Russian POD orbital debris collector

1

bb01e773.jpg

CleanSpace concept drawing (via EPFL)

 

Space is a messy place. According to NASA, it is littered with over ten million pieces of debris orbiting the Earth at a rate of around 36,000 km/h. That junk is potentially hazardous not only to astronauts but can damage or destroy spacecraft and satellites, as well. To combat this problem engineers from the Swiss Space Center at EPFL (Ecole Polytechnique Federale de Lausanne) have designed a satellite that performs a kind of intergalactic housekeeping. Called ‘CleanSpace One’, the satellite finds its target and latches on with a grappling mechanism. Once the garbage is taken hold of, CleanSpace One then de-orbits the Earth and both it and the garbage are harmlessly burned up in the planet’s atmosphere. To match the speed of the space junk in orbit, CleanSpace One will use a special ultra-compact motor that is being developed in EPFL labs to catch its target that travels anywhere from 28,000 to 36,000 km/h. The costs for developing and deploying CleanSpace One costs about $10,000,000 Swiss Francs and will be tested in the next five years with the retrieval of either the Swisscube picosatellite (launched in 2007) or the Tlsat (launched in 2010).

 

This development comes after a long line of other proposed space debris collection. Anime story line inspires many to clean up the skys. The Russian POD system is like a garbage truck in space. SETI will be used to track debris. NASA wants to use laser to shoot down larger pieces. The space station has to move constantly to avoid large bits flying into its path.

 

A Messy, and scary, place indeed.

 

Cabe

http://twitter.com/Cabe_e14

1

Video via Nasa

 

February 24th, 2011 a dexterous humanoid robot, Robonaut 2, was launched into space to be the first of its kind in space and the first United States robot to make its way to the international space station. NASA and General Motors have been working together to create a more human like robot that can simulate and execute human motions and actions. Succeeding in creating such a robot will allow it to perform current human tasks, potentially the dangerous ones or repetitive tasks while also allowing it to use current tools and technologies used by humans.

 

 

Currently, tests are being performed on the robot in order to calibrate it before it is put to use in carrying out missions. Calibrating it involves comparing the motions of the hardware in the 1G environment on Earth, and taking it to the 0G space environment. The first tests on the robot included booting it up and making sure all the circuitry and software made it to the space station in working condition. Just recently, they began testing the movement of the joints and hands. Ultimately, the robot is controlled by a set of software parameters to keep it safe. However, its actions and movements can be controlled from a location on Earth or the space station itself.

 

 

Robonaut 2 was built and equipped with a wide range of advantages over the former Robonaut 1. It is capable of carrying out tasks four times faster than the original. Its systems include built in infrared sensors, a high resolution camera, and has an advanced sensing system. Additionally, its movement technologies include extensive neck travel, ultra-high speed joint controllers, enhanced finger and thumb movements, and series elastic joint technology.

 

 

Robonaut 2 has an identical twin on the ground that will be used to simulate missions and tasks. It will be placed in a replica environment with panels and systems that simulate that of the space station itself. After the simulation is complete, the program can be then sent to the orbiting Robonaut for execution. Future plans for the robot include creating legs for it to navigate around the space station or possibly wheels and a rover base so it can travel across terrain on a different planet.

 

 

See more robots in the element14 Robotics Group.

 

 

Cabe

http://twitter.com/Cabe_e14

1

lares.jpg

LARES (via ESA & Stephane Covaja)

 

The Laser Relativity Satellite (LARES) was launched into orbit on February 13th to challenge Einstein's theory of relativity.  The satellite is made from tungsten and measures only 36 centimeters wide. In addition, it was constructed with many reflectors on its surface used to measure its position from Earth using lasers on the ground.

 

 

Past satellites were placed into space to challenge the exact same theory with varying results. One, Gravity Probe B Satellite (2004 - costing $750 million), brought in results within 19 percent while measuring the geodetic effect. This processes measures distortions in the fabric of space-time due to Earth's gravity field.  Scientists state that LARES should be able to produce precise measurements within one percent.

 

 

With such precise measurements, scientists and researchers will be able to put several theories to the test including gravitational laws, general relativity, and mainly the Lense-Thirring effect. The Lense-Thirring effect is derived from general relativity and describes how the rotation of nearby objects affects the rotation of other nearby objects. If the precision lasers pick up a disturbance in the orbit of LARES, it will verify relativity among other theories.

 

 

The satellite was launched by Vega, a small rocket used to economically launch lower mass satellites into orbit around Earth. The launching station is based in Kourou, French Guiana. The launch also has a secondary goal, to make Kaurou a ESA, and other space agencies, launch hot-spot. With NASA out of the shuttle business, Kourou is sure to be busy.

 

 

Cabe

http://twitter.com/Cabe_e14

2

workshop.jpg

Photo of MakeIt Labs from the inside caught the local government's eye (via Focusure Studios)

 

The first Hackerspace government shutdown too place in Nashua, New Hampshire in December 2010. Although, the exact reason for the shut down has not been described past the use of beaurocracy, some vague justifications have surfaced.

 

“We don’t shut places down unless we’re really concerned about the safety of people,” director of community development Katherine Hersh told the Nashua Telegraph.

 

“Their business is so varied, with a variety of different industrial processes – a kiln, automotive repair, cutting and welding – and along with each one of those comes a variety of concerns,” the local fire marshal Richard Wood explained.

 

The jealousy inducing 6,000 square foot MakeIt Labs was founded in July of 2010 by area “hackivists.” Their operation fits into an area of a old 25,500 square foot industrial building near the Crown Street railroad lines. The non-profit Makerspace has a hydraulic car lift, 3D printers, ceramic kiln, a laser cutting, and the standard set of tinkering tools.

 

The plan now is to get the building up to code. Installing Fixing the electrical system, plumbing, and ventilation will be needed before they can reopen. However, it is the bathroom that has cause the most concern. MakeIT Lab’s founders stated that the bathroom is considered new construction, and has a expansive set of regulations to follow. The Nashua officials stated that they want MakeIt Labs to stay in their town, but they want it to be safe. 

 

See more about MakeIT Labs at their website.

 

Cabe

http://twitter.com/Cabe_e14

1

low_earth_orbit-thumb-450x317.jpg

Trackable objects in Low Earth Orbit. One of these may be for communication freedom someday. (via European Space Agency)

 

At the Chaos Communication Congress in Berlin, an "unsensorable internet" via private satellite was proposed. The concept stems from telecom limitations and government sanctions, such as the Stop Online Piracy Act (SOPA). (SOPA is currently being reviewed by the House Judiciary Committee.) By using a satellite, no government or privatly controlled wires are need. Sidestepping earthly bonds may be the only way from true unregulated communication.

 

High altitude balloons have been launched with notable success. However, such a device can only handle a narrow slice of the planet's surface, by comparison to satellites. Some amateurs have placed satellites into low earth orbit. At that position, an object would circle the earth every 90 minutes. The only option is geostationary orbit above the equator.

 

Although outer space is not governed by any country that sits underneath, people are free to attack/disable satellites at will. In most cases, such an action would be taken as an act of war. The "free internet" people would not be able to do much more than hang their heads low after the event.

 

As a compliment to the satellite system, a ground based network was also proposed by the "Hackerspace Global Grid" (HGG). The vision is to create a "fallback infrastructure in case of natural and economic disaster to stay connected." Their system creates a land based network of base stations that keep a constant contact with the possible satellite, even in low orbit. There are already DIY systems for tracking satellite positions. Now it is just a matter of relaying the data. The goal is to provide these stations at around $130 USD. Cheap enough when everyone willing to host a node, could.

 

Both endeavors are plagued with the same stopping limitation, lack of funding. If this does come to fruition by some means, how would you feel to use an internet controlled by hackers?

 

Cabe

http://twitter.com/Cabe_e14

 

 

HGG also stated that they would like to place an amateur astronaut on the moon within the next 23 years. I think the Google Lunar X Prize, placing a robot on the moon, should be conquered first.

1

GRAIL_Poster_browse.jpg

GRAIL probes render. (via NASA)

 

According to the North American Aerospace Defense Command, there are over 9800+ man-made objects orbiting the Earth. As many now know, this is becoming an issue. Our reach does not stop at our geosynchronous orbits, the Earth's moon now has two satellites.

 

NASA launched two satellites that, as of December 31, 2011 and January 1, 2012, have taken their positions around the moon. The "GRAIL probes" launched back in September of 2011 for the dubious sole-goal of mapping the moon's gravitational field. The mission principal scientist, MIT's Maria Zuber, said the purpose best, "We don't actually know why the near side and far side are different."

 

Circling the moon at 55 km above its average surface, the GRAIL probes will use microwave signals to measure the distance between themselves that changes based on the gravitational differences on the surface of the planet.  Accuracy will be within a width of a human-hair. According to NASA, the maps will be "100 times" better than previous recorded near side gravity maps, and "1000 times" for the far side. Zuber again, "When we can improve by a factor of two, we can learn a lot, and improving by a factor of 1000 is transformative."

 

Currently the probes are collecting "better than expected" energy via their solar panels. Zuber stated that the team believes that the GRAIL satellites should be able to store enough energy to stay functional during the pending lunar eclipse in June of 2012. At which time the team will lower the probes to 25 km above the surface a perform a "treetop-skimming" study of the structures of craters. External mapping and internal structure are

 

Another purpose of the mission is to prove, or dis-prove, the University of California's claim that the Earth had two moons at one time. Where the current moon collided with its smaller, 1300 km diameter, sibling at low speeds. Where, instead of forming a typical crater, the strike merged the two. The far side is more mountainous that the front, and they aim to get to the bottom of the mystery.

 

Cabe

http://twitter.com/Cabe_e14

2

Satellite1.jpg

 

When Space Shuttle Endeavour launches for its final mission, a experimental type of satellite will be parts of its cargo. Three prototype 1-inch square satellites, each dubbed "Sprite," will be part of the Materials International Space Station Experiment (MISSE-8). Attached to the space station, they will sit in space for an undetermined number of years, to see how they stand up to the harsh environment. These micro-satellites were designed over the course of 3 years at Cornell University. Exact dates were not specified by the team. However, the prototypes were built by three students, Ryan Zhou, Zac Manchester, and Justin Atchison, when they were undergraduates. The latter two are now working on their doctorates. These "chip satellites" may have been made over 4 years ago.

 

Project leader, Mason Peck, talks about their potential, "[The] small size allows them to travel like space dust," said Peck. "Blown by solar winds (protons & electrons traveling at 600km/s, 370miles/s), they can 'sail' to distant locations without fuel. ... We're actually trying to create a new capability and build it from the ground up. ... We want to learn what's the bare minimum we can design for communication from space."

 

Peck's Sprites will be the first chip satellites launched into space. The goal now is to see how the communication system will work out, power, and overall tolerance to conditions. Then, Peck wants to launch a large number of Sprites and "sort out which is which."

 

Eavesdropper