Skip navigation

community

1 2 3 ... 11 Previous Next

News

163 Posts tagged with the test tag
1

 

There’s good news for those of you who need to destroy your data stored on your SSD’s quickly and efficiently in an emergency situation. RunCore (manufacturer of SSD’s) has unveiled their new line of InVincible Solid State Disc drives which feature two ways to ensure data destruction.

 

The first capability the drives feature is ‘Intelligent’ destruction which over-writes the data and returns the drive back to its factory default setting. According to the company there is no possible way to recover the original data stored on the drive once the drive is reset. This is the rather mundane approach as the second option for data elimination is much more fun and effective (as well as costly).

 

The second option of data deletion the drives feature is self-destruction. Essentially the drive over-volts itself and physically damages the NAND chips inside rendering the drive useless (like a bad CPU overclocking job). To initiate both data erasure and destruction, the InVincible drives feature a two push-button system that is physically attached to the drive with the green button for erasing and a red button for meltdown.

 

These new drives were designed for the military, as well as other companies and institutions where sensitive data is being used or stored, and come in varying sizes and capacities that can withstand a temperature range of -45 to 200 degrees Fahrenheit. The company hasn’t said when the InVincible line of will be available or how much they will go for, but chances are they will cost more than current SSD’s and be available before the year is out.

 

Cabe

http://twitter.com/Cabe_e14

1

dragon_pica.jpg

Dragon capsule (via SpaceX)

 

SpaceX (Space Exploration Technologies Corp.) has recently announced that they will launch their Dragon free-flying reusable space craft on Tuesday May 22nd. This will mark the first time in history that a commercial company has launched a manned space vehicle into space to rendezvous with the International Space Station.

 

The Dragon re-usable space craft was designed using three main components which feature a nosecone that’s used as a shield during lift-off and houses the docking adapter needed to connect to external hatches found on the ISS. The second component featured is the spacecraft itself and was designed to be configured based on payload specifications and houses the avionics, RCS (Reaction Control System or thruster control systems) system, parachutes and other un-pressurized cargo/systems. The third component featured on the spacecraft is the Trunk which is used for un-pressurized cargo, solar arrays and thermal radiators needed to power the craft.

 

The re-usable vehicle will be launched atop of SpaceX’s Falcon 9 two-stage heavy-lift rocket which uses 10 Merlin 1C liquid oxygen and kerosene motors (9 on the first stage and 1 on the second). The mission will bring much needed supplies to the ISS as well as challenge the Dragon in a series of tests designed to test the feasibility of using commercial craft for future missions contracted through NASA and other organizations. If all goes well the launch will take place at Cape Canaveral at 4:15 AM Eastern Time and is expected to return a few hundred miles off the coast of California two weeks later. For those interested in watching the launch head over to SpaceX.com which will start broadcasting 40 minutes prior to launch.

 

Update: The rocket was scheduled to launch this past Saturday, the 19th. However, the team discovered a faulty check valve on the "Merlin Engine." The component was swapped, and not the historic flight will take place this Tuesday, the 22nd. The post was updated to reflect the change.

 

Update 2: The Falcon 9 is now in orbit. The launch was successful.

 

Cabe

http://twitter.com/Cabe_e14

0

CortexA9.jpg

ARM Cortex A-9 (via TSMC)

 

Today's processor industry is largely controlled by two companies, Intel and ARM Holdings. Intel produces processors running in most of today’s laptops, desktops, and servers. On the other hand, ARM largely dominates the quickly growing mobile industry. Both are looking to invade each others markets soon by developing processors with high performance and low power consumption, or a strong performance per watt ratio.

 

 

Taiwan Semiconductor Manufacturing Company (TSMC) may have just made ARM Holdings future in the CPU market a bit more promising. At TSMC, they have recently ran a 28nm dual-core ARM Cortex A-9 processor at a max speed of 3.1GHz. The clock speed is 55% higher than present and is about twice as fast as its 40nm counterpart at TSMC. Additionally, the ARM chips also have the advantage of very little heat dissipation, giving them the ability to be densely packed together with one another.

 

 

Two of ARM's many partners include Nvidia and Calxeda, are both looking to produce ARM based processors to compete with Intel. Calxeda is working on producing chips for servers that work more efficiently. Such as implementing overlapping operations during each clock cycle to allow better speed handling. The method gives them an efficiency boost and may work to an advantage for large data retrieving applications such as web hosting.

 

 

TSMC also produces mobile chips for Nvidia. The successful high speed processing test can also mean good things for Nvidia. Nvidia is working on a custom ARM based processor to use in desktops and laptops to compete with Intel. The CPU project dubbed Project Denver has already been in development for some time, but TSMC's latest breakthrough could give the project a large boost.

 

 

The coming products produced from this “competition” should give us some interesting products in the future. Both companies will not easily be letting other companies invade their markets. The server market is worth $50 billion due to the rise of cloud computing and use of social networking. In addition, everyone can see the rise in the uses of tablets and smart phones.  The competition will lead us into the future of processor technology, which will be developed with these two companies paving the way.

 

Cabe

http://twitter.com/Cabe_e14

1

 

Augmented reality give a new way to interact with technology, and ambitious companies are clamoring to be firsts in the field. One of those concepts being developed by the software giant is called MirageTable. The system lets the user interact with objects in both the real and virtual worlds on a table top.

 

For instance; a person could set up a series of virtual bowling pins that could then be knocked over with a virtual ball with only using one pin as a real model to clone the others. The researchers developed MirageTable with the idea that two people could interact with each other in the same space without actually being with one another (think of it as being like Star Trek’s Holodeck). To do this, the researchers used an Acer H5360 3D stereoscopic projector (1280 X 720) to display objects, as well as the other person, onto a curved screen. A Kinect is positioned on top of the screen and captures the objects that are being projected and also tracks the eye movements of each corresponding user. This is to give the corresponding user the correct perspective of what’s in front of them. To view the objects in an augmented reality 3D environment each user wears a pair of Nvidia 3D shutter glasses which makes them appear spatially registered in conjunction with the real world. Any object can be scanned and then cloned for interaction by either of the two parties in both the real and virtual space.

 

-001.jpg

Virtual Bowling (via Microsoft)

 

Free-hand interaction (because no trackers, gloves or other hardware was implemented) with virtual objects in MirageTable was done by using software that takes all real-world objects and represents them as proxy particles, which are constantly updated and used for collision geometry in the virtual world. To process all of the dynamic physics constantly being updated the team relied on Nvidia’s GeForce GTX 580 along with their PhysX game software. This gives each person the ability to interact with both environments at the same time. The researchers admit that there are still limitations to overcome as the Kinect (at present) can only capture the front of an object and not all sides which leaves ‘gaps’ that make for bad texturing. Another problem the team faces is users can only scoop or catch objects from below instead of grasping or picking them up but hope to improve on these limitations with further development. I for one am very impressed at what they have already accomplished with MirageTable. What will its full capabilities be in the future if only as a gaming platform?

 

Cabe

http://twitter.com/Cabe_e14

0

Teaser_company.jpgFXI-withoutDOUBLECAP-2_withnumbering_2-300x187.png

Concept models (via FXI)

 

Only a short time after intensely successful Raspberry Pi hit the market, copy-cats came sweeping in to grab some of the frenzy.

 

FXI, a Norwegian hardware and software developer, has recently announced that the company plans to release their USB-stick sized computer later this month (May, 2012). The stick, dubbed Cotton Candy, is designed to connect to any screen and turn it into a personal computer. Does this sound familiar?

 

FXI states that the device can be used to complement mobile devices such as smartphones, tablets and notebooks but can also provide ‘smart’ capabilities to standalone screens such as TV’s. While Cotton Candy may be small in size, it none the less houses some pretty big hardware. Providing the computational power is an ARM Cortex A9 1.2GHz processor that’s coupled with a quad-core ARM Mali -400P GPU to deliver HD content (native support for MPEG-4, H.263/4) with resolutions up to 1080p on HD-capable screens. The device packs 1 GB of dedicated memory and the ability to upgrade to 64 GB through micro-SD cards for increased storage of media. Another impressive feature of Cotton Candy is its plethora of connection options that include USB (male) 2.0, micro-USB (female) 2.0 and HDMI. The software it uses is pretty much rounded out with Android 4.0 (Ice Cream Sandwich) and Ubuntu with a virtualization client for Windows, Linux and Mac (sorry no iOS). Content on-screen can be controlled in various ways with integrated keyboards found on tablets and notebooks, or wirelessly with the devices built-in Wi-Fi and Bluetooth connections that let you use your smartphone as the interface.

 

As it stands right now, only Scandinavians will be able to lay their hands on Cotton Candy at the end of May (2012), while the rest of us have to wait till the end of 2012 and should retail for about $200.00 US. The price is nearly 6 times that of the Raspberry Pi. Are the differences worth the extra $165?

 

Cabe

http://twitter.com/Cabe_e14

0

 

Have you ever been skiing and had to put up with the hassle of trying to answer your cell phone or listen to music? I have not, but Anthony Griesel has. This skier and software developer is recruiting people to contribute to his Kickstarter for a project Called Neva that will facilitate staying connected while outside in the cold elements.

 

 

The idea is simple, to avoid having to fumble with small devices while you are bundled up on the slopes, he has developed a smart ski pole that allows you to manage calls, SMS, and displays other useful information like time, temperature and elevation on a 0.96’’ extra bright OLED touch display placed directly on top of one of the ski poles. Of course, all of the electronics are kept safe inside by a waterproof seal.

 

 

The poles wirelessly communicate with Android and iPhone via a low power Bluetooth using a free downloadable app. This app has more features like using the GPS locations for calculating slope angle and aspect and can also track your route in Google Earth KML format.

 

 

The poles themselves are made with 7075 grade aluminum, which has properties comparable to mild steel. The included rechargeable battery is said to last 3 days between charges and will last about 500 charging cycles. It is charged using a generic USB connection, but this will not be included.

 

 

Griesel hopes that his system will prevent users from losing or damaging their devices, and he hopes that added features will provide valuable information as to avoid dangerous parts of the mountains or avalanche prone areas. He does mention  that there is no substitute for experience and good judgment.

 

 

So far Griesel's kickstarter has raised over $11,000, which is still far from the goal of $100,000 , but there are 21 days to go. The rewards for a pledge are very enticing. A modest contribution of just $150 will earn you your own set of Neva ski poles.

 

Eavesdropper

2

ctia_logo.gif

 

A new emergency alert system is set to go into effect in April geared towards mobile devices. Called the ‘Wireless Emergency Alerts’, the system was developed by FEMA (Federal Emergency Management Agency), the FCC (Federal Communications Commission) and most major wireless carriers to bring free emergency text alerts to mobile devices. The system is initiated by local, state or national officials who in-turn alerts a Federal aggregator (central hub) which translates the alert message into a specified software format that is able to be used by mobile carriers.

 

The translated alert is then sent to cell towers (if they haven’t been destroyed) in that particular area of disaster. CMAS-enabled (Commercial Mobile Alert System) mobile devices will then receive a special ring-tone and vibration in the geo-targeted area notifying the user of the emergency. As of now the WEA system will use three kinds of alert messages; Presidential: for national emergencies issues by the president or designee (terrorist, financial melt-downs and alien invasions?). Imminent Threat Alerts: NOAA severe weather alerts and other man-made or natural disasters. And finally Amber Alerts: for missing or exploited children. All messages are limited to 90 characters.

 

Unlike traditional text messages that aren’t point-aware, the WEA system is a point-to-multipoint generator meaning only those affected in that area (regardless of phone origin or area code) will receive that message. So, if you’re from Chicago but visiting Denver when an emergency occurs, you will be notified if you’re in the path of eminent doom. However, people will be able to opt-out of the imminent threat and amber alerts. Presidential alerts are mandatory.

 

According to the CTIA (International Wireless Association) the bulk of alerts will be weather related with advisements for tornados, earthquakes and floods and will give the user important information (such as seeking shelter) based on the specific alert. The system sounds like it will be very useful, but what happens if you’re riding out an earthquake while in the middle of a violent storm that produces a tornado?

 

Most mobile carriers will display the image below if the device is capable with the alert system.

weac_logo_v2.jpg

 

Eavesdropper

3

 

The Hybrid Memory Cube Consortium (HMCC) has recently announced that Microsoft has joined the conglomerate in an effort to integrate HMC technology into next generation systems. The HMCC are a group of electronic equipment manufacturers that include industry giants such as Samsung, IBM and Micron that are looking to develop and implement  advancement in DRAM memory technology called Hybrid Memory Cube (HMC).

 

The HMC features 15x the performance of DDR3 memory by utilizing a memory die that’s stacked using Through-silicon-VIA (Vertical Interconnect Access used to create 3D circuits- hence the ‘cube’). HMC technology has increased density that enables more memory to be packed into a space that’s 90% less over today’s DDR3 modules while utilizing 70% less energy per-bit.

 

The connections between the efficient stacked chips are shorter, which is why it takes up less of a foot-print over traditional DDR modules and is also significantly faster. This means that memory bandwidth and clock speeds can remain constant with each new iteration of CPU’s and GPU’s which isn’t limited to networks and PC’s but will also provide a performance boost for mobile devices such as smartphones and tablets as well. Microsoft has recently join the Consortium, hoping its resources will get the technology developed quicker. If the Consortium is successful in their developments, the future will indeed be ‘cubed’!

 

hmcstack.jpg

Actual image of a HMC (via HMCC)

 

Cabe

http://twitter.com/Cabe_e14

2

-010.jpg

(via Microsoft)

 

With the recent uncovering of toxic e-waste destroying the environment in Guiyu China, it was only a matter of time before huge companies started to rethink of what it actually means to be ‘green’. One such company is taking it rather seriously and is stepping up, becoming more environmentally conscious in every aspect of their business; Microsoft. The company will become completely carbon neutral by the beginning of the fiscal year, which starts on July 1st of this year (2012).

 

To do so, the company says that they are implementing an internal ‘carbon fee’ for each of their operations buildings in over 100 countries. Meaning each representative institution will be required to pay a fine (to Microsoft headquarters in Redmond) for carbon emissions based on renewable energy and carbon offsets. This will create an incentive among the data centers, office buildings and development labs to reduce or eliminate their carbon emissions. Some of the steps taken by Microsoft to become more environmentally friendly include ‘a smarter buldings pilot’ which entailed using software and technology to make Microsoft’s Redmond campus more energy efficient. Another step included using Carbonsystems Enterprise Sustainability Platform (ESP), which is an application that collects data from smart-meters, energy suppliers, waste processors and internal business systems to learn ways of reducing the global impact of carbon waste. Microsoft is even going as far as purchasing more renewable power agreements from various green conscious power companies and reducing air travel for business trips through based on the benefits incurred as each flight produces 1000kg of carbon emissions per trip. So far Microsoft is leading the way for a greener future , but we will have to wait and see if other companies follow suit in carbon-emission reduction.

 

Cabe

http://twitter.com/Cabe_e14

0

 

With today’s technology, it’s never been a better time to be a kid playing in a sandbox, and it's all thanks to researchers from UC Davis. The research team, headed by Oliver Kreylos, has designed an ‘Augmented Reality Sandbox’ as an interactive teaching tool for children to learn about earth sciences in places such as museums. The box can be configured for a myriad of topographical real-time representations at a scale of 1:100 and includes the ability to make it rain as well as water-flow simulations. To accomplish these feats, the team used a closed-looped Microsoft Kinect camera that grabs movement and objects at a rate of 30 fps. Then the system feeds the information to a computer running a combination of software derived from the Vrui VR development tool-kit and the Kinect 3D video processing framework.

 

The software, driven by a Nvidia GeForce 580 GTX, takes the information provided by the Kinect sensor and compiles a real-time topographical image complete with an elevation color map, topographical contour lines and simulated water based on how the sand is arranged inside the box itself. All the rendered graphics and real-time information is then projected back onto the sandbox using an overhead 3D data projector giving the viewer an unobstructed visual 3D model. While it may be a great learning tool, it makes me want to break out my MechWarrior Battle-Mechs and have a really cool war on a field with destructible terrain!

 

Cabe

http://twitter.com/Cabe_e14

0

 

With college tuition rising and more and more students taking online courses, it only made sense that  the more renowned schools would give the people what they want. MIT has partnered with Harvard to bring us edX, a "campus-based education" that is completely online. Last year MIT offered up free online classes (MITx) for those who wanted to expand their knowledge, and the faculty over at Harvard took notice.

 

Both prestigious institutions thought it beneficial to combine forces and create edX which provides interested users online classes (again for free) that feature video lessons, embedded quizzes and online laboratories. Those ‘super-interested’ individuals may be eligible for certificates of mastery in certain subjects. EdX is also a research tool for the combined faculty of both colleges in gaining valuable feedback data on how students learn which will improve existing classroom curricula and laboratory exercises through interaction of new technology.

 

The edX platform is open-source, through which other institutions and schools can contribute their material for offering additional courses as well as being an instruction tool. As it stands now only material from MITx and Harvardx will be available when online classes start this fall (2012), but that could change by the end of the school year.

 

Cabe

http://twitter.com/Cabe_e14

0

22474001817597138.png

Droplet (via MIT)

 

The Information Ecology group from MIT’s Media Lab was on-hand to demonstrate some innovations in light-based communications at MIT’s open house (2012). First on their list is a device called Droplet that lets you transfer information from a monitor or other hub to mobile devices such as tablets through the use of an RGB LED. The Droplet glows green and red depending on the time it takes to grab whatever information you want from the screen. For example, in the demonstration, the Droplet was placed on a screen to download an event on a calendar. The device blinks red when downloading and then turns green when the information is finished transferring at which point it acts as a countdown timer to that specific event. To check how much time is left simply place the droplet on any touch-capacitive device (that has the corresponding software needed installed) to see how much time is left as a digital read-out. You can also modify those settings with the Droplet.

 

The second demonstration centered on the groups StackAR device which also takes advantage of capacitive touch and light-based communication.  However, instead of using a timer like the Droplet, StackAR makes use of a LilyPad Arduino unit which can then be used to display a schematic of the Arduino on the touch-screen display using the integrated UI software. This lets easily see how to wire-up the circuitry of the Arduino based on whatever project you’re using it for. The UI can also be used for a programming the unit, where routines can then be instantly uploaded to the StackAR through the light-based connection. Sure these are only prototypes and proof-of-concept devices, but their potential uses for light-based data transfer are incredible.

 

Eavesdropper

0

 

Just a short blurb: Google Drive is now live, offering 5GB of online storage.

The best feature is connecting all the various Google apps with Drive. Sharing files larger than 20mb with friends/colleagues is also a big plus. Also, it's free. So, get started today.

 

This is not the only option for free cloud storage. Amazon Cloud Drive(5GB), Box (5GB), iCloud, and Dropbox (2GB) all come to mind.

 

Sign up for all of them and reap the combined 17GB. (excluding iCloud)

 

Cabe

http://twitter.com/Cabe_e14

1

The-European-Envisat-satellite-Credits-ESA1.jpegenvisat.jpg

Envisat concept art (via European Space Agency)

 

April 8th began the troubles for the European Space Agency (ESA). At a scheduled time, Envisat, a large environment satellite, did not make its transmission of data back home. The satellite is the largest and most expensive non-military satellite orbiting Earth. It measures in at 30 feet long, 16 feet wide, and also carries a large solar array that is about 16 feet wide and 46 feet long and collectively weighs in around 17,600 pounds (about 8,000 kilograms).

 

 

Although Envisat is not communicating as of the moment, efforts are being made to restore contact with the satellite. It is still floating around in a stable orbit and will be for 150 more years unless some outside force interferes with its path. Envisat was only planned to have a five year mission collecting data on environmental factors such as air quality, land masses, sea ice, atmosphere, and ocean conditions. However, the satellite lasted twice as long as planned and scientist were hoping it would  last until its predecessors could be launched and calibrated around the year 2014. 

 

 

Envisat supplied data using 10 different sophisticated instruments. The instruments used include a spectrometer, a radio meter that can measure the oceans temperature, and a radar altimeter. In addition, it used an interferometer which is a Fourier transforming  infrared spectrometer which transmits data about pressure and temperature along with information about atmospheric gases.

 

 

Scientists are worried about the gap in data that the loss of this satellite will cause. Envisat was the most advanced information collecting system in space. An agreement with Canada to use two of their satellites to continue collecting data is being looked into, however those two satellites combined will still not fill in all the missing information that Envisat would have provided.

 

 

For now scientist will have to get by with what they got. ESA has already been planning to launch newer satellites into space called Sentinels. The program will launch 5 different satellites into space over a period of 6 to 7 years. Hopefully engineers can find a way to fix Envisat, or else it will would become a billion dollar, bus-sized piece of technology added to the space junk collection.

 

Cabe

http://twitter.com/Cabe_e14

1

graphene_j-1z5bcpg.jpg

(Right) Professor Michael Weinert (Left) Graduate student Haihui Pu holding up a sculpture of the graphene monoxide (GMO) atomic structure

 

Graphene has been applied for a myriad of applications that include generators, solid state memory, and RF mixers to name a few. However, scientists from the University of Wisconsin have been successful at transforming graphene into a new substance which makes it ideal for use as a semiconductor.

 

The team of scientists and engineers were conducting experiments involving graphene-oxide heated inside a vacuum in order to reduce the oxygen content mixed throughout the on-atom thick material. Instead of eliminating the oxygen the team found that they created a new substance they call ‘graphene-monoxide’ (GMO). Actually, they succeeded in creating 4 new materials by varying the temperature inside the vacuum but all are collectively known as GMO. Graphene is extremely efficient when it comes to conducting electricity over gold and copper wiring, but until now the substance has only been applied as conductors and insulators.

 

GMO (graphene-monoxide), the team found, exhibits all three characteristics for electrical conductivity (conducting, insulating and semiconducting), which would be beneficial in making future electronics faster as we are reaching the end of how small we can go with silicon-based conductivity. The team is still exploring the exact details as to how they created this new substance and what the ideal conditions will be for its creation and destruction. Don’t expect GMO to be used as a semiconductor or implemented in near-future designs like new batteries anytime soon.

 

Eavesdropper

 

See more about graphene:

Girl Scout cookies to graphene

155Ghz graphene transistor

Graphene transistor from Nobel Prize winner

Transparent graphene transistor material stretches beyond all others

Graphene circuit auto-cool effect

Graphene made cheap and green

Cutting Costs and Cooling Efficiently With Graphene

Creating graphene with the help of pond scum

Researches can grow large sheets of graphene in one step


1 2 3 ... 11 Previous Next