Skip navigation

community

News

6 Posts tagged with the windows_phone tag
1

nokia front.JPGNokia_808_PureView_back_black.jpg

Nokia 808 (via Nokia)

 

There have been some pretty compelling smartphones showcased at this year’s Mobile World Congress. However, the crown of ‘best new mobile handset’ went to Nokia and their 808 PureView smartphone. The phone houses a 41 megapixel sensor with a Carl Zeiss lens which is able to cram 7 pixels into 1 (using Nokia’s proprietary technology) that helps the phone take 1080p pictures and HD movies at 30 frames per second! The images taken can then be uploaded to the net instantly to GetMeRated, Vimeo or a host of other social sites using apps downloaded from Nokia.

 

The 808 uses a Xenon flash that can capture video and images in low-light which is a problem for current smartphones. Another feature in the PureView is the ability to record sound with ultra-low bass at up to 140 decibels. The recorded bass can only be played back in true Dolby Surround sound (provided you have headphones capable to do so). As for the phones display screen; it uses a 4 inch AMOLED screen with a nHD resolution of (16:9) 640 X 360 capable of displaying 16.7 million colors.

 

(41 megapixel brings professional medium format digital photography to the masses. Everyone gets to be Ansel Adams with this sensor.)

 

The 808 PureView comes with everything you’d expect from a top of the line smartphone in terms of connections, including USB 2.0 (why not 3.0?), HDMI and Bluetooth 3.0. It also comes equipped with a dedicated GPU with OpenGL 2.0 that is capable of playing 3D games. A dual-core 1.3Ghz processor, 512MB of ram, and 16GB storage fill out the rest of its specs. The launching OS is Symbian Belle, an all but outdated platform. Though, we are sure to see the 41 MP camera on future Windows Phone handsets. The Nokia 808 PureView is available now (unlocked) for $895.00 US but should be available soon for most major carriers in the coming weeks or months.

 

For those who want to know:

35mm film = 10-16 megapixels

Medium format film = 31-62 megapixels

Large format film = 149 megapixels to 1.15 gigapixels

 

Cabe

http://twitter.com/Cabe_e14

2

 

For all those lost in the search for a scanty Raspberry Pi, don't forget to download and try the Windows 8 consumer preview.  It is the next level of OS HMI connectivity. Microsoft has ushered in the "Metro" style navigation in Windows Phone to the next incarnation of Windows.

 

Geared towards tablets and multitouch desktops, I am on the fence on how useful the interface is for a single mouse pointer. Easy access common applications are handy, but are they necessary? All in all, I am impressed with the preview. Give it a shot yourself here: http://windows.microsoft.com/en-US/windows-8/iso

 

Update: It appears that the Raspberry Pi does not meet the requirements to run Windows 8. How unfortunate. (Min specs 1Ghz CPU, 1GB ram)

 

Eavesdropper

1

app economy.JPG

(via TechNet study)

 

Some say the mobile device "app gold rush" is over. Both the iOS and Android markets have the better part of a million applications each, how can there be room for more? I disagree. I think the field is flush with possibilities. So far, 466,000 jobs have been created in the "app economy" business. There is room for more.

 

The App Economy generated $20 billion USD in 2011 alone, according to the TechNet study on the industry. The revenue includes app sales, in app advertising gains, virtual and physical goods sold due to apps. The major contributors to the app markets are not surprising: iOS, Android, Blackberry, Facebook site apps, and Windows Mobile/Phone. (I would say Blackberry may be a dwindling market for the developer, beware.)

 

jobs by region.JPGapp jobs by location.JPG

(Left) App jobs per state  (Right) App jobs per city (via TechNet study)

 

Geographical location was also obvious in the report. California state, USA, takes the crown having 23.8% of the jobs. New York, Washington, Texas, New Jersey, Illinois, Massachusetts, Georgia, Virginia, and Florida round out the top 10 in order. Being close to the OS company in Silicon Valley is a popular choice for app developers, while others want to be near advertising/media concentration in New York.

 

Growth is predicted, by the report, to be significant in the coming years. Between 2010 and 2011, an increase of 45% was seen in the job want ads. If you have the skill, the jobs are plentiful.

 

growth app.JPG

App career growth chart (via TechNet study)

 

With feature phones (dumb-phones) outnumbering Smartphones 4:1, globally, as of 2011, the app market has the potential to grow 400%. Take $20 billion and make it $80 billion to give another perspective. There are 82.2 million Smartphone users in the USA(2011), those numbers will only grow over time. I liken this to the adoption of computers in the home. At first slow, now every home has several.

 

Want to get started? Try the Goolge/MIT App Inventor. No coding needed.

 

Cabe

http://twitter.com/Cabe_e14

 

See the full TechNet study, attached to this post

1

 

What can one do when it is snowing outside, and one wants to fly a helicoptor? No worries you can now do it on your desk. If you have a Windows Phone and Kinect beta SDK, you are all set to fly! Not only do you not have to worry about crashing into anything, there are many other different applications that are pseudo-holographic.

The Kinect creates a pseudo-holographic by using a simple engine. This is not like a holographic card that needs to be physically move back and forth to get the effect. The Kinect recognizes where the viewer is positioned. After it figures out your position, the 3D engine adjusts the image in a view that gives the illusion of a real 3D object. To have better effects in real life, the 3D engine supports anaglyph 3D (red/cyan glasses). When controlling the application you simply use your Window Phone 7 app.


This particular demonstration shows a possibility for gaming in the near future Using the Kinect could immerse a user in the pseudo-3D world with projections on the wall. The rumored Kinect 2 may just have the resolution to keep track on head and even eye movement, to make sure 3D effects likes this one becomes real.


Looking for the original Youtube poster's, programming4fun's, "HoloController" source files have turned up nothing past a collection of videos. I am sure more will surface soon.


Cabe

http://twitter.com/Cabe_e14

0

phonegap.JPG

(Via PhoneGap)

 

Have idea for a simple phone app? Why not release it for the 4 big mobile operating systems at the same time: Windows Phone, Android, iOS, Blackberry, symbian, bada, and webOS.

 

PhoneGap 1.3 was recently released bringing along with it the most useful cross platform development environment to date. The new update mostly is to give Windows Phone 7.5 (Mango) full support of the features. The backbone of PhoneGap is based on web development standards, which innately bridges between the platforms already. The core relies  upon Java, HTML5, CSS and many native PhoneGap tools to get the job done. The best part is, PhoneGap is open-source. 

 

Originally developed by the company Nitobi, now part of Adobe, the PhoneGap framework (aka Apache Callback) has seen many contributors add to the project, most notably, RIM, IBM, and Microsoft. 

 

Unfortunately, according to the licensing agreement, PhoneGap can only be used on free apps. However, nothing says developers cannot make money with in-app advertisement. Take a look at the PhoneGap website to get started.

 

 

See more software development in the Knode OS forum.

 

Cabe

http://twitter.com/Cabe_e14

0

(Via Andrew Bragdon and Microsoft)

 

"It's true, Apple caught us all napping. It launched something that was very iconic, new and unseen with a very good user interface." - Microsoft UK Head of Mobility Phil Moore (December 2009)

 

Only a few years later Microsoft (MS) returns and innovates past the small screen with Microsoft Surface, Windows Phone, Windows 8, and into the third dimension with Kinect. The potential of all their innovations is still anchored in research. Surface is not in everyone's coffee table. Windows 8 is not out yet. Windows Phone's market share is still low. Kinect is isolated to gaming on the XBOX at the moment, with a Windows SDK out for those who wish to develop.

 

However, MS wants to bring all their new inventions into the business space with another research venture, Code Space. The effort combines touch, devices, and skeletal tracking in a conglomeration that appears quite useful. The goal is to literally get everyone on the same page, allows for interaction by all the parties, and brings synergy to new heights.

 

figure1.jpg

Depiction of all the devices at play. (Via Code Space)

 

The main screen is a touch interface, similar to Surface. A Windows Phone can be used as an input device, able to manipulate data on the main screen. The best part is the ability to move content to and from the phone itself. Laptops and computers can be used in the same way. The Kinect interface is the most clumsy looking (at the moment) of all the input options. If anyone has used the Kinect, they will know how slow the interactions can feel. However, a full range of gestures can be used by a presenter or even an audience member to control the main content.

 

The level of connectivity is what we all have wanted for as long as there was Science Fiction. I only wish development could go faster.

 

Cabe

http://twitter.com/Cabe_e14

 

More interaction research with Microsoft technology:

Windows 8 development

Microsoft Surface and robotics control

Holodesk, the virtual 3D desktop

The superficial human machine interface, Windows 8

Control your robot with Kinect

Robotic shopping cart, follows its user around

Control the web and Windows 7 with Kinect

Kinect and Surface, virtual physics engine

Advanced robot tech for the masses

Upgraded humanoid service robot, buy it now

Autonomous robot plays catch

Surgeons of the future might use robotic nurses