Load Google Translate Create and manage categories in Fluke. Removing a category will not remove content.
Create and manage announcements in Fluke. Try to limit the announcements to keep them useful.
| Subject | Author | Date | Actions |
|---|
Enter your announcement details below, including when you would like it to become active and expire. By default, announcements will become active immediately and expire in 7 days.
Loading...
![]() | The lightest, most rugged and easiest-to-use thermal imagers have now arrived.Perform infrared inspections faster and more efficiently with these new imagers. | |||
![]() | Fluke 700G Precision Pressure Gauge Calibrator »Introducing Fluke’s New Precision Pressure Gauge calibrators.
| |||
![]() | The new 430 Series II Three-Phase Power Quality and Energy Analyzers offer the best in power quality analysis and introduce, for the first time ever, the ability to monetarily quantify energy losses.The new Fluke 434, 435 and 437 Series II models help locate, predict, prevent, and troubleshoot power quality problems in three-phase and single-phase power distribution systems. Additionally, these models feature revolutionary power quality and energy measurement functions that help facilities reduce electrical power consumption, and improve the performance and lifespan of electro-mechanical equipment. | |||
![]() | Fluke 754/753 Documenting Process Calibrator »If you liked using the Fluke 743 or 744, you'll love our new Documenting Process Calibrators. The Fluke 753 and 754 bring you improved battery life, new DPCTrack 2™ Sample software, USB port, LCD graphical screen and much more.
*Only Fluke 754 | |||
| | TL175 TwistGuard™ Test Lead »The new Fluke TL175 TwistGuard™ Test Leads are the only test leads in the world with adjustable length test tips for use in different measurement environments.
| |||
Fluke 190 Series II Scopemeter »CAT IV, 60, 100 and 200 MHz portable oscilloscopes. For the first time, plant maintenance engineers and technicians can take a high performance two- or –four-channel scope into the harsh world of industrial electronics. The new Fluke 190 Series II scopes are the only portable oscilloscopes with independent isolated input channels, a CAT III 1000 V / CAT IV 600 V safety rating, and an IP 51 dust-proof and drip-proof rating. Safely troubleshoot three-phase systems like variable speed drives, UPS or back-up generators. Measure input, output and feedback signals simultaneously to diagnose industrial electronics. | ||||
| Jim Newell | ||
| Jim has worked for Fluke for a little over 31 years working in Manufacturing production and Quality assurance for the first 15 years. In the last 15 years he has focused on technical support as a Application Engineer for all of the Electrical Industrial products such as Handheld Oscilloscopes, Digital Mulitmeters and Power Quality Analyzers. He enjoys the challenge of helping people and the famous saying the only dumb question is the one you didn’t ask are often joked about among his customers. | ||
Process Tools Videos | |||
![]() | Fluke 719 Electric Pressure CalibratorLearn how to keep your process up and running »Product Information » | ![]() | Fluke 789 ProcessMeter™Check out this powerful tool that's a DMM and loop calibrator all in one »Product Information » |
Fluke 744 Documenting Process Calibrator-HARTLearn how to configure your HART 744 »Simple calibrating and adjusting techniques for your 744 » Product Information » | ![]() | Fluke 773 Milliamp Process Clamp MeterLearn how to troubleshoot without breaking the loop »Product Information » | |
Scopemeter VideosThe 190 Series II was built for the harsh, dirty world of industrial electronics. | |||
![]() | BrazilThis innovative sugar cane processor puts ScopeMeter to the test in a harsh, humid world.Watch now » | ![]() | BrazilTo keep the gondola in RIO running, engineers depend on the toughest scopes ever built.Watch now » |
![]() | U.S.Keithly Electronics’ stringent test standards demand an arsenal of high-performance test tools.Watch now » | ![]() | SwitzerlandHaeusler machines can bend steel 18” thick. They need an oscilloscope with as much muscle and precision.Watch now » |
|
|
Fluke Workshop Series 1 week ago | by amorse | |
|
|
Ten Things App Note.PDF 1 week ago | by amorse | |
|
|
Watch the Fluke 381 Clamp Meter in action 1 year ago | by Alistair Winning |
|
© 2009 Premier Farnell plc. All Rights Reserved
Premier Farnell plc, registered in England and Wales (no 00876412), registered office: Farnell House, Forge Lane, Leeds LS12 2NE