Skip navigation

community

0
1

 

Almost a year ago, the National Ignition Facility (The "NIF") started down the path to create a sustained fusion reaction, a cold fusion reactor. Over 200 tons of laser glass distributed across 192 lasers are used in the core. The goal is to start a fusion chain reaction in hydrogen pellet fuel. The heat produced the fusion will boil water that turns turbines.

 

The issue so far is the amount of power the lasers consume. One test fire, which was for a fraction of a second, used more power than the whole of the United States (during that fraction). According to the BBC, NIF Director Ed Moses said that other fractional tests consumed more power than the entire world combined during that time period.

 

Another issue is the amount of hydrogen fuel the reaction will need. Approximately 10 pellets per second, or over a million a day. However, 1,300 pounds of fuel could provide as much electricity as 2 million metric tons of coal.

 

Moses said we all should see major developments at NIF over the next 10 years. See more informative videos in NIF's Youtube channel.

 

Eavesdropper

0

USC fuel cell.gif

USC liberation method (via USC)

 

A problem with hydrogen for use as a fuel comes when the vehicle is in a crash. The hydrogen leaks out, and any sparks or fire will ignite the gas. Another problem is a hydrogen fire is invisible. (I toured a manufacturing facility once where they had hydrogen tanks for use in the factory. They had the "broom test" for testing if there is a hydrogen fire. People would walk down a hallway waiving brooms in front of them to see if the bristles catch fire. It is a scary thought. The same would happen with hydrogen vehicles.)

 

The use of hydrogen as a fuel is still on its way to reality. A common method of making hydrogen safe for transport is placing it into a harmless chemical. One method is a formic-acid storage. Another popular option is ammonia borane, a nitrogen-boron complex.

 

The University of Southern California (USC) has developed a way to extract hydrogen from ammonia borane. They took their research further and devised a way to extract the hydrogen at a rate that is usable as a fuel.  Unlike other boron and metal hydride hydrogen storage and release systems, the USC system is air-stable and re-usable. Read more of their findings at the Journal of the American Chemical Society.

 

You have liberated hydrogen, now you have to safe place to store it, and a great way to use it.

 

Eavesdropper

1

Mini-fission reactor

Posted by Eavesdropper Aug 31, 2011

11263nuclear.jpg

(Artist concept of the reactor. via Galaxy Wire)

 

NASA and the DOE are set to create a new type of power system for use in future space exploration. The concept is a mini-fission reactor that is 1.5 feet wide and 2.5 feet high.  "[It is] about the size of a carry on suitcase," said project leader James E. Werner at the 242nd National Meeting & Exposition of the American Chemical Society (ACS).

 

Werner continued, "The biggest difference between solar and nuclear reactors is that nuclear reactors can produce power in any environment. Fission power technology doesn't rely on sunlight, making it able to produce large, steady amounts of power at night or in harsh environments like those found on the Moon or Mars. A fission power system on the Moon could generate 40 kilowatts or more of electric power, approximately the same amount of energy needed to power eight houses on Earth."

 

No exact word was said about how the actual device operated past saying it had a power conversion system. With a device that size, and lack of water in the destined locations, a steam turbine could not be used. From what I can gather, it will use some sort of thermal heat to electricity method. A Peltier junction, for example, could do exactly what they need.

 

Space exploration is not ended like NASA's shuttle program, it is just waiting for advancements like this mini-reactor to become reality.

 

Eavesdropper

1

By adding gold nanoparticles to organic photovoltaic panels, a research team from UCLA, China, and Japan have increased the solar efficiency. By using the plasmonic effect, where the metal helps absorb more sunlight, the team pushed the overall light to energy output efficiently from 5.22 to 6.24, for a 20% increase. The construction places a gold layer between two light absorbing subcells, called a tandem polymer solar cell. Their method of layering has sidestepped all past difficulties of adding metal nanostructures into devices.

 

The success of the plasmonic effect of gold nanoparticles will lead to future development of polymer solar cells. The interlayer structure is being considered for other materials and "opening up opportunities" for higher efficiency, milt-stack, tandem solar cells. However, with gold currently at $1,800 USD per oz, the gains in efficiency may be diminished by manufacturing costs.

 

The project lead is professor Yang Yang of UCLA's Henry Samueli School of Engineering and Applied Science and director of the Nano Renewable Energy Center at UCLA's California NanoSystems Institute. The research team includes Xing Wang Zhang from the Key Lab of Semiconductor Materials Science at the Institute of Semiconductors at Beijing's Chinese Academy of Science and Ziruo Hong from the Graduate School of Science and Engineering at Japan's Yamagata University.

 

Three people, alone, changed organic solar cells forever.

 

Eavesdropper

0


Lithium titanate batteries contain a surface area at the anode of 100 square meters. Compared to the lithium ion surface area of 3 square meters, that is a sizable jump. The benefit comes in the ability to let in more charge, electron flow. five to ten times faster charging than li-on, over 25,000 cycles can be achieved with lithium-titanate. However, the rapid recharging comes at a cost, the potential battery has a low voltage, 1-2V typically. At $1.15 USD per kilo-watt hour, it is competitive with li-on`s $0.60 per. Researchers at the Oregon based EnerSol Energy Systems Solutions are banking on the battery to revolutionize the electric vehicle market and for an easy solution to alternative energy storage. At the moment, the 3 man operation seeks investors.
Yes, few people can make a big difference.
Eavesdropper

1

tatadysol.JPG

 

Rooftops globally are millions of acres of under tapped surface area prime for solar conversion. The structures are, in most cases, connected to the grid's of their respective countries, so energy distribution is built in. Many large companies are making the installation a standard for their sunniest stores. A certain new partnership seeks to make long roofing panels with integrated solar elements an option to traditional materials.

 

 

One of the world's top 10 steel manufacturers Tata Steel Corporation has partnered with a leading supplier of 3rd generation solar technology, Dyesol, in creating the world's largest dye-sensitized solar cell (DSSC)thin-film panel. The module measures over 3 meters in length and is 1 square meter in overall photovoltaic surface area. The innovative manufacturing process allows the Tata/Dyesol collaboration to print the solar cells directly to the steel. This allows for the manufacture of large volumes of cost effective cells to be made to exactly fit the shape of the structure. Tata Steel Operations Manager states that they have already "successfully produced hundreds of meters of printed steel and polymer film" used in the prototypes.

 

 

Dye-sensitized cell construction is printed in the following layers. The top layer, anode, is made of tin dioxide (SnO2:F) deposited on the back of glass. Below this is a layer of iodide electrolyte, sometime platinum, and is sealed with the next layer to prevent leaking. The next, and final, is a conducting layer of titanium dioxide (TiO2), dipped in a photosensitive dye, ruthenium-polypyridine.

 

 

The possibility for an electron to re-enter the dye after absorption is quite slow compared to the transfer from the platinum layer to the electrolyte. This differential is favorable allowing the cell to work in low light and cloudy day conditions. Even though DSSC panels have a 5%-12% efficiency rating the ability to charge for longer periods of time may make the cells more productive than their silicon counterparts (silicon cells rate at 12%-15%).

 

 

Tata/Dyesol finished the 3 year joint project in this June, 2011. 20 more people are needed for the team while they prepare for the pre-industrialization phase of the project. Like not recycling, the ease of the Tata/Dyesol panels make it almost a crime not to use rooftop solar collection. Great job Tata and Dyesol.

 

 

Eavesdropper


 

Picture via Tata/Dysol

2

Solar-Bikini.jpgsolar07.gif

 

Starting out as a joke about a beer chilling bikini, Andrew Schneider from New York University has created a solar power bikini that actually works. A melding of textile work and electrical engineering, 1" x 4" photovoltaic thin film solar cells have been sewn together with conductive thread. The power is then funneled through a 5V regulator and terminated into a standard female USB port. A thin connector bridges between the top and bottom of the suit to collect all power to one source. The overall power output is enough to charge a single MP3 player or cell phone, mostly due to the fact that overall surface area is rather skimpy. Although geared towards education, the Solar Bikini is currently being sold through the Solar Coterie website. Each one is custom, only $200 USD , so act fast.

 

Keep in mind, the number one issue with solar cells, even with thin film, is the buildup of heat in the cells themselves. Also, with the conductive thread, this suit can not get wet at all. So, no swimming or sweating allowed.

 

To actually deliver his original joke of cooling a beer, a male version of the solar suit will be made into a pair of board-shorts. The solar collector, with more surface area, will be able to charge a device as well as power a Peltier cooling device for chilling one drink.

 

Will these ever be able to enter the water? Schneider is hard are work to make it happen.

 

Eavesdropper

 

Pictures via Andrew Schneider

0

At present, both efficiency and output of solar thermal power plants are quite low and it's a big reason behind the high cost of kWh electricity produced in present day solar thermal power plants. The other reason is the high cost of maintenance of array of reflectors. But, this cost can be reduced to less than 1/3rd of the present day level. The way is using atmospheric or psychometric heat along with solar heat. The way is very very simple. First, evaporate the water with the help of a vacuum pump in such a way so that the latent heat of vaporization of water comes from the atmospheric heat and then heating the vapor produced in this manner with solar heat. It can be easily calculated that in a steam at temp 300ºC produced in the same manner as that of present day thermal and solar thermal power plants; latent heat of vaporization of water is about 2/3rd of the heat consumed by water in this process. By vacuum evaporation of water, the latent heat of vaporization of water comes from the atmosphere and heating the vapor by array of solar reflector would need 1/3rd of heat necessary before. Therefore, with just 1/3rd of the amount of solar reflecting arrays, we can get same efficiency and output. And in night too, less heat reserve will be necessary to run the power plant.

 

Vacuum evaporation of water is well tested in the experiments of open cycle OTEC. The vacuum pump in my project acts as the premium heat pump. It does so by vaporizing the water inside the Evaporator. On an experiment done by Prof. L.A.Vega, it was found that out of 1838 kW of gross output from 26.1 kg of steam, only 80 kW is spent on the compressor i.e. vacuum pump. From that experiment, it can be calculated to produce 1 kg of steam; approx. 3 kW of electricity is needed. This experiment proves that the c.o.p of the vacuum pump can be much higher; i.e. more than 22, according to the above mentioned experiment on open-cycle OTEC by Dr. Vega (resource: http://www.otecnews.org/articles/vega/07_landbased_OTEC.html). While the amount of power embedded in the 1 kg/sec vapor flow is (1000X550X4.2) W or 2.31 MW. In a conventional thermal power, all the heat necessary including the latent heat of vaporization have to be supplied by burning fossil fuel. On a steam of 300°C temp, 2/3rd of the amount of energy embedded is the latent heat of vaporization. If vapor can be produced in this way, then much less amount (in fact 1/3rd of less amount) of solar troughs will be needed to take the vapor to its desired temperature. But with that vapor, we can produce same level of electricity.

The latent heat of vaporization of water can be collected from atmosphere by means of heat conduction through the walls of the aluminum or aluminum alloy tubes attached to the Evaporator. Heat conductivity of aluminum is 2.37 W/m/ºK i.e. through an aluminum sheet of 1 sq meter and 1 mm thickness, 2.37 kW of heat would be passed with just 1ºK or 1ºC temp difference. Therefore, for conduction of 2.31 MW of heat with a 2.5ºK temp difference, just 4 sq meter of aluminum sheet is sufficient. Therefore, the cost of aluminum tubing wouldn’t be much.

The next part of the technology is almost like any other conventional solar thermal power plant electricity generation part. Therefore, there should be no difficulty in making and operating that part of this technology. Though, this technology has some little differences with conventional solar thermal power plants, but that difficulties can be overcome easily with available techniques. In short, there is no technological problem regarding the implementation of this technological idea.

 

Advantages of this technology are:-

1)      As much less solar reflectors are needed, the electricity produced by this technology will be cheaper than that produced by other solar thermal technologies available at present..

2)      As much less solar reflectors are used, therefore it takes much less area to construct in comparison to the other existing solar thermal power technology and also much less cost to operate.

3)      It can be made with present state of technology. No engineering or scientific breakthrough is needed.

4)      This technology uses the embedded heat that is stored in the lower part of the atmosphere. In effect it is a part of solar energy falling on earth. That’s why basic source of energy is unlimited and there would be less pressure on depleting reserves of fossil fuel like coal, oil, gas etc.

5)      Salt and fresh water are added bonus to this technology, if seawater is used.

6)      It can be source of low cost air conditioning for buildings of close proximity.

I am just giving here a short zest of the idea here. Anybody interested, who is willing to discuss this idea with me, can contact me at pranabjyoti_calcutta@rediffmail.com.

3

canadian-wind-farm.jpg

A Canadian Wind Farm

 

I had asked this questions before, do wind farms effect the global environment? I now have the answer.

 

Alex Kleidon of the Max Planck Institute for Biogeochemisty, Germany, theorizes that the overuse of wind/wave farms would have an impact as great as doubling the atmospheres concentration of CO2.

 

Kleidon states as we seek to replace the 17 Terawatts (TW), of the global 47 TW power consumption, of burning fossil fuels with renewable, we may end up depleting the amount of "Green Energy" the planet has to offer. It is a thermodynamic principal, as our wind farms generate electricity, it saps energy from the global system.

 

Energy from the sun hits the earth's atmosphere, and portions of it cause wind and ocean currents, evaporates water, moving condensation up into the atmosphere before it drops again. And the majority of the rest of the energy comes as heat, most of which is not harnessed. He says using wind/wave farms use a large portion of the sun's energy that reaches the earth.

 

Using models, Kleidon shows that the energy potential of wind power is reduced by a factor of 100 when wind farms are taken into account. He also shows that up to 70 TW of energy could be harvested from wind, but would destroy the natural global processes at the same time.

 

Although wind would not stop, his models have shown wind farms will effect turbulence, precipitation, and the amount of solar energy reaching the earth, over time. As Kleidon says, [as bad as] "doubling atmospheric concentrations of carbon dioxide."


 

What is a better option? More passive devices. A recent photosynthesis like breakthrough would not rob the world of kinetic energy at all. Plants have been doing it since the beginning.

 

Cabe

 

 

Read Alex Kleidon's abstract here.

3

saline_illus_news.jpg

 

Where fresh water meets saltwater there is a potential to harvest energy. Stanford University researchers have developed a device that can use this use the mixing of the two water types and pull out more energy that they put in. A container holds fresh water, with positive and negative electrodes at either end, is charged and then submerged in saltwater. The device allows the two waters to mix. Since  saltwater contains more ions of sodium and chlorine, the electrical potential between the electrodes increases.

 

Researcher Yi Cui elaborates, "The voltage really depends on the concentration of the sodium and chlorine ions you have. If you charge at low voltage in freshwater, then discharge at high voltage in sea water, that means you gain energy. You get more energy than you put in."

 

His idea is to place these devices when rivers, or other fresh water supplies, meet saltwater bodies, like the ocean. He claims that is every river mouth, estuaries, were tapped, 13% of the worlds electricity need would be met. (2 terawatts)

 

The battery could be 85% efficient, says Cui. To achieve this rating, the positive electrode is made of nanorods of manganese dioxide. This allows more surface area for the sodium ions to interact, move in and out, and speed up the process. This is not the first time electricity has been produces from the mix of saltwater and fresh water. However, this time both sodium and chlorine ions are used to generate power.

 

The next step for the team is to try this process with sewage water.

 

For the record, funding for Yi Cui's project has come from The King Abdullah University of Science and Technology (KAUST) and the U.S. Department of Energy.

 

Eavesdropper

5

Artificial-Photosynthesis-The-Latest-Way-To-Power-Your-Home.jpg

 

Sudden discoveries have lead to many different world changing technologies. For example, Penicillin came about through a cross contamination of two mold cultures in Dr. Alexander Flemings lab. X-rays were a surprise to researcher Wilhelm Conrad Roentgen for not putting a screen in front of a cathode ray tube he was studying. The list goes on and on.

 

The company SunCatalytix has made a discovery that has shown that the sun can be used to split water, and harvest the hydrogen. Researcher Daniel Nocera, from MIT, said that a jar of water could power a house. He also said that a swimming pool of water could meet the entire planet's electricity demand.

 

The idea works like photosynthesis. Sunlight gets absorbed and separates water. An artificial leaf made of Cobalt and Phosphate coated silicon is placed inside a jar of water, and the power output surpasses the best solar panel to date. It is discoveries like this that change the world. We will see more of this in the near future.

 

The Tata Group, a collection of companies that work to bring innovation to the world and the less fortunate, has partnered with SunCatalytix for an undisclosed amount. And they are receiving funding from other organizations to push the technology along.

 

See the SunCatalytix site for peer review links.

 

Eavesdropper

5

USA's largest solar farms

Posted by Eavesdropper Mar 29, 2011

CopperMountainSolar_Sempra.jpg

Copper Mountain Solar Installation via Sempra Generation

 

In Nevada, 40 miles southeast of Las Vegas, sits the United State's largest solar installation. Sempra Generation's 775,000 solar panels fill 380 acres generating 48 Mega-watts of electricity. This site is adjacent to an older 10 Mega-watt facility in El Dorado. Together, these sites will power 14,000 homes in California via Pacific Gas & Electric (PG&E) over the next 20 years.

 

MesquiteSolar.jpg

Mesquite Solar I planned location via Sempra Generation

 

Sempra Generation is not stopping here. Mesquite Solar I, a project in its first phase, is planned to eclipse the Nevada location by a factor of 12.5. 600 Mega-watts will pour from this Arlington Arizona based solar farm, powering up to 56,000 additional homes. This is a commendable effort.

 

 

Perhaps they should bring the panels to power each home directly. I decided to do a little math and figure out how much space and average price this may cost each person.

 

I will use the Kyocera KC175GT, a 175 watt solar panel.

I let it collect sunshine for 6 hours a day. Giving me a total of (175x6) 1050 watt hours. 1.05kwh

The size is 4.2 feet by 3.25 feet. Or 13.65 square feet.

An average home requires about 50kwh. (2 - 3 story home)

So I need approximately 48 panels to power the home. (50/1.05 = 47.62)

Which is a total of 655.2 square feet. And this is 1/66th of an acre.

Each panel costs $770 USD at the moment, on sale. Or $36,960 total for 48 panels.


Although that his a high price to pay to be green, I am sure Sempra Generation could provide each person with panels for far less. I hope they read this and get inspired to go individual generation someday.

 

Eavesdropper

1

pluglesspower.jpg

Evatran, USA Virginia state company, has unveiled their EV wireless charging stations. What every plug in hybrid needs, a way for the driver to not have to worry about where and how to plug in their cars. The "Plugless Power station" is a floor-mounted parking block that will automatically align itself with a an adapter mounted to the front of the EV. Through induction between the block and car mounted adapter, a charging circuit is completed. This is exactly like the Powermat or HP/Palm's Touchstone charging adapters. However, inducing current flow over such a distance come with a certain amount of loss. Currently Evatran's efficiency is at 80%, but Evatran plans to bump it up to 90% by the time production run models leave the assembly line.

 

Field testing, beta testing, has been underway since 2010. First run production models likely to ship in April 2011. The price for a unit will be $3,800 plus $500 for installation and adapter. There will be $2000 incentive in tax breaks. Can there be a price on park and forget on EVs?

 

Eavesdropper

0

uk-military-solar-uniform2011.jpg

 

A recent research project wants British soldiers to wear solar photovoltaic cells and a thermoelectric system to harness light or heat for 24/7 power. The goal is to lighten the packs soldiers carry by 50% and reduce the number of return trips to the base for recharging. An added benefit of the system is that after the various sources absorb all the energy across the electromagnetic spectrum, the soldiers will appear less obvious to infra-red surveillance equipment.

 

This project is a collaboration between the University of Glasgow and Strathclyde, Leeds, Reading, Loughborough, and Brunel Universities. Funding support is also coming from The Defense Science and Technology Laboratory (DSTL) and the Engineering and Physical Sciences Research Council (EPSRC). Many different disciplines are at work on this project, including chemists, material science, process, electrical, and design engineers. As you can see, everyone is quite serious about this endeavor.

 

Solar PV will harness light in the day, and thermoelectric devices will take over the same task at night. "Advanced" storage schemes will be used to store excess energy while still providing continuous power. Side note; the thermal harvesters should run 100% of the time. Daytime heat and the active soldier will generate much more power than in the evening, but the team will discover this soon.

 

Professor Ducan Gregory of Glasgow said they are planning to have a prototype within 2 years. He hopes the technology will filter into other categories, like medical transportation, satellites, or other space applications.

 

Good luck, see you all in 2 years.

 

Eavesdropper

1 2 3 ... 6 Previous Next