Skip navigation

community

Currently Being Moderated

Sustained fusion reaction ever closer

Posted by Eavesdropper on Sep 14, 2011 2:36:45 PM

 

Almost a year ago, the National Ignition Facility (The "NIF") started down the path to create a sustained fusion reaction, a cold fusion reactor. Over 200 tons of laser glass distributed across 192 lasers are used in the core. The goal is to start a fusion chain reaction in hydrogen pellet fuel. The heat produced the fusion will boil water that turns turbines.

 

The issue so far is the amount of power the lasers consume. One test fire, which was for a fraction of a second, used more power than the whole of the United States (during that fraction). According to the BBC, NIF Director Ed Moses said that other fractional tests consumed more power than the entire world combined during that time period.

 

Another issue is the amount of hydrogen fuel the reaction will need. Approximately 10 pellets per second, or over a million a day. However, 1,300 pounds of fuel could provide as much electricity as 2 million metric tons of coal.

 

Moses said we all should see major developments at NIF over the next 10 years. See more informative videos in NIF's Youtube channel.

 

Eavesdropper

Attributes

Comments (1)