Skip navigation

community

Alternative Energy Solutions & Technologies

13 Posts tagged with the energy_storage tag
0

USC fuel cell.gif

USC liberation method (via USC)

 

A problem with hydrogen for use as a fuel comes when the vehicle is in a crash. The hydrogen leaks out, and any sparks or fire will ignite the gas. Another problem is a hydrogen fire is invisible. (I toured a manufacturing facility once where they had hydrogen tanks for use in the factory. They had the "broom test" for testing if there is a hydrogen fire. People would walk down a hallway waiving brooms in front of them to see if the bristles catch fire. It is a scary thought. The same would happen with hydrogen vehicles.)

 

The use of hydrogen as a fuel is still on its way to reality. A common method of making hydrogen safe for transport is placing it into a harmless chemical. One method is a formic-acid storage. Another popular option is ammonia borane, a nitrogen-boron complex.

 

The University of Southern California (USC) has developed a way to extract hydrogen from ammonia borane. They took their research further and devised a way to extract the hydrogen at a rate that is usable as a fuel.  Unlike other boron and metal hydride hydrogen storage and release systems, the USC system is air-stable and re-usable. Read more of their findings at the Journal of the American Chemical Society.

 

You have liberated hydrogen, now you have to safe place to store it, and a great way to use it.

 

Eavesdropper

1

Mini-fission reactor

Posted by Eavesdropper Aug 31, 2011

11263nuclear.jpg

(Artist concept of the reactor. via Galaxy Wire)

 

NASA and the DOE are set to create a new type of power system for use in future space exploration. The concept is a mini-fission reactor that is 1.5 feet wide and 2.5 feet high.  "[It is] about the size of a carry on suitcase," said project leader James E. Werner at the 242nd National Meeting & Exposition of the American Chemical Society (ACS).

 

Werner continued, "The biggest difference between solar and nuclear reactors is that nuclear reactors can produce power in any environment. Fission power technology doesn't rely on sunlight, making it able to produce large, steady amounts of power at night or in harsh environments like those found on the Moon or Mars. A fission power system on the Moon could generate 40 kilowatts or more of electric power, approximately the same amount of energy needed to power eight houses on Earth."

 

No exact word was said about how the actual device operated past saying it had a power conversion system. With a device that size, and lack of water in the destined locations, a steam turbine could not be used. From what I can gather, it will use some sort of thermal heat to electricity method. A Peltier junction, for example, could do exactly what they need.

 

Space exploration is not ended like NASA's shuttle program, it is just waiting for advancements like this mini-reactor to become reality.

 

Eavesdropper

5

Artificial-Photosynthesis-The-Latest-Way-To-Power-Your-Home.jpg

 

Sudden discoveries have lead to many different world changing technologies. For example, Penicillin came about through a cross contamination of two mold cultures in Dr. Alexander Flemings lab. X-rays were a surprise to researcher Wilhelm Conrad Roentgen for not putting a screen in front of a cathode ray tube he was studying. The list goes on and on.

 

The company SunCatalytix has made a discovery that has shown that the sun can be used to split water, and harvest the hydrogen. Researcher Daniel Nocera, from MIT, said that a jar of water could power a house. He also said that a swimming pool of water could meet the entire planet's electricity demand.

 

The idea works like photosynthesis. Sunlight gets absorbed and separates water. An artificial leaf made of Cobalt and Phosphate coated silicon is placed inside a jar of water, and the power output surpasses the best solar panel to date. It is discoveries like this that change the world. We will see more of this in the near future.

 

The Tata Group, a collection of companies that work to bring innovation to the world and the less fortunate, has partnered with SunCatalytix for an undisclosed amount. And they are receiving funding from other organizations to push the technology along.

 

See the SunCatalytix site for peer review links.

 

Eavesdropper

0

uk-military-solar-uniform2011.jpg

 

A recent research project wants British soldiers to wear solar photovoltaic cells and a thermoelectric system to harness light or heat for 24/7 power. The goal is to lighten the packs soldiers carry by 50% and reduce the number of return trips to the base for recharging. An added benefit of the system is that after the various sources absorb all the energy across the electromagnetic spectrum, the soldiers will appear less obvious to infra-red surveillance equipment.

 

This project is a collaboration between the University of Glasgow and Strathclyde, Leeds, Reading, Loughborough, and Brunel Universities. Funding support is also coming from The Defense Science and Technology Laboratory (DSTL) and the Engineering and Physical Sciences Research Council (EPSRC). Many different disciplines are at work on this project, including chemists, material science, process, electrical, and design engineers. As you can see, everyone is quite serious about this endeavor.

 

Solar PV will harness light in the day, and thermoelectric devices will take over the same task at night. "Advanced" storage schemes will be used to store excess energy while still providing continuous power. Side note; the thermal harvesters should run 100% of the time. Daytime heat and the active soldier will generate much more power than in the evening, but the team will discover this soon.

 

Professor Ducan Gregory of Glasgow said they are planning to have a prototype within 2 years. He hopes the technology will filter into other categories, like medical transportation, satellites, or other space applications.

 

Good luck, see you all in 2 years.

 

Eavesdropper

0

DIY Wind Turbine, 200W

Posted by Eavesdropper Mar 23, 2011

turbine-autumn02.jpg

 

Applied Sciences is a group that has done a hand full of projects ranging widely, from making a top hat to a game console dance pad. Their latest project is a home build (DIY) wind turbine. The best part, the project is open source.

 

Called the Zoetrope, it functions as a vertical-axis wind turbine. Built from parts easily bought from hardware and home improvement stores, the turbine is able to produce up to 200W. In the Applied Science's guide for building this turbine, the energy generation comes from a self build alternator. Detailed descriptions on how to build a custom Stator in conjunction with the magnetic rotor. Some approximations are made in the number of turns and output voltage. EX: 320 turns 24 ga. ~= 100V @ 120RPM.

 

stator.JPG

 

Originally the Zoetrope was designed to run to supplement a water heater system. A high voltage is produced that the heating element could use. The Zoetrope outputs 3-phase AC which then needs to be converted to DC, which could power devices or charge batteries, or converted back into usable, single phase for example, AC.

 

Attached to this post in the design guide.

 

Some suggested improvements:

1. Make it safe to touch.

2. Enclose the alternator area.

3. Double the size of everything.

 

Great job Applied Sciences. I may just build one myself.

 

Eavesdropper

 

Zoetrope fun fact: The name of the turbine comes from an early

animation device that used a rotating cylinder with

slits in the side to give the illusion of moving

pictures. At certain speeds, the wind turbine gives

a similar effect.

0

GA.gif

 

I am conflicted. I want this to the future, and I also do not.


 

Ohio University's Geradine Botte, has demonstrated that "the most abundant waste on earth" can produce hydrogen with less than half the energy need with water. “During the electrochemical process the urea gets adsorbed on to the nickel electrod= surface, which passes the electrons needed to break up the molecule,” said Botte. The breakthrough comes in urine's constituent "urea." In which 4 loosely bonded hydrogen atoms are present per molecule. The required energy to break the molecule of Urea is 0.37V, while water needs 1.23V to split.


 

Botte wants to upscale the idea to be used in treating waste water. I wonder if Newcastle University included this sizeable volume of waste water in their calculations.


 

See more at the Royal Society of Chemistry journal Chemical Communications.


 

Eavesdropper

 

 

image via RSC Publishing

0

solarfpl.jpg

At the Florida Power & Light Co., 190,000 mirrors are used to concentrate the suns energy to heat synthetic oil to ~750 degrees. The oil is then used to boil water, creating steam to turn turbines. The $400 million dollar plant can generate 75 megawatts on peak days. This powers 11,000 homes. The plant in Indiantown, Florida, is the world first to combine solar thermal energy harvesting to a combined-cycle natural gas power station. The construction came in $75 million dollars under budget. The plant is not as ideal as it may sound. The plant needs 500 acres of land. Solar based systems always take up more land that its competitors. Despite being in the hurricane ally of the Gulf of Mexico, FPL claims their plant was tested and can withstand up to 130mph winds.


 

The team at Florida Power & Light Co. wants to build an additional 300 - 500 megawatt solar installation. Vice president of FPL, Eric Silagy said, "We believe that solar is a great addition to the fleet at FPL. We are the Sunshine State. We have proven that it works very well." That is an additional 73,000 homes powered. Still far shy of the 4.5 million customers FPL had, but it is a major step in the right direction.


 

Eavesdropper

0

GSR-110B-portable-retractable-solar-panel-1.jpg

 

From OS, Japan, comes a portable solar panel (GSR110B) using Fugi Electric Systems' flexible thin film solar technology. The system weighs approximately 3kg and is capable of generating 40W at 12V. Lithium-ion batteries store energy not being used, or to be charged before deploying. The most interesting feature is the ability to pair two together to produce 80W collectively. Although this is the cap, I ask why not combine more together for even higher wattage? OS's target for The GRS110B was be deployed as emergency power for communication equipment.  Of course, it can be used for anything else. These have been selling since January 2011 for 60,000 yen, or approximately $700 USD. A bit high, but can you put a price on 40W in a disaster?

 

Eavesdropper

0

100924121218.jpg

Developed originally at North Carolina State University, the Artificial Leaf uses a water-gel infused with plant chlorophyll to generate electricity when stimulated by light, similar to the way real plants generate sugars from light. With electrodes coated with carbon materials, a high efficiency and inexpensive solar panels can be produced. NC State's Dr. Orlin Velev says, "we believe that the concept of biologically inspired 'soft' devices for generating electricity may in the future provide an alternative for the present-day solid-state technologies."


NTU-researchers-asia-lab-300x200.jpg

Inspired by this technology, Nanyang Technological University has set up laboratories to convert water to hydrogen fuel. NTU President Bertil Andersson will use Artificial Leaf tech to use solar energy to separate oxygen and hydrogen. He claims that conventional methods to do the same thing require large amounts of energy to convert. With the greater efficiencies of the Artificial Leaf, this is proving to be the cheapest method for creation of the fuel. In other words, using free energy to create expensive fuel. NTU is hoping to fuel hydrogen-powered vehicles in 3 to 5 years from now.


 

Eavesdropper

0

 

“By taking-up this journey, I want to raise awareness about disability and tell people that we, despite our disability can achieve anything as an individual, if we are determined to try and have courage to do so," Said Haidar Taleb, as he attempts to beat his own world record of traveling 200 miles in a solar powered wheelchair. Taleb has had polio since the age of 4, but now wants to spread awareness to other people with disabilities that "there are no obstacles." Teamed up with Masdar, an alternative energy company, Taleb has shown that eco friendly solar powered wheelchairs are important and that "they can change the lives of persons with mobility problems." The chair can move at a constant 12mph. Taleb is set to break his previous 14-hour long 80 mile wheelchair trip. Good luck Haidar Taleb!

 

Eavesdropper

 

See E14's Technology for the Disabled group for other such technology.

0

e7c31e608543067b10ce4a2f8dd5f79f.jpg

 

Professor Zei Zhai and postdoctoral Jianhua Zou from the University of Central Floridahave taken carbon nanotubes forward a notch. Using nanotubes similar to the form of aerogel, aka "frozen smoke" The team has developed what they are boasting as a good way to detect pollution, toxins, improve robotic surgery, and to store energy. Zhai and Zou worked with Professors Saiful Knondaker, Quanfang Chen, and Sudipta Seal from UCF to make the multiwalled carbon nanotube (MWCNT) aerogel structure. The result was the construction of large surface area within the structure, and the material conducts electricity well, and is a thermal insulator. Applications could include measuring changes in pressure or other electrical properties. And the increased surface area could allow for increased capacity in supercapacitors and batteries. More here.

 

The biggest hold up of wide adoption of carbon nanotubes is the cost. The base form is still at $45-150/kg. Like everything, it will come down in price eventually.


Eavedropper

0

c0ee00640h-325-FOR-TRIDION_tcm18-198798.jpg

 

Korea Advanced Institute of Science and Technology has created a flexible battery based on grapheme that has very high potential. The cathode was “grown” onto a sheet of grapheme using pulsed laser reposition, material composition of V2O5.  The anode is lithium coated graphene. Lead developer Kisuk Kang said, “The electrode exhibits significantly improved electrochemical performance in almost all aspects of electrochemical properties, such as higher energy density, power density and better cycle life, compared with non-flexible conventional electrodes.”


 

The tech promises greater energy density and longer life performance. The target application is for flexible devices such as clothing, bendable displays and e-readers. More info at the abstract page.


 

Eavesdropper

0

mg20928014.800-1_300.jpg


Energy storage is a major issue when dealing with intermittent alternative energy such as wind or solar. With standard energy generation storage of energy is simple, let it sit in its raw form. Coal, oil, wood in its basic form is energy ready to burn. With a renewable source, energy has to be stored elsewhere. A tried and true way to store energy is via pumped-storage hydroelectricity. This works by pumping water to a high elevation. On demand the water can then be dropped through turbines, providing up to 85% efficiency. There is one major caveat, the location of the storage facility has to provide an elevation difference as well as a large area to hold water. This is not a convenient way to store other forms of renewable energy.

 

There are a few other options for storing energy from renewable sources. Batteries are simple method, but have proven to be quite expensive. Utsira, off the coast of Norway, use excess energy to separate hydrogen and oxygen to be stored in fuel cells. Precious metals in fuel cells make this option less attractive for most generation plants. Compressed air energy storage (CAES) uses energy generated to compress air placed in large storage tanks. CAES has been used in Huntorf Germany since 1978 and McIntosh Alabama from 1991. The size of these containers can be quite cumbersome and expensive to keep pressurized.

 

Now enters a new option. In Slough, UK, energy firm Scottish and Southern, at the Highview Power Storage facility, is storing energy from a 100-megawatt biomass plant in the form of liquid air, or cryogen. The generated energy from the plant is used to chill air to -190 °C and stored in a tank at regular atmospheric pressure, 1 bar. Then the energy is needed, the cryogen is pressurized to 70 bars and heated. The result is a high pressure gas used to spin turbines. On average the efficiency is 50%, but with using waste heat from another source efficiency goes up to 70%. This system is small enough to be placed anywhere, and the cost beats any other storage option.

 

A new liquefaction plant will be build on site, at Highview, in late march to produce its own cryogen. A large scale 2.5-megawatt station will be constructed by late 2012, and a 10-megawatt by 2014.

 

Eavesdropper

 

Pic via Jez Coulson at the Highview plant