Skip navigation

community

1 2 Previous Next

Alternative Energy Solutions & Technologies

16 Posts tagged with the on_campus tag
0

USC fuel cell.gif

USC liberation method (via USC)

 

A problem with hydrogen for use as a fuel comes when the vehicle is in a crash. The hydrogen leaks out, and any sparks or fire will ignite the gas. Another problem is a hydrogen fire is invisible. (I toured a manufacturing facility once where they had hydrogen tanks for use in the factory. They had the "broom test" for testing if there is a hydrogen fire. People would walk down a hallway waiving brooms in front of them to see if the bristles catch fire. It is a scary thought. The same would happen with hydrogen vehicles.)

 

The use of hydrogen as a fuel is still on its way to reality. A common method of making hydrogen safe for transport is placing it into a harmless chemical. One method is a formic-acid storage. Another popular option is ammonia borane, a nitrogen-boron complex.

 

The University of Southern California (USC) has developed a way to extract hydrogen from ammonia borane. They took their research further and devised a way to extract the hydrogen at a rate that is usable as a fuel.  Unlike other boron and metal hydride hydrogen storage and release systems, the USC system is air-stable and re-usable. Read more of their findings at the Journal of the American Chemical Society.

 

You have liberated hydrogen, now you have to safe place to store it, and a great way to use it.

 

Eavesdropper

1

By adding gold nanoparticles to organic photovoltaic panels, a research team from UCLA, China, and Japan have increased the solar efficiency. By using the plasmonic effect, where the metal helps absorb more sunlight, the team pushed the overall light to energy output efficiently from 5.22 to 6.24, for a 20% increase. The construction places a gold layer between two light absorbing subcells, called a tandem polymer solar cell. Their method of layering has sidestepped all past difficulties of adding metal nanostructures into devices.

 

The success of the plasmonic effect of gold nanoparticles will lead to future development of polymer solar cells. The interlayer structure is being considered for other materials and "opening up opportunities" for higher efficiency, milt-stack, tandem solar cells. However, with gold currently at $1,800 USD per oz, the gains in efficiency may be diminished by manufacturing costs.

 

The project lead is professor Yang Yang of UCLA's Henry Samueli School of Engineering and Applied Science and director of the Nano Renewable Energy Center at UCLA's California NanoSystems Institute. The research team includes Xing Wang Zhang from the Key Lab of Semiconductor Materials Science at the Institute of Semiconductors at Beijing's Chinese Academy of Science and Ziruo Hong from the Graduate School of Science and Engineering at Japan's Yamagata University.

 

Three people, alone, changed organic solar cells forever.

 

Eavesdropper

2

Solar-Bikini.jpgsolar07.gif

 

Starting out as a joke about a beer chilling bikini, Andrew Schneider from New York University has created a solar power bikini that actually works. A melding of textile work and electrical engineering, 1" x 4" photovoltaic thin film solar cells have been sewn together with conductive thread. The power is then funneled through a 5V regulator and terminated into a standard female USB port. A thin connector bridges between the top and bottom of the suit to collect all power to one source. The overall power output is enough to charge a single MP3 player or cell phone, mostly due to the fact that overall surface area is rather skimpy. Although geared towards education, the Solar Bikini is currently being sold through the Solar Coterie website. Each one is custom, only $200 USD , so act fast.

 

Keep in mind, the number one issue with solar cells, even with thin film, is the buildup of heat in the cells themselves. Also, with the conductive thread, this suit can not get wet at all. So, no swimming or sweating allowed.

 

To actually deliver his original joke of cooling a beer, a male version of the solar suit will be made into a pair of board-shorts. The solar collector, with more surface area, will be able to charge a device as well as power a Peltier cooling device for chilling one drink.

 

Will these ever be able to enter the water? Schneider is hard are work to make it happen.

 

Eavesdropper

 

Pictures via Andrew Schneider

3

canadian-wind-farm.jpg

A Canadian Wind Farm

 

I had asked this questions before, do wind farms effect the global environment? I now have the answer.

 

Alex Kleidon of the Max Planck Institute for Biogeochemisty, Germany, theorizes that the overuse of wind/wave farms would have an impact as great as doubling the atmospheres concentration of CO2.

 

Kleidon states as we seek to replace the 17 Terawatts (TW), of the global 47 TW power consumption, of burning fossil fuels with renewable, we may end up depleting the amount of "Green Energy" the planet has to offer. It is a thermodynamic principal, as our wind farms generate electricity, it saps energy from the global system.

 

Energy from the sun hits the earth's atmosphere, and portions of it cause wind and ocean currents, evaporates water, moving condensation up into the atmosphere before it drops again. And the majority of the rest of the energy comes as heat, most of which is not harnessed. He says using wind/wave farms use a large portion of the sun's energy that reaches the earth.

 

Using models, Kleidon shows that the energy potential of wind power is reduced by a factor of 100 when wind farms are taken into account. He also shows that up to 70 TW of energy could be harvested from wind, but would destroy the natural global processes at the same time.

 

Although wind would not stop, his models have shown wind farms will effect turbulence, precipitation, and the amount of solar energy reaching the earth, over time. As Kleidon says, [as bad as] "doubling atmospheric concentrations of carbon dioxide."


 

What is a better option? More passive devices. A recent photosynthesis like breakthrough would not rob the world of kinetic energy at all. Plants have been doing it since the beginning.

 

Cabe

 

 

Read Alex Kleidon's abstract here.

3

saline_illus_news.jpg

 

Where fresh water meets saltwater there is a potential to harvest energy. Stanford University researchers have developed a device that can use this use the mixing of the two water types and pull out more energy that they put in. A container holds fresh water, with positive and negative electrodes at either end, is charged and then submerged in saltwater. The device allows the two waters to mix. Since  saltwater contains more ions of sodium and chlorine, the electrical potential between the electrodes increases.

 

Researcher Yi Cui elaborates, "The voltage really depends on the concentration of the sodium and chlorine ions you have. If you charge at low voltage in freshwater, then discharge at high voltage in sea water, that means you gain energy. You get more energy than you put in."

 

His idea is to place these devices when rivers, or other fresh water supplies, meet saltwater bodies, like the ocean. He claims that is every river mouth, estuaries, were tapped, 13% of the worlds electricity need would be met. (2 terawatts)

 

The battery could be 85% efficient, says Cui. To achieve this rating, the positive electrode is made of nanorods of manganese dioxide. This allows more surface area for the sodium ions to interact, move in and out, and speed up the process. This is not the first time electricity has been produces from the mix of saltwater and fresh water. However, this time both sodium and chlorine ions are used to generate power.

 

The next step for the team is to try this process with sewage water.

 

For the record, funding for Yi Cui's project has come from The King Abdullah University of Science and Technology (KAUST) and the U.S. Department of Energy.

 

Eavesdropper

5

Artificial-Photosynthesis-The-Latest-Way-To-Power-Your-Home.jpg

 

Sudden discoveries have lead to many different world changing technologies. For example, Penicillin came about through a cross contamination of two mold cultures in Dr. Alexander Flemings lab. X-rays were a surprise to researcher Wilhelm Conrad Roentgen for not putting a screen in front of a cathode ray tube he was studying. The list goes on and on.

 

The company SunCatalytix has made a discovery that has shown that the sun can be used to split water, and harvest the hydrogen. Researcher Daniel Nocera, from MIT, said that a jar of water could power a house. He also said that a swimming pool of water could meet the entire planet's electricity demand.

 

The idea works like photosynthesis. Sunlight gets absorbed and separates water. An artificial leaf made of Cobalt and Phosphate coated silicon is placed inside a jar of water, and the power output surpasses the best solar panel to date. It is discoveries like this that change the world. We will see more of this in the near future.

 

The Tata Group, a collection of companies that work to bring innovation to the world and the less fortunate, has partnered with SunCatalytix for an undisclosed amount. And they are receiving funding from other organizations to push the technology along.

 

See the SunCatalytix site for peer review links.

 

Eavesdropper

0

uk-military-solar-uniform2011.jpg

 

A recent research project wants British soldiers to wear solar photovoltaic cells and a thermoelectric system to harness light or heat for 24/7 power. The goal is to lighten the packs soldiers carry by 50% and reduce the number of return trips to the base for recharging. An added benefit of the system is that after the various sources absorb all the energy across the electromagnetic spectrum, the soldiers will appear less obvious to infra-red surveillance equipment.

 

This project is a collaboration between the University of Glasgow and Strathclyde, Leeds, Reading, Loughborough, and Brunel Universities. Funding support is also coming from The Defense Science and Technology Laboratory (DSTL) and the Engineering and Physical Sciences Research Council (EPSRC). Many different disciplines are at work on this project, including chemists, material science, process, electrical, and design engineers. As you can see, everyone is quite serious about this endeavor.

 

Solar PV will harness light in the day, and thermoelectric devices will take over the same task at night. "Advanced" storage schemes will be used to store excess energy while still providing continuous power. Side note; the thermal harvesters should run 100% of the time. Daytime heat and the active soldier will generate much more power than in the evening, but the team will discover this soon.

 

Professor Ducan Gregory of Glasgow said they are planning to have a prototype within 2 years. He hopes the technology will filter into other categories, like medical transportation, satellites, or other space applications.

 

Good luck, see you all in 2 years.

 

Eavesdropper

0

30580_web.jpg

Xindi Yu, Professor Paul V. Braun and Huigang Zhang, University of Illinois at Urbana-Champaign

 

A step toward phones and laptops charging in seconds has been announced by the University of Illinois at Urbana-Champaign. Professor Paul Braun and his team at UIUC have created batteries that charge quick and retain a high energy density. Li-ion and NiMH, when rapidly charged, degrades the energy storage significantly over time. With Braun's battery, this is no longer an issue. The team have taken thin-film active material, like found in lithium-ion batteries, and wrap it into a three dimensional shape, which achieve high attractive volume and high current capabilities. Demonstrations in their lab have shown charge times in seconds. "10 to 100 times faster" than normal bulk electrodes, but perform exactly the same in existing devices.

 

 

The 3-D nano-structure of Braun's battery in self-assembling. Creating the material goes as such, a surface is coated with "tiny spheres" (Styrofoam) tightly packed to form a lattice. The space in between the spheres are filled with metal, then the spheres are melted (dissolved) to form a porous 3-D scaffold. Electropolishing uniformly etches the surface of the material, enlarging the pores, and making an open framework. Finally the frame is coated with a thin film active material. The result is a "bicontinuous electrode surface with small interconnects where lithium ions can move rapidly. The active material make the diffusion kinetics rapid. The metal framework makes for good conductivity.

 

 

Everyone would cheer if our gadgets charge in seconds using this battery form. But Braun has his eyes on automotive uses. Braun said, "If you had the ability to charge rapidly, instead of taking hours to charge the vehicle you could potentially have vehicles that would charge in similar times as needed to refuel a car with gasoline. If you had five-minute charge capability, you would think of this the same way you do an internal combustion engine. You would just pull up to a charging station and fill up." He is correct, the electric car would completely take over if the charge time was under 10 minutes.

 

 

Braun goes on, " We like that it's very universal, so if someone comes up with a better battery chemistry, this concept applies. This is not linked to one very specific kind of battery, but rather it's a new paradigm in thinking about a battery in three dimensions for enhancing properties."

 

 

Eavesdropper

 

pic L. Brian Stauffer, UIUC

0

GA.gif

 

I am conflicted. I want this to the future, and I also do not.


 

Ohio University's Geradine Botte, has demonstrated that "the most abundant waste on earth" can produce hydrogen with less than half the energy need with water. “During the electrochemical process the urea gets adsorbed on to the nickel electrod= surface, which passes the electrons needed to break up the molecule,” said Botte. The breakthrough comes in urine's constituent "urea." In which 4 loosely bonded hydrogen atoms are present per molecule. The required energy to break the molecule of Urea is 0.37V, while water needs 1.23V to split.


 

Botte wants to upscale the idea to be used in treating waste water. I wonder if Newcastle University included this sizeable volume of waste water in their calculations.


 

See more at the Royal Society of Chemistry journal Chemical Communications.


 

Eavesdropper

 

 

image via RSC Publishing

0

bioreactor.jpg

A brewery million gallon waste bioreactor

 

Among the waste water being turned into biofuels, Anheuser-Busch's beer facility has a sludge that looks quite potential to researchers. Cornell University's Largus T. Angenent and Jeffery J. Werner took samples at the InBev location around the USA to get a glimpse at the bacterial communities in the factory's bioreactors. From 9 locations they found thousands of species of bacteria.


 

Using genome analyzing software, the team took a look at 400,00 gene sequences of the microbes. 145 types were unique to each of the 9 facilities. "The cool thing we found was that if you're looking at these thousands of species of bacteria, it's a very dynamic system with things dying off and replacing them," Werner said. "There are certain signature populations that are resilient. Even if they get disturbed, they come right back up." In the million gallon tanks, the team plans to alter the environment to make the bacteria perform new functions.


 

One member of these bacterial communities currently produce high amounts of methane. Anheuser-Busch harness this byproduct to offset their heating bill by 20%, saving the company millions a year. However, the team wants to prevent the bacteria from producing methane, and make the colonies product carboxylates, a key component in alkanes of fuel. The hope is the biofuels produced will outstrip the energy potential of the methane produced. If it is accomplished, the thousands of distilleries globally may be large part of the emerging biofuel markets.


 

The Cornell team is also working with the University of Colorado in Boulder and Washington University in St. Louis. See more in the abstract.


 

Eavesdropper

 

2

hdr_wastewater.jpg

wastewater facility

 

Newcastle University in the U.K. is making new with their latest claim. The “United States flushes 12.5 Trillion gallons of energy down the drain.” They are referring to biofuels in sewage. Newcastle’s Elizabeth S. Heidrich says, “Instead of just processing and dumping this water, we suggest that in the future treatment facilities could convert its organic molecules into fuels, transforming their work from an energy drain to an energy source. Based on our research, we estimate that one gallon of wastewater contains enough energy to power a 100-watt light bulb for five minutes.” A quick internet search offers up thousands of "make your own biofuels at home" links. There are many vehicles that can run on the biofuel, biodiesel. With an ample source of sewage everywhere, biofuels is an option worth exploring. Thanks Newcastle.

 

algae-apium.jpg

micro-algae

 

One method of using wastewater to generate a biofuel from waste water is from algae. Researchers at the Rochester Institute of Technology, for example, use microalgae as a "renewable feedstock" in the process of making biodiesel. As the algae absorbs some of the wastewater elements they produce a tiny bit of biodiesel. One of the researchers, Jeff Lodge, explains further, " Algae will take out all the ammonia—99 percent—88 percent of the nitrate and 99 percent of the phosphate from the wastewater — all those nutrients you worry about dumping into the receiving water. In three to five days, pathogens are gone... We can start a new batch of algae about every seven days. It’s a more continuous source that could offset 50 percent of our total gas use for equipment that uses diesel." The team eventually extracts the lipids from the single cell algae Scenedesmus to make the biodiesel. Currently the team is only producing 100 gallons at a time, but hope to expand to 1000 by spring. Apply this  technique to trillions of gallons, and offseting fuel shortages it will. Good luck R.I.T.

 

Eavesdropper

0

100924121218.jpg

Developed originally at North Carolina State University, the Artificial Leaf uses a water-gel infused with plant chlorophyll to generate electricity when stimulated by light, similar to the way real plants generate sugars from light. With electrodes coated with carbon materials, a high efficiency and inexpensive solar panels can be produced. NC State's Dr. Orlin Velev says, "we believe that the concept of biologically inspired 'soft' devices for generating electricity may in the future provide an alternative for the present-day solid-state technologies."


NTU-researchers-asia-lab-300x200.jpg

Inspired by this technology, Nanyang Technological University has set up laboratories to convert water to hydrogen fuel. NTU President Bertil Andersson will use Artificial Leaf tech to use solar energy to separate oxygen and hydrogen. He claims that conventional methods to do the same thing require large amounts of energy to convert. With the greater efficiencies of the Artificial Leaf, this is proving to be the cheapest method for creation of the fuel. In other words, using free energy to create expensive fuel. NTU is hoping to fuel hydrogen-powered vehicles in 3 to 5 years from now.


 

Eavesdropper

0

e7c31e608543067b10ce4a2f8dd5f79f.jpg

 

Professor Zei Zhai and postdoctoral Jianhua Zou from the University of Central Floridahave taken carbon nanotubes forward a notch. Using nanotubes similar to the form of aerogel, aka "frozen smoke" The team has developed what they are boasting as a good way to detect pollution, toxins, improve robotic surgery, and to store energy. Zhai and Zou worked with Professors Saiful Knondaker, Quanfang Chen, and Sudipta Seal from UCF to make the multiwalled carbon nanotube (MWCNT) aerogel structure. The result was the construction of large surface area within the structure, and the material conducts electricity well, and is a thermal insulator. Applications could include measuring changes in pressure or other electrical properties. And the increased surface area could allow for increased capacity in supercapacitors and batteries. More here.

 

The biggest hold up of wide adoption of carbon nanotubes is the cost. The base form is still at $45-150/kg. Like everything, it will come down in price eventually.


Eavedropper

0

c0ee00640h-325-FOR-TRIDION_tcm18-198798.jpg

 

Korea Advanced Institute of Science and Technology has created a flexible battery based on grapheme that has very high potential. The cathode was “grown” onto a sheet of grapheme using pulsed laser reposition, material composition of V2O5.  The anode is lithium coated graphene. Lead developer Kisuk Kang said, “The electrode exhibits significantly improved electrochemical performance in almost all aspects of electrochemical properties, such as higher energy density, power density and better cycle life, compared with non-flexible conventional electrodes.”


 

The tech promises greater energy density and longer life performance. The target application is for flexible devices such as clothing, bendable displays and e-readers. More info at the abstract page.


 

Eavesdropper

2

ja-2010-10522x_0009.gif

advancedlithiumionbattery.jpg

Images of the cathode and anode

 

University of Rome Sapienza (Italy) and Hanyang University (South Korea) have teamed together to research new advancements in Lithium-Ion batteries. They have increased the battery performance from 120-150Wh/kg to 170Wh/kg(at 4.2V). This was done through a new combination of materials in the battery. The anode is made of tin-carbon and the cathode is made from lithium manganese oxide doped with cobalt and nickel. Through lab studies the combination was able to reach 100% charge-discharge efficiency. Team researchers Jusef Hassoun, ki-Soo Lee, Yang-Kook Sun, and Bruno Scrosati believe this new chemistry is best suited for electric vehicles due to the higher energy density.

 


Scrosati elaborated, "The battery has a high volumetric and gravimetric energy density, a high rate capability due to the nano-structured characteristics of the electrode materials, an excellent cycle life, and low cost due to the use of electrode materials based on abundant elements." Read the report after the link.


 

Eavesdropper


 

Image via Jusef Hassoun, et al. ©2011 American Chemical Society

1 2 Previous Next