Skip navigation

community

1 2 Previous Next

Alternative Energy Solutions & Technologies

16 Posts tagged with the solar_panel tag
1

By adding gold nanoparticles to organic photovoltaic panels, a research team from UCLA, China, and Japan have increased the solar efficiency. By using the plasmonic effect, where the metal helps absorb more sunlight, the team pushed the overall light to energy output efficiently from 5.22 to 6.24, for a 20% increase. The construction places a gold layer between two light absorbing subcells, called a tandem polymer solar cell. Their method of layering has sidestepped all past difficulties of adding metal nanostructures into devices.

 

The success of the plasmonic effect of gold nanoparticles will lead to future development of polymer solar cells. The interlayer structure is being considered for other materials and "opening up opportunities" for higher efficiency, milt-stack, tandem solar cells. However, with gold currently at $1,800 USD per oz, the gains in efficiency may be diminished by manufacturing costs.

 

The project lead is professor Yang Yang of UCLA's Henry Samueli School of Engineering and Applied Science and director of the Nano Renewable Energy Center at UCLA's California NanoSystems Institute. The research team includes Xing Wang Zhang from the Key Lab of Semiconductor Materials Science at the Institute of Semiconductors at Beijing's Chinese Academy of Science and Ziruo Hong from the Graduate School of Science and Engineering at Japan's Yamagata University.

 

Three people, alone, changed organic solar cells forever.

 

Eavesdropper

1

tatadysol.JPG

 

Rooftops globally are millions of acres of under tapped surface area prime for solar conversion. The structures are, in most cases, connected to the grid's of their respective countries, so energy distribution is built in. Many large companies are making the installation a standard for their sunniest stores. A certain new partnership seeks to make long roofing panels with integrated solar elements an option to traditional materials.

 

 

One of the world's top 10 steel manufacturers Tata Steel Corporation has partnered with a leading supplier of 3rd generation solar technology, Dyesol, in creating the world's largest dye-sensitized solar cell (DSSC)thin-film panel. The module measures over 3 meters in length and is 1 square meter in overall photovoltaic surface area. The innovative manufacturing process allows the Tata/Dyesol collaboration to print the solar cells directly to the steel. This allows for the manufacture of large volumes of cost effective cells to be made to exactly fit the shape of the structure. Tata Steel Operations Manager states that they have already "successfully produced hundreds of meters of printed steel and polymer film" used in the prototypes.

 

 

Dye-sensitized cell construction is printed in the following layers. The top layer, anode, is made of tin dioxide (SnO2:F) deposited on the back of glass. Below this is a layer of iodide electrolyte, sometime platinum, and is sealed with the next layer to prevent leaking. The next, and final, is a conducting layer of titanium dioxide (TiO2), dipped in a photosensitive dye, ruthenium-polypyridine.

 

 

The possibility for an electron to re-enter the dye after absorption is quite slow compared to the transfer from the platinum layer to the electrolyte. This differential is favorable allowing the cell to work in low light and cloudy day conditions. Even though DSSC panels have a 5%-12% efficiency rating the ability to charge for longer periods of time may make the cells more productive than their silicon counterparts (silicon cells rate at 12%-15%).

 

 

Tata/Dyesol finished the 3 year joint project in this June, 2011. 20 more people are needed for the team while they prepare for the pre-industrialization phase of the project. Like not recycling, the ease of the Tata/Dyesol panels make it almost a crime not to use rooftop solar collection. Great job Tata and Dyesol.

 

 

Eavesdropper


 

Picture via Tata/Dysol

2

Solar-Bikini.jpgsolar07.gif

 

Starting out as a joke about a beer chilling bikini, Andrew Schneider from New York University has created a solar power bikini that actually works. A melding of textile work and electrical engineering, 1" x 4" photovoltaic thin film solar cells have been sewn together with conductive thread. The power is then funneled through a 5V regulator and terminated into a standard female USB port. A thin connector bridges between the top and bottom of the suit to collect all power to one source. The overall power output is enough to charge a single MP3 player or cell phone, mostly due to the fact that overall surface area is rather skimpy. Although geared towards education, the Solar Bikini is currently being sold through the Solar Coterie website. Each one is custom, only $200 USD , so act fast.

 

Keep in mind, the number one issue with solar cells, even with thin film, is the buildup of heat in the cells themselves. Also, with the conductive thread, this suit can not get wet at all. So, no swimming or sweating allowed.

 

To actually deliver his original joke of cooling a beer, a male version of the solar suit will be made into a pair of board-shorts. The solar collector, with more surface area, will be able to charge a device as well as power a Peltier cooling device for chilling one drink.

 

Will these ever be able to enter the water? Schneider is hard are work to make it happen.

 

Eavesdropper

 

Pictures via Andrew Schneider

5

USA's largest solar farms

Posted by Eavesdropper Mar 29, 2011

CopperMountainSolar_Sempra.jpg

Copper Mountain Solar Installation via Sempra Generation

 

In Nevada, 40 miles southeast of Las Vegas, sits the United State's largest solar installation. Sempra Generation's 775,000 solar panels fill 380 acres generating 48 Mega-watts of electricity. This site is adjacent to an older 10 Mega-watt facility in El Dorado. Together, these sites will power 14,000 homes in California via Pacific Gas & Electric (PG&E) over the next 20 years.

 

MesquiteSolar.jpg

Mesquite Solar I planned location via Sempra Generation

 

Sempra Generation is not stopping here. Mesquite Solar I, a project in its first phase, is planned to eclipse the Nevada location by a factor of 12.5. 600 Mega-watts will pour from this Arlington Arizona based solar farm, powering up to 56,000 additional homes. This is a commendable effort.

 

 

Perhaps they should bring the panels to power each home directly. I decided to do a little math and figure out how much space and average price this may cost each person.

 

I will use the Kyocera KC175GT, a 175 watt solar panel.

I let it collect sunshine for 6 hours a day. Giving me a total of (175x6) 1050 watt hours. 1.05kwh

The size is 4.2 feet by 3.25 feet. Or 13.65 square feet.

An average home requires about 50kwh. (2 - 3 story home)

So I need approximately 48 panels to power the home. (50/1.05 = 47.62)

Which is a total of 655.2 square feet. And this is 1/66th of an acre.

Each panel costs $770 USD at the moment, on sale. Or $36,960 total for 48 panels.


Although that his a high price to pay to be green, I am sure Sempra Generation could provide each person with panels for far less. I hope they read this and get inspired to go individual generation someday.

 

Eavesdropper

0

uk-military-solar-uniform2011.jpg

 

A recent research project wants British soldiers to wear solar photovoltaic cells and a thermoelectric system to harness light or heat for 24/7 power. The goal is to lighten the packs soldiers carry by 50% and reduce the number of return trips to the base for recharging. An added benefit of the system is that after the various sources absorb all the energy across the electromagnetic spectrum, the soldiers will appear less obvious to infra-red surveillance equipment.

 

This project is a collaboration between the University of Glasgow and Strathclyde, Leeds, Reading, Loughborough, and Brunel Universities. Funding support is also coming from The Defense Science and Technology Laboratory (DSTL) and the Engineering and Physical Sciences Research Council (EPSRC). Many different disciplines are at work on this project, including chemists, material science, process, electrical, and design engineers. As you can see, everyone is quite serious about this endeavor.

 

Solar PV will harness light in the day, and thermoelectric devices will take over the same task at night. "Advanced" storage schemes will be used to store excess energy while still providing continuous power. Side note; the thermal harvesters should run 100% of the time. Daytime heat and the active soldier will generate much more power than in the evening, but the team will discover this soon.

 

Professor Ducan Gregory of Glasgow said they are planning to have a prototype within 2 years. He hopes the technology will filter into other categories, like medical transportation, satellites, or other space applications.

 

Good luck, see you all in 2 years.

 

Eavesdropper

3

sears_tower_willis_tower_chicago_01.jpg

 

The world famous Sears Tower, now Willis Tower, in Chicago is set to turn partially solar. A pilot project set to take place on the 56th floor of the Tower will feature photovoltaic glass from Pythagoras Solar. The insulating windows have a unique solar design. The PV cells lay 90 degrees from the glass's surface. Prisms in the glass reflect sunlight down into the horizontal PV cells, while diffused light still enters inside the building. This system makes the windows produce as much solar power as rooftop mounted panels.

 

 

willistowerg.jpg

 

If the project goes well, which I am sure it will, the solar windows will be expanded throughout the entire building. The equivalent solar surface of these windows, if applied to every window of the building, is approximately 10 acres, or about 8000 kW on sunny days.

 

Eavesdropper

0

Two years after the hurricane Katrina disaster in New Orleans, Louisiana, Brad Pitt toured the area and noticed most of the 4000 homes that were destroyed were not fixed, and the area abandoned. He promised the families he met there that he would "Make It Right." Like many, Pitt was let down by the lack of governmental help in the wake of the disaster. After meeting with local community groups and families Pitt established the "Make It Right Foundation," a non-profit organization set to build 150 green, affordable, high-quality homes that were closest to the levee breach, the lower 9th ward.


pitt clinton.JPG

Bill Clinton and Brad Pitt at the ground breaking in 2008


Make It Right broke ground in 2008, and since then have completed 70 homes. 21 local, national, and international architects designed the new homes, and donated the plans to the project. The designs have many green attributes. The homes feature a 2.7 to 3.0 kilowatt solar PV system, low-VOC paints, carpets, and other finishes, and recycled materials are used throughout. Metal roofs are used to reduce heat gain, it is hot down there, and capture rain water. Some feature green roofs. All internal materials are certified by Forest Stewardship. The homes have tankless waterheaters, Energy Star Rated appliances and light fixtures. The windows and doors have "low-e" coatings, to help reduce heat flow into the home.

 

NOLA2.jpghome2.JPG

2 of the finished homes. They look amazing.

 

Other interesting features include kevlar reinforced windows, advanced framing and engineered wall sections, all to withstand up to 130mph hurricane winds. And all the homes are built 6 to 8 feet off the ground to help in case of another flood.

 

Brad Pitt and Microsoft's Bing have pledged, together, $10 million dollars in matching funds for the project. For more information and links to donate, go to the Make It Right webpage.

 

I just found out about this program, and I am definitely going to donate.

 

Eavesdropper

0

US Marine PV installation

Posted by Eavesdropper Mar 21, 2011

solarmarinebase-450x337.jpg

 

1.4 megawatts from 6,3000 KD235, by Kyocra Solar Inc, are now powering the Pendleton USMC base camp. The system is expected to produce 2,400 MWh of electricity, enough power for about 400 average homes. The Naval Facilities Engineering Command (NAVFAC) is estimating this will save the Marine Corps $336,000 annually.

 

“The Box Canyon PV project is a very exciting venture that is making use of a previously unusable piece of real estate, and providing a renewable energy source to help Camp Pendleton meet its on-site renewable energy generation goals,” said Bernadette Rose, NAVFAC Southwest ROICC Construction Manager at Camp Pendleton.

 

The Navy has a goal it has to reach of 50% of their energy coming non-fossil fuels by 2020. The Navy is also using energy efficient lighting, alternatives for heating and cooling, and are on track to meeting their goal.

 

Eavesdropper

 

pic via Kyocera

0

thumb_230_1.jpgthumb_230_2.jpg

Nippon Telegraph and Telephone Copt (NTT), Toyko Japan, combines photovoltaic and thermal harvesting in the same container with an added benefit of up to 50% increase of current output. Sanyo Semiconductor Co's silicon PV cells are housed in a water-tight, transparent, enclosure in a staggered stair like configuration. This setup can provide power normally. However NTT fills the container with water, the water then refracts and reflects the light in such a way that the PV cells current output increases up to 50%. The PV cells absorb the visible light, while the water inside absorbs the infrared. The water is then heated and can be pumped out to be used.


 

The water has a similar effect like the "FUSION" film I wrote about in another post, but seems to have a greater effect. The film is cheap, while the NTT water enclosure is not. So, for now the water option will remain in the research lab. My question is, how deep does the water have to be to provide that effect?


 

I hope to see more from NTT.


 

Eavesdropper

0

GSR-110B-portable-retractable-solar-panel-1.jpg

 

From OS, Japan, comes a portable solar panel (GSR110B) using Fugi Electric Systems' flexible thin film solar technology. The system weighs approximately 3kg and is capable of generating 40W at 12V. Lithium-ion batteries store energy not being used, or to be charged before deploying. The most interesting feature is the ability to pair two together to produce 80W collectively. Although this is the cap, I ask why not combine more together for even higher wattage? OS's target for The GRS110B was be deployed as emergency power for communication equipment.  Of course, it can be used for anything else. These have been selling since January 2011 for 60,000 yen, or approximately $700 USD. A bit high, but can you put a price on 40W in a disaster?

 

Eavesdropper

0

before_after.jpghypersolar_concentrator.jpg

 

HyperSolar, has made a breakthrough in magnification of light on their solar panels, resulting in an increase in solar energy output. They plan to take the 1 cm thick solar product and place then right on top of existing, and aging, flat solar panels. The purposed increase of light magnification, 400%, reduces the number of solar cells inside of a panel which in turn reduces the cost. Though, I would wager that people would want to put the HyperSolar panels next to existing one. Even the smaller amount of energy from the old equipment is a little bit more you could harvest.


 

Tim Young, CEO of hyper solar, touts the new product, "Unlike current concentrated photovoltaic solutions that require bulky mirrors or lenses and sun tracking mechanisms, the HyperSolar concentrator will be a thin and flat self-tracking solar concentrator that conventional solar manufacturers can use in conventional flat solar panels. A HyperSolar concentrator is a concentrator like no other with a multi-billion square feet opportunity. Every square foot of solar panel demand is an opportunity to reduce the number of expensive solar cells by incorporating a square foot of HyperSolar."


 

See more at their site.

 



Eavesdropper

0

roof-blogSpan.jpgwal-mart-solar-panels.jpg

Walmart solar roof tops

 

 

Big companies need to participate in green initiatives, it is their ethical responsibility. Walmart, the world largest employer, is enthusiastic about alternative energy. Walmart partnered with The Environmental Defense Fund (EDF) in 2007 to provide a some momentum to photovoltaic technologies and research. They are particularly interested in thin-film solar. A few years later, Walmart has installed thin-film solar panels on top of several stores in California, Arizona, and Puerto Rico. Due to those locations receiving ample sun, they were logical choices. Currently, Walmart wishes to expand their solar stores to another 30 locations. The result is a reduction in each store's power demand by up to 30%. Collectively, Walmart produces 22.5 Million kWhs of energy. As they promote, "It is like taking 3000 cars off the road each year." Saving 11,650 metric tons of GHG from the atmosphere.


 

The thin-film solar panels come from First Solar and MiaSolé. Their products are far less expensive than silicon based solar panels. First Solar uses Cadmium Telluride and MiaSolé has copper, indium, selenide, and gallium based solar components. At 1 micron thick, their thin-film solar panels require less materials to manufacture, and are light weight and easy to install. They even work better than their silicon based counterparts on cloudy days, in smog and fog conditions. Thin-film even works with snow accumulation.


 

With the 8,350 Walmart locations, the chain has the potential to generate 6262.5 Million kWhs of energy, if they all produced at peak capacity. Walmart's vice president of energy, Kim Saylors, said " By leveraging our global scale to become a more efficient company, we are able to lower our expenses and help develop markets for new technologies. Developing and incorporating new renewable energy sources, like thin film, reduces energy price risk and aligns very well with our commitment to solving business challenges through technology.”



At an average of 1000kWh of energy a month per home (Based on California averages) Walmart could generate enough power 1/5 million homes for a year, to put it in perspective.



Cabe

0

fusionfilm clip.jpg

 

A new company called Genie Lens Technologies has just finished extensive testing on its "FUSION" film, made through a partner company SolOptics, at the National Renewable Energy Laboratory (NREL), a Golden Colorado research campus. Quite a basket of names and partnerships. More important is what FUSION film does. When applied to the surface of solar panels, the FUSION film traps light in to be absorbed by the solar cell. The light-bending properties of this film redirects the light along the surface of the semiconductor material of the cell for a greater chance of being absorbed. Tests at NREL shows that this film, applied to any solar cell, produces an efficiency gain of up to 12.5%. The FUSION films also helps in increasing light absorption even on cloudy days. As an added benefit, the film helps protect the surface of the solar panel, like a cell phone skin. No word on what will happen in areas where the film is damaged. Read more at Genie Lens's website.


Eavesdropper

0

 

“By taking-up this journey, I want to raise awareness about disability and tell people that we, despite our disability can achieve anything as an individual, if we are determined to try and have courage to do so," Said Haidar Taleb, as he attempts to beat his own world record of traveling 200 miles in a solar powered wheelchair. Taleb has had polio since the age of 4, but now wants to spread awareness to other people with disabilities that "there are no obstacles." Teamed up with Masdar, an alternative energy company, Taleb has shown that eco friendly solar powered wheelchairs are important and that "they can change the lives of persons with mobility problems." The chair can move at a constant 12mph. Taleb is set to break his previous 14-hour long 80 mile wheelchair trip. Good luck Haidar Taleb!

 

Eavesdropper

 

See E14's Technology for the Disabled group for other such technology.

0

stionalt_x220.jpg

A major issue with solar cells is the cost of each panel. In some cases it takes many years to recover the cost of a single panel, and even longer to have it produce more energy than it took to manufacture. Stion is attempting to reduce the cost of a cell by producing thin, stackable, and higher efficient solar film. The device is constructed in a way that significantly reduces cost, simplifies manufacturing and reduces materials utilization over traditional designs. The new panels are meant to be just as efficient as conventional silicon ones, but still significantly cheaper to manufacture. The funding is part of the Obama administration's recently announced Sun Shot initiative, which has the goal of reducing the cost of installed solar panels by 75 percent, to make solar power competitive with fossil fuels. Stion's existing panels convert 12 percent of the energy in sunlight into electricity. This is a high figure for thin-film solar panels, which typically have efficiencies that range from 6 to 11 percent. “The new panels use a tandem-solar-cell design to increase efficiencies to 15 to 18 percent,” says founder and chief technology officer Howard Lee. Pairing the cells increases the overall solar-panel efficiency and can drive down costs by reducing the number of panels that need to be installed. Tandem thin-film solar cells made of amorphous silicon have been made by other manufacturers, but they are far less efficient than the ones Stion is developing. When the sweet spot of price and efficiency is hit, the world will be a better place. Free Energy anywhere it's sunny.

Eavesdropper

1 2 Previous Next