Over the years, fingerprinting has evolved from an inky mess to pressing fingers on sensor screens to even a few touch-free systems that work at a short distance. Now a company, called Advanced Optical Systems Inc., has developed a prototype of a device that can scan fingerprints from up to two meters away, an approach that could prove especially useful at security checkpoints in places like Iraq and Afghanistan. It detects fingerprints by shining polarized light onto a person's hand and analyzing the reflection using two cameras configured to detect different polarizations. Slightly smaller than a square tissue box, AIRprint houses two 1.3 megapixel cameras and a source of polarized light. One camera receives horizontally polarized light, while the other receives vertically polarized light. When light hits a finger, the ridges of the fingerprint reflect one polarization of light, while the valleys reflect another. The prototype device, which scans a print in 0.1 seconds and processes it in about four seconds, can handle only one finger at a time. Also, the scanned finger must remain at a fixed distance from the device. I guess terrorists can circumvent this technology by being 2 1/2 meters away from the scanner. Or simply defeat it by not standing perfectly still. What do you all think, would you feel more safe or further violated with this device at airports? For more info on AIRprint visit: http://www.aos-inc.com/index.php/home
Zero