Skip navigation

community

Currently Being Moderated

Prolonging the Battery Life in WiFi Application

VERSION 1 
Created on: Oct 2, 2009 7:33 AM by tech1 - Last Modified:  Oct 2, 2009 7:44 AM by tech1

By Jack Gao – GTC China


WiFi has already been widely adopted in many applications; besides massive use in laptops and notebooks, it has also spread to the WiFi phone and VoIP applications. According to an authoritative report from Infonetics Research in 2007, the global distribution quantity of single mode WiFi phones had increased from 358,000 units in the previous year to 682,000 units, with a rate of growth of over 190% expected. However, WiFi/GSM Dual Mode VoIP phones are expected to have an even more rapid growth: from 2007 to 2010, the growth on the sales of these phones could reach as high as 1300%.

As WiFi applications becoming more popular, the coverage of the WiFi network become wider. More WiFi application will emerge in logistic management, home automation, building automation management and other portable devices. As Portable Mobile Electronics is cited as being one of the growth engines utilizing WiFi Technology, the requirement for longer battery lifetime will be one of the top priorities in these applications.

 

How to improve Battery Life?

 

There are three options to prolong battery life; increasing battery capacity, reduce WiFi product power consumption, and through some feasible control methods.

Increasing battery capacity is very simple; however, because of the technological limit, it may lead to a dramatic increase in the cost and physical size of the battery. Consequently, the other two options - reducing the power consumption of WiFi products and adding power control features are relatively feasible. To achieve low power consumption or even ultra low power consumption for WiFi products, an ultra-low power SoC has to be selected. The key features of three ultra low power WiFi chips which have gained relative popularity in the industry are listed in Table 1.

Part no.

GS1010

BCM4328

STLC4560

Vendor

Gainspan

BroadCom

ST-NXP

Single chip

Yes

Yes

Yes

Core

ARM7

ARM7

ARM9

Power Receive(mW)

-

295

275

Power Transmit(mW)

-

425

715

power sleep(mW)

0.018

5

1.5

Power   wise

Yes

Yes

Yes

Battery life Enhancement

Yes

No

No

RF   circuit

simple

complex

complex

Bluetooth

No

Yes

Yes

package

QFN102 (10 x 10 x 0.85 mm)

FPGA (10 mm x 10 mm)

LFBGA240 (8.5x8x1.4mm)

software support

GREENHILLS,    Keil, MDK, ARM,

WinCE, Linux, WinXP

Symbian,  WinCE, Linux

                                

                                                             Table 1

 

RF circuitry design for the GS1010 is very relatively simple (one 0805 part), even a system designer who has no any RF experience can complete the design easily. And because the GS1010 has an excellent battery life function, it consumes only 18µW in sleep mode. Gainspan claims that GS1010 can be powered for five to ten years on a single AA battery (depending on application).

The BCM4328 and STLC4560 both offer many advanced features and are provided with good software support. Therefore, designing a complex system which is software intensive (e.g., WiFi phone), the 328 or STLC4560 could be more likely to be chosen. But for a simple and low cost applications like a wireless sensor network, GS1010 could be the better choice.

 

 

              1.JPG

Figure 1

As shown in Figure 1, there is a vast gap in power consumption between active mode and standby mode. Based on that phenomenon, an idea for saving power is to prolong the time of standby and shorten the time of the active cycle is feasible. This requires designers to setup the response conditions accurately according to the request for system performance, reducing the possibilities that standby mode might be triggered by the system into active mode by mistake, and ensuring that the system returns to standby mode after all tasks are complete.

The techniques of low power consumption can dramatically prolong the battery life, but sound design solution is absolutely necessary to achieve this.

Attributes

Comments (0)

Bookmarked By (0)

Related Content


Related Products
Content
  • Retrieving data ...