picoPower AVR and RF transceiver on single-chip reduces overall system BOM and enables faster time-to-market without compromising performance
San Jose, CA, December 8, 2009 - Atmel® Corporation (Nasdaq: ATML), a leader in touch and microcontroller-based solutions, today announced a new family of AVR® wireless microcontroller (MCU) devices targeting wireless applications such as ZigBee® and IPv6/6LoWPAN. The ATmega128RFA1 is IEEE 802.15.4 compliant and combines Atmel's picoPower® AVR MCU and a 2.4 GHz RF transceiver. Atmel's picoPower technology offers ultra-low power consumption to ultimately enable longer battery life for wireless ZigBee applications, including smart energy, building automation, telecom and health care. ATmega128RFA1 is supported by Atmel's QTouch® Library, making it easy to combine capacitive touch functionality with RF in a single chip.
"The introduction of Atmel's new wireless MCU family further demonstrates its commitment to the ZigBee market," said Jagdish Rebello, PhD, Director and Principal Analyst, Wireless Communications, iSuppli Corporation. "As local governments, such as the state of California, pass Smart Grid legislation, local communities will begin to launch smart meters and other 'energy friendly' devices into their infrastructure. Many of these applications will require chips such as Atmel's new ATmega128RFA1. iSuppli forecasts that the ZigBee semiconductor market will grow to $636 million in 2013."
"As the ZigBee and smart metering markets continue to grow, our customers will demand lower power devices, lower bill of material (BOM) and higher performance, all combined in an integrated single chip solution," said Magnus Pedersen, Product Marketing Director of MCU Wireless Solutions at Atmel Corporation. "Atmel's ATmega128RFA1 solution addresses all these requirements for the low power, cost-sensitive ZigBee market. By combining our proprietary AVR technology, wireless know-how and integration expertise, we can now address all our customer needs in this market."
The ATmega128RFA1 combines Atmel's IEEE802.15.4 2.4 GHz transceiver with an AVR MCU on a single chip. The single-chip design enables designers to save board space and to bring down the overall system BOM so savings can be passed onto their customers. In addition, these devices include a low-power, high performance AVR MCU with embedded flash memory. Other key features include a long-range, high performance RF transceiver to ensure a reliable wireless link and a low current consumption for extended battery life. The MCUs in these devices run at a very low voltage operation without compromising performance. Finally, the wake-on-radio feature enables autonomous RF transmission and reception, further reducing power consumption keeping TRX RF active while the microcontroller is still in sleep mode.
Information, Availability and Pricing
For more information about Atmel's ATmega128RFA1, please click the following link:
http://www.atmel.com/wireless/single-chip.
The Atmel Atmega128RFA1 is available now with a suggested price of $4.78 for 10K quantities.
To download a high-resolution photo of the ATmega128RFA1, click the following link:
http://www.atmel.com/pressroom/photos/atmega128rfa1.jpg.
About Atmel
Atmel is a worldwide leader in the design and manufacture of capacitive touch solutions, microcontrollers, advanced logic, mixed-signal, nonvolatile memory and radio frequency (RF) components. Leveraging one of the industry's broadest intellectual property (IP) technology portfolios, Atmel is able to provide the electronics industry with complete system solutions focused on consumer, industrial, security, communications, computing and automotive markets.
© 2009 Atmel Corporation. All Rights Reserved. Atmel®, Atmel logo and combinations thereof, QTouch®, AVR®, AVR Studio®, picoPower® and others, are registered trademarks and others are trademarks of Atmel Corporation or its subsidiaries. Other terms and product names may be trademarks of others.