Skip navigation

community

Currently Being Moderated

Polycyclic Aromatic Hydrocarbons - PAH

VERSION 1 
Created on: Jun 22, 2010 8:59 AM by gnevison - Last Modified:  Jul 9, 2010 3:32 AM by gnevison

Polycyclic aromatic hydrocarbons (PAH) are a family of chemicals mainly derived from oil and coal but also

as by-products from burning a variety of materials. Therefore the main environmental sources are from coke

production, from petrol and diesel engine exhausts, from grilling meat and burning toast. Some PAH compounds,

such as Benzopyrene are carcinogens, mutagens and reproductive toxins. Very few have direct uses although

naphthalene was widely used at one time as mothballs and several are used as chemical intermediates to

manufacture pigments.

 

The only restriction today of PAH is from the Marketing and Use Directive (now Annex XVII

of the REACH Regulations) which bans the use of extender oil containing any of eight specified PAH in tyres.

Extender oils can contain PAH, although PAH-free extender oils are also available. Extender oils are used by the

electronics industry so that PAH may occur in electrical equipment although there are no restrictions except where

contact with food occurs (e.g. kitchen equipment). Analysis of a variety of materials has detected PAH in ABS,

polypropylene, paints, coatings and in natural materials such as wood, leather and bristles (brushes).

 

Soot is sometimes used as a black pigment and can contain PAH.TUV eco-labels now require certification that 16

PAH are below specified limits which is important for some types of products in certain countries. This has increased

interest in PAH and could result in pressure for legislation to further restrict it. REACH may be important here as the

regulation applies to commercial purity materials including any impurities.

 

In the meantime, the manufacturer of a particular product is the best source of information in respect of

PAH substance content

 

Attributes

Comments (0)

Bookmarked By (0)

Related Content


Related Products
Content
  • Retrieving data ...