Skip navigation

community

Currently Being Moderated

Alternative Energy Solutions - Solar LED Street Lighting

VERSION 2  Click to view document history
Created on: Feb 24, 2011 5:19 PM by Kcourtneynewark - Last Modified:  Sep 2, 2011 7:33 AM by RenfordNel

Alternative Energy Solutions - Solar LED Street Lighting

The sun is the biggest source of renewable energy on the planet. Solar power doesn't use fossil fuels, and is a non-renewable energy source. As the price of fossil fuels and other non-renewable energy sources skyrocket, consumers are being forced to think about other sources of energy. This is why, over the years, Solar Energy has found its way into our homes, offices, gardens and streets; while protecting the planet and helping us to save a fortune on our electricity bills.

 

Furthermore, the recent innovations in Solid State Lighting technology have made it possible for the mass adoption of high-efficacy energy efficient LED luminaires in conventional lighting applications. When equipped with solar power, LED street lighting offers a unique solution to reduction in electricity bills for city councils and Solar LED street lighting applications comprise of 3 phases: energy collection (solar panels), energy storage and energy conversion. Solar Panels form the core element of the design which collects and converts solar energy into electric energy which is then stored into the Energy Storage devices (e.g. high energy density batteries) during the day. During the night, power is fed into the LED arrays from the batteries through a DC/DC converter circuitry (or DC/AC if power is to be fed back into the energy grid). The entire operation from charging to monitoring the entire system is controlled by an MCU that supports a higher number of I/O pins to receive external control signals.

solar led street lighting.jpg

 

       
Visit >

 

AVAGO TECHNOLOGIESLEDSoldering and Handling of High BrightnessAN5334Click here
CIRRONETZigBee Module2.4 GHz ZigBee Transceiver ModuleZMN2430-R Click here
CREELEDLED_Lamp_PackagingP4LEDClick here
CREELEDLED_Lamp_Reliability_Test_StandardP4LEDClick here
CREELEDLED_Lamp_SolderingHandlingP4LEDClick here
FREESCALE SEMICONDUCTORMCUAN1986 Using the TRIAX Evaluation BoardAN1986MC68908Click here
FREESCALE SEMICONDUCTORMCUDeveloper's Serial Bootloader for M68HC08 and HCS08 MCUsAN2295MC68HC908Click here
FREESCALE SEMICONDUCTORMCUEEPROM Emulation Using FLASH in MC68HC908QY/QT MCUsAN2346MC68HC908Click here
FREESCALE SEMICONDUCTORMCUGenerating Clocks for HC908 MCU FamiliesAN2508MC68HC908Click here
FREESCALE SEMICONDUCTORMCUInitial Trimming of the MC68HC908 ICG AN2498MC68HC908Click here
FREESCALE SEMICONDUCTORMCULow-Cost Programming and Debugging Options for M68HC08 MCUsAN2317MC68HC908Click here
FREESCALE SEMICONDUCTORMCUMC68HC908EY16 ESCI LIN 1.3 DriversAN2575MC68HC908Click here
FREESCALE SEMICONDUCTORMCUSlave LIN Driver for the MC68HC908QT/QY FamilyAN2503MC68HC908Click here
FREESCALE SEMICONDUCTORMCUUsing FLASH as EEPROM on the MC68HC908GP32AN2183MC68HC908Click here
FREESCALE SEMICONDUCTORMCUUsing M68HC908 ROM-Resident RoutinesAN2874MC68HC908Click here
FREESCALE SEMICONDUCTORMCUUsing MC68HC908 On-Chip FLASH Programming Routines AN1831MC68HC908Click here
STMICROELECTRONICSLead-acid batterySolar-LED Streetlight Controller with 25 W LED Lamp Driver and 85 W Battery Charger Based on the STM32F101RxAN2946STM32F101RxClick here
MICROCHIPBattery Charger16HV785: Programmable Lead Acid Battery ChargerAN101516HV785Click here
MICROCHIPMCUAn I2C Network Protocol for Environmental MonitoringAN736PIC16CClick here
MICROCHIPBattery ChargerAN960-New Components and Design Methods Bring Intelligence to Battery Charger ManagementAN960Click here
MICROCHIPMCUMigrating Designs from PIC16C74A/74B to PIC18C442-I/P PIC16CClick here
MICROCHIPMCUMigrating Designs from PIC16C74A/74B to PIC18C442-I/P AN716PIC16CClick here
MICROCHIPMCUROM Code Submission Application NotePIC16CClick here
MICROCHIPMCUUsing the PICmicro MSSP Module for Master I2C CommunicationsPIC16CClick here
ON SEMICONDUCTORPower managementNCP1294: Solar Power Maximum Peak Power Tracking (MPPT) ControllerNCP1294Click here
TEXAS INSTRUMENTSSolar PowerMSP430x1xx Family User's GuideMSP430Click here
TEXAS INSTRUMENTSSolar PowerMSP430F11x1A Device ErrataMSP430Click here
ManufacturerProduct TypeAN TitleAN NumberPart NumberURL

Attributes

Comments (0)

Bookmarked By (0)

Related Content


Related Products
Content
  • Retrieving data ...