Skip navigation

community

Currently Being Moderated

Fortis Zd - Ruggedized high speed Backplane connector

VERSION 8  Click to view document history
Created on: Aug 16, 2011 2:49 AM by andy waller - Last Modified:  Aug 16, 2011 4:40 AM by andy waller
http://www.tycoelectronics.com/_TEincludes/ver/203/TEimages/leapfrog/te-logo.png

FORTIS ZD

 
FORTIS ZD high-speed backplane connector, designed for military and commercial  aerospace applications.
 
As demands on systems for real-time intelligence  intensifies, the importance of high performance interconnection becomes  critical. TE Connectivity set out to design a new connector system that  supports increasing bandwidth requirements in a ruggedized format to withstand  the increased shock and vibration requirements of emerging military  applications.
   
"The goal was to achieve a system that combined the seemingly contradictory  features of multi-gigabit speeds and extreme ruggedness," said Kevin Rock,  president, Aerospace, Defense & Marine, TE Connectivity. "Our development  engineering team has produced an outstanding product that more than met the  challenges set to them - providing a strong path for the next generation of  electronic systems in harsh environments."
 
TE Connectivity engineers provided ruggedization improvements in the  high-speed backplane connector designs by marrying an electrically  sophisticated, high-speed contact leadframe with a robust, industry-proven  separable contact interface. A metal shell offers an even higher degree of  robustness, both in the mating interface and the outer shell of the connector.
   
By combining the best features of commercial high-speed backplane connectors  with proven MIL-SPEC contacts, the new high performance FORTIS ZD connector  allows data rates of 10 Gbs+ and is designed to enable improved communications,  unmatched situational awareness, and technologically superior command/control  and training.
 
For more information and to follow all the latest news on the FORTIS ZD,  visit www.TheFutureUnleashed.com
  

APPLICATIONS
Motherboard / Daughtercard applications used in:

  • Commercial  aerospace
  • Ground defence
  • UAV - Unmanned Aerial vehicle
  • Fighter Jets
  • Other severe mechanical       environments

 
KEY  FEATURES

  • Allows 10 Gb/s+ data rates
  • Extreme mechanical and electrical performance for the most demanding applications
  • Modular design allows for user configurability and modular evolution
  • M55302 heritage Mini-Box separable interface provides 4 points of contact on all sides of the pin
  • Three shell varieties for application versatility, including plastic, shielded and machined  metal shell
  • 3-Pair and 2-Pair versions available to accommodate multiple slot pitches
  • Space compatible materials
  • Proven compliant pin board attach facilitates manufacturing efficiency, repairability, and  superior electrical performance
  • Staggered daughtercard pin field supports 2 level maintenance
  • Protected pin field on backplane for reliability and durability
fortis zd 2
fortis zd 3
    
View the products or buy:

Europe      US     Asia
 
Fortis Zd uses TE MIL-Spec Mini-Box PCB Connectors
Industry proven in high reliability applications
terminal
fortis zd

(MIL-DTL-55302)
Four-Beam Box Contact

helecopter
jet
plane


FORTIS, TE Connectivity and the TE Connectivity LOGO are trademarks of the  TE Connectivity group of companies and its licensors



Visit or Join Interconnect group
(New technologies, discussions, help)

Attributes

Comments (1)

Bookmarked By (0)

Related Content


Related Products
Content
  • Retrieving data ...