Show fans have a chance to channel their inner pinball wizard and win one of four autographed pinball circuit board prototypes on the element14 community
CHICAGO – Nov. 7, 2011 – element14, the first collaborative community and electronics store for design engineers and electronics enthusiasts, and modding guru Ben Heck, pull out all the stops in round two of Pinball Wars on this week’s episode of “The Ben Heck Show.” Special guest and pinball designer John Popadiuk returns to the studio with a 1950’s-inspired pinball build, Ben Heck’s Zombie Adventureland, starring none other than Ben Heck, himself.
“My love for pinball is no secret, and I'm beyond excited to be involved with this build,” said Ben. “Not only is it fun for me to use my skills in this challenging field, but it’s also an honor to be featured in a game designed and built by the legendary John Popadiuk.”
The team begins by stripping down an original Super Mario Bros. pinball machine to create the test play field for the new game. Using a breadboard configuration in the driver system, a design wired by hand using blank PCBs or wire-wrap, the team is able to test individual components such as the Arduino mega-compatible brain and parallax propellers, before assembling them together on the motherboard. In addition, John’s standard prototype “Italian Bottom” is composed using foam and paper, in lieu of the usual wood and metal, to make for a much quicker build time.
“Ben’s passion for pinball is obvious in this segment,” said Kevin Yapp, chief marketing officer, Premier Farnell. “With no more than the simple exchange of ideas, a little DIY finesse and access to element14’s wide array of design solutions and electronics components, the team inspires one another to build an amazing machine.”
Known for pinball machines such as Bally’s Cirqus Voltaire™ and Theatre of Magic™, John teams up with Ben to design the “super secret” playfield geometry, 304 stainless Adventureland mechanisms and amazing thematic elements for the final design—from Ben’s weapon of choice, an atomic neon glue gun, to King Arthur, the once-stray, good luck cat that finds his way into all of John’s builds. Pinball enthusiasts across the globe are sure to be impressed with Ben Heck’s Zombie Adventureland, and even more excited to learn that John will be taking preorders for the full-size custom build that features Ben beginning in January 2012.
Show fans are also invited to join the element14 community to send Ben a challenge for a future build, engage with community members, and enter for a chance to win one of four pinball circuit board prototypes autographed by Ben himself.