Skip navigation

community

Currently Being Moderated

How Cell Phones Work

VERSION 1 
Created on: Dec 14, 2011 3:57 PM by squadMCU - Last Modified:  Dec 14, 2011 4:10 PM by squadMCU

Millions of people in the United States and around the world use cellular phones. They are such great gadgets -- with a cell phone, you can talk to anyone on the planet from just about anywhere! These days, cell phones provide an incredible array of functions, and new ones are being added at a breakneck pace. But have you ever wondered how a cell phone works? What makes it different from a regular phone?


To start with, one of the most interesting things about a cell phone is that it is actually a radio -- an extremely sophisticated radio, but a radio nonetheless. That’s why a good way to understand the sophistication of a cell phone is to compare it to a CB radio or a walkie-talkie.


  • Full-duplex vs. half-duplex - Both walkie-talkies and CB radios are half-duplex devices. That is, two people communicating on a CB radio use the same frequency, so only one person can talk at a time. A cell phone is a full-duplex device. That means that you use one frequency for talking and a second, separate frequency for listening. Both people on the call can talk at once.
  • Channels - A walkie-talkie typically has one channel, and a CB radio has 40 channels. A typical cell phone can communicate on 1,664 channels or more!
  • Range - A walkie-talkie can transmit about 1 mile (1.6 km) using a 0.25-watt transmitter. A CB radio, because it has much higher power, can transmit about 5 miles (8 km) using a 5-watt transmitter. Cell phones operate within cells, and they can switch cells as they move around. Cells give cell phones incredible range. Someone using a cell phone can drive hundreds of miles and maintain a conversation the entire time because of the cellular approach.


All cell phones have special codes associated with them. These codes are used to identify the phone, the phone's owner and the service provider. Let's say you have a cell phone, you turn it on and someone tries to call you. Here is what happens to the call:

1. When you first power up the phone, it listens for an SID (see sidebar) on the control channel. The control channel is a special frequency that the phone and base station use to talk to one another about things like call set-up and channel changing. If the phone cannot find any control channels to listen to, it knows it is out of range and displays a "no service" message.

2. When it receives the SID, the phone compares it to the SID programmed into the phone. If the SIDs match, the phone knows that the cell it is communicating with is part of its home system.

3. Along with the SID, the phone also transmits a registration request, and the MTSO keeps track of your phone's location in a database -- this way, the MTSO (Mobile Telephone Switching Office) knows which cell you are in when it wants to ring your phone.

4. The MTSO gets the call, and it tries to find you. It looks in its database to see which cell you are in.

5. The MTSO picks a frequency pair that your phone will use in that cell to take the call.

6. The MTSO communicates with your phone over the control channel to tell it which frequencies to use, and once your phone and the tower switch on those frequencies, the call is connected. Now, you are talking by two-way radio to a friend.

 

cellphone.png

 

SOURCE: howstuffworks.com

Attributes

Comments (0)

Bookmarked By (0)

Related Content


Related Products
Content
  • Retrieving data ...