Skip navigation

community

Currently Being Moderated

MPC551x to MPC560xB/C, SPC560Bx/Cx Migration*

VERSION 1 
Created on: Jan 31, 2012 12:48 PM by iLOVEautomotive - Last Modified:  Jan 31, 2012 12:54 PM by iLOVEautomotive

The MPC551x family has introduced features into a
Power Architecture family of devices that support
reduced current consumption, specifically to assist the
power-sensitive body electronics system space. The
power consumption can be tuned during dynamic
operating modes, where code execution and actuation are
supported, and also in static modes, where the minimum
power consumption is necessary.
Freescale has recently introduced the MPC560x family
in a joint development program with
STMicroelectronics. This family shares many
low-power features with the MPC551x family, but users
migrating from one family to the other need to be aware
of key differences between them.
This document outlines the differences between the
MPC551x and the MPC560x familes

The MPC551x family has introduced features into a Power Architecture family of devices that support reduced current consumption, specifically to assist the power-sensitive body electronics system space. The power consumption can be tuned during dynamic operating modes, where code execution and actuation are supported, and also in static modes, where the minimum power consumption is necessary.

 

Application Note for MPC551x family

 

Freescale has recently introduced the MPC560x family in a joint development program with STMicroelectronics. This family shares many low-power features with the MPC551x family, but users migrating from one family to the other need to be aware of key differences between them. This document outlines the differences between the MPC551x and the MPC560x familes.

Attributes

Comments (0)

Bookmarked By (0)

Related Content


Related Products
Content
  • Retrieving data ...