(Via Vincent Founier & Ariane stock photography)
This is not a UFO, but it is part of a space bound vehicle. It is a fuel storage system for the Ariane 5 heavy-lift launcher rocket, aka- Automated Transfer Vehicle, a resupply spacecraft for the International Space Station. The "cryogenic stage" pod contains 132.27 metric tons of liquid oxygen and 25.84 metric tons of liquid hydrogen. After the fuel is spent, the pod is designed to re-enter the atmosphere for an oceanic splashdown.

(Via Arianespace)
The Ariane 5 rocket can carry 20 tonnes of equipment into low earth orbit. Additionally, it can boost 10 tonnes into geostationary orbit (36,000 km).
The next Ariane 5 launch (the 5th of 2011) will take 2 satellites into orbit. One is the Arab Satellite Communication Organization's "Arabsat 5C" communication satellite (weighing in at 4.6 tonnes). The second is the North America servicing SES-2 communication satellite delivering "advanced digital media" to the USA and Caribbean. The U.S. Airforce is also tacking on an experimental wide-field-of-view infrared missile tracking system on the SES-2. (Watch the latest fall season TV or shoot down missiles? I am in for both.)
Eavesdropper