Skip navigation

community

Defense and Aerospace

10 Posts tagged with the eavesdropper tag
0

ariane.jpg

(Via Vincent Founier & Ariane stock photography)

 

This is not a UFO, but it is part of a space bound vehicle. It is a fuel storage system for the Ariane 5 heavy-lift launcher rocket, aka- Automated Transfer Vehicle, a resupply spacecraft for the International Space Station. The "cryogenic stage" pod contains 132.27 metric tons of liquid oxygen and 25.84 metric tons of liquid hydrogen. After the fuel is spent, the pod is designed to re-enter the atmosphere for an oceanic splashdown.

 

a5-overview.jpg

(Via Arianespace)

 

The Ariane 5 rocket can carry 20 tonnes of equipment into low earth orbit. Additionally, it can boost 10 tonnes into geostationary orbit (36,000 km).

 

The next Ariane 5 launch (the 5th of 2011) will take 2 satellites into orbit. One is the Arab Satellite Communication Organization's "Arabsat 5C" communication satellite (weighing in at 4.6 tonnes). The second is the North America servicing SES-2 communication satellite delivering "advanced digital media" to the USA and Caribbean. The U.S. Airforce is also tacking on an experimental wide-field-of-view infrared missile tracking system on the SES-2. (Watch the latest fall season TV or shoot down missiles? I am in for both.)

 

Eavesdropper

1

 

(video via BAE Systems)

 

Today's modern wars are fought with a severe technology disparity between the factions. One side is making improvised explosive devices while the other uses augmented reality to call in air strikes. Despite the differences, the modern countries continue to innovate against a possible war with its hi-tech peers. BAE Systems has just released its "Adaptiv" vehicle camouflage that mimics the heat signatures in its surroundings.

 

The Adaptiv technology consists of hexagonal "pixels." An onboard camera samples the background and displays the IR-image on the pixels accordingly. The process happens fast enough for a moving vehicle to not even make an impression under IR surveillance. The pixels can also be arranged to make the vehicle look like another. In the video example, a tank is make to look like a Jeep.  The pixels could also be used to display words or a message, if need be.

 

The project is funded by the Swedish Defense Materiel Administration, who wanted a focus on IR cloaking. However, the BAE engineers combined the Adaptiv pixels with other electro-magnetic spectrum cloaking devices to provide further stealth coverage.

 

BAE plans on adapting the technology for warships and buildings. For this application, larger panels will be used.

 

I would like to see similar technology for use on soldiers. Seeing soldiers get taken out by UAVs at night, via infrared cameras, is disturbing. Again, the battles are usually one sided anyway. I have never heard of a drone on drone battle in any war.

 

Eavesdropper

 

0

scell.JPG

SIlver Cell construction (via The Autralian NAtional University)

 

Soldiers carry a lot of weight. With radios, night-vision devices, flashlights, communication systems, ammunition, and other basic supplies the weight approaches the point of hurting the person carrying it all. In fact, major-general of the Australian army said, "It's not good for a soldier's back to be carrying that much weight."

 

One area that can benefit from advancing technology has been the size of the electronics and the power systems. In the distant past, communications were powered by heavy lead-acid batteries. Later came lighter weight battery packs that have been getting smaller and more energy dense every year. The progress does not stop here. The Australian army is testing the possible use of lightweight solar panels, eliminating the need for any large battery pack.

 

The new solar cells are a bit different than standard silicon based panels. Called "Silver Cells," the panel arranges the photovoltaic elements in thinly sliced pieces, vertically, in a silicon frame. The cells use 90% less silicon than other mono crystalline cells of equivalent output. In other words, the costs are lower.

 

The elements are 50 to 100mm long, 1 - 2mm wide, and 45micrometers thick. Both sides of the element can absorb light. Due to the bifacial response of the Silver cell, the optimal angles are increased. And the cells work well on curved surfaces. Open circuit voltage of the cell is in the 600 - 700mV range. Connected in series or parallel, for whatever voltage the application needs, the cells are capable of 140 Watts per square meter.

 

The plan is to cover soldier's helmets, tents, and clothing. Testing will be conducted over a few years before acceptance for true field use. What they will soon discover is that the reflective nature of solar panels will not be good for concealing soldiers or objects. Much like flashing the sun off a mirror at your enemies. I would imagine a whole group of soldiers would look like they are sparkling. Not the most intimidating look out there.

 

Eavesdropper

1

Printable UAV Aircraft

Posted by Eavesdropper Jul 29, 2011

A team from the University of Southampton has used 3D printing techniques to build a working UAV from the ground up in just under a week. The team, led by Andy Keane and Jim Scanlan, demonstrated their effort at an air strip just a little down the road from Stonehenge. The 1.5 meter wing span, ultra-low-drag, aircraft successfully flew showing it is possible to build for each individual application.


At 100 micrometers (4 thousands) at a time, a laser traces out the 2D cross section of the design. The laser can "print" with many different types of materials, from polyamide plastic to stainless steel or titanium powder. When forming parts with the metallic powder, the team stated that it is as strong as if the parts were machined from raw/bare metal. To create a stronger formed part, an electron laser sintering is used, instead of the conventional laser, to melt the powder completely.


Of course, the electronics in the craft are not printed. At least not yet. http://www.element14.com/community/community/doittogetherblog/blog/2011/07/14/grow-electronics-by-the-molecule


Eavesdropper

2

SpaceX, a California company, had tested their Falcon 9 rocket and capsule successfully back in November 2010. Now they are planning a docking of their new Dragon capsule aboard the International Space Station (ISS) in December of this year, 2011. The Falcon Heavy rocket will launch on November 30th, and the capsule will then take a week long tour around the planet before docking on the ISS.


Following the shutdown of the shuttle program, the ISS will need another way to receive supplies. This is SpaceX's mission, to provide an alternative to sending supplies, satellites, and people into space. Being the only alternative to Russian Soyuz missions to get people into orbit, SpaceX is sure to make enormous profits.


SpaceX also stated that their Dragon capsule is far safer than the former shuttle program, "astronauts flying on Dragon will be considerably safer." I do hope this is true. There has been far to many shuttle disasters to date.


Eavesdropper

2

Serious threat of space debris on the space station
In the past three years the International Space Station (ISS) had to change its orbit five time to avoid orbiting "junk" from ripping right through the station vital and fragile shell. In fact on June 28th astronauts took shelter in a heavily fortified section of the space station as a object was detected only fourteen hours before an expected impact. Although it passed one thousand feet from the outside of the station, the countless objects remain a continuous threat.


Russia has blown up many off their satellites which happen to fall within the ISS orbit band, placing thousands of objects in direct line for impact. In 2007 China demonstrated their capabilities to destroy satellites with the take down of one of their own. Thousands of additional objects have been added to the frey. In 2009 an American and a Russian satellite collided producing thousands more for the orbiting path. In other words, the ISS is under constant danger.


With an estimated 1 in 8 chance of an impact, the ISS may end up becoming a short lived destination for space travelers. There are some thin kevlar based protective shields placed over critical components, they will not be able to protect against larger objects. Perhaps collecting space garbage is imperative.

Http://www.element14.com/community/message/19899#19899


Though it may all come too late. The ISS is scheduled to be abandoned in 2020.


Eavesdropper

0

boeing747-8.jpg

Boeing 747-8 via Boeing

 

Seeing a trend in aircraft biofuel usage?

 

Boeing has recently demonstrated the use of a camelina-based biofuel in one of their unmodified 747-8 Freighter airplanes. The camelina biofuel is a mixture of 85% kerosene fuel, called Jet-A, and 15% processed oils from the camelina organic plant. Camelina plant seeds have an oil content in the range of 37-41%, and it is rich in omega-3 fatty acids. When the oils are heated in the excess of 450°C in the absence of air (oxygen), it causes the molecules to break forming chemical compounds similar to those found in petrodiesel. This process is called pyrolysis, and sometimes thermal cracking or cracking.

 

220px-Camelina_sativa_eF.jpg

Camelina plant, via Camelina Wiki

 

The camelina plant was grown in Montana, USA, and Honeywell's UOP processed the plant into the biofuel used in the demonstration. The 747-8 cargo plane made its 4,989 mile transatlantic flight without a single issue. The fuel comes from a 5 year program that Boeing and several other aircraft companies started as a way to develop sustainable biofuels.

 

Eavesdropper

0

klm.jpg

KLM Passenger Jet via KLM

 

The oldest airline with the same name since it started, KLM Royal Dutch Airlines founded in the Netherlands in 1919, is showing off the first use of a biofuel blend on a commercial passenger aircraft. 170 passengers on a Boeing 737-800 flew from Amsterdam to Paris on June 22, 2011. KLM managing director Camiel Eurlings spoke about the use of the fuel, "In November 2009 we demonstrated that it was technically possible to fly on biokerosene. Now, a year and a half after our first demonstration flight on Camelina, a new phase has been entered around the world, that of certification. Authorisation will soon be granted to operate commercial flights on biofuel. I am especially proud to announce that KLM will take this substantial step in September."

 

Biokerosene if a 50/50 blend of kerosene and biofuel made from used cooking oil produced by Dynamic Fuels, a Tyson Foods and Syntroleum Corporation partnership. The Biokerosene met the same specifications of standard kerosene, and required no modification to the aircraft. The end result was a substantial reduction of CO2 emissions and a minimum negative impact on biodiversity and the food supply due to the fuel source.

 

KLM's consortium that is seeking out and developing sustainable aviation biofuel, SkyNRG, supplied the fuel. After seeking the advice of an independent sustainability board consisting of Solidaridad, Copernicus Institute of the University of Utrecht, and the World Wide Fund for Nature, they were given the OK on the mix of Biokerosene.

 

KLM admits that the price of the Biokerosene is very high. To meet true sustainability, the price of the fuel has to "come down substantially and permanently." However, KLM's demonstration is an indicator of big changes on the way. No wonder KLM has been a sector leader of the Dow Jones Sustainability Index for the past six years.

 

Perhaps they should look into algae, as in the recent U.S. Navy's recent biofuel helicopter test fight.

 

Eavesdropper

0

5f526603-5973-4c93-bcd1-7e25c71f39a2.Large.jpg05e83f05-9be2-49d0-9cf1-4fa2b5b2e23c.Large.jpg

BiPod on its test flight and car via Scaled Composites

 

While Terrafugia takes pre-orders on their Airplane Car, and Trek Aerospace consider civilian transport, Burt Rutan tests his last airplane before his retirement. BiPod, the flying car from Scaled Composites. A two seater, dual 15 kW motor driven hybrid-electric airplane that just happens to be drivable on the road. 

 

In just four months from the inception of the BiPod, the craft took its first flight on March 30, 2011. Able to reach a 200mph speed, the BiPod can fly a distance of 530 miles. It also have an "overdrive mode," that lets the user fly 760 miles at a slower 100mph. In ground driving mode it can go 35 miles on battery charge alone, or up to 820 miles on a single tank of gas. Batteries in the nose of the craft privide enough power for takeoff, and a reserve of two possible landing attempts for safety.

 

Two 450CC internal-combustion engines, one in each fuselage, drive generators that in turn power electric motors on the driving wheels and propellers. The driving of a generator by a gasoline motor is also the concept behind the Chevy Volt, under certain conditions. Four propellers, one on each wing and two on the horizontal stabilizer linkage on the tails.

 

Flight and driving controls are separated between the two fuselage sections. Left side are the flight controls, and right side is for driving. When in driving mode, the wings must be removed and stored between the two halves.

 

Scaled Composites announced the ambitious project to gauge the response and viability of the BiPod. All the while Burt Rutan spends most of his time working away on his final legacy. Scaled Composite's President Doug Shane said, "[Rutan] was here all the time - he worked really damned hard - and that was a good lesson to all our young engineers that you don't get something for nothing."

 

fb4f5683-9fc9-49d0-9160-1d0d79fe3b78.Large.jpga81881f7-1421-44cc-9005-af0847ac4f6c.Large.jpg

Concept design for the BiPod via Scaled Composites

 

 

You might recognize some of the past eclectic airplane designs from Burt Rutan and the team at Scaled Composites in the below video. Now you know where they all came from.



 

Eavesdropper

0

RRM2.jpg

The Robotic Refueling Mission via NASA

 

Despite the retiring of the space shuttle program, NASA sent up a space craft refueling and repairing platform. The Robotic Refueling Mission (RRM) sent on the Atlantis space shuttle on July 8th, 2011 and installed in 15 minutes on the International Space Station. The RRM features a twin-armed robot dubbed "Dextre." The Dextre, Special Purpose Dexterous Manipulator, will be controlled by a person located on Earth. Using Dextre will make repairs and refueling to cost far lower than with an astronaut on a spacewalk. Overall, the RRM with Dextre will prolong space travel for crafts already orbiting the planet.

 

Another use of the RRM comes in repairing satellites, where there are already hundreds out of commission at the moment. This is a service never before attempted. NASA's Satellite Servicing Capabilities Officer Benjamin Reed said, "We anticipate [the RRM] enabling future missions, future capabilities, for the international aerospace community."

 

We're going to make this data available to everybody," said RRM project manager at the Satellite Servicing Capabilities Office Frank Cepollina. "That is, all commercial industry that may want to leap off and start their own ventures."

 

080626-aresv-flight-02.jpg

Heavy-Lift rocket concept via NASA

 

On related space news, the U.S. Congress demands to know why a new heavy lifting rocket is not completed by now. With the cancellation of some space programs by the Obama administration has led to many delays. Since the retirement of the shuttle program a new type of space craft is needed to get satellites, equipment, and people out of the atmosphere. The Space Launch System heavy-lift rocket is what President Obama is now backing as a contender for a new vehicle. However, current plans will not have a manned mission aboard the new craft until 2020. Which could be in line with President Obama's wishes for a manned mission to an asteroid by 2025 and to Mars by 2035.

 

Eavesdropper