Skip navigation

community

Defense and Aerospace

5 Posts tagged with the space tag
0

ariane.jpg

(Via Vincent Founier & Ariane stock photography)

 

This is not a UFO, but it is part of a space bound vehicle. It is a fuel storage system for the Ariane 5 heavy-lift launcher rocket, aka- Automated Transfer Vehicle, a resupply spacecraft for the International Space Station. The "cryogenic stage" pod contains 132.27 metric tons of liquid oxygen and 25.84 metric tons of liquid hydrogen. After the fuel is spent, the pod is designed to re-enter the atmosphere for an oceanic splashdown.

 

a5-overview.jpg

(Via Arianespace)

 

The Ariane 5 rocket can carry 20 tonnes of equipment into low earth orbit. Additionally, it can boost 10 tonnes into geostationary orbit (36,000 km).

 

The next Ariane 5 launch (the 5th of 2011) will take 2 satellites into orbit. One is the Arab Satellite Communication Organization's "Arabsat 5C" communication satellite (weighing in at 4.6 tonnes). The second is the North America servicing SES-2 communication satellite delivering "advanced digital media" to the USA and Caribbean. The U.S. Airforce is also tacking on an experimental wide-field-of-view infrared missile tracking system on the SES-2. (Watch the latest fall season TV or shoot down missiles? I am in for both.)

 

Eavesdropper

2

SpaceX, a California company, had tested their Falcon 9 rocket and capsule successfully back in November 2010. Now they are planning a docking of their new Dragon capsule aboard the International Space Station (ISS) in December of this year, 2011. The Falcon Heavy rocket will launch on November 30th, and the capsule will then take a week long tour around the planet before docking on the ISS.


Following the shutdown of the shuttle program, the ISS will need another way to receive supplies. This is SpaceX's mission, to provide an alternative to sending supplies, satellites, and people into space. Being the only alternative to Russian Soyuz missions to get people into orbit, SpaceX is sure to make enormous profits.


SpaceX also stated that their Dragon capsule is far safer than the former shuttle program, "astronauts flying on Dragon will be considerably safer." I do hope this is true. There has been far to many shuttle disasters to date.


Eavesdropper

2

Serious threat of space debris on the space station
In the past three years the International Space Station (ISS) had to change its orbit five time to avoid orbiting "junk" from ripping right through the station vital and fragile shell. In fact on June 28th astronauts took shelter in a heavily fortified section of the space station as a object was detected only fourteen hours before an expected impact. Although it passed one thousand feet from the outside of the station, the countless objects remain a continuous threat.


Russia has blown up many off their satellites which happen to fall within the ISS orbit band, placing thousands of objects in direct line for impact. In 2007 China demonstrated their capabilities to destroy satellites with the take down of one of their own. Thousands of additional objects have been added to the frey. In 2009 an American and a Russian satellite collided producing thousands more for the orbiting path. In other words, the ISS is under constant danger.


With an estimated 1 in 8 chance of an impact, the ISS may end up becoming a short lived destination for space travelers. There are some thin kevlar based protective shields placed over critical components, they will not be able to protect against larger objects. Perhaps collecting space garbage is imperative.

Http://www.element14.com/community/message/19899#19899


Though it may all come too late. The ISS is scheduled to be abandoned in 2020.


Eavesdropper

0

RRM2.jpg

The Robotic Refueling Mission via NASA

 

Despite the retiring of the space shuttle program, NASA sent up a space craft refueling and repairing platform. The Robotic Refueling Mission (RRM) sent on the Atlantis space shuttle on July 8th, 2011 and installed in 15 minutes on the International Space Station. The RRM features a twin-armed robot dubbed "Dextre." The Dextre, Special Purpose Dexterous Manipulator, will be controlled by a person located on Earth. Using Dextre will make repairs and refueling to cost far lower than with an astronaut on a spacewalk. Overall, the RRM with Dextre will prolong space travel for crafts already orbiting the planet.

 

Another use of the RRM comes in repairing satellites, where there are already hundreds out of commission at the moment. This is a service never before attempted. NASA's Satellite Servicing Capabilities Officer Benjamin Reed said, "We anticipate [the RRM] enabling future missions, future capabilities, for the international aerospace community."

 

We're going to make this data available to everybody," said RRM project manager at the Satellite Servicing Capabilities Office Frank Cepollina. "That is, all commercial industry that may want to leap off and start their own ventures."

 

080626-aresv-flight-02.jpg

Heavy-Lift rocket concept via NASA

 

On related space news, the U.S. Congress demands to know why a new heavy lifting rocket is not completed by now. With the cancellation of some space programs by the Obama administration has led to many delays. Since the retirement of the shuttle program a new type of space craft is needed to get satellites, equipment, and people out of the atmosphere. The Space Launch System heavy-lift rocket is what President Obama is now backing as a contender for a new vehicle. However, current plans will not have a manned mission aboard the new craft until 2020. Which could be in line with President Obama's wishes for a manned mission to an asteroid by 2025 and to Mars by 2035.

 

Eavesdropper

0

fusion pro.jpg

 

At the IEEE Symposium in Chicago this week, Nasa physicist John J. Chapman suggested that boron could be used as an "aneutronic" fuel, a fusion power source where neutrons carry no more than 1% of the total released energy (Wiki). What he implied was a new type of fusion thruster.

 

Using an off the shelf laser directed on to a thick metal foil, the energy is used to accelerate protons. The then rush of electrons leaved behind an overly positive charge. Which creates an imbalance with the protons left behind, resulting in a micro explosion. The explosion will send protons from the metal sheet to a second sheet made up of thin sliced Boron-11.

 

When the protons interact with the Boron-11, carbon nuclei are formed, but then decays to Helium-4 & beryllium nucleuses. All this would then decay to a pair of alpha particles, which is two protons and two neutrons bound together into a particle identical to a helium nucleus (alpha particles are incredibly dangerous to living cells). Each reaction creates 3 alpha particle, and according to Chapman the process is "very efficient." Electromagnetic force would then channel the alpha particles and all matter they touch through a nozzle. Chapman believe that this fusion thruster would be more efficient that current ion propulsion, but does not see his idea emerging for at least another 10 years.

 

Where would be we if we all did not speculate from time to time?

 

Eavesdropper