Skip navigation

community

Defense and Aerospace

5 Posts tagged with the university tag
0

scell.JPG

SIlver Cell construction (via The Autralian NAtional University)

 

Soldiers carry a lot of weight. With radios, night-vision devices, flashlights, communication systems, ammunition, and other basic supplies the weight approaches the point of hurting the person carrying it all. In fact, major-general of the Australian army said, "It's not good for a soldier's back to be carrying that much weight."

 

One area that can benefit from advancing technology has been the size of the electronics and the power systems. In the distant past, communications were powered by heavy lead-acid batteries. Later came lighter weight battery packs that have been getting smaller and more energy dense every year. The progress does not stop here. The Australian army is testing the possible use of lightweight solar panels, eliminating the need for any large battery pack.

 

The new solar cells are a bit different than standard silicon based panels. Called "Silver Cells," the panel arranges the photovoltaic elements in thinly sliced pieces, vertically, in a silicon frame. The cells use 90% less silicon than other mono crystalline cells of equivalent output. In other words, the costs are lower.

 

The elements are 50 to 100mm long, 1 - 2mm wide, and 45micrometers thick. Both sides of the element can absorb light. Due to the bifacial response of the Silver cell, the optimal angles are increased. And the cells work well on curved surfaces. Open circuit voltage of the cell is in the 600 - 700mV range. Connected in series or parallel, for whatever voltage the application needs, the cells are capable of 140 Watts per square meter.

 

The plan is to cover soldier's helmets, tents, and clothing. Testing will be conducted over a few years before acceptance for true field use. What they will soon discover is that the reflective nature of solar panels will not be good for concealing soldiers or objects. Much like flashing the sun off a mirror at your enemies. I would imagine a whole group of soldiers would look like they are sparkling. Not the most intimidating look out there.

 

Eavesdropper

1

Printable UAV Aircraft

Posted by Eavesdropper Jul 29, 2011

A team from the University of Southampton has used 3D printing techniques to build a working UAV from the ground up in just under a week. The team, led by Andy Keane and Jim Scanlan, demonstrated their effort at an air strip just a little down the road from Stonehenge. The 1.5 meter wing span, ultra-low-drag, aircraft successfully flew showing it is possible to build for each individual application.


At 100 micrometers (4 thousands) at a time, a laser traces out the 2D cross section of the design. The laser can "print" with many different types of materials, from polyamide plastic to stainless steel or titanium powder. When forming parts with the metallic powder, the team stated that it is as strong as if the parts were machined from raw/bare metal. To create a stronger formed part, an electron laser sintering is used, instead of the conventional laser, to melt the powder completely.


Of course, the electronics in the craft are not printed. At least not yet. http://www.element14.com/community/community/doittogetherblog/blog/2011/07/14/grow-electronics-by-the-molecule


Eavesdropper

0

klm.jpg

KLM Passenger Jet via KLM

 

The oldest airline with the same name since it started, KLM Royal Dutch Airlines founded in the Netherlands in 1919, is showing off the first use of a biofuel blend on a commercial passenger aircraft. 170 passengers on a Boeing 737-800 flew from Amsterdam to Paris on June 22, 2011. KLM managing director Camiel Eurlings spoke about the use of the fuel, "In November 2009 we demonstrated that it was technically possible to fly on biokerosene. Now, a year and a half after our first demonstration flight on Camelina, a new phase has been entered around the world, that of certification. Authorisation will soon be granted to operate commercial flights on biofuel. I am especially proud to announce that KLM will take this substantial step in September."

 

Biokerosene if a 50/50 blend of kerosene and biofuel made from used cooking oil produced by Dynamic Fuels, a Tyson Foods and Syntroleum Corporation partnership. The Biokerosene met the same specifications of standard kerosene, and required no modification to the aircraft. The end result was a substantial reduction of CO2 emissions and a minimum negative impact on biodiversity and the food supply due to the fuel source.

 

KLM's consortium that is seeking out and developing sustainable aviation biofuel, SkyNRG, supplied the fuel. After seeking the advice of an independent sustainability board consisting of Solidaridad, Copernicus Institute of the University of Utrecht, and the World Wide Fund for Nature, they were given the OK on the mix of Biokerosene.

 

KLM admits that the price of the Biokerosene is very high. To meet true sustainability, the price of the fuel has to "come down substantially and permanently." However, KLM's demonstration is an indicator of big changes on the way. No wonder KLM has been a sector leader of the Dow Jones Sustainability Index for the past six years.

 

Perhaps they should look into algae, as in the recent U.S. Navy's recent biofuel helicopter test fight.

 

Eavesdropper

0

5f526603-5973-4c93-bcd1-7e25c71f39a2.Large.jpg05e83f05-9be2-49d0-9cf1-4fa2b5b2e23c.Large.jpg

BiPod on its test flight and car via Scaled Composites

 

While Terrafugia takes pre-orders on their Airplane Car, and Trek Aerospace consider civilian transport, Burt Rutan tests his last airplane before his retirement. BiPod, the flying car from Scaled Composites. A two seater, dual 15 kW motor driven hybrid-electric airplane that just happens to be drivable on the road. 

 

In just four months from the inception of the BiPod, the craft took its first flight on March 30, 2011. Able to reach a 200mph speed, the BiPod can fly a distance of 530 miles. It also have an "overdrive mode," that lets the user fly 760 miles at a slower 100mph. In ground driving mode it can go 35 miles on battery charge alone, or up to 820 miles on a single tank of gas. Batteries in the nose of the craft privide enough power for takeoff, and a reserve of two possible landing attempts for safety.

 

Two 450CC internal-combustion engines, one in each fuselage, drive generators that in turn power electric motors on the driving wheels and propellers. The driving of a generator by a gasoline motor is also the concept behind the Chevy Volt, under certain conditions. Four propellers, one on each wing and two on the horizontal stabilizer linkage on the tails.

 

Flight and driving controls are separated between the two fuselage sections. Left side are the flight controls, and right side is for driving. When in driving mode, the wings must be removed and stored between the two halves.

 

Scaled Composites announced the ambitious project to gauge the response and viability of the BiPod. All the while Burt Rutan spends most of his time working away on his final legacy. Scaled Composite's President Doug Shane said, "[Rutan] was here all the time - he worked really damned hard - and that was a good lesson to all our young engineers that you don't get something for nothing."

 

fb4f5683-9fc9-49d0-9160-1d0d79fe3b78.Large.jpga81881f7-1421-44cc-9005-af0847ac4f6c.Large.jpg

Concept design for the BiPod via Scaled Composites

 

 

You might recognize some of the past eclectic airplane designs from Burt Rutan and the team at Scaled Composites in the below video. Now you know where they all came from.



 

Eavesdropper

0

mg21128195.100-1_300.jpg

MyCopter Concept Image via Jan Kranendonk

 

Personal aerial vehicles (PAV) are coming in droves. Does it make sense to let the general populous fly them all over the place? The European Commission (EC) wants to know.

 

A €4.3 million euro EC research project called "MyCopter" will focus helicopter-style PAVs. The project will feature automatically flying vehicles as they swarm around each other. The choice of helicopter based transport is due to the fact a runway is not needed, a vertical takeoff is possible from a parking space. Unlike the 2,500 feet need for the Terrafugia Airplane Car.

 

MyCopter will start with 10 quad-copter robots. A research team from the University of Liverpool, UK, and the Swiss Federal Institute of Technology in Lausanne (EDFL) will be going over sensing, collision avoidance, communications, and speed and reliability of other wireless services like GPS for autonomous flight. Dario Floreano's team from EPFL have created 360 degree vision and acoustic systems for the 10 bots in the study. When visibility is low Floreano said, "You can work out the speed and direction of approaching aircraft from the sound they make [via the acoustic sensors]."

 

A set of rules for autonomous flight will eventually come from this research project. Will all of us start fly flying around anytime soon though?

 

Eavesdropper