It had been a busy weekend. On the Friday I'd been down to Mum's after work to pack some tiems away before the builders came. Saturday saw me off doing another of my weekend activities on Wensleydale Railway, where what I'd hoped to be a nice relaxing day saw track work at the crossing I was manning - so much for peace and quiet.
On arriving home I found a couple of parts on my doorstep. Ah yes. Time to do a bit of repair work. My HF vertical had become poorly over the winter, it had gained rather a lopsided look. Plan A had been to sleeve where it was joined to the insulating section at the base, but when we took it into the workshop it was just two of the rivets that had loosened up. So these were drilled out and replaced. The feed point was doing most of the support work here, so we added another rivet here.
Why not just bolt the thing together? Well unless you like to try to fit a nut and washer 12 inches inside a 2 1/2 diameter tube we didn't think there would be any point.
Okay so what effect did it have? Well I landed 9A9RR on EU-136 with a 57 report despite me showing about a 2.5:1 SWR on 14.260MHz. Now the case was that the antenna had been tuned up at the digital portions of the bands (40, 20, 15 & 10) as that's my usual mode of working. So the conclusion is that it's now a lot happier, the bandwidth has dropped, possible as now the electrical connection between the feed and the element is somewhat better. There are tuned radials fitted, I've not adjusted them this time, and they are about 8 ft off the ground. This antenna is no longer made (EVX-4000) as it's required regular maintainance, plenty of silicone to stop water getting into the 20m trap and the plentiful use of self amalgamating tape where the tubes are jointed. I can't complain, I have 6 years use out of it so far and my squeeze a couple more out yet until I decide what to replace it with. My postage stamp garden suits this one, although when I lower it on the mast I haven't much room at the end of the garden to play with.
Sunday was busy too - this time near Dent in Cumbria. To provide communications to the ambulance at the bottom of the hill at Lea Yeat, I was stationed not far from the summit of the Coal Road to Garsdale with my 6m/20ft portable mast and a talkthrough radio. In the end we only had messages relating to them arriving, setting up and finishing without incident, but they are in a hole radio wise.
I haven't decided what to do with the temperamental 6m beam as yet. I will however give it another try before I think about getting rid and sorting a HB9CV for the band. I have one for 2m, it's been used portable, and got me into Southern England from home on the 20ft mast with 30W on SSB.