Skip navigation

community

1 2 3 ... 5 Previous Next

Black Box Network Services

71 Posts tagged with the black_box tag
0

Remote access is the ability to access a network, a personal computer, a server, or other device from a distance for the purpose of controlling it or to access data. Today, remote access is usually accomplished over the Internet, although a local IP network, telephone lines, cellular service, or leased lines may also be used.

 

Remote access is a very general term that covers a wide range of applications from telecommuting to resetting a distant server. Here are just a few of the applications that fall under the remote access umbrella:

 

Remote network access
A common use for remote access is to provide corporate network access to employees who work at home or are in sales or other traveling positions. This kind of remote access typically uses IPsec VPN tunnels to authenticate and secure connections.

 

Remote desktop access
Remote desktop access enables users to access a computer remotely from another computer and take control of it as if it were local. This kind of remote control requires that special software—which is included with most operating systems—be installed and enabled. It’s often used by those who travel frequently to access their “home” computer, and by network administrators for remote server access. This remote access method has some inherent security concerns and is usually incompatible with firewalls, so it’s important to be aware of its limitations and use adequate security precautions.

Remote KVM access
A common application in organizations that maintain servers across multiple sites is server administration through an IP-enabled KVM switch. These IP-addressable switches support one or more servers and have an integral Web server, enabling users to access them over the Internet through a Web browser. Because they’re intended for Internet use, these switches offer authentication and encryption for secure connections.

Remote power management
Anyone who’s ever had to get out of bed in the middle of the night to go switch a server off and back on again to reset it can appreciate the convenience of remote power management. Remote power managers have a wide range of capabilities ranging from simple power switching to reboot a device to sophisticated power monitoring, reporting, and management functions.

Remote environmental security monitoring
Remote environmental and security monitoring over the Internet is increasingly popular, largely because of the cost savings of using existing network infrastructure rather than a proprietary security system. This application requires IP-addressable hubs that support a variety of sensors ranging from temperature and humidity to power monitors. Some models even support surveillance cameras.

 

Cost savings for you

With today’s ubiquitous Internet availability, remote access is increasingly popular and often results in significant cost savings by enabling greater network access and reducing travel to remote sites.

0

Voice over Internet Protocol, or VoIP, is a great cost-saving alternative to traditional telephone services that enables voice data to be transported over IP networks, like the Internet, instead of the public switched telephone network (PSTN) or a cellular network.

 

Because VoIP is inexpensive, has a worldwide reach, and operates on a few simple principles, it’s exploded in popularity in recent years—especially among both small and large businesses that incur significant long-distance telephone expenses. However, it’s not all fun and free calls. Below are six things to consider when you’re deciding whether or not to invest in VoIP.

1. Regulation vagaries
Much of the government regulation of VoIP is still being worked out. The U.S. government hasn’t decided whether VoIP is going to be regulated as phone service or whether to tax it. VoIP isn’t available worldwide because some governments fear the loss of tax revenue or control.

2. Compatibility
Although older VoIP equipment may still have some compatibility issues, current VoIP products from different vendors generally work together.

3. Cost
For all the popular talk about VoIP being free, it isn’t truly free. Any VoIP system has costs associated with its implementation—equipment, high-speed Internet access, and gateway service. So, although it’s inexpensive, it’s a long way from being free. For organizations with a high volume of long-distance calls, especially to international locations, VoIP almost always pays for itself quickly. However, private users or organizations with a low volume of long-distance calls primarily within the U.S., may find that a standard service is actually more economical in the short- to mid-term.

4. QoS
VoIP depends on having a fast, reliable network to operate. A fast network connection with guaranteed bandwidth is not a problem in a corporate intranet where you have complete control over the network. However, if you’re using the Internet for VoIP, you’re using a public network that may be subject to slowdowns that cause drop-outs and distortion. You may find that your high-speed Internet connection is faster than the actual Internet and that the quality of your connection is generally unacceptable or is unacceptable at times when Internet usage is high.

There are four common network issues that can cause problems with a VoIP system:
- Latency is a delay in data transmission. With VoIP, this usually results in people speaking over one another because neither can tell when the other is finished talking.
- Loss. Losing a small percentage of voice transmission doesn’t affect VoIP, but too much (more than 1%) compromises the quality of the call.
- Jitter—is common to congested networks with bursty traffic. Jitter can be managed to some degree with software buffers.
- Sequence errors—or changes in the order of packets when they’re recompiled at the receiving station, degrades sound quality.

5. Emergency services
If you subscribe to a VoIP gateway service that enables you to use your VoIP phone like a regular phone, be aware that you may not be able to call 911 for emergencies. If 911 service is important to you because you don’t have an alternative way to call 911, shop for a VoIP provider who does provide this service.

Consider, too, that VoIP needs both working Internet access and power to work. If you lose your Internet service, your phone goes, too. And, unlike regular phone service that can keep basic telephones working when the power goes out, VoIP needs power—if you lose power, you lose your phone.

6. Moving forward
Before VoIP technology becomes truly universal; the current worldwide PSTN will have to migrate to a packet-based IP equivalent. Industry inertia alone dictates this will not occur instantly. The current worldwide PSTN system has grown to what it is over a period of 125 years. Given the sheer complexity of the existing PSTN, the migration to an IP packet network will probably occur during several decades.

As migration from the PSTN to IP-based networks proceeds, businesses and home users will gradually discover reasons of their own to implement VoIP. It won’t happen right away, but we predict that VoIP will become a big part of telecommunications in the not-so-distant future.

Although it’s not quite as convenient as conventional phone service, VoIP can offer serious savings—particularly if you now regularly pay for multiple overseas phone calls. Keep in mind though, VoIP isn’t a one-size-fits-all solution. But with a little planning, VoIP could spell savings for you.

0

Fiber optic cable not only gives you immunity to interference and greater signal security, but it’s also constructed to insulate the fiber’s core from the stress associated with use in harsh environments.

The core is a very delicate channel that’s used to transport data signals from an optical transmitter to an optical receiver. To help reinforce the core, absorb shock, and provide extra protection against cable bends, fiber cable contains a coating of acrylate plastic.

In an environment free from the stress of external forces such as temperature, bends, and splices, fiber optic cable can transmit light pulses with minimal attenuation. And although there will always be some attenuation from external forces and other conditions, there are two methods of cable construction to help isolate the core: loose-tube and tight-buffer construction.

In a loose-tube construction, the fiber core literally floats within a plastic gel-filled sleeve. Surrounded by this protective layer, the core is insulated from temperature extremes, as well as from damaging external forces such as cutting and crushing.

In a tight-core construction, the plastic extrusion method is used to apply a protective coating directly over the fiber coating. This helps the cable withstand even greater crushing forces. But while the tight-buffer design offers greater protection from core breakage, it’s more susceptible to stress from temperature variations. Conversely, while it’s more flexible than loose-tube cable, the tight-buffer design offers less protection from sharp bends or twists.

 

Resources:

White Paper - Fiber Optic Technology

Fiber Cable Selector

Multicolor Fiber Optic Patch Cables Data Sheet

0

The National Electrical Manufacturers’ Association (NEMA) issues guidelines and ratings for an enclosure’s level of protection against contaminants that might come in contact with its enclosed equipment.

There are many numerical NEMA designations; we’ll discuss NEMA enclosures relevant to our on-line catalog: NEMA 3, NEMA 3R, NEMA 4, NEMA 4X, and NEMA 12.

NEMA 3 enclosures, designed for both indoor and outdoor use, provide protection against falling dirt, windblown dust, rain, sleet, and snow, as well as ice formation.

The NEMA 3R rating is identical to NEMA 3 except that it doesn’t specify protection against windblown dust.

NEMA 4 and 4X enclosures, also designed for indoor and outdoor use, protect against windblown dust and rain, splashing and hose-directed water, and ice formation. NEMA 4X goes further than NEMA 4, specifying that the enclosure will also protect against corrosion caused by the elements.

NEMA 12 enclosures are constructed for indoor use only and are designed to provide protection against falling dirt, circulating dust, lint, fibers, and dripping or splashing noncorrosive liquids. Protection against oil and coolant seepage is also a prerequisite for NEMA 12 designation.

 

Additional resources:

How NEMA standards are developed

How to read a NEMA standard

0

Driving data? Better check the transmission.

Line drivers can operate in any of four transmission modes: 4-wire full-duplex, 2-wire full-duplex, 4-wire half-duplex, and 2-wire half-duplex. In fact, most models support more than one type of operation.

So how do you know which line driver to use in your application?

The deal with duplexing.
First you must decide if you need half- or full-duplex transmission. In half-duplex transmission, voice or data signals are transmitted in only one direction at a time, as in a CB radio conversation. In full-duplex operation, voice or data signals are transmitted in both directions at the same time, as in a telephone conversation.

The entire bandwidth is available for your transmission in half-duplex mode. In full-duplex mode, however, the bandwidth must be split in two because data travels in both directions simultaneously.

Two wires or not two wires? That is the question.
The second consideration you have is the type of twisted-pair cable you need to complete your data transmissions. Generally you need twisted-pair cable with either two or four wires. Often the type of cabling that’s already installed in a building dictates what kind of a line driver you use. For example, if two twisted pairs of UTP cabling are available, you can use a line driver that operates in 4-wire applications, such as the Short-Haul Modem-B Async. Otherwise, you might choose a line driver that works for 2-wire applications, such as the Short-Haul Modem-B Async, 2-wire.

If you have the capabilities to support both 2- and 4-wire operation in half- or full-duplex mode, we even offer line drivers that support all four types of operation.

Still unsure? Consult our Technical Support experts and they’ll help you make your decision.

0

The Fiber Optic Association released Version 1.0.1 of its LossCalc app for the iPhone®, iPad®, and iPod®. This app estimates the optical loss of a fiber optic link. This saves the installer time in determining whether or not test results are reasonable or are pass/fail. The app can also help link designers determine if communications equipment will operate over the link. This second version of the app fixes a bug in saving reports. You can download the app from iTunes®. The app enables users to calculate end-to-end link loss for single-mode and multimode links based on the length of the link, number of connections, and number of splices.

0

The “parts” of a digital signage project can become a tangled web of technologies if not understood as standalone elements and then as a whole. “The 7 Key Elements of Digital Signage” provides clarity and a way to connect the dots on any and all digital signage projects. Keep in mind that every digital signage system contains all of the 7 Key Elements in one form or another and if ignored, can become the weak link in the chain.

 

The following are major questions are broken down into ”The 7 Key Elements of Digital Signage.” By answering each one, you increase your knowledge about the requirements of a project and you increase your probability of success.

 

Hardware

Will the players be mounted in or behind the displays, or in a data closet? How exactly will the displays and appliances be mounted? How many hours a day will the screens be in use? Based on display locations, will you have potential security issues? Do you want to remotely control the display(s)? Will you need to protect screens and equipment from dust, debris, and the elements, as well extremes in temperature or moisture? Will your digital signage installation meet all local and federal codes and requirements?

 

Software

Are you considering a hosted or software as a service (SaaS) solution or a single purchase licensed software solution? Do you want to display information crawls or RSS news feeds to audiences? Does the player software support this? Is the system capable of generating automated e-mail alerts in case of system and/or screen failure? Does the system perform status checks of connected devices and log content play out for reporting purposes? Will touch screens be used in your application, and will the software support them?

 

Connectivity

What is the network configuration? Are there any bandwidth limitations? Will you be sharing a network with other applications outside digital signage? Who specifically will be responsible for installing the equipment and connecting it to the network? For screens located far from a source, what kind of signal distribution are you considering? Are you looking to integrate video from another source into your content feed? Will you be locating signage in an island kiosk or aisle end caps? How do you plan to distribute audio as well as serial control signals?

 

Content

Are there existing content resources to draw from? Who will be responsible for the overall “look and feel” of the content? Do you have graphic designers on staff or the services of a design firm? Can suppliers, vendors, or partners of yours help supply content? Will you need to add audio with your content? Is audio permissible in the environment that you have chosen for the digital signage system?

 

Operations

Will you have a single person administer or multiple people who require passwords and permissions for any specific content? Will you need to integrate additional building operations, such as paging, security, or fire alarms into the digital signage? Will you have someone on-staff to troubleshoot issues and be dispatched to get a screen or player up and running? Are their provisions for proper system backup for operation and storage of content? Have you properly estimated the amount of time it takes not to just implement a system, but also manage it and update it with fresh, relevant content later?

 

Design

Who is the intended audience/viewer? What information do you want to communicate? Are you looking to deploy the signage in more than one location? Looking to deploy your digital signage internationally? Are you planning an incremental roll-out? Do you have a lead person designated to evaluate and test the system?

 

Business

What is the timeline for judgment and what are the repercussions for failure or success? Is the digital signage system based on ROI? Is the digital signage system based on attainment of objectives, aka ROO, and if so, what is the business plan and strategy? Are there participating partners in the project and if so, what is the division of responsibilities and metrics of completion of tasks? When evaluating a supplier for your digital signage system, also ask:

• What does the price include? What are the options?

• Is technical support extra, and who provides that support?

• What are the shipping terms, return policies, and warranties?

• Is training available at no charge, and how good is it?

• How is customer service handled, and how are complaints adjudicated?

 

Being able to understand and answer each of these questions will certainly help you on your journey to digital signage success! Comments? Questions? You can always reach out to one of our Digital Signage Success Managers at 724-873-6553.

0

Networking equipment—especially servers—generates a lot of heat in a relatively small area. Today’s servers are smaller and have faster CPUs than ever. Because most of the power used by these devices is dissipated into the air as heat, they can really strain the cooling capacity of your data center. The components housed in a medium-sized data center can easily generate enough heat to heat a house in the dead of winter!

 

So cool you must, because when network components become hot, they’re prone to failure and a shortened lifespan. Damage caused by heat is not always immediately evident as a catastrophic meltdown—signs of heat damage include node crashes and hardware failures that can happen over a period of weeks or even moths, leading to chronic downtime.

 

It’s also important to ensure that individual cabinets used for network equipment provide adequate ventilation. The temperature inside a cabinet is affected by many variables, including door perforations, cabinet size, and the types of components housed within the cabinet.

 

The most direct way to cool network equipment is to ensure adequate airflow. The goal is that every server, every router, every switch has the necessary amount of air no matter how high or low it is in the cabinet. It takes a certain volume of air to cool a device to within its ideal temperature range. Equipment manufacturers provide very little guidance about how to do this; however, there are some very basic methods you can use to maximize the ventilation within your cabinets.

 

Open it up

Most major sever manufactures recommend that the front and back cabinet doors have at least 63% open area for airflow. You can achieve this by either removing cabinet doors altogether or by buying cabinets that have perforated doors. Because most servers, as well as other network devices, are equipped with internal fans, open or perforated doors may be the only ventilation you need as long as your data center has enough air-conditioning to dissipate the heat load. You may also want to choose cabinets with side panels to keep the air within each cabinet from mixing with hot air from an adjacent cabinet.

 

Equipment placement

Don’t overload the cabinet by trying to fit in too many servers—75% to 80% of capacity is about right. Maintain at least a 1.5” clearance between equipment and the front and back of the cabinet. And finally, ensure all unused rack space is closed off with blank panels to prevent mixing of hot and cold air.

 

Fans and fan placement

You can increase ventilation even more by installing fans to actively circulate air through cabinets. The most common cabinet fans are top-mounted fan panels that pull air from the bottom of the cabinet or through the doors. For spot cooling, use a fan or fan panel that mounts inside the cabinet.

 

For very tightly packed cabinets, chose an enclosure blower—a specialized high speed fan that mounts in the bottom of the cabinet to pull a column of cool air from the floor across the front of your servers or other equipment. An enclosure blower requires a solid or partially vented front door with adequate space—usually at least 4 inches—between the front of your equipment and the cabinet door for air movement.

 

When using fans to cool a cabinet, keep in mind that cooling the outside of a component doesn’t necessarily cool its inside. The idea is to be sure that the air circulates where your equipment’s air intake is. Also, beware of installing fans within the cabinets that work against the small fans in your equipment and overwhelm them.

 

Air conditioning

Air-conditioned cabinets keep equipment cool and save energy because you cool just the cabinet and not the entire room or IT center. ClimateCab models are perfect for harsh environments and remote locations without cooling infrastructures.

 

Temperature monitoring

To ensure that your components are operating within their approved temperature range, it’s important to monitor conditions within your cabinets. The most direct method is to put a thermometer into your cabinet and check it regularly. This simple and inexpensive method can work well for small installations, but it does have its drawbacks—a cabinet thermometer can’t tell you what the temperature inside individual components is, it can’t raise the alarm if the temperature goes out of range, and it must be checked manually.

 

Another simple and inexpensive addition to a cabinet is a thermostat that automatically turns on a fan when the cabinet’s temperature exceeds a predetermined limit.

 

Many network devices come with SNMP or IP-addressable internal temperature sensors to tell you what the internal temperature of the component is. And, there are also cabinet temperature sensors that can alert you over your network.

 

The AlertWerks Environmental Monitor System not only monitors temperature within a cabinet, but also humidity, the presence of water or smoke, airflow, and security as well.

 

It’s easy!

Keeping your data and server cabinets cool doesn’t have to be complicated. Just remember not to overcrowd the cabinets, be sure to provide adequate ventilation, and always monitor conditions within your cabinets.

0

Our VGA Wireless Video Presentation System is back and better than ever! Stop swapping cables every time an individual is ready to present. Go wireless! If you have a meeting room with a VGA projector and you want a roomful of people to have a simple way to share their screens with others, then this affordable, plug-and-play receiver is your solution.

 

This latest version of the popular Wi-Fi receiver not only supports presentation sharing through 4-to-1 split-screen and 1-to-4 projection, it also provides 802.11n Wi-Fi support—delivering up to five times the throughput and greater range of earlier Wi-Fi technology. The 802.11b/g/n compatibility means it can communicate with the latest mobile devices, too. This includes computers, PDA’s or any wireless mobile hand held device running with windows mobile. Plus, the system works as a wireless access point, so laptop users can even access and stream information from the Internet or a wireless LAN.

 

Ideal for college classrooms, auditoriums, business meetings, places of worship, presentations, and video conferencing. It even boasts a range of 300 feet and includes a kit that contains the necessary equipment for wall mounting. For more information on this simple way to improve collaboration in large meeting rooms, go to blackbox.com/go/VPS or watch the demo video below.

 

0

These switches perform as promised year after year, using internal mirrors to optically move data between fiber ports. Air-gap isolation provides a physical break in circuit connections for secure communications. This makes them ideal for government, healthcare, or other applications where a private, data-sensitive network connects to a publicly accessible one.

 

Unlike conventional electronic switches, these switches are not complex devices with vulnerable circuits that you need to closely monitor and protect from intrusion, component failure, or interference.

 

Even without the complexity, they’re reliable in mission-critical environments. Their jewel-like micro-mirrors are bonded to precise positioning servos, controlling the reflections of the optical data beams. Data passes through, maintaining optical communications even when power is removed. The “latching” versions latch mirror movement mechanically into a selected position and hold it there without the need for continuous electrical power.

 

The A/B switch has unique loopback capabilities. Using loopbacks, you can verify the integrity of your backup fiber link while still connected to your primary fiber link. This is especially useful in failover applications where you want to continuously test the “unused” circuit to ensure that it’s available if needed.

 

All Fiber Optic AB, ABC, and ABCD Switches are designed to pass fiber wavelengths and data formats transparently now and in the future. Because they’re compatible with all formats and speeds, there’s no need to upgrade or replace them when your data protocols change and your speeds increase.

0

Session Initiation Protocol (SIP) is used for controlling multimedia communication sessions over an IP network. Common applications include voice over IP (VoIP), videoconferencing, streaming multimedia, on-line gaming, and instant messaging. SIP is the protocol of choice for VoIP, and is used to create, modify, and terminate VoIP sessions, including functions such as call transfer, conference calls, and call hold.

 

This very high-level protocol operates primarily in the Application Layer (Layer 7) of the OSI model. Because SIP runs independently of the Transport Layer (Layer 4), it works with most transport protocols, including TCP and UDP.

 

Much like HTTP, SIP is a text-based protocol. SIP messages contain only as much information as is needed for each session, so it’s very efficient and can expand and contract to meet each application’s specific requirements. This extensibility makes SIP incredibly versatile, enabling it to cover functions ranging from simple VoIP calls to complex multi-user videoconferencing.

 

SIP uses proxy servers to route requests, authenticate users, and provide features such as voice mail. SIP performs five basic functions:

  1. User Location finds another user by way of an address, not unlike an e-mail address.
  2. User Availability determines whether a user answers a request to communicate. A user may be registered under several addresses, in which case SIP may transfer an unanswered call to another address, which may be another device or an application such as voicemail.
  3. User Capabilities checks for compatibility between clients.
  4. Session Setup establishes session parameters for both called and calling party.
  5. Session management handles changes to the call status, including transfer and termination of sessions, modifying session parameters, and invoking new services.
0

This is the fifth and last post in our series on counterfeit and substandard cable.

 

Because of all the publicity counterfeit and substandard cable has  garnered, especially in the past year, we want to explain how Black Box  addresses performance and safety issue through ETL Verification and  independent burn testing.

 

Every three months, an independent Intertek inspector visits us. He goes into our warehouse where he randomly selects  GigaBase® CAT5e and GigaTrue® CAT6 channel components for ETL testing. To ensure that “good” product isn’t  pulled only from the most popular items, he mixes up his product  selection. In one visit, he may choose green jacks to be tested with  white cable. The next, he may choose gray cable and yellow jacks. The  items are then sealed up and sent to the ETL lab for testing.

 

At the same time, he also pulls two CMP cables, 1 CMR cable, and 1 CM  cable, which Black Box sends to an independent testing burn facility to  verify that the bulk cable meets the safely listing marked on the cable  jacket.

 

For more information on our ETL Verified and burn-tested cable, you can go to our product pages for CAT5e and CAT6 cable:
GigaBase CAT5e Cable (EYN844A-PB-1000–EYN861A-PB-1000 series)
GigaTrue CAT6 Cable (EYN864A-PB-1000–EYN881A-PB-1000 series)

 

Want to verify it for yourself? We receive the results every quarter.  If you want more information on our test results, please contact Tech Support.

0

One of the most aggravating infrastructure challenges occurs when you get asked to put a workstation in some inconvenient, too far, difficult-to-wire spot. If there’s a room at the far end of some unused hallway, or a shack at the edge of campus, chances are you’re going to get a request for an Ethernet port there.

 

Whenever you need to put a connection in one of these types of places, your first move should be to check to see if there’s any existing cable that can be adapted for Ethernet by using Ethernet extenders. Most modern buildings have unused voice-grade wires or unused coax. Additionally, many campuses have installed 25- or 50-pair telephone trunk cables between buildings. You can hijack these unused wires for Ethernet use.

 

Ethernet extenders are easy to set up—all you need to do is to plug in one at each end of the twisted-pair wire or coax. Sometimes you’ll also need to set a DIP switch for local or remote operation. Once the Ethernet extenders are installed, there’s nothing to configure, and the extenders are transparent to network operation.

 

Ethernet extenders can often save you the time, aggravation, and expense of pulling new cable. If you have the right cable already installed, Ethernet extenders are definitely the way to go when it comes to putting your network into out-of-the-way or distant locations. Best of all, when you pull off that difficult install, you look like a miracle worker!

0

1. UL® number and hologram: None, fake, or illegitimate. If there is no UL® number or hologram, that's an instant tip-off. Even if there is a number or hologram, you can look up the cable on-line at UL® to see if it's verified. Sometimes, even if there is a legit UL® number, it's possible that it was copied from "good" cable. UL also posts alerts on unauthorized numbers on its website.

 

2. ETL logos. Counterfeiters use them whether they are earned or not. Ask the seller for the ETL test results. You can also check the ETL website for a directory of verified cables.

 

3. Printing/Legend. Is the printing poorly done on the box and the cable? Are there any typographical or grammatical errors?  Check the UL® logo. It should have the letters UL arranged diagonally (descending left to right) with a circle with a small ® symbol directly below the U. Does the cable legend also have the proper markings?

 

4. Color. Does the color match previously bought cable?

 

5. Jacket/construction. Does the cable look like previously purchased cable? Are the conductors straight or oddly "twisty"? Does the jacket feel like a riser or plenum cable? Use a magnet to check that you're getting copper conductors instead of aluminum conductors. Just cut a few pieces of cable and see if a magnet picks them up. If it does, your cable is copper, not aluminum.

 

6. Weight. If the cable box/spool feels light, compare its weight to cable you know performs up to standard. Counterfeit cable and substandard cable often have undersized copper conductors or copper-clad aluminum conductors that weigh half as much as genuine cable.

0

Video standards are changing, moving from analog video to digital video. Digital Video Interface, or DVI, was developed by the Digital Display Working Group (DDWG) to replace the VGA connector standard, the "legacy analog technology." [1]

 

There are some very simple differences between analog and digital video, and simple advantages to switching to digital.

 

Analog signals travel in a sine-like wave form, and digital signals travel in a square-like waveform. Digital signals offer advantages over analog because the wave shape offers multiple places to read the signal and is more accurate. Digital signals are also far less vulnerable to EMI and RFI interference, especially when fiber cable is used to transmit the signals.

 

As a result, systems and KVM switches are moving from HD15 or VGA connectors to DVI connectors. The DVI connectors can either support both analog or digital signals depending on the pinning. DVI-I supports both analog and digital signals while DVI-D only supports digital.

 

Standard resolutions with analog video initially were designed to only 640 x 480 or 800 x 600. They were later stretched to higher resolutions, but the image quality became dependent on many physical factors of the transmission link, and hence more vulnerable to distortion and signal degradation. Upgrading to digital video brings higher resolutions, usually about 1920 x 1200. Using dual-link video effectively doubles the power of transmission and provides an increase in speed and signal quality. Dual-link video resolutions can display resolutions of 2048 x 1536 or even 2560 x 1600. This resolution is supported on high-definition displays, such as 30" LCD monitors and digital signage displays.

 

DVI-D extenders reach up to 460 feet over CATx cable and up to 40 km over single-mode fiber. These distances will improve as the technology for extending signals improves.

 

Black Box offers a number of products for digital video extension, including ServSwitch™ DKM switches and extenders the ServSwitch Agility, and the ServSwitch Wizard Dual-Link DVI.

 

Sources:

[1] http://en.wikipedia.org/wiki/Digital%E2%80%93visual_interface

1 2 3 ... 5 Previous Next