Skip navigation

community

1 2 Previous Next

Black Box Network Services

21 Posts tagged with the cable tag
0

Hopefully most of you don't rely on Big Lots for your cable. At the end of March 2012, UL issued a public warning about the unauthorized use of the UL® mark on packages of CAT5e and USB patch cable. In the warning, UL states that “The products bear an unauthorized UL Mark on the product packaging. The products have not been evaluated by UL to the applicable Standard for Safety and it is unknown if they comply with the UL safety requirements. ”

 

The cables listed in the notices are TriQuest 15-foot CAT5e patch cable, model number 60-0102, and TriQuest 10-foot USB 2.0 patch cable, model number 60-0302. The notice reports that the CAT5e cables first went into production in March 2010 and that 124,300 units were produced. The USB cables went into production in February 2010 and 95,120 units were produced. The cables are manufactured by Sela Products, LLC, and they are made in China.

 

The back of the cable packages is marked with the UL mark in a circle and the words UL Approved. They are not approved, and the use of the UL mark is fraudulent.

 

You can see photos of the cables and read the notice at the UL Website.

ul_mark.jpg

0

Watch this informative video to learn how to identify counterfeit cable. In this short, 3-minute video, Andy Schmeltzer, the “Cable Guy” at Black Box, explains what to look for when you purchase cable. Some tip-offs that a cable may be non-compliant or counterfeit can include a price that seems too good to be true, specs or lack thereof, a lighter weight than expected, and more.

 

If you have questions about cable construction and specs, contact our FREE, 24-hour tech support at 724-746-5500.

 

0

When most people think of counterfeit and substandard cable, they think of bulk cable and their backbone and horizontal runs. But don’t underestimate the importance of patch cables in your channel. Patch cables are the most overlooked component of the Channel Link. Remember the saying, “A chain is only a strong as its weakest link?” The same principle applies to the Channel Link. If a patch cable is non-compliant, it can ruin expensive electronics, invalidate warranties, cause poor network performance, and lead to a loss in productivity. Risky business.

 

The CCCA did large-scale performance testing of Category 6 copper patch cords. Test results showed an 85% failure rate in cables produced offshore by companies who are largely unknown in North America. 78% of the failing samples failed NEXT tests by a margin of 3 dB or more. A second sample set of Category 6 copper patch cords produced by multiple, well-recognized manufacturers was also tested and showed a 0% failure rate.

 

Other patch cord issues include non-compliant plugs that don't meet requirements. Problems can include substandard gold plating on the contacts, plating that erodes and corrodes, and contact spacing and dimensional issues that can cause intermittent connections and link loss. If you have poor network performance, the cost to identify the problem and to replace all your patch cables could be quite expensive indeed.

 

How can you spot substandard patch cable?

Patch cables are usually not supplied by the structured cabling installer but instead they're often purchased by someone in the IT department, who frequently buys them on-line based on price. Just because a cable is advertised as CAT6, it doesn’t mean it’s compliant. Your first tip-off that a cable is substandard is price. If it’s significantly less than what you would expect to pay at Black Box (or any other brand-name manufacturer), it's probably counterfeit. In a recent sampling of patch cable on the Web, we found significant differences in prices. For a 3-foot CAT5e cable, our suspect cable came in at $.85 as compared to $5.45 for our premium GigaBase® cable. For CAT6 cable, we found a 3-foot cable priced at $1.10 as compared to $9.45 for our premium GigaTrue® cable. These low prices are a serious indication the cable is substandard.

 

Another way to check for inferior cable is to smell it. Some non-compliant cables have a plasticizer issue with the jacketing, which can produce a bad odor. See if the cable feels oily or too stiff. Both are indicators of counterfeit cable. Check the modular plug. It should be intact and not cracked. It should also be made for a fire-resistant plastic. To test this, put a lighter to the clip. If it catches fire and does not self-extinguish, it is substandard. The gold contacts should not be too shiny. Often substandard contacts appear shinier than true gold contacts. Lastly, check the boot to make sure it is not pinching or crushing the cable.

2

Thought you knew your fiber stuff? Check out these four myths:

 

Myth #1: Fiber is too expensive.

Fiber used to be more expensive than copper. Today, however, because manufacturing costs are down and terminations are easier, fiber is often less expensive than the equivalent copper installation. Once installed, fiber optic maintenance costs are significantly less than copper ones.

 

Myth #2: Fiber is difficult to install.

In the old days of grind-and-polish connectors, installing fiber optic cable was a difficult, precise business that required a specialist. But improvements in fiber optic terminations and technologies have made them as easy to terminate as CATx connectors, and now many technicians prefer to install fiber because of its smaller diameter, lighter weight, and ease of testing.

 

Myth #3: Fiber is fragile.

Although terminating fiber cable does require some care to avoid breaking the glass core, in other respects, fiber is actually more robust than copper. Fiber optic cable can withstand a higher pulling tension than copper, is rated for larger temperature ranges, and is immune to EMI/RFI interference. In fact, one of the reasons the military prefers fiber is for its ruggedness and survivability. 

 

Myth #4: Fiber is impossible to hack.

Because a copper cable “leaks” electromagnetic signals, a hacker can read data nearby without actually touching the cable. A fiber cable, on the other hand, uses light that stays within the cable, so a hacker must physically tap into it to gain access to data. So it’s true that fiber cable is more secure than copper cable, but it’s not true that it’s impossible to hack—all that’s needed is a network tap and physical access to the cable. For this reason, it’s important to secure fiber optic cable by protecting it from unauthorized tampering and by encrypting data that must be kept private.

0

Fiber optic cable not only gives you immunity to interference and greater signal security, but it’s also constructed to insulate the fiber’s core from the stress associated with use in harsh environments.

The core is a very delicate channel that’s used to transport data signals from an optical transmitter to an optical receiver. To help reinforce the core, absorb shock, and provide extra protection against cable bends, fiber cable contains a coating of acrylate plastic.

In an environment free from the stress of external forces such as temperature, bends, and splices, fiber optic cable can transmit light pulses with minimal attenuation. And although there will always be some attenuation from external forces and other conditions, there are two methods of cable construction to help isolate the core: loose-tube and tight-buffer construction.

In a loose-tube construction, the fiber core literally floats within a plastic gel-filled sleeve. Surrounded by this protective layer, the core is insulated from temperature extremes, as well as from damaging external forces such as cutting and crushing.

In a tight-core construction, the plastic extrusion method is used to apply a protective coating directly over the fiber coating. This helps the cable withstand even greater crushing forces. But while the tight-buffer design offers greater protection from core breakage, it’s more susceptible to stress from temperature variations. Conversely, while it’s more flexible than loose-tube cable, the tight-buffer design offers less protection from sharp bends or twists.

 

Resources:

White Paper - Fiber Optic Technology

Fiber Cable Selector

Multicolor Fiber Optic Patch Cables Data Sheet

0

This is the fifth and last post in our series on counterfeit and substandard cable.

 

Because of all the publicity counterfeit and substandard cable has  garnered, especially in the past year, we want to explain how Black Box  addresses performance and safety issue through ETL Verification and  independent burn testing.

 

Every three months, an independent Intertek inspector visits us. He goes into our warehouse where he randomly selects  GigaBase® CAT5e and GigaTrue® CAT6 channel components for ETL testing. To ensure that “good” product isn’t  pulled only from the most popular items, he mixes up his product  selection. In one visit, he may choose green jacks to be tested with  white cable. The next, he may choose gray cable and yellow jacks. The  items are then sealed up and sent to the ETL lab for testing.

 

At the same time, he also pulls two CMP cables, 1 CMR cable, and 1 CM  cable, which Black Box sends to an independent testing burn facility to  verify that the bulk cable meets the safely listing marked on the cable  jacket.

 

For more information on our ETL Verified and burn-tested cable, you can go to our product pages for CAT5e and CAT6 cable:
GigaBase CAT5e Cable (EYN844A-PB-1000–EYN861A-PB-1000 series)
GigaTrue CAT6 Cable (EYN864A-PB-1000–EYN881A-PB-1000 series)

 

Want to verify it for yourself? We receive the results every quarter.  If you want more information on our test results, please contact Tech Support.

0

1. UL® number and hologram: None, fake, or illegitimate. If there is no UL® number or hologram, that's an instant tip-off. Even if there is a number or hologram, you can look up the cable on-line at UL® to see if it's verified. Sometimes, even if there is a legit UL® number, it's possible that it was copied from "good" cable. UL also posts alerts on unauthorized numbers on its website.

 

2. ETL logos. Counterfeiters use them whether they are earned or not. Ask the seller for the ETL test results. You can also check the ETL website for a directory of verified cables.

 

3. Printing/Legend. Is the printing poorly done on the box and the cable? Are there any typographical or grammatical errors?  Check the UL® logo. It should have the letters UL arranged diagonally (descending left to right) with a circle with a small ® symbol directly below the U. Does the cable legend also have the proper markings?

 

4. Color. Does the color match previously bought cable?

 

5. Jacket/construction. Does the cable look like previously purchased cable? Are the conductors straight or oddly "twisty"? Does the jacket feel like a riser or plenum cable? Use a magnet to check that you're getting copper conductors instead of aluminum conductors. Just cut a few pieces of cable and see if a magnet picks them up. If it does, your cable is copper, not aluminum.

 

6. Weight. If the cable box/spool feels light, compare its weight to cable you know performs up to standard. Counterfeit cable and substandard cable often have undersized copper conductors or copper-clad aluminum conductors that weigh half as much as genuine cable.

0

Earlier this year, the CCCA (Communications Cable and Connectivity Association) commissioned a white paper after it tested cables from offshore manufacturers and found that many failed to comply with fire safety specifications. It found that many of the cables are made from low-fire performing materials making them highly combustible. This means trouble for contractors.

 

The paper was commissioned from the law firm of Crowell Moring to look at potential liability for contractors who install communications cables that do not comply with NEC (National Electrical Code) requirements.

 

In the white paper, Crowell Moring studied the laws in Connecticut, Virginia, and Florida.  Because each state incorporates NEC into its building codes, a violation of those codes is a state violation. Crowell Moring explains, “Any installed cable that fails to meet the NEC standards, whether known, apparent, or not, opens a contractor up to penalties for those failures.”

 

The paper concludes that contractors who install CMR or CMP cable may face liability based on violations of building codes. If a contractor installs non-compliant cable that causes damage, such as a fire, the contractor can also be held liable in civil lawsuits.

 

The paper states that "A contractor need not have actual knowledge that the cable is non-compliant to be found negligent. If a contractor knew it installed non-compliant cable, but said it was compliant, the contractor can be charged with fraud. And lastly, if a contractor installs non-compliant cable, either knowingly or unknowingly, the contractor is liable for breach of contract and warranty claims.”

 

As a contractor you may face exposure to legal liability. The white paper says you can avoid this liability by carefully, “selecting, purchasing, and installing cable that complies with NEC standards.”  In addition to the white paper, information on non-compliant cables and best practices for purchasing compliant cables can be found at the CCCA website.

0

One of the hottest topics during the past year has been the legal wrangling over counterfeit cable. Last year, Anixter sued Commodity Cables, Inc. The suit alleges that Commodity Cables sold substandard off-shore-manufactured cable that did not meet flame- and fire-resistance standards established by UL® and the National Fire Protection Association. Some of the cable in question was marked as being UL® certified or ETL Verified. Anixter is seeking $1 million in damages plus punitive damages for false advertising, unfair competition, breach of contact, and deceptive trade practices.

 

The basis of the suit stems from when Anixter said it discovered numerous boxes of cable with apparently fraudulent UL marks. Anixter sent the cables to UL for burn testing, which they failed. In December 2010, Anixter recalled all its Commodity Cables products from customers. Anixter has also worked with many customers to remove and replace the substandard cable.

 

In June 2011, Commodity Cables countersued Anixter. The counterclaim is a defamation allegation.

 

More information on the history of the suits can be found at Cabling, Installation & Maintenance. Or, read more about how to avoid unsafe, unapproved, or counterfeit cable.

0

Here at Inside the Box, we’re always trying to find stellar content and industry news. One of the hottest topics in the cabling industry today is the prevalence of counterfeit cable. In a nutshell, counterfeit cable is imported cable marked and advertised as compliant to North American fire codes and industry standards, but it's not—even though the cable may carry UL® and ETL marks. The subject is extremely serious because of public safety and liability issues about fire and network performance. In addition, there are also legal and cost issues related to contractor liability.

 

Today, we want to share the presentation given at the September 2011 BICSI conference by the CCCA (Communications Cable & Connectivity Association). The presentation, titled Non-Compliant Cabling Products: How Big Is the Problem and What Can be Done?, focuses on codes and standards in the cabling industry, as well as what your risks are when installing non-compliant cable.

 

Founded in 2007, the CCCA is a non-profit association committed to ensuring all cabling products in North America comply with existing codes and standards. The association is growing, and members include many of the industry's top cabling manufacturers.

 

The CCCA has also done other studies on counterfeit and substandard cables. The results point to the importance of purchasing cable from known sources (such as us!). You can also check verified cable directories on the UL® and ETL websites. Look for authentic marks and labels on the cable, too. For example, in October 2010, UL® started requiring the use of holographic labels on cable.

 

For more studies and presentations by the CCCA, check out their blog.

0

Most cables are constructed with standard polymer jackets, which are combustible. Copper and aluminum are the most common metals used as conductors. Unfortunately, they’re good conductors of heat. The conductors can spread a fire by igniting surrounding flammable materials, such as the cable jacket. Then the jacket burns away, the conductors melt together, and the size of the cable bundle shrinks and causes gaps to develop within the cabling opening. This can be a major fire risk.

 

Firestopping is a term used to describe sealing and protecting openings and other joints between the cable and edges of the floor, wall, or ceiling. Firestopping was first practiced on U.S. combat ships in the 1960s. The walls and floors of the ships had steel tubes, which allowed conduits to pass through. Then, non-burning material was stuffed between the gaps, preventing the spread of fire and smoke. It wasn’t until the 1970s when larger companies began producing firestopping materials.

 

A successful firestop plan requires careful planning. Here are three tips to help you meet the needs of future cabling requirements and fire protection:

 

#1. Think long term

Most people tend to underestimate the size of the openings required for cabling and often forget about future expansion. When planning on how large to make the opening to run your cable, you must consider the diameter of the cable itself, how much room you need for firestopping materials, and whether you’ll be adding more cables in the future.

#2.  Different cabling systems require different firestops
There are two basic types of cabling systems: permanent and retrofittable. Permanent cabling systems, such as electrical cables, do not change. But most cabling systems, such as data and voice, have to accommodate moves, adds, and changes so they need to be retrofittable. You use different firestops with each system.

In permanent installations, a sealant is used in and around the cables. This is also appropriate for external areas, including conduits and sleeves.

In retrofittable systems, firestops need to be removed and reinstalled easily as cable needs change. Common firestops include pillows, putty, and fire-rated pathways. These products are packed in and around a cable bundle rather than being injected the way sealant is. The product to use often depends on the size of the cable opening and the frequency of changes.

 

#3. Use the proper materials

There are two basic types of materials used in firestopping: Passive firestopping uses nonintumescent materials, which draw heat away or insulate the cables. Passive materials include mortars, silicone sealants, foam, and grout. Cabling runs with passive firestopping are generally thicker and are more limited in the types of cables they can protect.

Intumescent materials expand when exposed to heat or fire and compensate for the loss of mass in cable bundles. They’re a good choice for sealing and surrounding cable holes and runs.

0

We’ve focused on the importance of network security before, and if you remember, it all starts with getting physical. Now you can boost your physical network security starting at the port. Here’s one of the simplest and inexpensive, yet most effective ways you can increase your Layer 1 security. Lock up your network ports with LockPORT Security Locking Patch Cables. They stay locked in place until you take them out. Or, as Christina Hansen from CableOrganizer.com’s Product Showcase says, “removal only with approval.”

 

If people—whether they’re personnel, visitors, or those with evil on their mind—can’t disconnect your network cables, they can’t tamper with your network and bring it down. Another danger to your network are cable connections that work loose over time or are accidentally knocked out. Loose and poor cable connections are one of the biggest causes of network downtime. And, it’s why the first question Help Desk technicians ask is: “Did you check the cable connection?” Whether from accidental or intentional disconnects, once your network goes down, you could spend hours and hours trying to pinpoint where the problem lies.

 

Two levels of security

LockPORT gives you two different locking cable choices. Both feature the same patented LockPORT boot. What differs are the patented clip inserts. Best of all, the clips are interchangeable so if you're application changes, all you do is move a clip from one cable to another instead of buying more cables.

 

For absolute port security, choose the red Key Locking cable. It secures cables in place and can only be removed by you with the Removal Tool. This is the “removal only with approval” lock.

 

To prevent accidental disconnects, but to give people access to ports, use the green Secure Locking cable. It holds the cable in place and eliminates disconnects from jostling and general wear and tear.

 

Publicly perfect.

Use LockPORT cables to prevent network tampering in public areas like hospitals, airports, hotels, and shops. It’s perfect for educational settings as well, providing a foolproof way to secure network connections in classrooms and training rooms. And, it’s a great and inexpensive way to turn your CAT5e/6 and fiber cables into a Layer 1 security tool.

 

Download the LockPORT Brochure, or see how LockPORT cables can secure your network ports in the video below:

 

0

There are two primary organizations dedicated to developing and setting structured cabling standards. In North America, standards are issued by the Telecommunications Industry Association (TIA), which is accredited by the American National Standards Institute (ANSI). The TIA was formed in April 1988 after a merger with the Electronics Industry Association (EIA). That’s why its standards are commonly known as ANSI/TIA/EIA, TIA/EIA, or TIA.

Globally, the organizations that issue standards are the International Electrotechnical Commission (IEC) and the International Organization for Standardization (ISO). Standards are often listed as ISO/IEC. Other organizations include the Canadian Standards Association (CSA), CENELEC (European Committee for Electrotechnical Standardizations), and the Japanese Standards Association (JSA/JSI).

The committees of all these organizations work together and the performance requirements of the standards are very similar. But there is some confusion in terminology.

The TIA cabling components (cables, connecting hardware, and patch cords) are labeled with a “category.” These components together form a permanent link or channel that is also called a “category.” The ISO/IEC defines the link and channel requirements with a “class” designation. But the components are called a “category.” Follow?

The Standards
Category 5 (CAT5), ratified in 1991, was the de facto standard for 100-Mbps networks during the 1990s. It is no longer recognized by the TIA/EIA for use in data networking.

Category 5e (CAT5e)–ISO/IEC 11801 Class D, ratified in 1999, is designed to enable twisted-pair cabling to support full-duplex, 4-pair transmission in 100-MHz applications. The CAT5e standard added more headroom and established new requirements to support Gigabit Ethernet over a worst case four-connector channel. These include stricter specs for Near-End Crosstalk (NEXT) and Return Loss (RL). The standard also introduced the required measurements for Power Sum Near-End Crosstalk (PS-NEXT), Equal-Level Far-End Crosstalk (EL-FEXT), and Power Sum Equal-Level Far-End Crosstalk (PS-ELFEXT). CAT5e is still used in many organizations, although it is no longer recognized for new installations.

Category 6 (CAT6)–Class E has a specified frequency of 250 MHz, significantly improved bandwidth capacity over CAT5e, and easily handles Gigabit Ethernet transmissions. In recent years, it has been the cable of choice for new structured cabling systems. CAT6 supports 1000BASE-T and, depending on the installation, 10GBASE-T (10-GbE).

10-GbE over CAT6 introduces the problem of Alien Crosstalk (ANEXT), the unwanted coupling of signals between adjacent pairs and cables. Because ANEXT in CAT6 10-GbE networks is so dependent on installation practices, TSB-155 qualifies 10-GbE over CAT6 up to 55 meters and requires it to be 100% tested. To mitigate ANEXT in CAT6, it is recommended that you unbundle the cables and increase the separation between the cables.

Augmented Category 6 (CAT6a)–Class Ea was ratified in February 2008. This standard calls for 10-Gigabit Ethernet data transmission over a 4-pair copper cabling system up to 100 meters. CAT6a extends CAT6 electrical specifications from 250 MHz to 500 MHz. It introduces the ANEXT requirement. It also replaces the term Equal Level Far-End Crosstalk (ELFEXT) with Attenuation to Crosstalk Ratio, Far-End (ACRF) to mesh with ISO terminology. CAT6a provides improved insertion loss over CAT6. It is a good choice for noisy environments with lots of EMI. CAT6a is also well-suited for use with PoE+.

CAT6a UTP cable is significantly larger than CAT6 cable. It features larger conductors, usually 22 AWG, and is designed with more space between the pairs to minimize ANEXT. The outside diameter of CAT6a cable averages 0.29–0.35" compared to 0.21–0.24" for CAT6 cable. This reduces number of cables you can fit in a conduit. At a 40% fill ratio, you can run three CAT6a cables in a 3/4" conduit vs. five CAT6 cables.

There are two types of CAT6a cable, UTP and F/UTP. For a discussion of the differences, see the white paper in our Resources section.

Category 7 (CAT7)–Class F was published in 2002 by the ISO/IEC. It is not a TIA recognized standard. Class 7 specifies minimum performance standards for fully shielded cable (individually shielded pairs surrounded by an overall shield) transmitting data at rates up to 600 MHz. It offers greater capacity for demanding applications such as broadband video. It’s also well suited for applications where fiber optic cable would typically be used—but it costs less. Because each CAT7 pair is fully shielded, it's ideal for areas prone to EMI/RFI. Class 7 cable offers two connector styles: the standard RJ plug and a non-RJ-style plug and socket interface specified in IEC 61076-2-104:2.

Category 7a (CAT7a)–Class Fa is currently in ISO standards for channel performance in Amendment 1, recently component performance has been ratified in Amendment 2. The formal names are ISO 11801 Amendment 1 (2008) and ISO 11801 Amendment 2 (2010). Class Fa cable is a fully shielded cable that extends frequency from 600 MHz to 1000 MHz. It can easily handle 10-GbE and offers users a lifespan of 15 years or more. It has even been discussed that Class Fa cable is the future for 40GBASE-T or more.

 

Now that you’ve memorized the alphabet soup of cabling, how about a test? Just kidding. For a comparison chart of category performance standards, see the Buyer's Guide in the Resources section. Questions? E-mail info@blackbox.com.

0

Configurators and Selectors are interactive tools that make it even easier for you to get the solutions you need. Whether it’s cables, cabinets, or KVM, we provide simple to use guides that help make your decisions a snap.

CATx Cable Selector
Quickly find the exact CAT5/5e/6/6a/7 cable you need.

Custom Cable and Adapter Configurator
Design your custom cable or adapter and submit your request to our engineers for review. A Black Box representative will contact you, typically in 24 hours or less, to confirm your order.

KVM Switch Selector
Find the perfect ServSwitch™ KVM solution for your application.

Cabinet Configurator
Twenty seconds to configure, two days to ship. Build your ideal cabinet, configured to your specs and shipped in two business days.

Wallmount Cabinet Selector
Select wallmount features in the order of your priorities and get a list of matching cabinets.

0

If you’re accustomed to certifying copper cable, you’ll be pleasantly surprised at how easy it is to certify fiber optic cable because it’s immune to electrical interference. You only need to check a few measurements.

 

Attenuation (or decibel loss)—Measured in decibels/kilometer (dB/km), this is the decrease of signal strength as it travels through the fiber cable. Generally, attenuation problems are more common on multimode fiber optic cables.

 

Return loss—This is the amount of light reflected from the far end of the cable back to the source. The lower the number, the better. For example, a reading of -60 decibels is better than -20 decibels. Like attenuation, return loss is usually greater with multimode cable.

 

Graded refractive index—This measures how the light is sent down the fiber. This is commonly measured at wavelengths of 850 and 1300 nanometers. Compared to other operating frequencies, these two ranges yield the lowest intrinsic power loss (NOTE: This is valid for multimode fiber only.)

 

Propagation delay—This is the time it takes a signal to travel from one point to another over a transmission channel.

 

Optical time-domain reflectometry (OTDR)—This enables you to isolate cable faults by transmitting high-frequency pulses onto a cable and examining their reflections along the cable. With OTDR, you can also determine the length of a fiber optic cable because the OTDR value includes the distance the optic signal travels.

 

There are many fiber testers on the market today. Basic fiber optic testers function by shining a light down on end of the cable. At the other end, there’s a receiver calibrated to the strength of the light source. With this test, you can measure how much light is going to the other end of the cable. Generally these testers give you the results in dB lost, which you can then compare to the loss budget. If the measured loss is less than the number calculated by your loss budget, you installation is good.

 

Newer fiber optic testers have an even broader range of capabilities. They can test both 850- and 1300-nanometer signals at the same time and can even check your cable for compliance with specific standards.

 

Precautions to take when using fiber

 

Intrinsic power loss—As the optic signal travels through the fiber core, the signal inevitably loses some speed through absorption, reflection, and scattering. This problem is easy to manage by making sure your splices are good and your connections are clean.

 

Microbending—These are minute deviations in fiber caused by excessive bends, pinches, and kinks. Using cable with reinforcing fibers and other special manufacturing techniques minimizes this problem.

 

Connector loss—This occurs when two fiber segments are misaligned. This problem is commonly caused by poor splicing. Scratches and dirt introduced during the splicing process can also cause connector loss.

 

Coupling loss—Similar to connector loss, coupling loss results in reduced signal power and is from poorly terminated connector couplings. Remember to be careful and use common sense when installing fiber cable. Use clean components. Keep dirt and dust to a minimum. Don’t pull the cable excessively or bend it too sharply around corners.

 

These properties particular to fiber optic cable can cause problems if you aren’t careful during installation.

 

For more cabling tips visit our resources page.

1 2 Previous Next