Hopefully most of you don't rely on Big Lots for your cable. At the end of March 2012, UL issued a public warning about the unauthorized use of the UL® mark on packages of CAT5e and USB patch cable. In the warning, UL states that “The products bear an unauthorized UL Mark on the product packaging. The products have not been evaluated by UL to the applicable Standard for Safety and it is unknown if they comply with the UL safety requirements. ”
The cables listed in the notices are TriQuest 15-foot CAT5e patch cable, model number 60-0102, and TriQuest 10-foot USB 2.0 patch cable, model number 60-0302. The notice reports that the CAT5e cables first went into production in March 2010 and that 124,300 units were produced. The USB cables went into production in February 2010 and 95,120 units were produced. The cables are manufactured by Sela Products, LLC, and they are made in China.
The back of the cable packages is marked with the UL mark in a circle and the words UL Approved. They are not approved, and the use of the UL mark is fraudulent.
You can see photos of the cables and read the notice at the UL Website.