Skip navigation

community

Black Box Network Services

5 Posts tagged with the kvm_switch tag
0

Remote access is the ability to access a network, a personal computer, a server, or other device from a distance for the purpose of controlling it or to access data. Today, remote access is usually accomplished over the Internet, although a local IP network, telephone lines, cellular service, or leased lines may also be used.

 

Remote access is a very general term that covers a wide range of applications from telecommuting to resetting a distant server. Here are just a few of the applications that fall under the remote access umbrella:

 

Remote network access
A common use for remote access is to provide corporate network access to employees who work at home or are in sales or other traveling positions. This kind of remote access typically uses IPsec VPN tunnels to authenticate and secure connections.

 

Remote desktop access
Remote desktop access enables users to access a computer remotely from another computer and take control of it as if it were local. This kind of remote control requires that special software—which is included with most operating systems—be installed and enabled. It’s often used by those who travel frequently to access their “home” computer, and by network administrators for remote server access. This remote access method has some inherent security concerns and is usually incompatible with firewalls, so it’s important to be aware of its limitations and use adequate security precautions.

Remote KVM access
A common application in organizations that maintain servers across multiple sites is server administration through an IP-enabled KVM switch. These IP-addressable switches support one or more servers and have an integral Web server, enabling users to access them over the Internet through a Web browser. Because they’re intended for Internet use, these switches offer authentication and encryption for secure connections.

Remote power management
Anyone who’s ever had to get out of bed in the middle of the night to go switch a server off and back on again to reset it can appreciate the convenience of remote power management. Remote power managers have a wide range of capabilities ranging from simple power switching to reboot a device to sophisticated power monitoring, reporting, and management functions.

Remote environmental security monitoring
Remote environmental and security monitoring over the Internet is increasingly popular, largely because of the cost savings of using existing network infrastructure rather than a proprietary security system. This application requires IP-addressable hubs that support a variety of sensors ranging from temperature and humidity to power monitors. Some models even support surveillance cameras.

 

Cost savings for you

With today’s ubiquitous Internet availability, remote access is increasingly popular and often results in significant cost savings by enabling greater network access and reducing travel to remote sites.

0

A KVM switch enables you to control multiple servers and other equipment from one keyboard, monitor, and mouse workstation. KVM switches give you the flexibility to access servers that are down the hall or across “the pond.” How you access your servers depends on a number of things. Before you choose a KVM switching solution, you need to consider some important issues…

 

What type of connection does the controlling keyboard, video display, and mouse have?

Depending on whether they are PS/2®, USB, or some combination of both, your connections determine what type of cabling you need.

 

If you are using USB devices, like keyboards and mice, make sure to purchase a KVM switch with USB support. Older KVMs usually only support PS/2 connections.

 

Do your CPUs require keyboard or keyboard and mouse emulation?

Keyboard emulation and keyboard and mouse emulation are enhanced features of most KVM switches. They enable each CPU to communicate with the switch as if it were directly attached to the controlling keyboard or mouse.

 

What operating system (OS) software do your computers use?

Are all your computers running the same OS? Or, like many organizations, do you have multiple CPUs running different OSs? With the right KVM switch, interconnecting multiple CPUs running different OSs is easy.

 

How close are your users to your servers?

If servers and users are physically close to each other, an analog KVM system will meet your needs. On the other hand, if users require access from remote locations because they travel, or if an IT manager needs to manage a distant data center, a KVM over IP (KVMoIP) system is going to be the best fit for your organization.

 

How many ports do you need? What will your future needs be?

It is advisable to purchase a KVM switch with more ports than you currently need. This way, when you expand your server room or add users, you don’t need to completely replace a small KVM switch with a larger one with more ports. Also, although many KVM switches are cascadable, a KVMoIP system simplifies configuration, usually requiring the addition of IP addresses and updating the authentication database. KVMoIP makes adding servers fast and free of complications (to learn how to do more with less, listen to our recorded webinar on KVMoIP).

 

What are your security needs?

Network security must never be compromised, yet authorized personnel need access. KVM switches use a combination of user authentication, an operating system’s internal security, and Secure Socket Layer (SSL) encryption—among other security features—to ensure that users receive access to those devices to which they are allowed.

 

We have KVM switches that support both USB and PS/2, as well as USB-only models. We also provide multiplatform KVM switches so you can interconnect multiple CPUs that are running on various OSs.  Pick and choose what you need/want with our KVM Selector. Or, call our 24/78/365 Tech Support.

0

Configurators and Selectors are interactive tools that make it even easier for you to get the solutions you need. Whether it’s cables, cabinets, or KVM, we provide simple to use guides that help make your decisions a snap.

CATx Cable Selector
Quickly find the exact CAT5/5e/6/6a/7 cable you need.

Custom Cable and Adapter Configurator
Design your custom cable or adapter and submit your request to our engineers for review. A Black Box representative will contact you, typically in 24 hours or less, to confirm your order.

KVM Switch Selector
Find the perfect ServSwitch™ KVM solution for your application.

Cabinet Configurator
Twenty seconds to configure, two days to ship. Build your ideal cabinet, configured to your specs and shipped in two business days.

Wallmount Cabinet Selector
Select wallmount features in the order of your priorities and get a list of matching cabinets.

0

It should come as no surprise that the federal government is concerned about signal leakage. In fact, its interest goes back to the days of World War II when the Army was trying to exploit weaknesses of enemy combat phones and radio transmitters. Since then, the scope of the government’s interest has broadened beyond the battlefield. In the last 40 years, the National Security Agency (NSA) has taken several industry measurement standards for signal protection and greatly enhanced them.

 

These enhanced criteria are commonly referred to as the TEMPEST standards (although the NSA also calls them EMSEC standards, short for “emissions security”). TEMPEST pertains to technical security countermeasures, standards, and instrumentation that prevent or minimize the exploitation of vulnerable data communications equipment by technical surveillance (AKA eavesdropping!). It involves designing circuits to minimize emanations. Another set of testing standards is called Common Criteria (EAL4+). Both standards are important, but they test for different things.

 

TEMPEST

Many things put your data communications at risk. Any device with a microchip generates an electromagnetic field, often called a “compromising emanation” by security experts. With the proper surveillance equipment, these emanations can be intercepted and the signal reconstructed and analyzed. Unprotected equipment can, in fact, emit a signal into the air like a radio station—and nobody wants to risk his or her job and a whole lot more by broadcasting national security or trade secrets to the wrong people.

 

Some of the most vulnerable equipment includes speakerphones, printers, fax machines, scanners, external disc drives, and other high-speed, high-bandwidth peripherals. And if the snoop is using a high-quality interception devices, your equipment’s signals can be acquired up to several hundred feet away.

 

TEMPEST testing, while classified, is regarded as a process that assesses the threat of data linking by various covert electromagnetic eavesdropping mechanisms. TEMPEST testing and certification is often required by military organizations, and ensures that equipment is designed to minimize emanation.

 

The TEMPEST standards require red/black separation. In military and government IT setups, that is the most common segregation between secure and non-secure networks. “Red” circuits are normal, unsecured circuits and equipment. Separation is ensured by maintaining physical distance or installing shielding between “red” and “black” circuits and equipment.

 

TEMPEST is vital for areas where physical security is either not possible or limited. When equipment is on a vehicle or deployed in an active zone, use of TEMPEST-rated equipment is a must when sensitive data is involved. It can be a user’s only line of protection.

 

Common Criteria (EAL4+)

Common Criteria is an international standardized process for information technology security evaluation, validation, and certification. The Common Criteria scheme is supported by the National Security Agency through the National Information Assurance Program (NIAP).

 

Common Criteria defines a common set of tests regarding the process of design, testing, verification, and shipping of new security products. Common Criteria enables customers to assess a level of trust in how a product has been designed, tested, built, and shipped.

 

When shopping, be sure to get secure KVM switching for networks with multiple security classifications. For more information, visit the Secure KVM section of blackbox.com.

0

Directors of command and control centers listen up. Now switching between four separate computer systems is as simple as moving a mouse from one monitor to another! The new ServSwitch Freedom™ enables a single user to access information and control operations  across numerous systems and screens. Before, desks were messy and time  was wasted trying to control multiple systems and screens. With just one USB keyboard and USB mouse, it can fulfill functions that previously required four separate sets.

 

The ServSwitch Freedom features True Emulation technology, which ensures that the full characteristics of the connected USB keyboard and mouse are passed to every system.

This versatile product is also ideal for professionals in command and  control applications, such as those in finance on a trading room floor.  Not only can users switch between several computers just by moving the  mouse with the Glide and Switch feature, they can also simultaneously  access a mix of USB peripherals, including high-speed USB 2.0 devices.

 

The  keyboard/mouse, audio, and the two individual USB channels can be  collectively or separately switched through to each computer system. You  can, for instance, create e-mails on one system, listen to audio on a  second system, print from a third computer, and scan documents on  another—all at the same time.

Even better, there’s no need to  install any software on the connected computers. Because there is no software involved, security issues are minor, which can be a real  concern for those of you in government, healthcare, and banking industries.

Stop wasting valuable time and space. To learn more about the ServSwitch Freedom visit http://www.blackbox.com/go/Freedom.