Skip navigation

community

Black Box Network Services

1 Post tagged with the liquid_cooling tag
0

Cooling in the data center can be a  lot like a black money hole, in that it’s a big energy sucker. How can  you keep it cool and balance your budget by using efficient cooling  technology? We know that the growing demand for power is a challenge, so  choosing the best system for your data center is important.

 

Fortunately,  there are a number of cooling methods to choose from, whether you are  building a new data center or retrofitting one. And emerging green  technologies offer exciting possibilities for advances in efficiency and  cost savings.

 

Whether  under the floor, above the floor, in the rack, or above the rack, the  requirement of data center cooling remains the same: Warm air must be  moved away from equipment and cool air towards it. Understanding the  factors that can hinder or even prevent this from happening is one of  the first steps to improving data center efficiency.

 

Air conditioners and air handlers
The familiar air conditioner (AC) unit, installed in the data center  and connected to outside condensing units, uses a fan system to move  cool and hot air where they need to be. It’s much like the systems used  in residential settings except that, in building, cooling, the  evaporator coil and blower are separate from the condenser coil,  compressor, and condenser blower, while in electronics cooling they are  packaged together in one unit.

 

Computer  room air handlers (CRAH) work much the same way except that they use  chilled water instead of refrigerant to remove heat from the air.

 

You might think that the drier the data center, the better. But, in fact, the American Society of Heating, Refrigerating, and Air-Conditioning Engineers (ASHRAE) has a recommended range of humidity levels to help ensure longevity.

 

Hot aisle/cold aisle
The idea of hot aisle/cold aisle seems simple, but it’s a little  tricky. Ideally, cool air passes in front of parallel rows of racks,  being drawn in toward equipment, and hot air comes out the back of the  rack or overhead and is exhausted out of the room, producing constant  air circulation.

 

Most  major server manufacturers recommend that cabinet doors used in hot  aisle/cold aisle installations have at least 63% open area for airflow.  You can achieve this by either removing cabinet doors altogether or by  buying cabinets that have mesh doors. Also, cabinets with side panels  keep the air within each cabinet from mixing with hot air from an  adjacent cabinet.

 

Because  most servers and other network devices are equipped with internal fans,  open or mesh doors may be the only ventilation you need as long as your  data center has enough air-conditioning to dissipate the heat load.

 

Here’s  where the tricky part comes in. Cool air can escape through various  holes like cable cutouts, and some hot air doesn’t get exhausted and may  enter the cold aisle, resulting in inefficient air handling and the  presence of hot spots. These problems can be overcome through various  analyses and equipment modifications.

 

Blanking panels,  for example, can prevent cold air from passing through a cabinet too  quickly or in the wrong direction and are a simple and economical way to  direct cold air through equipment and prevent it from mixing with hot  air. Brush strips, although not airtight, can cut down on air leakage while keeping dust and other contaminants out of cabinets.

 

You can increase ventilation by installing fans to actively circulate air through cabinets. The most common cabinet fans are top-mounted fan panels that pull air from the bottom of the cabinet or through the doors. Or  you can use a fan or fan panel that mounts inside the cabinet or choose  cabinet doors with built-in fans. For very tightly packed cabinets, an enclosure blower is a specialized high-speed fan that mounts in the bottom of the  cabinet to pull cool air from a raised floor across the front of the  cabinet where it can be used by equipment. An enclosure blower requires a  solid front door with adequate space—usually at least four  inches—between the front of your equipment and the cabinet door for air  movement. If you’re housing components outside of a  temperature-controlled area, you may want a cabinet with its own air conditioner.

 

Hot aisle/cold aisle containment
In hot aisle/cold aisle containment,  barriers are used to enclose the aisles, ensuring cold air and hot air  stay where they should be to maximize AC efficiency. Cold air stays near  the server intake, and hot air exhaust is shuttled to in-row air  conditioners, conditioned, and then returned to the cold aisle.

 

To  keep cool air from mixing with arm air, row ends are closed off with an  airflow barrier. This barrier can range from makeshift arrangements of  plastic strips to doors made specifically for this purpose.

 

Because  cold aisle containment concentrates cool air at the front of equipment  where it’s most needed, it’s a great cooling method. Cold aisle  containment significantly reduces energy costs, lowering power bills as  well as reducing data centers’ carbon footprints.

 

http://bboxblog.files.wordpress.com/2011/04/hotaisle-coldaisle.jpg

Liquid cooling
Liquid cooling systems are air conditioners that use a liquid to dissipate heat. That  may be cold water or refrigerant, but the difference is that the liquid  is closer to the heat source, resulting in even more efficient cooling.

 

Green cooling
The world of data center cooling is evolving alongside “green” or  sustainable technologies, as data center managers contend with power,  cooling, and space limitations.

 

Servers  designed to handle higher temperatures are an example of so-called  “adaptive” cooling. “Free” cooling, on the other hand, is almost like  simply opening a data center window, except the windows are filters and  louvers for cleanliness and air control. In the right environment,  methods such as these can save tremendous amounts of money and energy.

 

Geothermal  cooling is an example of a more involved green system. In traditional  chilled water system, a majority of the water can be lost to  evaporation. With geothermal cooling, evaporation can be cut to zero.

 

Power demands generally vary throughout the day, and system with variably frequency drives can adjust the power as needed.

 

Chill out!
These and other evolving technologies may drastically change the way  data centers are cooled in the future. Choosing the right cooling system  saves money and protects your investment. How do you keep your data  center cool? What advice would you offer to others looking to build or  retrofit their data center?

 

Data center resources:
Quiet Fan Panels: Equipment cooling without the noise (PDF)
Video: How to pick a cabinet
White Paper: Extending the Life of Your Data Center