Skip navigation

community

Black Box Network Services

2 Posts tagged with the media_converters tag
1

#1. Repurpose unused phone wires for Ethernet.

Campus phone systems are usually built around 25- and 50-pair trunk cable. Most of these wire pairs are redundant and not used as phone lines. These spare pairs can be commandeered for Ethernet through the use of Ethernet extenders, which not only transparently establish a network connection on phone cable, but can also extend links farther than the usual 100-meter limit for Ethernet on copper. Ethernet extenders are an ideal solution for linking isolated workstations without laying new cable.

 

#2. Upgrade to fiber on your existing copper ports.

Fiber optic cable has many advantages, including speed, distance, and resistance to EMI/RFI, plus it’s now usually less expensive to install than the equivalent copper infrastructure. What usually stops the installation of fiber is the prospect of having to replace expensive network switches with fiber switches and having to install fiber NICs in PCs.

 

Media converters are a simple way to convert the RJ-45 ports on existing equipment to fiber. Because media converters are transparent to data, they’re “invisible” to the network—literally plug-and-play. In the data center, modular media converter systems feature powered chassis that house and power multiple media converters—a whole switch’s worth of copper ports can be converted to fiber without cluttering the rack. On the desktop side, tiny USB-powered media converters bring fiber to the desktop without the driver issues and incompatibilities created by fiber NICs.

 

#3. Take advantage of PoE without buying new switches.

Adding power over Ethernet (PoE) devices such as VoIP phones, wireless access points, and security cameras doesn’t have to mean an investment in a new PoE switch. PoE injectors enable you to add power to one or more Ethernet runs using your existing copper-based Ethernet switches. Injectors are particularly useful when adding just one or two PoE devices such as security cameras to a network.

 

#4. Accommodate larger equipment in the cabinets you have now.

Sometimes upgrading servers or switches can lead to a space problem when new, larger equipment restricts cabinet cabling space. These tight squeezes can often be solved by using right-angle patch cables, which can save up to 4" of cabling space over ordinary patch cable, eliminating the expense and difficulty of replacing data cabinets.

 

#5. Bring legacy equipment with serial interfaces into today’s network.

Devices such as machine tools, restaurant equipment, and scientific instrumentation often have a useful life that spans decades. Although newer industrial devices now come equipped with Ethernet, older equipment often has an RS-232, RS-422, or RS-485 serial interface. These serial devices can be brought into the Ethernet network through the use of a device server. Once legacy devices are on Ethernet, they can be accessed from a central location, enabling control, real-time diagnostics, data capture, and alerts.

0

Media converters interconnect different cable types such as twisted pair, fiber, and coax within an existing network. They are often used to connect newer Ethernet equipment to legacy cabling. They can also be used in pairs to insert a fiber segment into copper networks to increase cabling distances and enhance immunity to electromagnetic interference (EMI).

 

Traditional media converters are purely Layer 1 devices that only convert electrical signals and physical media. They don’t do anything to the data coming through the link so they’re totally transparent to data. These converters have two ports—one port for each media type. Layer 1 media converters only operate at one speed and cannot, for instance, support both 10-Mbps and 100-Mbps Ethernet.

 

Some media converters are more advanced Layer 2 Ethernet devices that, like traditional media converters, provide Layer 1 electrical and physical conversion. But, unlike traditional media converters, they also provide Layer 2 services—in other words, they’re really switches. This kind of media converter often has more than two ports, enabling you to, for instance, extend two or more copper links across a single fiber link. They also often feature autosensing ports on the copper side, making them useful for linking segments operating at different speeds.

 

Media converters are often used to connect newer 100-Mbps, Gigabit Ethernet, or ATM equipment to existing networks, which are generally 10BASE-T, 100BASE-T, or a mixture of both. They can also be used in pairs to insert a fiber segment into copper networks to increase cabling distances and enhance immunity to electromagnetic interference.

 

Media converters are available in standalone models that convert between two different media types and in chassis-based models that connect many different media types in a single housing.

Rent an apartment

Standalone converters convert between two media. But, like a small apartment, they can be outgrown. Consider your current and future applications before selecting a media converter. Standalone converters are available in many configurations, including 10BASE-T to multimode or single-mode fiber, 10BASE-T to Thin coax (ThinNet), 10BASE-T to thick coax (standard Ethernet), CDDI to FDDI, and Thin coax to fiber. 100BASE-T and 100BASE-FX models that connect UTP to single- or multimode fiber are also available. With the development of Gigabit Ethernet (1000 Mbps), media converters have been created to make the transition to high-speed networks easier.


...or buy a house.

Chassis-based or modular media converters are normally rackmountable and have slots that house media converter modules. Like a well-planned house, the chassis gives you room to grow. These are used when many Ethernet segments of different media types need to be connected in a central location. Modules are available for the same conversions performed by the standalone converters, and 10BASE-T, 100BASE-TX, 100BASE-FX, and Gigabit modules may also be mixed. Although enterprise-level, chassis-based systems generally have modules that can only be used in a chassis; many midrange systems feature modules that can be used individually or in a chassis as well.

 

Still on the fence about renting or buying? Call us at 724-746-5500 or e-mail techsupport@blackbox.com and we’ll help you decide. Consider us your own personal real estate agent. Just don’t ask us about what school district the kids will be in…