Skip navigation

community

Black Box Network Services

12 Posts tagged with the network_security tag
1

A common vulnerability in wireless networks is in their ability to create unexpected connections that can result in security gaps. Here are five common wireless security bandits to watch out for:

 

1.   The rogue access point (AP). A rogue access point is an unauthorized access point connected to your wired network, generally connected by someone in your organization trying to set up do-it-yourself wireless service. Although rogue access points are usually installed innocently enough, they can provide an unsecured gateway right into the heart of your network.

 

2.   The ad-hoc client. Ad-hoc mode is the ability of wireless devices to connect directly with other wireless devices without accessing an access point. If a computer on your wired network sets up an ad-hoc wireless connection to another computer, that other computer can gain access to your network through the ad-hoc computer.

 

3.   The out-of-compliance access point. Older access points that have not been updated to the latest firmware release may open your network to hackers. Keeping all the equipment on your network up to date with firmware releases will protect your network from attack to known vulnerabilities. Not doing this can weaken security and reduce network performance. Out-of-compliance access points tend to be a problem in organizations that do not have a security policy that addresses keeping all equipment up to date on their firmware releases.

 

4. The mis-associated client. This is a problem, not with your wireless network, but with nearby wireless networks. When a wireless client has more than one wireless network to choose from, it may accidentally connect to the wrong network. This kind of mis-association, especially if it’s by a laptop also connected to your wired network, creates a security breach. Although mis-association is usually accidental, a hacker may deliberately create a decoy wireless network that looks like yours in order to fool users into logging on. This connection then allows the hacker to steal passwords and attack your wired network.

 

5. The non-traditional wireless device. It’s easy to focus on laptop computers and forget about other wireless clients such as personal Bluetooth® devices, cell phones, bar-code readers, and printers that may also use your wireless network. All these devices are vulnerable to cracking and may present an entry to your network to an enterprising hacker.

 

Your best defense against these common security bandits is a cohesive security strategy that includes network access control, regular site surveys, and a consistent, up-to-date security policy. A centrally managed wireless system makes planning and enforcing network security far more efficient than in “traditional” wireless networks with autonomous access points. Managed systems can often be set to independently handle tasks such as network access control and rogue mitigation, making life far easier for time-stressed IT managers.

0

We’ve focused on the importance of network security before, and if you remember, it all starts with getting physical. Now you can boost your physical network security starting at the port. Here’s one of the simplest and inexpensive, yet most effective ways you can increase your Layer 1 security. Lock up your network ports with LockPORT Security Locking Patch Cables. They stay locked in place until you take them out. Or, as Christina Hansen from CableOrganizer.com’s Product Showcase says, “removal only with approval.”

 

If people—whether they’re personnel, visitors, or those with evil on their mind—can’t disconnect your network cables, they can’t tamper with your network and bring it down. Another danger to your network are cable connections that work loose over time or are accidentally knocked out. Loose and poor cable connections are one of the biggest causes of network downtime. And, it’s why the first question Help Desk technicians ask is: “Did you check the cable connection?” Whether from accidental or intentional disconnects, once your network goes down, you could spend hours and hours trying to pinpoint where the problem lies.

 

Two levels of security

LockPORT gives you two different locking cable choices. Both feature the same patented LockPORT boot. What differs are the patented clip inserts. Best of all, the clips are interchangeable so if you're application changes, all you do is move a clip from one cable to another instead of buying more cables.

 

For absolute port security, choose the red Key Locking cable. It secures cables in place and can only be removed by you with the Removal Tool. This is the “removal only with approval” lock.

 

To prevent accidental disconnects, but to give people access to ports, use the green Secure Locking cable. It holds the cable in place and eliminates disconnects from jostling and general wear and tear.

 

Publicly perfect.

Use LockPORT cables to prevent network tampering in public areas like hospitals, airports, hotels, and shops. It’s perfect for educational settings as well, providing a foolproof way to secure network connections in classrooms and training rooms. And, it’s a great and inexpensive way to turn your CAT5e/6 and fiber cables into a Layer 1 security tool.

 

Download the LockPORT Brochure, or see how LockPORT cables can secure your network ports in the video below:

 

0

Because wireless networks are particularly vulnerable to attacks, security is a primary concern. Wireless networks can be hacked by “war drivers“—who cruise around looking for a wireless signal to exploit. Usually war drivers are just looking for free Internet access, but sometimes they’re looking for confidential information such as credit card numbers.

Although a wireless network can never be totally secure, there are important steps you can take to minimize the risk:


1. Know how far your signal extends.
When you install a wireless network near public areas, it’s very important to know where your signal is going. If it’s easily picked up outside your business—perhaps from a parked car across the street or from the building next door—then you’ve got a security problem. If you send a strong wireless signal into the coffee house next door to your business, chances are someone is going to try to take advantage of it.

A wireless analyzer can help you map exactly where your access points are sending their signals. This can help you arrange the access points in your network in order to minimize signals in public areas and maximize signals to your users. A wireless analyzer can also spot unauthorized wireless access points attached to your network as well as other wireless networks broadcasting in your area. A wireless analyzer may be a freestanding application or may be part of a wireless management suite. Newer wireless mesh products often feature cloud-based management that includes wireless analysis.

 

2. Separate your wired network from your wireless network.
To add a layer of security to your wireless network, separate it from your wired network by gathering all your wireless access points into a separate LAN connected to the DMZ port of your firewall. This makes the wireless network accessible, yet safely outside of your main wired LAN. Once you separate the wireless from the wired network, insist that anything that needs to be kept secure stay on the wired network. This includes confidential data such as credit card numbers, sensitive financial data, or corporate secrets of any kind. You can, however, freely use the wireless network for less-sensitive applications such as notebook computers for taking notes at meetings, PCs for temporary workers, computer hookups for trade show booths, and bar-code readers for inventory.

 

3. Use encryption to lock out unauthorized users.
Any wireless signal, no matter how heavily encrypted, can be broken into eventually. Encryption isn’t perfect, but it can go a long way towards discouraging the casual hacker—the trick is to make breaking into your network so difficult that the hackers don’t bother. Be sure to use encryption and, rather than easily hacked WEP, use higher-level encryption schemes such as Extensible Authentication Protocol-Transport Layer Security (EAP-TLS).

4. Have a security plan and implement it. Seriously.
With a wireless network, as in any other network, it’s important to have a security plan and then implement it. The biggest security problem with wireless security is that network administrators often fail to take even the simplest of steps to ensure security, do not activate encryption at all, or fail to change the default passwords. When you fail to take these basic precautions, you leave your wireless network extremely vulnerable to casual hacking.

Yes, a wireless network is less secure than a wired network, but if you pay attention to your wireless network and implement a sensible security plan, you won’t find yourself blindsided by its vulnerabilities.

0

Is your company concerned about being connected to the Internet? If  so, you’re not alone. It’s the fear of being successfully hacked that’s  keeping many companies and their employees off the Internet. In fact,  according to Infosecurity News, over 25% of all companies polled  responded that hackers have tried to gain unauthorized access from  outside the corporate network.

 

What else keeps companies disconnected? Hackers are no longer just  techies with a hobby. Hackers are no often highly trained professionals  in places like Eastern Europe, Russia, or China, and they’re out to make  a profit on you. There’s a mystique to being hacked. It’s the new crime, it’s the hottest news. And it’s fun…according to hacking group Lulz Security, whose motto claims they are, “The world’s leaders in high-quality entertainment at your expense.” Well  they sure aren’t fun for you. If anything, this hype from the media  watchers and technical experts, should be keeping you on your toes.

 

So why the mystique? Our ever-growing, ever-faster cyberworld makes  protecting your network from intruders ever more difficult. Many people,  including company executives,  lack a fundamental understanding of technology. Mix this with the  complexities of network security issues and you can see why many  companies haven’t ventured onto the Information Superhighway. However,  what you don’t know really can hurt you.

 

On the other side of the spectrum, there are many companies with  executives who have “Teflon sensibilities.” Media hype doesn’t stick to  them. Unfortunately, neither does the advice of company network  administrators who want network security problems addressed. These  companies go about their connected-to-the-Net business until the  inevitable compromise in security happens. And when something valuable  is swiped, the executives worry.

 

“We’ve taken steps to make sure something like this never happens  again!” is the boilerplate reaction. Otherwise, they say, heads will  roll. For companies that have been hacked, the cost of information security now equals the cost of the incident plus the cost of countermeasures.

 

So protect yourself from hackers while getting the Internet access  you need. You’ll never be 100% secure, but you can dramatically reduce  your risk and proactively defend your organization by containing and  controlling threats, vulnerabilities, and assets. Just use the 4Ds:

    • Threats need to be detected, deterred, defended against, and defeated in real-time or expect downtime.
    • Vulnerabilities need to be detected, deterred, defended against, and defeated (i.e. removed by system hardening, reconfiguration, patching, etc.) as quickly as possible or expect to be exploited.
    • Assets need to be controlled—which ones gain access to your  network/infrastructure and those that are trusted but weak or infected  need to be quarantined in real-time or expect malware propagation.

 

It’s a fine balancing act, but you can protect data and keep  out the unwanted while still giving your staff access they need. A  network, as it turns out, is only as secure as the people who run it,  use it, and fund its protection. Find out more about protecting your  data infrastructure at www.blackbox.com/go/Security.

0

Is your hospital using a PACS system? Although this way of digitally sending images eliminates the need to manually retrieve and transports files, your PACS system may not be performing as quickly as your organization needs. If these images are being transmitted to another facility in another town, state, or even country, the latency of your connection can cause the transfer to take FOREVER. And in emergency situations where there are life-or-death implications, this delay is unacceptable.

 

Many healthcare institutions with multiple locations have experienced slow DICOM transmission across their WAN links, and have looked for solutions to improve transmission speeds (usually due to the critical nature and timeliness of the transmissions). WAN acceleration or WAN optimization devices help speed up these transmissions. But are your devices packing the 1-2-3 punch that Black Box provides?

 

While some traditional WAN acceleration or optimization technologies have been used by healthcare organizations and have provided some relief in certain situations, there are two basic technological or architectural problems that are limiting the benefits of these technologies in other applications.

 

Punch #1 and #2 – Cashing and Compression

Most WAN acceleration or optimization technologies involve caching or compressions. This approach can help in some cases, but in others it can be very limiting. Caching benefits transmission speeds by taking frequently requested data and storing it locally (instead of sending it across the internet each time you need it); this can help with web pages or other frequently used info, but doesn’t help much if the information being requested is unique medical images. Compressions can help by shrinking the file size of the data being sent, but many PACS systems have modes where they pre-compress the data before sending it. In this case, the compression attempts by other WAN accelerator appliances can actually slow down the transmissions.

 

Punch #3 – Protocol Optimization

Black Box can help PACS systems communicate across multiple locations with one or both of the following products:

 

Opti-WAN: A family of WAN Acceleration appliances, the Opti-WAN does not use compression or caching to achieve its speed gains. The Opti-WAN is specifically designed for long-distance or high-latency WAN connections. It accelerates links from a 1-Mb to a 1-Gb connection by accelerating and making more efficient all TCP/IP transmissions. Speed improvements can be as small as 20% or as high as 10x or more (depending on latency and other factors). DICOM traffic is one of the many formats that are helped by Opti-WAN.

 

Optinet:  A family of secure web gateways, the Optinet provides packet-level visibility into the traffic going through your Internet gateway.  By gaining this visibility, it allows the organization to identify critical traffic and accelerate it through the gateway.  The ability to take DICOM transmissions from a PACS system and elevate it past all e-mail and general web browsing traffic can substantially increase the throughput.  Traditional gateways don't have the Layer-7 inspection capabilities of Optinet, and would have trouble identifying and selectively prioritizing unique traffic such as DICOM.

 

Think of all of the archived charts, pictures, x-rays, and other important files in your organization. Plus, many times a patient's records involve several pictures in a series, from different angles, or with different filters. With the proper WAN appliances, PACS can efficiently deliver critical information; saving time, money, and lives.

0

Every network administrator is faced with this dilemma: The Internet can be a risky thing for your network, but your network needs to be connected to  it.

 

Attacks are surprisingly common. We’re just hearing more about it these days (Hi there Epsilon and Sony)  because they’re now affecting larger companies and millions of people. Before, outbreaks may have gone unreported, except at the Web sites of  antivirus software vendors.

 

What makes you want to pull your hair out even more is that every time you learn to defend against one kind of attack, hackers seem to come up with new and more creative ways to send spam. And if hackers on the Internet aren’t enough to worry about, you also have to worry about your own network users deliberately or inadvertently causing damage.

 

Although this perpetual onslaught can overwhelm you and make you feel like you’re fighting a losing battle, the reality is that with some basic precautions, you can defend your network against the vast majority of threats.

 

Have a plan

Start by making a security plan. Generally, the larger the network you’re administering, the more formalized the plan should be.

 

Your security plan should include:

  • Education — Teach network users how to avoid threats.
  • Access policies — Control physical access to the network through lock and key or password protection.
  • Software   — This includes the software required to protect your network and the scheduling of regular updates of both antivirus software and patches issued by software vendors.
  • Firewall   — If a firewall is needed, consider what kind of a firewall is needed and schedule regular reviews of firewall policies.
  • Backups — In case your network does fail, you should be ready to repair the damage and restore lost data.

 

Education

Keep on top of the latest hoaxes and viruses and make sure your network users know about them. Teach your network users to be suspicious of and report anything that doesn’t look “right.”

 

This may seem like common sense, but common sense isn’t always common place. Be sure network users know never to reply to or forward spam. Hoaxes and scams run rampant across the Internet. Any e-mail that promises money, asks for personal information, asks you to forward or respond to something, or tells you something bad will happen if you don’t respond should always be deleted.

 

Warn your network users about bad neighborhoods on the Internet. If they start poking around on sites that offer pornography, gambling, and too-good-to-be true (It just fell off the back of a truck, really?) deals, they’re more likely to be exposed to viruses and scams. Although you can use a firewall to deny users access to dubious sites, it’s virtually impossible to filter out all of them so network users should be aware that dangerous sites are out there.

Access policies

Be aware that security breaches happen “at home,” too. Anyone with network access can steal or damage your data or networking devices. Take the time to look at who has access to what, keep essential network devices under lock and key, and implement password access to sensitive data.


Software protection

An important line of defense for your network is antivirus software. Buy a well-known brand and update it often. There are two major types of antivirus software: scanners and checksummers.

Scanners, the most popular variety of antivirus software, scan your hard drive or scan each file in real time as it’s accessed. Scanners work by comparing files to known viruses. They’re easy to use but must be kept up-to-date with the latest virus information to remain effective.

 

Because viruses change files, checksummers look for these changes to find signs of infection. They have the advantage of detecting unknown viruses that a scanner can’t detect; however, they also have trouble distinguishing between legitimate change and a virus infection. Another marked disadvantage of checksummers is that they can only detect infection after it happens-they’re useless for virus prevention. There is no such thing as ideal antivirus software, and different products have different strengths and weaknesses. For the most effective protection, it’s a good idea to use more than one antivirus program.

 

In addition to using antivirus software, it’s also wise to always install software patches as they’re issued. Modern software is very complex, making it difficult to thoroughly test for security holes. Often these holes are discovered after software has been out for a while. At this point, the vendor will release a software patch, usually available on its Web site. Many computer break-ins can be prevented simply by keeping your software patches up-to-date. Regularly schedule a check of software patches issued by your software vendors and use them where needed. Do NOT install software patches that arrive unsolicited through your e-mail, as many viruses masquerade as software patches.

 

Firewalls

Hackers probe computer networks for open ports looking for a way in. Your goal is to make sure that unused ports are blocked and that your network only accepts legitimate requests for service. This is where a firewall comes in.

 

The firewall blocks unwanted traffic while letting through the traffic you want. It makes decisions that allow or deny access to services and ports on your firewall. A firewall enforces your access control policy, but it’s up to you to decide what that access control policy is. You can block whole ranges of ports-everything that you do not require to be open.

 

Firewalls generally come preconfigured to deny all access to all ports. It’s then up to you to instruct your firewall to allow network traffic through to specific ports on specific PCs in your network. When a request for a service is made, the firewall inspects the request to make sure the type of request matches an available port.

 

Backup and recovery

Back up your files on a regular basis so if your network is invaded, you can replace corrupt or infected files with your backup copies. With regular nightly backups, even the worst disaster will never cause the loss of more than a day’s data. Backup copies should always be stored on hard media in a separate location-NOT on a server connected to the network.

 

Do you have a plan to cover an unexpected disaster?

0

It should come as no surprise that the federal government is concerned about signal leakage. In fact, its interest goes back to the days of World War II when the Army was trying to exploit weaknesses of enemy combat phones and radio transmitters. Since then, the scope of the government’s interest has broadened beyond the battlefield. In the last 40 years, the National Security Agency (NSA) has taken several industry measurement standards for signal protection and greatly enhanced them.

 

These enhanced criteria are commonly referred to as the TEMPEST standards (although the NSA also calls them EMSEC standards, short for “emissions security”). TEMPEST pertains to technical security countermeasures, standards, and instrumentation that prevent or minimize the exploitation of vulnerable data communications equipment by technical surveillance (AKA eavesdropping!). It involves designing circuits to minimize emanations. Another set of testing standards is called Common Criteria (EAL4+). Both standards are important, but they test for different things.

 

TEMPEST

Many things put your data communications at risk. Any device with a microchip generates an electromagnetic field, often called a “compromising emanation” by security experts. With the proper surveillance equipment, these emanations can be intercepted and the signal reconstructed and analyzed. Unprotected equipment can, in fact, emit a signal into the air like a radio station—and nobody wants to risk his or her job and a whole lot more by broadcasting national security or trade secrets to the wrong people.

 

Some of the most vulnerable equipment includes speakerphones, printers, fax machines, scanners, external disc drives, and other high-speed, high-bandwidth peripherals. And if the snoop is using a high-quality interception devices, your equipment’s signals can be acquired up to several hundred feet away.

 

TEMPEST testing, while classified, is regarded as a process that assesses the threat of data linking by various covert electromagnetic eavesdropping mechanisms. TEMPEST testing and certification is often required by military organizations, and ensures that equipment is designed to minimize emanation.

 

The TEMPEST standards require red/black separation. In military and government IT setups, that is the most common segregation between secure and non-secure networks. “Red” circuits are normal, unsecured circuits and equipment. Separation is ensured by maintaining physical distance or installing shielding between “red” and “black” circuits and equipment.

 

TEMPEST is vital for areas where physical security is either not possible or limited. When equipment is on a vehicle or deployed in an active zone, use of TEMPEST-rated equipment is a must when sensitive data is involved. It can be a user’s only line of protection.

 

Common Criteria (EAL4+)

Common Criteria is an international standardized process for information technology security evaluation, validation, and certification. The Common Criteria scheme is supported by the National Security Agency through the National Information Assurance Program (NIAP).

 

Common Criteria defines a common set of tests regarding the process of design, testing, verification, and shipping of new security products. Common Criteria enables customers to assess a level of trust in how a product has been designed, tested, built, and shipped.

 

When shopping, be sure to get secure KVM switching for networks with multiple security classifications. For more information, visit the Secure KVM section of blackbox.com.

0

Here's the fourth weapon in your 10-part reseller arsenal:

 

Education solutions for the K-12 budgeting season in progress now!

 

Show your K-12 customers how they can:

- Improve communications and emergency notification at their schools.

- Raise academic performance with smarter classroom technology.

- Increase the range of their network without running new cables.

- Safeguard studnets and staff from accessing inappropriate Web content.

- Cut IT power consumption up to 25% and prevent outages.

- Product expensive data equipment from high temperatures and theft.

- Save on cabling costs and labor when extending an ethernet network.

 

Get started:
VirtuaCore™ Computer Sharing
Turns one CPU into two or four workstations and saves money, space, and  energy. Ideal in classrooms and education settings where cost savings  are vital. Hardware savings up to 60%; energy savings up to 60%.

 

Economy Laptop Carts
The most economical way to transport and store up to 16 laptops.  Perfect for classrooms—just roll from room to room. Guaranteed for life!

 

Enterprise Wireless
SmartPath delivers enterprise-class wireless at half the cost of  comparable solutions. Help your education customers get the wireless  infrastructure they need.

 

Wireless Video Presentation System
Transforms a wired projector into a high-end wireless one—and streams  from a PDA. Features Plug & Show setup, 4-to-1 split screen display,  simple conference control, and support for PDA wireless projection.

 

iCOMPEL™ Digital Signage
No other medium makes it possible to deliver compelling content at the  right location at the right time for maximum impact. Schools can use to  inform and notify students in their buildings and on their campuses,  whether for event promotion, disseminating important up-to-date  information, or broadcasting emergency alerts.

0

It's estimated that up to 20% of the cable for sale is now unsafe, unapproved, or counterfeit. Chances are that you've bought illegitimate cable and haven't even realized it! Cheap cable can really hurt you (literally) in the long run. Let's take a trip back in time to 1980. Remember the MGM Grand fire in Las Vegas? The fire spread so rapidly that eighty-four people perished. An electrical ground fault was to blame. What if counterfeit cable causes an accident where you work?

 

Below we've listed a few pro-tips of what are the sure signs of counterfeit or cheap cable:

  1. Look for the UL number. If there is no UL umber, that's an instant tip-off. Even if there is a UL number, look it up to see if it's legit.
  2. Look for the ETL logo. Ask the seller for the ETL test results and check the ETL website.
  3. How is the printing? Is it poorly done on the box and cable?
  4. Check for product manuals. Legitimate products will always include brochures or manuals.
  5. Does the color match previous bought cable?
  6. Compare the weight to cable you know performs up to standard.

 

Use these tips when you shop around for your next batch of cable. The last thing we want is for you to get burned on counterfeit cable. For more information and tips on how to avoid unsafe cable, listen to our "Complete Cabling Solutions" podcast, coming soon.

 

Do you have any cable horror stories? Share it with us so we can pass your wisdom on to others!

0

http://now.eloqua.com/eloquaimages/clients/BlackBox/%7B0639fe35-85ff-47ff-9d60-1c5f6a75642b%7D_WP00033-Whitepaper-template_hdr.jpg

Understand attack methodologies and develop a more proactive approach to defense.

 

Most network breaches come from malware. Learn about the many  ways  it can invade your network and why traditional countermeasures all   fail. Then learn what to do about it. This white paper shows you how to dramatically reduce your risk of a  network breach  from malware by defending against threats, detecting  vulnerabilities,  and controlling your assets. Discover how increasing  employee awareness  and training, setting up strong encryption, using  physical and network  access control, and implementing a host-based  intrusion prevention  system are all part of a smart security plan.

0

Is your organization protecting itself in the new digital age? Unauthorized devices joining the network through an open port or a wireless network is a real threat. With an ever-increasing number of mobile devices—laptop computers, notebooks, smartphones, PDAs, even video game systems—network managers are finding that portable devices are creating a real security threat. Controlling access is what Network Access Control (NAC) is all about.

NAC has a special place in a network security plan because, unlike a firewall, which offers perimeter protection, it monitors the inside of your network. A firewall stops the hacker in Poland from getting to your network through the Internet. NAC stops the hacker inside your building or in the parking lot from getting to your network through an Ethernet port or a wireless access point.

Learn how your organization can protect itself. Attend our next webinar and learn to:

• Prevent network breaches from unauthorized network connections and out-of-compliance devices.

• Stop rogue laptop connections and unauthorized wireless access devices from accessing your network.

Go to http://www.blackbox.com/Store/LP/veri-nacwebinar.aspx to view the webinar schedule and choose the time that’s best for you.  In addition, be sure to visit our Veri-NAC resources page.

0

 

The Massachusetts Data Breach Law that took effect on March 1, 2010 requires you to adequately secure your data. This means hardening your systems, preventing intrusions, and documenting policies.

But besides the fact that you are now required by law to do so, there are many other reasons to have a comprehensive security plan in place. For example, according to the Ponemon Institute, the average data breach costs $6.75 million.

Black Box can help you implement your comprehensive security plan with effective security solutions that aren’t going to break the bank.

The Veri-NAC™ appliance for network access control helps you comply with this new law by enabling you to find and fix network holes, and prevent unauthorized access to confidential citizen records. It also comes with templates for producing security policies for documenting due care and due diligence. Veri-NAC is a plug-and-play, agentless, and non-inline appliance, designed to provide rock-solid security. Best of all, it requires no infrastructure upgrade like some other NAC solutions do. For more information, go to blackbox.com/go/Veri-NAC.

To see many other practical security solutions from Black Box, visit blackbox.com/go/Security.