Skip navigation

community

Black Box Network Services

4 Posts tagged with the new_products tag
0

When news about e-mail marketer Epsilon’s data breach hit the streets, people were both surprised and concerned. How many other businesses out there have been using third party sites to handle their customer information? The reality is that…It’s a lot. Given the global size of networks out there today, companies are forced to utilize third party carriers. In doing so, these third party service vendors introduce additional vulnerabilities.

 

Even if third party vendors aren’t used, more and more organizations are using the Internet to send data to branch offices. Authentication is critical, but many companies don’t encrypt their data because it’s traveling on a “safe” MPLS network. Although MPLS networks provide more reliable connections than the Internet and aren’t as public, you can’t put all your eggs in the MPLS basket.

 

When vendors say MPLS is secure, what they mean is that the traffic is kept separate from other traffic. Separate data is not the same as data security, and separate traffic is even easier for hackers to attack. The vendor might have processes in place to prevent unauthorized data snooping, and tell you that their employees probably aren’t going to snoop either. In fact, your data probably won’t be stolen on an MPLS network, but you have no way of being sure and no way to tell if your data has been breached.

 

The only way to ensure data security over an MPLS network is by encrypting data as it travels across the WAN. This is accomplished through a traditional IPsec VPN. Although this approach is fairly simple to set up between only two points, when remote sites multiply, the number of tunnels increases exponentially. A tunnel is needed between each pair of sites, leading to administrative hassles every time a remote site is added. With growth comes the addition of personnel, router and re-structuring costs. Not to mention, a lag in network performance.

 

Enterprises can stop bleeding money and still deploy network-wide data protection without compromising performance. EncrpyTight™ is an encryption solution that overcomes the limitations associated with IPsec VPN tunnels. It brings you air-tight encryption across a WAN—even the Internet—without the hassle of setting up a VPN tunnel for each connection. Plus, EncrypTight doesn’t add latency to bog down network operations—it’s totally transparent. 

 

The “stealth” Layer 4 encryption capability leaves packet headers intact, making encrypted data far more compatible with network operations. Other advantages of Layer 4 include:

  • Ability to pass encrypted data through NAT devices. VPN tunnels, which encapsulate the Layer 3 address, of often don’t work with NAT.
  • Compatibility with policy-based routing and load balancing that require Layer 3 addresses to be intact.
  • Layer 4 encryption leaves Layer 3 headers intact, making it possible to troubleshoot a network without turning off encryption. Because heads are intact, data looks encrypted, making it possible to use within countries that restrict encrypted data.

 

Because there are no tunnels to set up, it’s easy to deploy EncrypTight across large WANs. For instance, an organization with many sites around the world could add a new site to its WAN without having to establish a VPN tunnel to every other site.

 

Additionally, EncrypTight Management Software enables network administrators to centrally manage security across the entire WAN using a simple drag-and-drop interface. A company’s headquarters in the United States can have all the control over encryption polices and key generation and distribution, but still protect sensitive data being transported to branch offices in Europe and Asia.

 

Visit www.blackbox.com/go/EncrypTight or request a call from one of our experts see if EncrypTight WAN Encryption would fit your industry needs.

0

Last week, USA Today posted an article discussing the increase of tablet computers in the business world.  This shouldn’t come as a surprise. Tablet computers are cheaper than laptops and can easily be carried around showrooms and offices. With fewer laptops and more space, companies are even saving money on the ever increasing, and seemingly unavoidable, checked bag fee.

 

What does come as a surprise is that many business execs are buying these tablet computers by the hundreds and even thousands. Often, this is without consulting their IT department.  IT Techs suddenly find themselves scrambling to adjust the design and management of their company’s wireless system. Businesses return to their Wi-Fi supplier (because they have to) to purchase expensive controllers and more APs, only to do the same a few years later due to company growth. This everlasting sales cycle becomes time consuming, expensive, and not to mention, annoying.

 

Now there is a way to break the cycle and keep pace with company growth and industry trends while still maintaining costs. SmartPath Enterprise Wireless system is unlike ordinary wireless systems. Not only does it provide fast, seamless 802.11n throughput, SmartPath APs are considered “equals” in a wired network. With all APs as equals, there is no need for a central controller.

 

Each SmartPath AP has its own “brain.” It behaves as a high-end switch, sorting packets and sending them to where they’re needed—broadcasted wirelessly to a nearby laptop, passed on to another access point in a wireless mesh arrangement, or sent through the wired network to another endpoint.  Because there is no controller, the system scales from two or three APs to thousands of APs—with no hidden upgrade costs.

 

By being completely self aware, Smartpath APs are able to track a user moving from one AP to another, so you never drop off a network. Thinking you’ll be in trouble if one stops working? They also automatically arrange a failure path with other access points.  

 

With older 802.11a/b/g devices, faster devices would be at the mercy of slower ones. This is not the case with a SmartPath AP. Its advanced circuitry and algorithms allocate air time efficiently, enabling older devices to share the network without slowing down 802.11n connectivity.

 

Why it’s ideal for your industry:

-          Healthcare: Doctors and nurses stay connected; improving patient care. Also track assets for more efficient delivery. 

-          Education: Speedy wireless allows students and staff to become more hands-on in the classroom.

-          Manufacturing: Keep track of inventory wirelessly—without the nightmare of a possible controller failure.

-          Hospitality: A full-featured guest management system allows you to manage who can and can’t access your network.

-          Government: Robust security and policy enforcement, including firewall and NAC functionality.

 

Now is the time to update your wireless infrastructure. Thinking about switching to cloud? The management functionality is available as a cloud-based service or standalone appliance, which enables you to manage the entire system from a single, user-friendly GUI consol.

 

For more information on SmartPath Enterprise Wireless go to www.blackbox.com/go/SmartPath. Not completely convinced? Play around with one of our demo units by calling 1-877-877-2269.

 

Do you have any plans on upgrading??

0

Do you work for a bank, insurance company, or financial management firm that needs to adhere to good timekeeping practices? Help prevent illegal backdated financial transactions with the Auto-Sync Time Clock. It ensures financial institutions’ compliance with FINRA OATS Rule 7430, and offers the highest-quality OATS-compliant time stamp available.

 

The time clock automatically syncs directly to National Institute of Standards and Technology (NIST) or any other NTP time source. It provides notification of a time synchronization failure via stamp imprint, LCD display, e-mail or SNMP traps, and can schedule up to 12 sync times a day.

 

With plug-and-play installation set up is quick and easy. You can manage the time clock via a Web browser over your network and configure and manage each clock through its embedded Web server. You can even save files and generate reports on time sync events, which are important for audits.

To learn more, visit blackbox.com/go/AutoSync, where you can also download the free white paper Making Networks Run on Time.

0

The 35th Anniversary Edition of the Black Box Big Book is hot off the presses and on its way to you and your customers. This year’s Big Book is bigger and better than ever. It’s packed with buyer’s guides, diagrams, illustrations, tips, how-to’s, and more than 211 new products.

Learn more about our 35th Anniversary Big Book and many of our new products by attending an introductory webinar on Thursday, September 2, 2010.

 

September 2, 2010 1:00 p.m., Eastern Daylight Time (New York, GMT-04:00)

September 2, 2010 12:00 p.m., Central Daylight Time (Chicago, GMT-05:00)

September 2, 2010 11:00 a.m., Mountain Daylight Time (Denver, GMT-06:00

September 2, 2010 10:00 a.m., Pacific Daylight Time (San Francisco, GMT-07:00)

 

Click here to register!

 

**If you are unable to attend, the webinar will be recorded and a link will be made available for your listening and viewing enjoyment.